]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/commit
remoteproc/omap: add support for runtime auto-suspend/resume
authorSuman Anna <s-anna@ti.com>
Fri, 2 Mar 2018 03:06:44 +0000 (21:06 -0600)
committerSuman Anna <s-anna@ti.com>
Mon, 4 Mar 2019 16:17:26 +0000 (10:17 -0600)
commit7405d551db8e9153e1467839d40a901b744109a4
treed77eed368528ea05c51fe3e47baa9f4d784afdd7
parent7c282f0c9667adba595780eb9f154f4a65d48346
remoteproc/omap: add support for runtime auto-suspend/resume

This patch enhances the PM support in the OMAP remoteproc driver to
support the runtime auto-suspend. A remoteproc may not be required to
be running all the time, and typically will need to be active only
during certain usecases. As such, to save power, it should be turned
off during potential long periods of inactivity between usecases.
This suspend and resume of the device is a relatively heavy process
in terms of latencies, so a remoteproc should be suspended only after
a certain period of prolonged inactivity. The OMAP remoteproc driver
leverages the runtime pm framework's auto_suspend feature to accomplish
this functionality. This feature is automatically enabled when a remote
processor has successfully booted. The 'autosuspend_delay_ms' for each
device dictates the inactivity period/time to wait for before
suspending the device.

The runtime auto-suspend design relies on marking the last busy time
on every communication (virtqueue kick) to and from the remote processor.
When there has been no activity for 'autosuspend_delay_ms' time, the
runtime PM framework invokes the driver's runtime pm suspend callback
to suspend the device. The remote processor will be woken up on the
initiation of the next communication message through the runtime pm
resume callback. The current auto-suspend design also allows a remote
processor to deny a auto-suspend attempt, if it wishes to, by sending a
NACK response to the initial suspend request message sent to the remote
processor as part of the suspend process. The auto-suspend request is
also only attempted if the remote processor is idled and in standby at
the time of inactivity timer expiry. This choice is made to avoid
unnecessary messaging, and the auto-suspend is simply rescheduled to
be attempted again after a further lapse of autosuspend_delay_ms.

The runtime pm callbacks functionality in this patch reuses most of the
core logic from the suspend/resume support code, and make use of an
additional auto_suspend flag to differentiate the logic in common code
from system suspend. The system suspend/resume sequences are also updated
to reflect the proper pm_runtime statuses, and also to really perform a
suspend/resume only if the remoteproc has not been auto-suspended at the
time of request. The remote processor is left in suspended state on a
system resume if it has been auto-suspended before, and will be woken up
only when a usecase needs to run. The other significant change in this
patch is to reset the remoteproc device's pm_domain so as to avoid
conflicts with the ordering sequences in the device pm_domain's runtime
callbacks and the reset management and clock management implemented
within the runtime callbacks in the driver.

The OMAP remoteproc driver currently uses a default value of 10 seconds
for all OMAP remoteprocs, and a different value can be chosen either by
choosing a positive value for the 'autosuspend_delay' in the device's
omap_rproc_fw_data in the driver match data or by updating the
'autosuspend_delay_ms' field at runtime through the sysfs interface.
    Eg: To use 25 seconds for IPU2 on DRA7xx,
      echo 25000 > /sys/bus/platform/devices/55020000.ipu/power/autosuspend_delay_ms

The runtime suspend feature can also be similarly enabled or disabled by
writing 'auto' or 'on' to the device's 'control' power field. The default
is enabled.
    Eg: To disable auto-suspend for IPU2 on DRA7xx SoC,
      echo on > /sys/bus/platform/devices/55020000.ipu/power/control

Signed-off-by: Suman Anna <s-anna@ti.com>
drivers/remoteproc/omap_remoteproc.c