]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/commit
ARM: dts: AM4372: Add PRUSS MDIO controller node
authorAndrew F. Davis <afd@ti.com>
Tue, 30 Jan 2018 21:08:46 +0000 (15:08 -0600)
committerSuman Anna <s-anna@ti.com>
Sun, 24 Feb 2019 01:20:49 +0000 (19:20 -0600)
commitc378d163f2abf60222d049bb8a324e512ddf149e
treeeaca44e6a2c29846a0312fb2fd37073385061453
parent9518252590d63b66af1f68d07e522500d8b175fa
ARM: dts: AM4372: Add PRUSS MDIO controller node

The PRU-ICSS1 instance on AM437x SoCs has a MDIO sub-module that
can be used to control external PHYs associated with the Industrial
Ethernet peripherals within the PRUSS. The MDIO module used within
this PRU-ICSS is an instance of the MDIO Controller used in TI
Davinci SoCs. The same bus frequency of 1 MHz is chosen as the
regular MDIO node. Note that there is no MDIO node added to the
smaller PRU-ICSS0 instance as the MDIO pins are not pinned out.

The node is added to the common am4372 dtsi file and is disabled.
This needs to be enabled in the respective board files using the
relevant AM437x SoCs supporting PRUSS and where the ethernet is
pinned out and connected properly.

Signed-off-by: Andrew F. Davis <afd@ti.com>
[s-anna@ti.com: fix reg address, add commit description]
Signed-off-by: Suman Anna <s-anna@ti.com>
arch/arm/boot/dts/am4372.dtsi