]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/commit
ARM: dts: am572x-idk-common: Add CMA pools and enable IPU & DSP rprocs
authorSuman Anna <s-anna@ti.com>
Thu, 22 Feb 2018 17:38:23 +0000 (11:38 -0600)
committerSuman Anna <s-anna@ti.com>
Mon, 4 Mar 2019 16:02:39 +0000 (10:02 -0600)
commitfb756be57b8c1c9cd06f5152a5635d101794d1a5
treec71ede195d58088669bd00c429120e8b2dc38527
parentb4a2b39f3b58c89096545ea77aafb078adfdf463
ARM: dts: am572x-idk-common: Add CMA pools and enable IPU & DSP rprocs

The CMA reserved memory nodes have been added for all the IPU and DSP
remoteproc devices in the am572x-idk-common.dtsi file that is common to
both the AM572x and AM574x IDK boards. These nodes are assigned to the
respective rproc device nodes, and all the IPU and DSP remote processors
are enabled.

The current CMA pools and sizes are defined statically for each device.
The addresses chosen are the same as the respective processors on
the AM57xx EVM board to maintain firmware compatibility between the
two boards. The CMA pools and sizes are defined using 64-bit values
to support LPAE. The starting addresses are fixed to meet current
dependencies on the remote processor firmwares, and this will go
away when the remote-side code has been improved to gather this
information runtime during its initialization.

An associated pair of the rproc node and its CMA node can be disabled
later on if there is no use-case defined to use that remote processor.

Signed-off-by: Suman Anna <s-anna@ti.com>
arch/arm/boot/dts/am572x-idk-common.dtsi