summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: fb9e801)
raw | patch | inline | side by side (parent: fb9e801)
author | Suman Anna <s-anna@ti.com> | |
Fri, 15 Feb 2019 18:20:35 +0000 (12:20 -0600) | ||
committer | Suman Anna <s-anna@ti.com> | |
Sun, 24 Feb 2019 01:20:48 +0000 (19:20 -0600) |
The AM437x SoCs have a second smaller PRU-ICSS subsystem (PRUSS0)
in addition to the primary PRUSS1 instance. The PRUSS0 is another
instantiation of the IP, but is not identical to PRUSS1. It is
essentially a cut-down version of the IP, with less DRAM per PRU,
no Shared DRAM etc. It also does not have direct access to L3 bus
regions, there is a single interface to L3 for both PRUSS0 and
PRUSS1, and it would have to go through the PRUSS1's interface.
The PRUSS_SYSCFG register is reserved on PRUSS0, so any external
access requires the programming the corresponding PRUSS_SYSCFG
register in PRUSS1. It does have its own dedicated I/O lines
though. Note that this instance does not support any PRU Ethernet
related usecases.
The PRUSS remoteproc drivers have been enhanced to support this
smaller PRUSS0 instance using instance-specific data. The adaptation
uses a newly introduced pruss_match_private_data structure and the
pruss_get_private_data() function to retrieve a PRUSS instance
specific data using a device-name based lookup logic. The reset
and the L3 external access are managed by the common PRUSS SoC bus
driver so that PRUSS1 and PRUSS0 can be independently supported.
The initial names for the firmware images for each PRU core are
retrieved from DT nodes, and can be adjusted through sysfs if
required.
Signed-off-by: Andrew F. Davis <afd@ti.com>
Signed-off-by: Suman Anna <s-anna@ti.com>
in addition to the primary PRUSS1 instance. The PRUSS0 is another
instantiation of the IP, but is not identical to PRUSS1. It is
essentially a cut-down version of the IP, with less DRAM per PRU,
no Shared DRAM etc. It also does not have direct access to L3 bus
regions, there is a single interface to L3 for both PRUSS0 and
PRUSS1, and it would have to go through the PRUSS1's interface.
The PRUSS_SYSCFG register is reserved on PRUSS0, so any external
access requires the programming the corresponding PRUSS_SYSCFG
register in PRUSS1. It does have its own dedicated I/O lines
though. Note that this instance does not support any PRU Ethernet
related usecases.
The PRUSS remoteproc drivers have been enhanced to support this
smaller PRUSS0 instance using instance-specific data. The adaptation
uses a newly introduced pruss_match_private_data structure and the
pruss_get_private_data() function to retrieve a PRUSS instance
specific data using a device-name based lookup logic. The reset
and the L3 external access are managed by the common PRUSS SoC bus
driver so that PRUSS1 and PRUSS0 can be independently supported.
The initial names for the firmware images for each PRU core are
retrieved from DT nodes, and can be adjusted through sysfs if
required.
Signed-off-by: Andrew F. Davis <afd@ti.com>
Signed-off-by: Suman Anna <s-anna@ti.com>
drivers/soc/ti/pruss.c | patch | blob | history |
diff --git a/drivers/soc/ti/pruss.c b/drivers/soc/ti/pruss.c
index 86805a3328be00520e0c0266635c7142bc3f9152..b88c1d596a933059eac2d95eaf2b1e95e1d5a711 100644 (file)
--- a/drivers/soc/ti/pruss.c
+++ b/drivers/soc/ti/pruss.c
#include <linux/of_device.h>
#include <linux/pruss_driver.h>
+/**
+ * struct pruss_private_data - PRUSS driver private data
+ * @has_no_sharedram: flag to indicate the absence of PRUSS Shared Data RAM
+ */
+struct pruss_private_data {
+ bool has_no_sharedram;
+};
+
+/**
+ * struct pruss_match_private_data - private data to handle multiple instances
+ * @device_name: device name of the PRUSS instance
+ * @priv_data: PRUSS driver private data for this PRUSS instance
+ */
+struct pruss_match_private_data {
+ const char *device_name;
+ const struct pruss_private_data *priv_data;
+};
+
+static const
+struct pruss_private_data *pruss_get_private_data(struct platform_device *pdev)
+{
+ const struct pruss_match_private_data *data;
+
+ if (!of_device_is_compatible(pdev->dev.of_node, "ti,am4376-pruss"))
+ return NULL;
+
+ data = of_device_get_match_data(&pdev->dev);
+ for (; data && data->device_name; data++) {
+ if (!strcmp(dev_name(&pdev->dev), data->device_name))
+ return data->priv_data;
+ }
+
+ return ERR_PTR(-ENODEV);
+}
+
static int pruss_probe(struct platform_device *pdev)
{
struct device *dev = &pdev->dev;
struct pruss *pruss;
struct resource res;
int ret, i, index;
+ const struct pruss_private_data *data;
const char *mem_names[PRUSS_MEM_MAX] = { "dram0", "dram1", "shrdram2" };
if (!node) {
return -ENODEV;
}
+ data = pruss_get_private_data(pdev);
+ if (IS_ERR(data)) {
+ dev_err(dev, "missing private data\n");
+ return -ENODEV;
+ }
+
ret = dma_set_coherent_mask(dev, DMA_BIT_MASK(32));
if (ret) {
dev_err(dev, "dma_set_coherent_mask: %d\n", ret);
}
for (i = 0; i < ARRAY_SIZE(mem_names); i++) {
+ if (data && data->has_no_sharedram &&
+ !strcmp(mem_names[i], "shrdram2"))
+ continue;
+
index = of_property_match_string(np, "reg-names", mem_names[i]);
if (index < 0) {
of_node_put(np);
return 0;
}
+/* instance-specific driver private data */
+static const struct pruss_private_data am437x_pruss1_priv_data = {
+ .has_no_sharedram = false,
+};
+
+static const struct pruss_private_data am437x_pruss0_priv_data = {
+ .has_no_sharedram = true,
+};
+
+static const struct pruss_match_private_data am437x_match_data[] = {
+ {
+ .device_name = "54400000.pruss",
+ .priv_data = &am437x_pruss1_priv_data,
+ },
+ {
+ .device_name = "54440000.pruss",
+ .priv_data = &am437x_pruss0_priv_data,
+ },
+ {
+ /* sentinel */
+ },
+};
+
static const struct of_device_id pruss_of_match[] = {
{ .compatible = "ti,am3356-pruss", .data = NULL, },
- { .compatible = "ti,am4376-pruss", .data = NULL, },
+ { .compatible = "ti,am4376-pruss", .data = &am437x_match_data, },
{ /* sentinel */ },
};
MODULE_DEVICE_TABLE(of, pruss_of_match);