summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 24ebd0e)
raw | patch | inline | side by side (parent: 24ebd0e)
author | Roger Quadros <rogerq@ti.com> | |
Fri, 26 Mar 2021 20:43:53 +0000 (15:43 -0500) | ||
committer | Suman Anna <s-anna@ti.com> | |
Fri, 26 Mar 2021 20:43:53 +0000 (15:43 -0500) |
Some firmwares expect the OS drivers to configure the CTABLE
entries publishing dynamically allocated memory regions. For
example, the PRU Ethernet firmwares use the C28 and C30 entries
for retrieving the Shared RAM and System SRAM (OCMC) areas
allocated by the PRU Ethernet client driver.
Provide a way for users to do that through a new API,
pru_rproc_set_ctable(). The API returns 0 on success and
a negative value on error.
NOTE:
The programmable CTABLE entries are typically re-programmed by
the PRU firmwares when dealing with a certain block of memory
during block processing. This API provides an interface to the
PRU client drivers to publish a dynamically allocated memory
block with the PRU firmware using a CTABLE entry instead of a
negotiated address in shared memory. Additional synchronization
may be needed between the PRU client drivers and firmwares if
different addresses needs to be published at run-time reusing
the same CTABLE entry.
Co-developed-by: Andrew F. Davis <afd@ti.com>
Signed-off-by: Andrew F. Davis <afd@ti.com>
Co-developed-by: Suman Anna <s-anna@ti.com>
Signed-off-by: Suman Anna <s-anna@ti.com>
Signed-off-by: Roger Quadros <rogerq@ti.com>
Co-developed-by: Grzegorz Jaszczyk <grzegorz.jaszczyk@linaro.org>
Signed-off-by: Grzegorz Jaszczyk <grzegorz.jaszczyk@linaro.org>
entries publishing dynamically allocated memory regions. For
example, the PRU Ethernet firmwares use the C28 and C30 entries
for retrieving the Shared RAM and System SRAM (OCMC) areas
allocated by the PRU Ethernet client driver.
Provide a way for users to do that through a new API,
pru_rproc_set_ctable(). The API returns 0 on success and
a negative value on error.
NOTE:
The programmable CTABLE entries are typically re-programmed by
the PRU firmwares when dealing with a certain block of memory
during block processing. This API provides an interface to the
PRU client drivers to publish a dynamically allocated memory
block with the PRU firmware using a CTABLE entry instead of a
negotiated address in shared memory. Additional synchronization
may be needed between the PRU client drivers and firmwares if
different addresses needs to be published at run-time reusing
the same CTABLE entry.
Co-developed-by: Andrew F. Davis <afd@ti.com>
Signed-off-by: Andrew F. Davis <afd@ti.com>
Co-developed-by: Suman Anna <s-anna@ti.com>
Signed-off-by: Suman Anna <s-anna@ti.com>
Signed-off-by: Roger Quadros <rogerq@ti.com>
Co-developed-by: Grzegorz Jaszczyk <grzegorz.jaszczyk@linaro.org>
Signed-off-by: Grzegorz Jaszczyk <grzegorz.jaszczyk@linaro.org>
drivers/remoteproc/pru_rproc.c | patch | blob | history | |
include/linux/pruss.h | patch | blob | history |
index e138787014e7ab4f0e0e4726b5ab31e7728d25e5..3ceb3e9b8e860c0f632b5a447a309dca7b905f28 100644 (file)
* @mapped_irq: virtual interrupt numbers of created fw specific mapping
* @pru_interrupt_map: pointer to interrupt mapping description (firmware)
* @pru_interrupt_map_sz: pru_interrupt_map size
+ * @rmw_lock: lock for read, modify, write operations on registers
* @dbg_single_step: debug state variable to set PRU into single step mode
* @dbg_continuous: debug state variable to restore PRU execution mode
* @evt_count: number of mapped events
unsigned int *mapped_irq;
struct pru_irq_rsc *pru_interrupt_map;
size_t pru_interrupt_map_sz;
+ spinlock_t rmw_lock; /* register access lock */
u32 dbg_single_step;
u32 dbg_continuous;
u8 evt_count;
writel_relaxed(val, pru->mem_regions[PRU_IOMEM_CTRL].va + reg);
}
+static inline
+void pru_control_set_reg(struct pru_rproc *pru, unsigned int reg,
+ u32 mask, u32 set)
+{
+ u32 val;
+ unsigned long flags;
+
+ spin_lock_irqsave(&pru->rmw_lock, flags);
+
+ val = pru_control_read_reg(pru, reg);
+ val &= ~mask;
+ val |= (set & mask);
+ pru_control_write_reg(pru, reg, val);
+
+ spin_unlock_irqrestore(&pru->rmw_lock, flags);
+}
+
static struct rproc *__pru_rproc_get(struct device_node *np, int index)
{
struct device_node *rproc_np = NULL;
}
EXPORT_SYMBOL_GPL(pru_rproc_put);
+/**
+ * pru_rproc_set_ctable() - set the constant table index for the PRU
+ * @rproc: the rproc instance of the PRU
+ * @c: constant table index to set
+ * @addr: physical address to set it to
+ *
+ * Return: 0 on success, or errno in error case.
+ */
+int pru_rproc_set_ctable(struct rproc *rproc, enum pru_ctable_idx c, u32 addr)
+{
+ struct pru_rproc *pru = rproc->priv;
+ unsigned int reg;
+ u32 mask, set;
+ u16 idx;
+ u16 idx_mask;
+
+ if (IS_ERR_OR_NULL(rproc))
+ return -EINVAL;
+
+ if (!rproc->dev.parent || !is_pru_rproc(rproc->dev.parent))
+ return -ENODEV;
+
+ /* pointer is 16 bit and index is 8-bit so mask out the rest */
+ idx_mask = (c >= PRU_C28) ? 0xFFFF : 0xFF;
+
+ /* ctable uses bit 8 and upwards only */
+ idx = (addr >> 8) & idx_mask;
+
+ /* configurable ctable (i.e. C24) starts at PRU_CTRL_CTBIR0 */
+ reg = PRU_CTRL_CTBIR0 + 4 * (c >> 1);
+ mask = idx_mask << (16 * (c & 1));
+ set = idx << (16 * (c & 1));
+
+ pru_control_set_reg(pru, reg, mask, set);
+
+ return 0;
+}
+EXPORT_SYMBOL_GPL(pru_rproc_set_ctable);
+
static inline u32 pru_debug_read_reg(struct pru_rproc *pru, unsigned int reg)
{
return readl_relaxed(pru->mem_regions[PRU_IOMEM_DEBUG].va + reg);
pru->pruss = platform_get_drvdata(ppdev);
pru->rproc = rproc;
pru->fw_name = fw_name;
+ spin_lock_init(&pru->rmw_lock);
mutex_init(&pru->lock);
for (i = 0; i < ARRAY_SIZE(mem_names); i++) {
diff --git a/include/linux/pruss.h b/include/linux/pruss.h
index 1a97856b463a586764e410f508a410263fb98b18..e1740ff069626d9d671c41b939440022155626d0 100644 (file)
--- a/include/linux/pruss.h
+++ b/include/linux/pruss.h
PRUSS_NUM_PRUS,
};
+/*
+ * enum pru_ctable_idx - Configurable Constant table index identifiers
+ */
+enum pru_ctable_idx {
+ PRU_C24 = 0,
+ PRU_C25,
+ PRU_C26,
+ PRU_C27,
+ PRU_C28,
+ PRU_C29,
+ PRU_C30,
+ PRU_C31,
+};
+
struct device_node;
+struct rproc;
#if IS_ENABLED(CONFIG_PRU_REMOTEPROC)
struct rproc *pru_rproc_get(struct device_node *np, int index,
enum pruss_pru_id *pru_id);
void pru_rproc_put(struct rproc *rproc);
+int pru_rproc_set_ctable(struct rproc *rproc, enum pru_ctable_idx c, u32 addr);
#else
static inline void pru_rproc_put(struct rproc *rproc) { }
+static inline int pru_rproc_set_ctable(struct rproc *rproc,
+ enum pru_ctable_idx c, u32 addr)
+{
+ return -EOPNOTSUPP;
+}
+
#endif /* CONFIG_PRU_REMOTEPROC */
static inline bool is_pru_rproc(struct device *dev)