summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: ea922c7)
raw | patch | inline | side by side (parent: ea922c7)
author | Suman Anna <s-anna@ti.com> | |
Fri, 15 Feb 2019 01:54:48 +0000 (19:54 -0600) | ||
committer | Suman Anna <s-anna@ti.com> | |
Sun, 24 Feb 2019 01:20:48 +0000 (19:20 -0600) |
The remoteproc core creates certain standard debugfs entries,
that does not give a whole lot of useful information for the
PRUs. The PRU remoteproc driver is enhanced to add additional
debugfs entries for PRU. These will be auto-cleaned up when
the parent rproc debug directory is removed.
The enhanced debugfs support adds two new entries: 'regs' and
'single_step'. The 'regs' dumps out the useful CTRL sub-module
registers as well as each of the 32 GPREGs and CT_REGs registers.
The GPREGs and CT_REGs though are printed only when the PRU is
halted and accessible as per the IP design.
The 'single_step' utilizes the single-step execution of the PRU
cores. Writing a non-zero value performs a single step, and a
zero value restores the PRU to execute in the same mode as the
mode before the first single step. (note: if the PRU is halted
because of a halt instruction, then no change occurs).
Logic for setting the PC and jumping over a halt instruction shall
be added in the future.
Signed-off-by: Suman Anna <s-anna@ti.com>
that does not give a whole lot of useful information for the
PRUs. The PRU remoteproc driver is enhanced to add additional
debugfs entries for PRU. These will be auto-cleaned up when
the parent rproc debug directory is removed.
The enhanced debugfs support adds two new entries: 'regs' and
'single_step'. The 'regs' dumps out the useful CTRL sub-module
registers as well as each of the 32 GPREGs and CT_REGs registers.
The GPREGs and CT_REGs though are printed only when the PRU is
halted and accessible as per the IP design.
The 'single_step' utilizes the single-step execution of the PRU
cores. Writing a non-zero value performs a single step, and a
zero value restores the PRU to execute in the same mode as the
mode before the first single step. (note: if the PRU is halted
because of a halt instruction, then no change occurs).
Logic for setting the PC and jumping over a halt instruction shall
be added in the future.
Signed-off-by: Suman Anna <s-anna@ti.com>
drivers/remoteproc/pru_rproc.c | patch | blob | history |
index a7adcd4d5d8089ea0628eb5ec0e2e201eb9fade7..d23f9d5654652ce1406dbe31fddca99a613ccc26 100644 (file)
*/
#include <linux/bitops.h>
+#include <linux/debugfs.h>
#include <linux/interrupt.h>
#include <linux/module.h>
#include <linux/of_device.h>
#define CTRL_CTRL_SINGLE_STEP BIT(8)
#define CTRL_CTRL_RUNSTATE BIT(15)
+/* PRU_ICSS_PRU_DEBUG registers */
+#define PRU_DEBUG_GPREG(x) (0x0000 + (x) * 4)
+#define PRU_DEBUG_CT_REG(x) (0x0080 + (x) * 4)
+
/* PRU Core IRAM address masks */
#define PRU0_IRAM_ADDR_MASK 0x34000
#define PRU1_IRAM_ADDR_MASK 0x38000
* @sdram_da: device address of secondary Data RAM for this PRU
* @shrdram_da: device address of shared Data RAM
* @fw_name: name of firmware image used during loading
+ * @dbg_single_step: debug state variable to set PRU into single step mode
+ * @dbg_continuous: debug state variable to restore PRU execution mode
*/
struct pru_rproc {
int id;
u32 sdram_da;
u32 shrdram_da;
const char *fw_name;
+ u32 dbg_single_step;
+ u32 dbg_continuous;
};
static void *pru_d_da_to_va(struct pru_rproc *pru, u32 da, int len);
writel_relaxed(val, pru->mem_regions[PRU_IOMEM_DEBUG].va + reg);
}
+static int regs_show(struct seq_file *s, void *data)
+{
+ struct rproc *rproc = s->private;
+ struct pru_rproc *pru = rproc->priv;
+ int i, nregs = 32;
+ u32 pru_sts;
+ int pru_is_running;
+
+ seq_puts(s, "============== Control Registers ==============\n");
+ seq_printf(s, "CTRL := 0x%08x\n",
+ pru_control_read_reg(pru, PRU_CTRL_CTRL));
+ pru_sts = pru_control_read_reg(pru, PRU_CTRL_STS);
+ seq_printf(s, "STS (PC) := 0x%08x (0x%08x)\n", pru_sts, pru_sts << 2);
+ seq_printf(s, "WAKEUP_EN := 0x%08x\n",
+ pru_control_read_reg(pru, PRU_CTRL_WAKEUP_EN));
+ seq_printf(s, "CYCLE := 0x%08x\n",
+ pru_control_read_reg(pru, PRU_CTRL_CYCLE));
+ seq_printf(s, "STALL := 0x%08x\n",
+ pru_control_read_reg(pru, PRU_CTRL_STALL));
+ seq_printf(s, "CTBIR0 := 0x%08x\n",
+ pru_control_read_reg(pru, PRU_CTRL_CTBIR0));
+ seq_printf(s, "CTBIR1 := 0x%08x\n",
+ pru_control_read_reg(pru, PRU_CTRL_CTBIR1));
+ seq_printf(s, "CTPPR0 := 0x%08x\n",
+ pru_control_read_reg(pru, PRU_CTRL_CTPPR0));
+ seq_printf(s, "CTPPR1 := 0x%08x\n",
+ pru_control_read_reg(pru, PRU_CTRL_CTPPR1));
+
+ seq_puts(s, "=============== Debug Registers ===============\n");
+ pru_is_running = pru_control_read_reg(pru, PRU_CTRL_CTRL) &
+ CTRL_CTRL_RUNSTATE;
+ if (pru_is_running) {
+ seq_puts(s, "PRU is executing, cannot print/access debug registers.\n");
+ return 0;
+ }
+
+ for (i = 0; i < nregs; i++) {
+ seq_printf(s, "GPREG%-2d := 0x%08x\tCT_REG%-2d := 0x%08x\n",
+ i, pru_debug_read_reg(pru, PRU_DEBUG_GPREG(i)),
+ i, pru_debug_read_reg(pru, PRU_DEBUG_CT_REG(i)));
+ }
+
+ return 0;
+}
+
+DEFINE_SHOW_ATTRIBUTE(regs);
+
+/*
+ * Control PRU single-step mode
+ *
+ * This is a debug helper function used for controlling the single-step
+ * mode of the PRU. The PRU Debug registers are not accessible when the
+ * PRU is in RUNNING state.
+ *
+ * Writing a non-zero value sets the PRU into single-step mode irrespective
+ * of its previous state. The PRU mode is saved only on the first set into
+ * a single-step mode. Writing a zero value will restore the PRU into its
+ * original mode.
+ */
+static int pru_rproc_debug_ss_set(void *data, u64 val)
+{
+ struct rproc *rproc = data;
+ struct pru_rproc *pru = rproc->priv;
+ u32 reg_val;
+
+ val = val ? 1 : 0;
+ if (!val && !pru->dbg_single_step)
+ return 0;
+
+ reg_val = pru_control_read_reg(pru, PRU_CTRL_CTRL);
+
+ if (val && !pru->dbg_single_step)
+ pru->dbg_continuous = reg_val;
+
+ if (val)
+ reg_val |= CTRL_CTRL_SINGLE_STEP | CTRL_CTRL_EN;
+ else
+ reg_val = pru->dbg_continuous;
+
+ pru->dbg_single_step = val;
+ pru_control_write_reg(pru, PRU_CTRL_CTRL, reg_val);
+
+ return 0;
+}
+
+static int pru_rproc_debug_ss_get(void *data, u64 *val)
+{
+ struct rproc *rproc = data;
+ struct pru_rproc *pru = rproc->priv;
+
+ *val = pru->dbg_single_step;
+
+ return 0;
+}
+DEFINE_SIMPLE_ATTRIBUTE(pru_rproc_debug_ss_fops, pru_rproc_debug_ss_get,
+ pru_rproc_debug_ss_set, "%llu\n");
+
+/*
+ * Create PRU-specific debugfs entries
+ *
+ * The entries are created only if the parent remoteproc debugfs directory
+ * exists, and will be cleaned up by the remoteproc core.
+ */
+static void pru_rproc_create_debug_entries(struct rproc *rproc)
+{
+ if (!rproc->dbg_dir)
+ return;
+
+ debugfs_create_file("regs", 0400, rproc->dbg_dir,
+ rproc, ®s_fops);
+ debugfs_create_file("single_step", 0600, rproc->dbg_dir,
+ rproc, &pru_rproc_debug_ss_fops);
+}
+
/* start a PRU core */
static int pru_rproc_start(struct rproc *rproc)
{
goto free_rproc;
}
+ pru_rproc_create_debug_entries(rproc);
+
dev_info(dev, "PRU rproc node %s probed successfully\n", np->full_name);
return 0;