summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 969d02d)
raw | patch | inline | side by side (parent: 969d02d)
author | Suman Anna <s-anna@ti.com> | |
Thu, 21 Feb 2019 02:43:27 +0000 (20:43 -0600) | ||
committer | Suman Anna <s-anna@ti.com> | |
Mon, 25 Feb 2019 19:31:39 +0000 (13:31 -0600) |
The K3 AM65x family of SoCs have the next generation of the PRU-ICSS
processor subsystem, commonly referred to as ICSSG. Each ICSSG processor
subsystem contain two primary PRU cores and two new auxiliary PRU cores
called RTUs. Each RTU core has its own dedicated IRAM (smaller than a
PRU), Control and debug feature sets, but is different in terms of
sub-modules integrated around it and does not have the full capabilities
associated with a PRU core. The RTU core is typically used to aid a
PRU core in accelerating data transfers, but can also be used to run
independent applications. The RTU cores though share the same Data RAMs
as the PRU cores, so the memories have to be partitioned carefully
between different applications. The new cores also support a new
sub-module called Task Manager to support two different context thread
executions.
Enhance the existing PRU remoteproc driver to support these new PRU
and RTU cores by using specific compatibles. The initial names for the
firmware images for each PRU core are retrieved from DT nodes, and can
be adjusted through sysfs if required.
The PRU remoteproc driver has to be specifically modified to use a
custom ELF loader implementation for these new cores in order to
overcome a limitation with copying data into each of the core's IRAM
memories. These memory ports support only 4-byte writes, and any
sub-word order byte writes clear out the remaining bytes other than
the bytes being written within the containing word. The default ARM64
memcpy also cannot be used as it throws an exception when the preferred
8-byte copy operation is attempted.
The ICSSG instances on AM65x SoCs also have more System Events, Interrupt
Channels and Host Interrupts compared to the previous generation PRUSS
instances on other SoCs. The logic in pru_rproc_get() function to parse
and program the interrupts from DT is also updated to use proper values
relevant for K3 SoCs by using a state flag that is set only on K3 SoCs.
This can be reworked to use match data to scale beyond current SoCs if
needed.
Signed-off-by: Suman Anna <s-anna@ti.com>
processor subsystem, commonly referred to as ICSSG. Each ICSSG processor
subsystem contain two primary PRU cores and two new auxiliary PRU cores
called RTUs. Each RTU core has its own dedicated IRAM (smaller than a
PRU), Control and debug feature sets, but is different in terms of
sub-modules integrated around it and does not have the full capabilities
associated with a PRU core. The RTU core is typically used to aid a
PRU core in accelerating data transfers, but can also be used to run
independent applications. The RTU cores though share the same Data RAMs
as the PRU cores, so the memories have to be partitioned carefully
between different applications. The new cores also support a new
sub-module called Task Manager to support two different context thread
executions.
Enhance the existing PRU remoteproc driver to support these new PRU
and RTU cores by using specific compatibles. The initial names for the
firmware images for each PRU core are retrieved from DT nodes, and can
be adjusted through sysfs if required.
The PRU remoteproc driver has to be specifically modified to use a
custom ELF loader implementation for these new cores in order to
overcome a limitation with copying data into each of the core's IRAM
memories. These memory ports support only 4-byte writes, and any
sub-word order byte writes clear out the remaining bytes other than
the bytes being written within the containing word. The default ARM64
memcpy also cannot be used as it throws an exception when the preferred
8-byte copy operation is attempted.
The ICSSG instances on AM65x SoCs also have more System Events, Interrupt
Channels and Host Interrupts compared to the previous generation PRUSS
instances on other SoCs. The logic in pru_rproc_get() function to parse
and program the interrupts from DT is also updated to use proper values
relevant for K3 SoCs by using a state flag that is set only on K3 SoCs.
This can be reworked to use match data to scale beyond current SoCs if
needed.
Signed-off-by: Suman Anna <s-anna@ti.com>
drivers/remoteproc/Kconfig | patch | blob | history | |
drivers/remoteproc/pru_rproc.c | patch | blob | history |
index 1919cf005e5ada2c2cb48434a35b3c553668d681..414f5c6215c77961702ce8cda04b8cd9baa1dc4d 100644 (file)
depends on TI_PRUSS
default TI_PRUSS
select MAILBOX
- select OMAP2PLUS_MBOX if ARCH_OMAP2PLUS
+ select OMAP2PLUS_MBOX if ARCH_OMAP2PLUS || ARCH_K3
help
Support for TI PRU remote processors present within a PRU-ICSS
subsystem via the remote processor framework.
index 9857715faaba3dad466759d27c1a110ddb0b01a2..2981d5520201f534e36b8c31b0f10558c6b6cdcf 100644 (file)
#define PRU_DEBUG_GPREG(x) (0x0000 + (x) * 4)
#define PRU_DEBUG_CT_REG(x) (0x0080 + (x) * 4)
-/* PRU Core IRAM address masks */
+/* PRU/RTU Core IRAM address masks */
#define PRU0_IRAM_ADDR_MASK 0x34000
#define PRU1_IRAM_ADDR_MASK 0x38000
+#define RTU0_IRAM_ADDR_MASK 0x4000
+#define RTU1_IRAM_ADDR_MASK 0x6000
/**
* enum pru_iomem - PRU core memory/register range identifiers
* @dbg_single_step: debug state variable to set PRU into single step mode
* @dbg_continuous: debug state variable to restore PRU execution mode
* @fw_has_intc_rsc: boolean flag to indicate INTC config through firmware
+ * @is_k3: boolean flag used to indicate the core has increased number of events
+ * @is_rtu: boolean flag to indicate the core is a RTU core
*/
struct pru_rproc {
int id;
u32 dbg_single_step;
u32 dbg_continuous;
unsigned int fw_has_intc_rsc : 1;
+ unsigned int is_k3 : 1;
+ unsigned int is_rtu : 1;
};
static void *pru_d_da_to_va(struct pru_rproc *pru, u32 da, int len);
struct device_node *np = pru->client_np;
struct property *prop;
const char *prop_name = "ti,pru-interrupt-map";
+ u8 max_system_events, max_pru_channels, max_pru_host_ints;
int ret = 0, i;
int dt_irqs;
u32 *arr;
goto out;
}
+ max_system_events = pru->is_k3 ?
+ MAX_PRU_SYS_EVENTS_K3 : MAX_PRU_SYS_EVENTS;
+ max_pru_channels = pru->is_k3 ? MAX_PRU_CHANNELS_K3 : MAX_PRU_CHANNELS;
+ max_pru_host_ints = pru->is_k3 ? MAX_PRU_HOST_INT_K3 : MAX_PRU_HOST_INT;
+
for (i = 0; i < ARRAY_SIZE(pru->intc_config.sysev_to_ch); i++)
pru->intc_config.sysev_to_ch[i] = -1;
continue;
if (arr[i + 1] < 0 ||
- arr[i + 1] >= MAX_PRU_SYS_EVENTS) {
+ arr[i + 1] >= max_system_events) {
dev_err(dev, "bad sys event %d\n", arr[i + 1]);
ret = -EINVAL;
goto out;
}
if (arr[i + 2] < 0 ||
- arr[i + 2] >= MAX_PRU_CHANNELS) {
+ arr[i + 2] >= max_pru_channels) {
dev_err(dev, "bad channel %d\n", arr[i + 2]);
ret = -EINVAL;
goto out;
}
if (arr[i + 3] < 0 ||
- arr[i + 3] >= MAX_PRU_HOST_INT) {
+ arr[i + 3] >= max_pru_host_ints) {
dev_err(dev, "bad irq %d\n", arr[i + 3]);
ret = -EINVAL;
goto out;
return ERR_PTR(-EPROBE_DEFER);
/* TODO: replace the crude string based check to make sure it is PRU */
- if (!strstr(dev_name(&pdev->dev), "pru")) {
+ if (!strstr(dev_name(&pdev->dev), "pru") &&
+ !strstr(dev_name(&pdev->dev), "rtu")) {
put_device(&pdev->dev);
return ERR_PTR(-ENODEV);
}
return;
/* TODO: replace the crude string based check to make sure it is PRU */
- if (!strstr(dev_name(rproc->dev.parent), "pru"))
+ if (!strstr(dev_name(rproc->dev.parent), "pru") &&
+ !strstr(dev_name(rproc->dev.parent), "rtu"))
return;
pru = rproc->priv;
return -EINVAL;
/* TODO: replace the crude string based check to make sure it is PRU */
- if (!strstr(dev_name(rproc->dev.parent), "pru"))
+ if (!strstr(dev_name(rproc->dev.parent), "pru") &&
+ !strstr(dev_name(rproc->dev.parent), "rtu"))
return -EINVAL;
pru = rproc->priv;
struct pru_rproc *pru = rproc->priv;
int ret;
mbox_msg_t msg = (mbox_msg_t)vq_id;
+ const char *name = pru->is_rtu ? "RTU" : "PRU";
- dev_dbg(dev, "kicking vqid %d on PRU%d\n", vq_id, pru->id);
+ dev_dbg(dev, "kicking vqid %d on %s%d\n", vq_id, name, pru->id);
if (pru->irq_kick > 0) {
ret = pruss_intc_trigger(pru->irq_kick);
{
struct device *dev = &rproc->dev;
struct pru_rproc *pru = rproc->priv;
+ const char *name = pru->is_rtu ? "RTU" : "PRU";
u32 val;
int ret;
- dev_dbg(dev, "starting PRU%d: entry-point = 0x%x\n",
- pru->id, (rproc->bootaddr >> 2));
+ dev_dbg(dev, "starting %s%d: entry-point = 0x%x\n",
+ name, pru->id, (rproc->bootaddr >> 2));
if (!list_empty(&pru->rproc->rvdevs)) {
if (!pru->mbox && (pru->irq_vring <= 0 || pru->irq_kick <= 0)) {
{
struct device *dev = &rproc->dev;
struct pru_rproc *pru = rproc->priv;
+ const char *name = pru->is_rtu ? "RTU" : "PRU";
u32 val;
- dev_dbg(dev, "stopping PRU%d\n", pru->id);
+ dev_dbg(dev, "stopping %s%d\n", name, pru->id);
val = pru_control_read_reg(pru, PRU_CTRL_CTRL);
val &= ~CTRL_CTRL_EN;
.da_to_va = pru_da_to_va,
};
+/*
+ * Custom memory copy implementation for ICSSG PRU/RTU Cores
+ *
+ * The ICSSG PRU/RTU cores have a memory copying issue with IRAM memories, that
+ * is not seen on previous generation SoCs. The data is reflected properly in
+ * the IRAM memories only for integer (4-byte) copies. Any unaligned copies
+ * result in all the other pre-existing bytes zeroed out within that 4-byte
+ * boundary, thereby resulting in wrong text/code in the IRAMs. Also, the
+ * IRAM memory port interface does not allow any 8-byte copies (as commonly
+ * used by ARM64 memcpy implementation) and throws an exception. The DRAM
+ * memory ports do not show this behavior. Use this custom copying function
+ * to properly load the PRU/RTU firmware images on all memories for simplicity.
+ *
+ * TODO: Improve the function to deal with additional corner cases like
+ * unaligned copy sizes or sub-integer trailing bytes when the need arises.
+ */
+static int pru_rproc_memcpy(void *dest, const void *src, size_t count)
+{
+ const int *s = src;
+ int *d = dest;
+ int size = count / 4;
+ int *tmp_src = NULL;
+
+ /* limited to 4-byte aligned addresses and copy sizes */
+ if ((long)dest % 4 || count % 4)
+ return -EINVAL;
+
+ /* src offsets in ELF firmware image can be non-aligned */
+ if ((long)src % 4) {
+ tmp_src = kmemdup(src, count, GFP_KERNEL);
+ if (!tmp_src)
+ return -ENOMEM;
+ s = tmp_src;
+ }
+
+ while (size--)
+ *d++ = *s++;
+
+ kfree(tmp_src);
+
+ return 0;
+}
+
+static int
+pru_rproc_load_elf_segments(struct rproc *rproc, const struct firmware *fw)
+{
+ struct device *dev = &rproc->dev;
+ struct elf32_hdr *ehdr;
+ struct elf32_phdr *phdr;
+ int i, ret = 0;
+ const u8 *elf_data = fw->data;
+
+ ehdr = (struct elf32_hdr *)elf_data;
+ phdr = (struct elf32_phdr *)(elf_data + ehdr->e_phoff);
+
+ /* go through the available ELF segments */
+ for (i = 0; i < ehdr->e_phnum; i++, phdr++) {
+ u32 da = phdr->p_paddr;
+ u32 memsz = phdr->p_memsz;
+ u32 filesz = phdr->p_filesz;
+ u32 offset = phdr->p_offset;
+ void *ptr;
+
+ if (phdr->p_type != PT_LOAD)
+ continue;
+
+ dev_dbg(dev, "phdr: type %d da 0x%x memsz 0x%x filesz 0x%x\n",
+ phdr->p_type, da, memsz, filesz);
+
+ if (filesz > memsz) {
+ dev_err(dev, "bad phdr filesz 0x%x memsz 0x%x\n",
+ filesz, memsz);
+ ret = -EINVAL;
+ break;
+ }
+
+ if (offset + filesz > fw->size) {
+ dev_err(dev, "truncated fw: need 0x%x avail 0x%zx\n",
+ offset + filesz, fw->size);
+ ret = -EINVAL;
+ break;
+ }
+
+ /* grab the kernel address for this device address */
+ ptr = rproc_da_to_va(rproc, da, memsz,
+ RPROC_FLAGS_ELF_PHDR | phdr->p_flags);
+ if (!ptr) {
+ dev_err(dev, "bad phdr da 0x%x mem 0x%x\n", da, memsz);
+ ret = -EINVAL;
+ break;
+ }
+
+ /* skip the memzero logic performed by remoteproc ELF loader */
+ if (!phdr->p_filesz)
+ continue;
+
+ ret = pru_rproc_memcpy(ptr, elf_data + phdr->p_offset, filesz);
+ if (ret) {
+ dev_err(dev, "PRU custom memory copy failed for da 0x%x memsz 0x%x\n",
+ da, memsz);
+ break;
+ }
+ }
+
+ return ret;
+}
+
/*
* compute PRU id based on the IRAM addresses. The PRU IRAMs are
* always at a particular offset within the PRUSS address space.
* hardware property to define it in DT), and the id can always be
* computated using this inherent address logic.
*/
-static int pru_rproc_set_id(struct pru_rproc *pru)
+static int pru_rproc_set_id(struct device_node *np, struct pru_rproc *pru)
{
int ret = 0;
u32 mask1 = PRU0_IRAM_ADDR_MASK;
u32 mask2 = PRU1_IRAM_ADDR_MASK;
- if ((pru->mem_regions[PRU_IOMEM_IRAM].pa & mask1) == mask1)
- pru->id = PRUSS_PRU0;
- else if ((pru->mem_regions[PRU_IOMEM_IRAM].pa & mask2) == mask2)
+ if (of_device_is_compatible(np, "ti,am654-rtu")) {
+ mask1 = RTU0_IRAM_ADDR_MASK;
+ mask2 = RTU1_IRAM_ADDR_MASK;
+ pru->is_rtu = 1;
+ }
+
+ if ((pru->mem_regions[PRU_IOMEM_IRAM].pa & mask2) == mask2)
pru->id = PRUSS_PRU1;
+ else if ((pru->mem_regions[PRU_IOMEM_IRAM].pa & mask1) == mask1)
+ pru->id = PRUSS_PRU0;
else
ret = -EINVAL;
spin_lock_init(&pru->rmw_lock);
mutex_init(&pru->lock);
+ if (of_device_is_compatible(np, "ti,am654-pru") ||
+ of_device_is_compatible(np, "ti,am654-rtu")) {
+ /* use generic elf ops for undefined platform driver ops */
+ rproc->ops->load = pru_rproc_load_elf_segments;
+
+ pru->is_k3 = 1;
+ }
+
/* XXX: get this from match data if different in the future */
pru->iram_da = 0;
pru->pdram_da = 0;
pru->mem_regions[i].size, pru->mem_regions[i].va);
}
- ret = pru_rproc_set_id(pru);
+ ret = pru_rproc_set_id(np, pru);
if (ret < 0)
goto free_rproc;
{ .compatible = "ti,am4376-pru", },
{ .compatible = "ti,am5728-pru", },
{ .compatible = "ti,k2g-pru", },
+ { .compatible = "ti,am654-pru", },
+ { .compatible = "ti,am654-rtu", },
{},
};
MODULE_DEVICE_TABLE(of, pru_rproc_match);