summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: a34939a)
raw | patch | inline | side by side (parent: a34939a)
author | Tero Kristo <t-kristo@ti.com> | |
Tue, 19 Feb 2019 23:12:16 +0000 (17:12 -0600) | ||
committer | Suman Anna <s-anna@ti.com> | |
Sun, 24 Feb 2019 01:20:51 +0000 (19:20 -0600) |
Add documentation for the common properties that can be used by the
PRU consumer/application nodes and supported by the PRU remoteproc
driver. These are used to configure the PRU hardware for specific
user applications.
The application nodes themselves should define their own bindings.
Signed-off-by: Tero Kristo <t-kristo@ti.com>
[s-anna@ti.com: some binding updates]
Signed-off-by: Suman Anna <s-anna@ti.com>
PRU consumer/application nodes and supported by the PRU remoteproc
driver. These are used to configure the PRU hardware for specific
user applications.
The application nodes themselves should define their own bindings.
Signed-off-by: Tero Kristo <t-kristo@ti.com>
[s-anna@ti.com: some binding updates]
Signed-off-by: Suman Anna <s-anna@ti.com>
Documentation/devicetree/bindings/remoteproc/ti,pru-rproc.txt | patch | blob | history |
diff --git a/Documentation/devicetree/bindings/remoteproc/ti,pru-rproc.txt b/Documentation/devicetree/bindings/remoteproc/ti,pru-rproc.txt
index 021516864e500b684f82b954f4e2395a501976f9..f299395c528916c429d184782d93ed43bdc1f1c6 100644 (file)
"kick" - for HOST to PRU virtqueue signalling
+Application/Consumer Nodes
+==========================
+A PRU application/consumer/user node typically uses one or more PRU device nodes
+to implement a PRU application/functionality. Each application/client node would
+need a reference to at least a PRU node, and optionally define some properties
+needed for hardware/firmware configuration. The below properties are a list of
+common properties supported by the PRU remoteproc infrastructure.
+
+The application nodes shall define their own bindings like regular platform
+devices, so below are in addition to each node's bindings.
+
+Required Properties:
+--------------------
+- prus : phandles to the PRU nodes used
+
+Optional Properties:
+--------------------
+- firmware-name : firmwares for the PRU cores, the default firmware
+ for the core from the PRU node will be used if not
+ provided. The firmware names should correspond to
+ the PRU cores listed in the 'prus' property
+- ti,pruss-gp-mux-sel : array of values for the GP_MUX_SEL under PRUSS_GPCFG
+ register for a PRU. This selects the internal muxing
+ scheme for the PRU instance. If not provided, the
+ default out-of-reset value (0) for the PRU core is
+ used. Values should correspond to the PRU cores listed
+ in the 'prus' property
+- ti,pru-interrupt-map : PRU interrupt mappings, containing an array of entries
+ with each entry consisting of 4 cell-values. First one
+ is an index towards the "prus" property to identify the
+ PRU core for the interrupt map, second is the PRU
+ System Event id, third is the PRU interrupt channel id
+ and fourth is the PRU host interrupt id. If provided,
+ this map will supercede any other configuration
+ provided through firmware
+
+
Example:
--------
};
};
};
+
+3: /* PRU application node example */
+ app_node: app_node {
+ ...
+ prus = <&pru0>, <&pru1>;
+ firmware-name = "pruss-app-fw", "pruss-app-fw-2";
+ ti,pruss-gp-mux-sel = <2>, <1>;
+ /* setup interrupts for prus:
+ prus[0] => pru1_0: ev=16, chnl=2, host-irq=7,
+ prus[1] => pru1_1: ev=19, chnl=1, host-irq=3 */
+ ti,pru-interrupt-map = <0 16 2 7 >, <1 19 1 3>;
+ }