summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 1e35777)
raw | patch | inline | side by side (parent: 1e35777)
author | Suman Anna <s-anna@ti.com> | |
Thu, 22 Nov 2018 11:39:03 +0000 (13:39 +0200) | ||
committer | Suman Anna <s-anna@ti.com> | |
Sun, 24 Feb 2019 02:56:38 +0000 (20:56 -0600) |
The PRUSS CFG module's SYSCFG register is used for managing the
PRCM clock management settings at the PRU-ICSS subsystem level,
and is being programmed for the PRCM Idle/Standby protocol properly
during probe and remove. The register is also programmed to enable
the OCP master ports (disable MStandby) by default during probe now
to allow the PRUs access to on-chip memories and peripherals outside
the PRUSS without having to do it in firmware (primarily for the PRU
Ethernet usecase currently, the firmware is not programming this
register).
NOTE:
1. The AM57xx TRM suggests to enable "No Standby" during the
Idle + Standby state to an Active/Normal state, but this
sequence is not documented in either of AM33xx and AM437x
SoCs. Furthermore, it did not have an impact on the working
of Ethernet Rx, so is left out.
2. This has an impact on the PM suspend/resume operation usually
(same bit is used to trigger PRU standby), and even when the
PRU cores are in halted state. The STANDBY_INIT has to be
re-programmed to initiate a standby sequence and have the PM
suspend/resume functional when PRUs are halted. This is already
handled in commit c1d6b33cb8f7 ("soc: ti: pruss: Fix system
suspend/MStandby config issues").
Signed-off-by: Suman Anna <s-anna@ti.com>
PRCM clock management settings at the PRU-ICSS subsystem level,
and is being programmed for the PRCM Idle/Standby protocol properly
during probe and remove. The register is also programmed to enable
the OCP master ports (disable MStandby) by default during probe now
to allow the PRUs access to on-chip memories and peripherals outside
the PRUSS without having to do it in firmware (primarily for the PRU
Ethernet usecase currently, the firmware is not programming this
register).
NOTE:
1. The AM57xx TRM suggests to enable "No Standby" during the
Idle + Standby state to an Active/Normal state, but this
sequence is not documented in either of AM33xx and AM437x
SoCs. Furthermore, it did not have an impact on the working
of Ethernet Rx, so is left out.
2. This has an impact on the PM suspend/resume operation usually
(same bit is used to trigger PRU standby), and even when the
PRU cores are in halted state. The STANDBY_INIT has to be
re-programmed to initiate a standby sequence and have the PM
suspend/resume functional when PRUs are halted. This is already
handled in commit c1d6b33cb8f7 ("soc: ti: pruss: Fix system
suspend/MStandby config issues").
Signed-off-by: Suman Anna <s-anna@ti.com>
drivers/soc/ti/pruss_soc_bus.c | patch | blob | history |
index 89711993cdddcc0f9d6b79cc966ba8b3a90ee5dd..47545fc13b3710c3ccf9f327b63e3eadc1479624 100644 (file)
* outside of the PRU-ICSS. The function has to wait for the PRCM to
* acknowledge through the monitoring of the PRUSS_SYSCFG.SUB_MWAIT bit.
*/
-static
-int __maybe_unused pruss_soc_bus_enable_ocp_master_ports(struct device *dev)
+static int pruss_soc_bus_enable_ocp_master_ports(struct device *dev)
{
struct pruss_soc_bus *psoc_bus = dev_get_drvdata(dev);
u32 syscfg_val, i;
pruss_soc_bus_rmw(psoc_bus->syscfg, SYSCFG_STANDBY_MODE_MASK,
SYSCFG_STANDBY_MODE_SMART);
+ /* enable OCP master ports/disable MStandby */
+ ret = pruss_soc_bus_enable_ocp_master_ports(dev);
+ if (ret)
+ pruss_disable_module(dev);
+
return ret;
}