rpmsg: pru: add a PRU RPMsg driver
authorJason Reeder <jreeder@ti.com>
Fri, 3 Feb 2017 02:48:57 +0000 (20:48 -0600)
committerSuman Anna <s-anna@ti.com>
Sun, 24 Feb 2019 05:19:16 +0000 (23:19 -0600)
An RPMsg driver that exposes interfaces to user space, to
allow applications to communicate with the PRU processors
on available TI SoCs has been added. This is restricted to
SoCs that have the PRUSS remoteproc support.

Signed-off-by: Jason Reeder <jreeder@ti.com>
[s-anna@ti.com: various cleanups, rpmsg rebase fixes for 4.19]
Signed-off-by: Suman Anna <s-anna@ti.com>
drivers/rpmsg/Kconfig
drivers/rpmsg/Makefile
drivers/rpmsg/rpmsg_pru.c [new file with mode: 0644]

index 720bf328c0b6cd6f5e6ad31d51dcd8e08c4faa81..c41d8157b079236a91ec3db51b933785919ae6c1 100644 (file)
@@ -68,6 +68,17 @@ config RPMSG_RPC
          remote calls to more power-efficient remote processors. This is
          currently available only on OMAP4+ systems.
 
          remote calls to more power-efficient remote processors. This is
          currently available only on OMAP4+ systems.
 
+config RPMSG_PRU
+       tristate "PRU RPMsg Communication driver"
+       depends on RPMSG_VIRTIO
+       depends on REMOTEPROC
+       depends on PRU_REMOTEPROC
+       help
+         An rpmsg driver that exposes interfaces to user space, to allow
+         applications to communicate with the PRU processors on available
+         TI SoCs. This is restricted to SoCs that have the PRUSS remoteproc
+         support.
+
          If unsure, say N.
 
 endmenu
          If unsure, say N.
 
 endmenu
index 0aea724c00d32be82dcd1c9c3533ce0531e10454..6666c8d6327e2a6eb1b7e12cd207261f4fca4f9c 100644 (file)
@@ -1,6 +1,7 @@
 # SPDX-License-Identifier: GPL-2.0
 obj-$(CONFIG_RPMSG)            += rpmsg_core.o
 obj-$(CONFIG_RPMSG_CHAR)       += rpmsg_char.o
 # SPDX-License-Identifier: GPL-2.0
 obj-$(CONFIG_RPMSG)            += rpmsg_core.o
 obj-$(CONFIG_RPMSG_CHAR)       += rpmsg_char.o
+obj-$(CONFIG_RPMSG_PRU)                += rpmsg_pru.o
 obj-$(CONFIG_RPMSG_QCOM_GLINK_RPM) += qcom_glink_rpm.o
 obj-$(CONFIG_RPMSG_QCOM_GLINK_NATIVE) += qcom_glink_native.o
 obj-$(CONFIG_RPMSG_QCOM_GLINK_SMEM) += qcom_glink_smem.o
 obj-$(CONFIG_RPMSG_QCOM_GLINK_RPM) += qcom_glink_rpm.o
 obj-$(CONFIG_RPMSG_QCOM_GLINK_NATIVE) += qcom_glink_native.o
 obj-$(CONFIG_RPMSG_QCOM_GLINK_SMEM) += qcom_glink_smem.o
diff --git a/drivers/rpmsg/rpmsg_pru.c b/drivers/rpmsg/rpmsg_pru.c
new file mode 100644 (file)
index 0000000..137af59
--- /dev/null
@@ -0,0 +1,350 @@
+// SPDX-License-Identifier: GPL-2.0
+/*
+ * PRU Remote Processor Messaging Driver
+ *
+ * Copyright (C) 2015-2019 Texas Instruments Incorporated - http://www.ti.com/
+ *     Jason Reeder <jreeder@ti.com>
+ *     Suman Anna <s-anna@ti.com>
+ */
+
+#include <linux/kernel.h>
+#include <linux/rpmsg.h>
+#include <linux/slab.h>
+#include <linux/fs.h>
+#include <linux/init.h>
+#include <linux/cdev.h>
+#include <linux/module.h>
+#include <linux/kfifo.h>
+#include <linux/uaccess.h>
+#include <linux/mutex.h>
+#include <linux/poll.h>
+#include <linux/rpmsg/virtio_rpmsg.h>
+
+#define PRU_MAX_DEVICES                                (16)
+/* Matches the definition in virtio_rpmsg_bus.c */
+#define RPMSG_BUF_SIZE                         (512)
+#define MAX_FIFO_MSG                           (32)
+#define FIFO_MSG_SIZE                          RPMSG_BUF_SIZE
+
+/**
+ * struct rpmsg_pru_dev - Structure that contains the per-device data
+ * @rpdev: rpmsg channel device that is associated with this rpmsg_pru device
+ * @dev: device
+ * @cdev: character device
+ * @locked: boolean used to determine whether or not the device file is in use
+ * @devt: dev_t structure for the rpmsg_pru device
+ * @msg_fifo: kernel fifo used to buffer the messages between userspace and PRU
+ * @msg_len: array storing the lengths of each message in the kernel fifo
+ * @msg_idx_rd: kernel fifo read index
+ * @msg_idx_wr: kernel fifo write index
+ * @wait_list: wait queue used to implement the poll operation of the character
+ *             device
+ *
+ * Each rpmsg_pru device provides an interface, using an rpmsg channel (rpdev),
+ * between a user space character device (cdev) and a PRU core. A kernel fifo
+ * (msg_fifo) is used to buffer the messages in the kernel that are
+ * being passed between the character device and the PRU.
+ */
+struct rpmsg_pru_dev {
+       struct rpmsg_device *rpdev;
+       struct device *dev;
+       struct cdev cdev;
+       bool locked;
+       dev_t devt;
+       struct kfifo msg_fifo;
+       u32 msg_len[MAX_FIFO_MSG];
+       int msg_idx_rd;
+       int msg_idx_wr;
+       wait_queue_head_t wait_list;
+};
+
+static struct class *rpmsg_pru_class;
+static dev_t rpmsg_pru_devt;
+static DEFINE_MUTEX(rpmsg_pru_lock);
+static DEFINE_IDR(rpmsg_pru_minors);
+
+static int rpmsg_pru_open(struct inode *inode, struct file *filp)
+{
+       struct rpmsg_pru_dev *prudev;
+       int ret = -EACCES;
+
+       prudev = container_of(inode->i_cdev, struct rpmsg_pru_dev, cdev);
+
+       mutex_lock(&rpmsg_pru_lock);
+       if (!prudev->locked) {
+               prudev->locked = true;
+               filp->private_data = prudev;
+               ret = 0;
+       }
+       mutex_unlock(&rpmsg_pru_lock);
+
+       if (ret)
+               dev_err(prudev->dev, "Device already open\n");
+
+       return ret;
+}
+
+static int rpmsg_pru_release(struct inode *inode, struct file *filp)
+{
+       struct rpmsg_pru_dev *prudev;
+
+       prudev = container_of(inode->i_cdev, struct rpmsg_pru_dev, cdev);
+       mutex_lock(&rpmsg_pru_lock);
+       prudev->locked = false;
+       mutex_unlock(&rpmsg_pru_lock);
+       return 0;
+}
+
+static ssize_t rpmsg_pru_read(struct file *filp, char __user *buf,
+                             size_t count, loff_t *f_pos)
+{
+       int ret;
+       u32 length;
+       struct rpmsg_pru_dev *prudev;
+
+       prudev = filp->private_data;
+
+       if (kfifo_is_empty(&prudev->msg_fifo) &&
+           (filp->f_flags & O_NONBLOCK))
+               return -EAGAIN;
+
+       ret = wait_event_interruptible(prudev->wait_list,
+                                      !kfifo_is_empty(&prudev->msg_fifo));
+       if (ret)
+               return -EINTR;
+
+       ret = kfifo_to_user(&prudev->msg_fifo, buf,
+                           prudev->msg_len[prudev->msg_idx_rd], &length);
+       prudev->msg_idx_rd = (prudev->msg_idx_rd + 1) % MAX_FIFO_MSG;
+
+       return ret ? ret : length;
+}
+
+static ssize_t rpmsg_pru_write(struct file *filp, const char __user *buf,
+                              size_t count, loff_t *f_pos)
+{
+       int ret;
+       struct rpmsg_pru_dev *prudev;
+       static char rpmsg_pru_buf[RPMSG_BUF_SIZE];
+
+       prudev = filp->private_data;
+
+       if (count > RPMSG_BUF_SIZE - sizeof(struct rpmsg_hdr)) {
+               dev_err(prudev->dev, "Data too large for RPMsg Buffer\n");
+               return -EINVAL;
+       }
+
+       if (copy_from_user(rpmsg_pru_buf, buf, count)) {
+               dev_err(prudev->dev, "Error copying buffer from user space");
+               return -EFAULT;
+       }
+
+       ret = rpmsg_send(prudev->rpdev->ept, (void *)rpmsg_pru_buf, count);
+       if (ret)
+               dev_err(prudev->dev, "rpmsg_send failed: %d\n", ret);
+
+       return ret ? ret : count;
+}
+
+static unsigned int rpmsg_pru_poll(struct file *filp,
+                                  struct poll_table_struct *wait)
+{
+       int mask;
+       struct rpmsg_pru_dev *prudev;
+
+       prudev = filp->private_data;
+
+       poll_wait(filp, &prudev->wait_list, wait);
+
+       mask = POLLOUT | POLLWRNORM;
+
+       if (!kfifo_is_empty(&prudev->msg_fifo))
+               mask |= POLLIN | POLLRDNORM;
+
+       return mask;
+}
+
+static const struct file_operations rpmsg_pru_fops = {
+       .owner = THIS_MODULE,
+       .open = rpmsg_pru_open,
+       .release = rpmsg_pru_release,
+       .read = rpmsg_pru_read,
+       .write = rpmsg_pru_write,
+       .poll = rpmsg_pru_poll,
+};
+
+static int rpmsg_pru_cb(struct rpmsg_device *rpdev, void *data, int len,
+                       void *priv, u32 src)
+{
+       u32 length;
+       struct rpmsg_pru_dev *prudev;
+
+       prudev = dev_get_drvdata(&rpdev->dev);
+
+       if (kfifo_avail(&prudev->msg_fifo) < len) {
+               dev_err(&rpdev->dev, "Not enough space on the FIFO\n");
+               return -ENOSPC;
+       }
+
+       if ((prudev->msg_idx_wr + 1) % MAX_FIFO_MSG ==
+               prudev->msg_idx_rd) {
+               dev_err(&rpdev->dev, "Message length table is full\n");
+               return -ENOSPC;
+       }
+
+       length = kfifo_in(&prudev->msg_fifo, data, len);
+       prudev->msg_len[prudev->msg_idx_wr] = length;
+       prudev->msg_idx_wr = (prudev->msg_idx_wr + 1) % MAX_FIFO_MSG;
+
+       wake_up_interruptible(&prudev->wait_list);
+
+       return 0;
+}
+
+static int rpmsg_pru_probe(struct rpmsg_device *rpdev)
+{
+       int ret;
+       struct rpmsg_pru_dev *prudev;
+       int minor_got;
+
+       prudev = devm_kzalloc(&rpdev->dev, sizeof(*prudev), GFP_KERNEL);
+       if (!prudev)
+               return -ENOMEM;
+
+       mutex_lock(&rpmsg_pru_lock);
+       minor_got = idr_alloc(&rpmsg_pru_minors, prudev, 0, PRU_MAX_DEVICES,
+                             GFP_KERNEL);
+       mutex_unlock(&rpmsg_pru_lock);
+       if (minor_got < 0) {
+               ret = minor_got;
+               dev_err(&rpdev->dev, "Failed to get a minor number for the rpmsg_pru device: %d\n",
+                       ret);
+               goto fail_alloc_minor;
+       }
+
+       prudev->devt = MKDEV(MAJOR(rpmsg_pru_devt), minor_got);
+
+       cdev_init(&prudev->cdev, &rpmsg_pru_fops);
+       prudev->cdev.owner = THIS_MODULE;
+       ret = cdev_add(&prudev->cdev, prudev->devt, 1);
+       if (ret) {
+               dev_err(&rpdev->dev, "Unable to add cdev for the rpmsg_pru device\n");
+               goto fail_add_cdev;
+       }
+
+       prudev->dev = device_create(rpmsg_pru_class, &rpdev->dev, prudev->devt,
+                                   NULL, "rpmsg_pru%d", rpdev->dst);
+       if (IS_ERR(prudev->dev)) {
+               dev_err(&rpdev->dev, "Unable to create the rpmsg_pru device\n");
+               ret = PTR_ERR(prudev->dev);
+               goto fail_create_device;
+       }
+
+       prudev->rpdev = rpdev;
+
+       ret = kfifo_alloc(&prudev->msg_fifo, MAX_FIFO_MSG * FIFO_MSG_SIZE,
+                         GFP_KERNEL);
+       if (ret) {
+               dev_err(&rpdev->dev, "Unable to allocate fifo for the rpmsg_pru device\n");
+               goto fail_alloc_fifo;
+       }
+
+       init_waitqueue_head(&prudev->wait_list);
+
+       dev_set_drvdata(&rpdev->dev, prudev);
+
+       dev_info(&rpdev->dev, "new rpmsg_pru device: /dev/rpmsg_pru%d",
+                rpdev->dst);
+
+       return 0;
+
+fail_alloc_fifo:
+       device_destroy(rpmsg_pru_class, prudev->devt);
+fail_create_device:
+       cdev_del(&prudev->cdev);
+fail_add_cdev:
+       mutex_lock(&rpmsg_pru_lock);
+       idr_remove(&rpmsg_pru_minors, minor_got);
+       mutex_unlock(&rpmsg_pru_lock);
+fail_alloc_minor:
+       return ret;
+}
+
+static void rpmsg_pru_remove(struct rpmsg_device *rpdev)
+{
+       struct rpmsg_pru_dev *prudev;
+
+       prudev = dev_get_drvdata(&rpdev->dev);
+
+       kfifo_free(&prudev->msg_fifo);
+       device_destroy(rpmsg_pru_class, prudev->devt);
+       cdev_del(&prudev->cdev);
+       mutex_lock(&rpmsg_pru_lock);
+       idr_remove(&rpmsg_pru_minors, MINOR(prudev->devt));
+       mutex_unlock(&rpmsg_pru_lock);
+}
+
+/* .name matches on RPMsg Channels and causes a probe */
+static const struct rpmsg_device_id rpmsg_driver_pru_id_table[] = {
+       { .name = "rpmsg-pru" },
+       { },
+};
+MODULE_DEVICE_TABLE(rpmsg, rpmsg_driver_pru_id_table);
+
+static struct rpmsg_driver rpmsg_pru_driver = {
+       .drv.name       = KBUILD_MODNAME,
+       .id_table       = rpmsg_driver_pru_id_table,
+       .probe          = rpmsg_pru_probe,
+       .callback       = rpmsg_pru_cb,
+       .remove         = rpmsg_pru_remove,
+};
+
+static int __init rpmsg_pru_init(void)
+{
+       int ret;
+
+       rpmsg_pru_class = class_create(THIS_MODULE, "rpmsg_pru");
+       if (IS_ERR(rpmsg_pru_class)) {
+               pr_err("Unable to create class\n");
+               ret = PTR_ERR(rpmsg_pru_class);
+               goto fail_create_class;
+       }
+
+       ret = alloc_chrdev_region(&rpmsg_pru_devt, 0, PRU_MAX_DEVICES,
+                                 "rpmsg_pru");
+       if (ret) {
+               pr_err("Unable to allocate chrdev region\n");
+               goto fail_alloc_region;
+       }
+
+       ret = register_rpmsg_driver(&rpmsg_pru_driver);
+       if (ret) {
+               pr_err("Unable to register rpmsg driver");
+               goto fail_register_rpmsg_driver;
+       }
+
+       return 0;
+
+fail_register_rpmsg_driver:
+       unregister_chrdev_region(rpmsg_pru_devt, PRU_MAX_DEVICES);
+fail_alloc_region:
+       class_destroy(rpmsg_pru_class);
+fail_create_class:
+       return ret;
+}
+
+static void __exit rpmsg_pru_exit(void)
+{
+       unregister_rpmsg_driver(&rpmsg_pru_driver);
+       idr_destroy(&rpmsg_pru_minors);
+       mutex_destroy(&rpmsg_pru_lock);
+       class_destroy(rpmsg_pru_class);
+       unregister_chrdev_region(rpmsg_pru_devt, PRU_MAX_DEVICES);
+}
+
+module_init(rpmsg_pru_init);
+module_exit(rpmsg_pru_exit);
+
+MODULE_AUTHOR("Jason Reeder <jreeder@ti.com>");
+MODULE_DESCRIPTION("PRU Remote Processor Messaging Driver");
+MODULE_LICENSE("GPL v2");