summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 9d98b91)
raw | patch | inline | side by side (parent: 9d98b91)
author | Suman Anna <s-anna@ti.com> | |
Fri, 15 Feb 2019 23:07:52 +0000 (17:07 -0600) | ||
committer | Suman Anna <s-anna@ti.com> | |
Sat, 23 Feb 2019 17:39:59 +0000 (11:39 -0600) |
The Programmable Real-Time Unit Subsystem (PRUSS) contains an
interrupt controller (INTC) that can handle various system input
events and post interrupts back to the device-level initiators.
The INTC can support upto 64 input events with individual control
configuration and hardware prioritization. These events are mapped
onto 10 interrupt signals through two levels of many-to-one mapping
support. Different interrupt signals are routed to the individual
PRU cores or to the host CPU.
The PRUSS INTC platform driver manages this PRUSS interrupt
controller and implements an irqchip driver to provide a Linux
standard way for the PRU client users to enable/disable/ack/
re-trigger a PRUSS system event. The system events to interrupt
channels and host interrupts relies on the mapping configuration
provided through a firmware resource table for now. This will be
revisited and enhanced in the future for a better interface. The
mappings will currently be programmed during the boot/shutdown
of the PRU.
The PRUSS INTC module is reference counted during the interrupt
setup phase through the irqchip's irq_request_resources() and
irq_release_resources() ops. This restricts the module from being
removed as long as there are active interrupt users.
The driver currently supports the AM335x SoC, and support for other
TI SoCs will be added in subsequent patches.
Signed-off-by: Suman Anna <s-anna@ti.com>
Signed-off-by: Andrew F. Davis <afd@ti.com>
Signed-off-by: Roger Quadros <rogerq@ti.com>
interrupt controller (INTC) that can handle various system input
events and post interrupts back to the device-level initiators.
The INTC can support upto 64 input events with individual control
configuration and hardware prioritization. These events are mapped
onto 10 interrupt signals through two levels of many-to-one mapping
support. Different interrupt signals are routed to the individual
PRU cores or to the host CPU.
The PRUSS INTC platform driver manages this PRUSS interrupt
controller and implements an irqchip driver to provide a Linux
standard way for the PRU client users to enable/disable/ack/
re-trigger a PRUSS system event. The system events to interrupt
channels and host interrupts relies on the mapping configuration
provided through a firmware resource table for now. This will be
revisited and enhanced in the future for a better interface. The
mappings will currently be programmed during the boot/shutdown
of the PRU.
The PRUSS INTC module is reference counted during the interrupt
setup phase through the irqchip's irq_request_resources() and
irq_release_resources() ops. This restricts the module from being
removed as long as there are active interrupt users.
The driver currently supports the AM335x SoC, and support for other
TI SoCs will be added in subsequent patches.
Signed-off-by: Suman Anna <s-anna@ti.com>
Signed-off-by: Andrew F. Davis <afd@ti.com>
Signed-off-by: Roger Quadros <rogerq@ti.com>
drivers/irqchip/Makefile | patch | blob | history | |
drivers/irqchip/irq-pruss-intc.c | [new file with mode: 0644] | patch | blob |
include/linux/pruss_driver.h | patch | blob | history |
index fbd1ec8070efa89e5439321f410af09579e76b1e..b49c2470fa94ad76df1be15c6b4ac7a969485772 100644 (file)
--- a/drivers/irqchip/Makefile
+++ b/drivers/irqchip/Makefile
obj-$(CONFIG_NDS32) += irq-ativic32.o
obj-$(CONFIG_QCOM_PDC) += qcom-pdc.o
obj-$(CONFIG_SIFIVE_PLIC) += irq-sifive-plic.o
+obj-$(CONFIG_TI_PRUSS) += irq-pruss-intc.o
diff --git a/drivers/irqchip/irq-pruss-intc.c b/drivers/irqchip/irq-pruss-intc.c
--- /dev/null
@@ -0,0 +1,571 @@
+// SPDX-License-Identifier: GPL-2.0
+/*
+ * PRU-ICSS INTC IRQChip driver for various TI SoCs
+ *
+ * Copyright (C) 2016-2019 Texas Instruments Incorporated - http://www.ti.com/
+ * Andrew F. Davis <afd@ti.com>
+ * Suman Anna <s-anna@ti.com>
+ */
+
+#include <linux/irq.h>
+#include <linux/irqchip/chained_irq.h>
+#include <linux/irqdomain.h>
+#include <linux/module.h>
+#include <linux/of_device.h>
+#include <linux/platform_device.h>
+#include <linux/pruss_driver.h>
+
+/*
+ * Number of host interrupts reaching the main MPU sub-system. Note that this
+ * is not the same as the total number of host interrupts supported by the PRUSS
+ * INTC instance
+ */
+#define MAX_HOST_NUM_IRQS 8
+
+/* PRU_ICSS_INTC registers */
+#define PRU_INTC_REVID 0x0000
+#define PRU_INTC_CR 0x0004
+#define PRU_INTC_GER 0x0010
+#define PRU_INTC_GNLR 0x001C
+#define PRU_INTC_SISR 0x0020
+#define PRU_INTC_SICR 0x0024
+#define PRU_INTC_EISR 0x0028
+#define PRU_INTC_EICR 0x002C
+#define PRU_INTC_HIEISR 0x0034
+#define PRU_INTC_HIDISR 0x0038
+#define PRU_INTC_GPIR 0x0080
+#define PRU_INTC_SRSR0 0x0200
+#define PRU_INTC_SRSR1 0x0204
+#define PRU_INTC_SECR0 0x0280
+#define PRU_INTC_SECR1 0x0284
+#define PRU_INTC_ESR0 0x0300
+#define PRU_INTC_ESR1 0x0304
+#define PRU_INTC_ECR0 0x0380
+#define PRU_INTC_ECR1 0x0384
+#define PRU_INTC_CMR(x) (0x0400 + (x) * 4)
+#define PRU_INTC_HMR(x) (0x0800 + (x) * 4)
+#define PRU_INTC_HIPIR(x) (0x0900 + (x) * 4)
+#define PRU_INTC_SIPR0 0x0D00
+#define PRU_INTC_SIPR1 0x0D04
+#define PRU_INTC_SITR0 0x0D80
+#define PRU_INTC_SITR1 0x0D84
+#define PRU_INTC_HINLR(x) (0x1100 + (x) * 4)
+#define PRU_INTC_HIER 0x1500
+
+/* HIPIR register bit-fields */
+#define INTC_HIPIR_NONE_HINT 0x80000000
+
+static const char * const irq_names[] = {
+ "host2", "host3", "host4", "host5", "host6", "host7", "host8", "host9",
+};
+
+/**
+ * struct pruss_intc - PRUSS interrupt controller structure
+ * @pruss: back-reference to parent PRUSS structure
+ * @irqs: kernel irq numbers corresponding to PRUSS host interrupts
+ * @base: base virtual address of INTC register space
+ * @irqchip: irq chip for this interrupt controller
+ * @domain: irq domain for this interrupt controller
+ * @config_map: stored INTC configuration mapping data
+ * @lock: mutex to serialize access to INTC
+ * @host_mask: indicate which HOST IRQs are enabled
+ */
+struct pruss_intc {
+ struct pruss *pruss;
+ unsigned int irqs[MAX_HOST_NUM_IRQS];
+ void __iomem *base;
+ struct irq_chip *irqchip;
+ struct irq_domain *domain;
+ struct pruss_intc_config config_map;
+ struct mutex lock; /* PRUSS INTC lock */
+ u32 host_mask;
+};
+
+static inline u32 pruss_intc_read_reg(struct pruss_intc *intc, unsigned int reg)
+{
+ return readl_relaxed(intc->base + reg);
+}
+
+static inline void pruss_intc_write_reg(struct pruss_intc *intc,
+ unsigned int reg, u32 val)
+{
+ writel_relaxed(val, intc->base + reg);
+}
+
+static int pruss_intc_check_write(struct pruss_intc *intc, unsigned int reg,
+ unsigned int sysevent)
+{
+ if (!intc)
+ return -EINVAL;
+
+ if (sysevent >= MAX_PRU_SYS_EVENTS)
+ return -EINVAL;
+
+ pruss_intc_write_reg(intc, reg, sysevent);
+
+ return 0;
+}
+
+static struct pruss_intc *to_pruss_intc(struct pruss *pruss)
+{
+ struct device_node *parent = pruss->dev->of_node;
+ struct device_node *np;
+ struct platform_device *pdev;
+ struct pruss_intc *intc = NULL;
+
+ np = of_get_child_by_name(parent, "interrupt-controller");
+ if (!np) {
+ dev_err(pruss->dev, "pruss does not have an interrupt-controller node\n");
+ return NULL;
+ }
+
+ pdev = of_find_device_by_node(np);
+ if (!pdev) {
+ dev_err(pruss->dev, "no associated platform device\n");
+ goto out;
+ }
+
+ intc = platform_get_drvdata(pdev);
+out:
+ of_node_put(np);
+ return intc;
+}
+
+/**
+ * pruss_intc_configure() - configure the PRUSS INTC
+ * @pruss: the pruss instance
+ * @intc_config: PRU core-specific INTC configuration
+ *
+ * Configures the PRUSS INTC with the provided configuration from
+ * a PRU core. Any existing event to channel mappings or channel to
+ * host interrupt mappings are checked to make sure there are no
+ * conflicting configuration between both the PRU cores. The function
+ * is intended to be used only by the PRU remoteproc driver.
+ *
+ * Returns 0 on success, or a suitable error code otherwise
+ */
+int pruss_intc_configure(struct pruss *pruss,
+ struct pruss_intc_config *intc_config)
+{
+ struct device *dev = pruss->dev;
+ struct pruss_intc *intc = to_pruss_intc(pruss);
+ int i, idx, ret;
+ s8 ch, host;
+ u64 sysevt_mask = 0;
+ u32 ch_mask = 0;
+ u32 host_mask = 0;
+ u32 val;
+
+ if (!intc)
+ return -EINVAL;
+
+ mutex_lock(&intc->lock);
+
+ /*
+ * configure channel map registers - each register holds map info
+ * for 4 events, with each event occupying the lower nibble in
+ * a register byte address in little-endian fashion
+ */
+ for (i = 0; i < ARRAY_SIZE(intc_config->sysev_to_ch); i++) {
+ ch = intc_config->sysev_to_ch[i];
+ if (ch < 0)
+ continue;
+
+ /* check if sysevent already assigned */
+ if (intc->config_map.sysev_to_ch[i] != -1) {
+ dev_err(dev, "event %d (req. channel %d) already assigned to channel %d\n",
+ i, ch, intc->config_map.sysev_to_ch[i]);
+ ret = -EEXIST;
+ goto unlock;
+ }
+
+ intc->config_map.sysev_to_ch[i] = ch;
+
+ idx = i / 4;
+ val = pruss_intc_read_reg(intc, PRU_INTC_CMR(idx));
+ val |= ch << ((i & 3) * 8);
+ pruss_intc_write_reg(intc, PRU_INTC_CMR(idx), val);
+ sysevt_mask |= BIT_ULL(i);
+ ch_mask |= BIT(ch);
+
+ dev_dbg(dev, "SYSEV%d -> CH%d (CMR%d 0x%08x)\n", i, ch, idx,
+ pruss_intc_read_reg(intc, PRU_INTC_CMR(idx)));
+ }
+
+ /*
+ * set host map registers - each register holds map info for
+ * 4 channels, with each channel occupying the lower nibble in
+ * a register byte address in little-endian fashion
+ */
+ for (i = 0; i < ARRAY_SIZE(intc_config->ch_to_host); i++) {
+ host = intc_config->ch_to_host[i];
+ if (host < 0)
+ continue;
+
+ /* check if channel already assigned */
+ if (intc->config_map.ch_to_host[i] != -1) {
+ dev_err(dev, "channel %d (req. intr_no %d) already assigned to intr_no %d\n",
+ i, host, intc->config_map.ch_to_host[i]);
+ ret = -EEXIST;
+ goto unlock;
+ }
+
+ /* check if host intr is already in use by other PRU */
+ if (intc->host_mask & (1U << host)) {
+ dev_err(dev, "%s: host intr %d already in use\n",
+ __func__, host);
+ ret = -EEXIST;
+ goto unlock;
+ }
+
+ intc->config_map.ch_to_host[i] = host;
+
+ idx = i / 4;
+
+ val = pruss_intc_read_reg(intc, PRU_INTC_HMR(idx));
+ val |= host << ((i & 3) * 8);
+ pruss_intc_write_reg(intc, PRU_INTC_HMR(idx), val);
+
+ ch_mask |= BIT(i);
+ host_mask |= BIT(host);
+
+ dev_dbg(dev, "CH%d -> HOST%d (HMR%d 0x%08x)\n", i, host, idx,
+ pruss_intc_read_reg(intc, PRU_INTC_HMR(idx)));
+ }
+
+ dev_info(dev, "configured system_events = 0x%016llx intr_channels = 0x%08x host_intr = 0x%08x\n",
+ sysevt_mask, ch_mask, host_mask);
+
+ /* enable system events, writing 0 has no-effect */
+ pruss_intc_write_reg(intc, PRU_INTC_ESR0, lower_32_bits(sysevt_mask));
+ pruss_intc_write_reg(intc, PRU_INTC_SECR0, lower_32_bits(sysevt_mask));
+ pruss_intc_write_reg(intc, PRU_INTC_ESR1, upper_32_bits(sysevt_mask));
+ pruss_intc_write_reg(intc, PRU_INTC_SECR1, upper_32_bits(sysevt_mask));
+
+ /* enable host interrupts */
+ for (i = 0; i < MAX_PRU_HOST_INT; i++) {
+ if (host_mask & BIT(i))
+ pruss_intc_write_reg(intc, PRU_INTC_HIEISR, i);
+ }
+
+ /* global interrupt enable */
+ pruss_intc_write_reg(intc, PRU_INTC_GER, 1);
+
+ intc->host_mask |= host_mask;
+
+ mutex_unlock(&intc->lock);
+ return 0;
+
+unlock:
+ mutex_unlock(&intc->lock);
+ return ret;
+}
+EXPORT_SYMBOL_GPL(pruss_intc_configure);
+
+/**
+ * pruss_intc_unconfigure() - unconfigure the PRUSS INTC
+ * @pruss: the pruss instance
+ * @intc_config: PRU core specific INTC configuration
+ *
+ * Undo whatever was done in pruss_intc_configure() for a PRU core.
+ * It should be sufficient to just mark the resources free in the
+ * global map and disable the host interrupts and sysevents.
+ */
+int pruss_intc_unconfigure(struct pruss *pruss,
+ struct pruss_intc_config *intc_config)
+{
+ struct device *dev = pruss->dev;
+ struct pruss_intc *intc = to_pruss_intc(pruss);
+ int i;
+ s8 ch, host;
+ u64 sysevt_mask = 0;
+ u32 host_mask = 0;
+
+ if (!intc)
+ return -EINVAL;
+
+ mutex_lock(&intc->lock);
+
+ for (i = 0; i < ARRAY_SIZE(intc_config->sysev_to_ch); i++) {
+ ch = intc_config->sysev_to_ch[i];
+ if (ch < 0)
+ continue;
+
+ /* mark sysevent free in global map */
+ intc->config_map.sysev_to_ch[i] = -1;
+ sysevt_mask |= BIT_ULL(i);
+ }
+
+ for (i = 0; i < ARRAY_SIZE(intc_config->ch_to_host); i++) {
+ host = intc_config->ch_to_host[i];
+ if (host < 0)
+ continue;
+
+ /* mark channel free in global map */
+ intc->config_map.ch_to_host[i] = -1;
+ host_mask |= BIT(host);
+ }
+
+ dev_info(dev, "unconfigured system_events = 0x%016llx host_intr = 0x%08x\n",
+ sysevt_mask, host_mask);
+
+ /* disable system events, writing 0 has no-effect */
+ pruss_intc_write_reg(intc, PRU_INTC_ECR0, lower_32_bits(sysevt_mask));
+ pruss_intc_write_reg(intc, PRU_INTC_ECR1, upper_32_bits(sysevt_mask));
+ /* clear any pending status */
+ pruss_intc_write_reg(intc, PRU_INTC_SECR0, lower_32_bits(sysevt_mask));
+ pruss_intc_write_reg(intc, PRU_INTC_SECR1, upper_32_bits(sysevt_mask));
+
+ /* disable host interrupts */
+ for (i = 0; i < MAX_PRU_HOST_INT; i++) {
+ if (host_mask & BIT(i))
+ pruss_intc_write_reg(intc, PRU_INTC_HIDISR, i);
+ }
+
+ intc->host_mask &= ~host_mask;
+ mutex_unlock(&intc->lock);
+
+ return 0;
+}
+EXPORT_SYMBOL_GPL(pruss_intc_unconfigure);
+
+static void pruss_intc_init(struct pruss_intc *intc)
+{
+ int i;
+
+ /* configure polarity to active high for all system interrupts */
+ pruss_intc_write_reg(intc, PRU_INTC_SIPR0, 0xffffffff);
+ pruss_intc_write_reg(intc, PRU_INTC_SIPR1, 0xffffffff);
+
+ /* configure type to pulse interrupt for all system interrupts */
+ pruss_intc_write_reg(intc, PRU_INTC_SITR0, 0);
+ pruss_intc_write_reg(intc, PRU_INTC_SITR1, 0);
+
+ /* clear all 16 interrupt channel map registers */
+ for (i = 0; i < 16; i++)
+ pruss_intc_write_reg(intc, PRU_INTC_CMR(i), 0);
+
+ /* clear all 3 host interrupt map registers */
+ for (i = 0; i < 3; i++)
+ pruss_intc_write_reg(intc, PRU_INTC_HMR(i), 0);
+}
+
+static void pruss_intc_irq_ack(struct irq_data *data)
+{
+ struct pruss_intc *intc = irq_data_get_irq_chip_data(data);
+ unsigned int hwirq = data->hwirq;
+
+ pruss_intc_check_write(intc, PRU_INTC_SICR, hwirq);
+}
+
+static void pruss_intc_irq_mask(struct irq_data *data)
+{
+ struct pruss_intc *intc = irq_data_get_irq_chip_data(data);
+ unsigned int hwirq = data->hwirq;
+
+ pruss_intc_check_write(intc, PRU_INTC_EICR, hwirq);
+}
+
+static void pruss_intc_irq_unmask(struct irq_data *data)
+{
+ struct pruss_intc *intc = irq_data_get_irq_chip_data(data);
+ unsigned int hwirq = data->hwirq;
+
+ pruss_intc_check_write(intc, PRU_INTC_EISR, hwirq);
+}
+
+static int pruss_intc_irq_retrigger(struct irq_data *data)
+{
+ struct pruss_intc *intc = irq_data_get_irq_chip_data(data);
+ unsigned int hwirq = data->hwirq;
+
+ return pruss_intc_check_write(intc, PRU_INTC_SISR, hwirq);
+}
+
+static int pruss_intc_irq_reqres(struct irq_data *data)
+{
+ if (!try_module_get(THIS_MODULE))
+ return -ENODEV;
+
+ return 0;
+}
+
+static void pruss_intc_irq_relres(struct irq_data *data)
+{
+ module_put(THIS_MODULE);
+}
+
+static int pruss_intc_irq_domain_map(struct irq_domain *d, unsigned int virq,
+ irq_hw_number_t hw)
+{
+ struct pruss_intc *intc = d->host_data;
+
+ irq_set_chip_data(virq, intc);
+ irq_set_chip_and_handler(virq, intc->irqchip, handle_level_irq);
+
+ return 0;
+}
+
+static void pruss_intc_irq_domain_unmap(struct irq_domain *d, unsigned int virq)
+{
+ irq_set_chip_and_handler(virq, NULL, NULL);
+ irq_set_chip_data(virq, NULL);
+}
+
+static const struct irq_domain_ops pruss_intc_irq_domain_ops = {
+ .xlate = irq_domain_xlate_onecell,
+ .map = pruss_intc_irq_domain_map,
+ .unmap = pruss_intc_irq_domain_unmap,
+};
+
+static void pruss_intc_irq_handler(struct irq_desc *desc)
+{
+ unsigned int irq = irq_desc_get_irq(desc);
+ struct irq_chip *chip = irq_desc_get_chip(desc);
+ struct pruss_intc *intc = irq_get_handler_data(irq);
+ u32 hipir;
+ unsigned int virq;
+ int i, hwirq;
+
+ chained_irq_enter(chip, desc);
+
+ /* find our host irq number */
+ for (i = 0; i < MAX_HOST_NUM_IRQS; i++)
+ if (intc->irqs[i] == irq)
+ break;
+ if (i == MAX_HOST_NUM_IRQS)
+ goto err;
+
+ i += MIN_PRU_HOST_INT;
+
+ /* get highest priority pending PRUSS system event */
+ hipir = pruss_intc_read_reg(intc, PRU_INTC_HIPIR(i));
+ while (!(hipir & BIT(31))) {
+ hwirq = hipir & GENMASK(9, 0);
+ virq = irq_linear_revmap(intc->domain, hwirq);
+
+ /*
+ * XXX: manually ACK any system events that do not have a
+ * handler mapped yet
+ */
+ if (unlikely(!virq))
+ pruss_intc_check_write(intc, PRU_INTC_SICR, hwirq);
+ else
+ generic_handle_irq(virq);
+
+ /* get next system event */
+ hipir = pruss_intc_read_reg(intc, PRU_INTC_HIPIR(i));
+ }
+err:
+ chained_irq_exit(chip, desc);
+}
+
+static int pruss_intc_probe(struct platform_device *pdev)
+{
+ struct device *dev = &pdev->dev;
+ struct platform_device *ppdev = to_platform_device(dev->parent);
+ struct pruss_intc *intc;
+ struct resource *res;
+ struct irq_chip *irqchip;
+ int i, irq;
+
+ intc = devm_kzalloc(dev, sizeof(*intc), GFP_KERNEL);
+ if (!intc)
+ return -ENOMEM;
+ platform_set_drvdata(pdev, intc);
+
+ res = platform_get_resource(pdev, IORESOURCE_MEM, 0);
+ intc->base = devm_ioremap_resource(dev, res);
+ if (IS_ERR(intc->base)) {
+ dev_err(dev, "failed to parse and map intc memory resource\n");
+ return PTR_ERR(intc->base);
+ }
+
+ dev_dbg(dev, "intc memory: pa %pa size 0x%zx va %pK\n", &res->start,
+ (size_t)resource_size(res), intc->base);
+
+ mutex_init(&intc->lock);
+
+ for (i = 0; i < ARRAY_SIZE(intc->config_map.sysev_to_ch); i++)
+ intc->config_map.sysev_to_ch[i] = -1;
+
+ for (i = 0; i < ARRAY_SIZE(intc->config_map.ch_to_host); i++)
+ intc->config_map.ch_to_host[i] = -1;
+
+ intc->pruss = platform_get_drvdata(ppdev);
+ pruss_intc_init(intc);
+
+ irqchip = devm_kzalloc(dev, sizeof(*irqchip), GFP_KERNEL);
+ if (!irqchip)
+ return -ENOMEM;
+
+ irqchip->irq_ack = pruss_intc_irq_ack;
+ irqchip->irq_mask = pruss_intc_irq_mask;
+ irqchip->irq_unmask = pruss_intc_irq_unmask;
+ irqchip->irq_retrigger = pruss_intc_irq_retrigger;
+ irqchip->irq_request_resources = pruss_intc_irq_reqres;
+ irqchip->irq_release_resources = pruss_intc_irq_relres;
+ irqchip->name = dev_name(dev);
+ intc->irqchip = irqchip;
+
+ /* always 64 events */
+ intc->domain = irq_domain_add_linear(dev->of_node, MAX_PRU_SYS_EVENTS,
+ &pruss_intc_irq_domain_ops, intc);
+ if (!intc->domain)
+ return -ENOMEM;
+
+ for (i = 0; i < MAX_HOST_NUM_IRQS; i++) {
+ irq = platform_get_irq_byname(ppdev, irq_names[i]);
+ if (irq < 0) {
+ dev_err(dev->parent, "platform_get_irq_byname failed for %s : %d\n",
+ irq_names[i], irq);
+ goto fail_irq;
+ }
+
+ intc->irqs[i] = irq;
+ irq_set_handler_data(irq, intc);
+ irq_set_chained_handler(irq, pruss_intc_irq_handler);
+ }
+
+ return 0;
+
+fail_irq:
+ irq_domain_remove(intc->domain);
+ return irq;
+}
+
+static int pruss_intc_remove(struct platform_device *pdev)
+{
+ struct pruss_intc *intc = platform_get_drvdata(pdev);
+ unsigned int hwirq;
+
+ if (intc->domain) {
+ for (hwirq = 0; hwirq < MAX_PRU_SYS_EVENTS; hwirq++)
+ irq_dispose_mapping(irq_find_mapping(intc->domain,
+ hwirq));
+ irq_domain_remove(intc->domain);
+ }
+
+ return 0;
+}
+
+static const struct of_device_id pruss_intc_of_match[] = {
+ { .compatible = "ti,am3356-pruss-intc", },
+ { /* sentinel */ },
+};
+MODULE_DEVICE_TABLE(of, pruss_intc_of_match);
+
+static struct platform_driver pruss_intc_driver = {
+ .driver = {
+ .name = "pruss-intc",
+ .of_match_table = pruss_intc_of_match,
+ },
+ .probe = pruss_intc_probe,
+ .remove = pruss_intc_remove,
+};
+module_platform_driver(pruss_intc_driver);
+
+MODULE_AUTHOR("Andrew F. Davis <afd@ti.com>");
+MODULE_AUTHOR("Suman Anna <s-anna@ti.com>");
+MODULE_DESCRIPTION("PRU-ICSS INTC Driver");
+MODULE_LICENSE("GPL v2");
index 874c61be8a0739aa3b1618d99784fb05228e33f1..fe7d513ea8e7322abc16aef070d3de342b64e291 100644 (file)
#ifndef _PRUSS_DRIVER_H_
#define _PRUSS_DRIVER_H_
+/* maximum number of system events */
+#define MAX_PRU_SYS_EVENTS 64
+
+/* maximum number of interrupt channels */
+#define MAX_PRU_CHANNELS 10
+
+/* minimum starting host interrupt number for MPU */
+#define MIN_PRU_HOST_INT 2
+
+/* maximum number of host interrupts */
+#define MAX_PRU_HOST_INT 10
+
/**
* enum pruss_mem - PRUSS memory range identifiers
*/
size_t size;
};
+/**
+ * struct pruss_intc_config - INTC configuration info
+ * @sysev_to_ch: system events to channel mapping information
+ * @ch_to_host: interrupt channel to host interrupt information
+ */
+struct pruss_intc_config {
+ s8 sysev_to_ch[MAX_PRU_SYS_EVENTS];
+ s8 ch_to_host[MAX_PRU_CHANNELS];
+};
+
/**
* struct pruss - PRUSS parent structure
* @dev: pruss device pointer
struct pruss_mem_region mem_regions[PRUSS_MEM_MAX];
};
+int pruss_intc_configure(struct pruss *pruss,
+ struct pruss_intc_config *intc_config);
+int pruss_intc_unconfigure(struct pruss *pruss,
+ struct pruss_intc_config *intc_config);
+
#endif /* _PRUSS_DRIVER_H_ */