]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/commitdiff
remoteproc/omap: add support for system suspend/resume
authorSuman Anna <s-anna@ti.com>
Thu, 22 Feb 2018 23:57:17 +0000 (17:57 -0600)
committerSuman Anna <s-anna@ti.com>
Mon, 4 Mar 2019 16:17:26 +0000 (10:17 -0600)
This patch adds the support for system suspend/resume to the
OMAP remoteproc driver so that the OMAP remoteproc devices can
be suspended/resumed during a system suspend/resume. The support
is added through the driver PM .suspend/.resume callbacks, and
requires appropriate support from the OS running on the remote
processors.

The IPU & DSP remote processors typically have their own private
modules like registers, internal memories, caches etc. The context
of these modules need to be saved and restored properly for a
suspend/resume to work. These are in general not accessible from
the MPU, so the remote processors themselves have to implement
the logic for the context save & restore of these modules.

The OMAP remoteproc driver initiates a suspend by sending a mailbox
message requesting the remote processor to save its context and
enter into an idle/standby state. The remote processor should
usually stop whatever processing it is doing to switch to a context
save mode. The OMAP remoteproc driver detects the completion of
the context save by checking the module standby status for the
remoteproc device. It also stops any resources used by the remote
processors like the timers. The timers need to be running only
when the processor is active and executing, and need to be stopped
otherwise to allow the timer driver to reach low-power states. The
IOMMUs are automatically suspended by the PM core during the late
suspend stage, after the remoteproc suspend process is completed by
putting the remote processor cores into reset. Thereafter, the Linux
kernel can put the domain into further lower power states as possible.

The resume sequence undoes the operations performed in the PM suspend
callback, by starting the timers and finally releasing the processors
from reset. This requires that the remote processor side OS be able to
distinguish a power-resume boot from a power-on/cold boot, restore the
context of its private modules saved during the suspend phase, and
resume executing code from where it was suspended. The IOMMUs would
have been resumed by the PM core during early resume, so they are
already enabled by the time remoteproc resume callback gets invoked.

The remote processors should save their context into System RAM (DDR),
as any internal memories are not guaranteed to retain context as it
depends on the lowest power domain that the remote processor device
is put into. The management of the DDR contents will be managed by
the Linux kernel.

Signed-off-by: Suman Anna <s-anna@ti.com>
drivers/remoteproc/omap_remoteproc.c
drivers/remoteproc/omap_remoteproc.h

index 3e34778c2cebe81efa8436cc63d48cfc1ed66e66..0d35efb96cc122b6f97c460a017fd5041627de09 100644 (file)
@@ -16,6 +16,7 @@
 #include <linux/kernel.h>
 #include <linux/module.h>
 #include <linux/err.h>
+#include <linux/io.h>
 #include <linux/of_device.h>
 #include <linux/of_address.h>
 #include <linux/of_reserved_mem.h>
@@ -24,6 +25,7 @@
 #include <linux/remoteproc.h>
 #include <linux/mailbox_client.h>
 #include <linux/omap-mailbox.h>
+#include <linux/omap-iommu.h>
 #include <linux/regmap.h>
 #include <linux/mfd/syscon.h>
 #include <clocksource/timer-ti-dm.h>
@@ -84,6 +86,9 @@ struct omap_rproc_timer {
  * @num_timers: number of rproc timer(s)
  * @timers: timer(s) info used by rproc
  * @rproc: rproc handle
+ * @pm_comp: completion primitive to sync for suspend response
+ * @standby_addr: kernel address of the register having module standby status
+ * @suspend_acked: state machine flag to store the suspend request ack
  */
 struct omap_rproc {
        struct mbox_chan *mbox;
@@ -94,6 +99,9 @@ struct omap_rproc {
        int num_timers;
        struct omap_rproc_timer *timers;
        struct rproc *rproc;
+       struct completion pm_comp;
+       void __iomem *standby_addr;
+       bool suspend_acked;
 };
 
 /**
@@ -344,6 +352,11 @@ static void omap_rproc_mbox_callback(struct mbox_client *client, void *data)
        case RP_MBOX_ECHO_REPLY:
                dev_info(dev, "received echo reply from %s\n", name);
                break;
+       case RP_MBOX_SUSPEND_ACK:
+       case RP_MBOX_SUSPEND_CANCEL:
+               oproc->suspend_acked = msg == RP_MBOX_SUSPEND_ACK;
+               complete(&oproc->pm_comp);
+               break;
        default:
                if (msg >= RP_MBOX_READY && msg < RP_MBOX_END_MSG)
                        return;
@@ -534,6 +547,171 @@ static const struct rproc_ops omap_rproc_ops = {
        .da_to_va       = omap_rproc_da_to_va,
 };
 
+#ifdef CONFIG_PM
+static bool _is_rproc_in_standby(struct omap_rproc *oproc)
+{
+       static int standby_mask = (1 << 18);
+
+       return readl(oproc->standby_addr) & standby_mask;
+}
+
+/* 1 sec is long enough time to let the remoteproc side suspend the device */
+#define DEF_SUSPEND_TIMEOUT 1000
+static int _omap_rproc_suspend(struct rproc *rproc)
+{
+       struct device *dev = rproc->dev.parent;
+       struct platform_device *pdev = to_platform_device(dev);
+       struct omap_rproc_pdata *pdata = dev_get_platdata(dev);
+       struct omap_rproc *oproc = rproc->priv;
+       unsigned long to = msecs_to_jiffies(DEF_SUSPEND_TIMEOUT);
+       unsigned long ta = jiffies + to;
+       int ret;
+
+       reinit_completion(&oproc->pm_comp);
+       oproc->suspend_acked = false;
+       ret = mbox_send_message(oproc->mbox, (void *)RP_MBOX_SUSPEND_SYSTEM);
+       if (ret < 0) {
+               dev_err(dev, "PM mbox_send_message failed: %d\n", ret);
+               return ret;
+       }
+
+       ret = wait_for_completion_timeout(&oproc->pm_comp, to);
+       if (!oproc->suspend_acked)
+               return -EBUSY;
+
+       /*
+        * The remoteproc side is returning the ACK message before saving the
+        * context, because the context saving is performed within a SYS/BIOS
+        * function, and it cannot have any inter-dependencies against the IPC
+        * layer. Also, as the SYS/BIOS needs to preserve properly the processor
+        * register set, sending this ACK or signalling the completion of the
+        * context save through a shared memory variable can never be the
+        * absolute last thing to be executed on the remoteproc side, and the
+        * MPU cannot use the ACK message as a sync point to put the remoteproc
+        * into reset. The only way to ensure that the remote processor has
+        * completed saving the context is to check that the module has reached
+        * STANDBY state (after saving the context, the SYS/BIOS executes the
+        * appropriate target-specific WFI instruction causing the module to
+        * enter STANDBY).
+        */
+       while (!_is_rproc_in_standby(oproc)) {
+               if (time_after(jiffies, ta))
+                       return -ETIME;
+               schedule();
+       }
+
+       ret = pdata->device_shutdown(pdev);
+       if (ret)
+               return ret;
+
+       ret = omap_rproc_disable_timers(rproc, false);
+       if (ret) {
+               dev_err(dev, "disabling timers during suspend failed %d\n",
+                       ret);
+               goto enable_device;
+       }
+
+       return 0;
+
+enable_device:
+       pdata->device_enable(pdev);
+       return ret;
+}
+
+static int _omap_rproc_resume(struct rproc *rproc)
+{
+       struct device *dev = rproc->dev.parent;
+       struct platform_device *pdev = to_platform_device(dev);
+       struct omap_rproc_pdata *pdata = dev_get_platdata(dev);
+       struct omap_rproc *oproc = rproc->priv;
+       int ret;
+
+       /* boot address could be lost after suspend, so restore it */
+       if (oproc->boot_data) {
+               ret = omap_rproc_write_dsp_boot_addr(rproc);
+               if (ret) {
+                       dev_err(dev, "boot address restore failed %d\n", ret);
+                       goto out;
+               }
+       }
+
+       ret = omap_rproc_enable_timers(rproc, false);
+       if (ret) {
+               dev_err(dev, "enabling timers during resume failed %d\n",
+                       ret);
+               goto out;
+       }
+
+       ret = pdata->device_enable(pdev);
+       if (ret)
+               goto disable_timers;
+
+       return 0;
+
+disable_timers:
+       omap_rproc_disable_timers(rproc, false);
+out:
+       return ret;
+}
+
+static int __maybe_unused omap_rproc_suspend(struct device *dev)
+{
+       struct platform_device *pdev = to_platform_device(dev);
+       struct rproc *rproc = platform_get_drvdata(pdev);
+       int ret = 0;
+
+       mutex_lock(&rproc->lock);
+       if (rproc->state == RPROC_OFFLINE)
+               goto out;
+
+       if (rproc->state == RPROC_SUSPENDED)
+               goto out;
+
+       if (rproc->state != RPROC_RUNNING) {
+               ret = -EBUSY;
+               goto out;
+       }
+
+       ret = _omap_rproc_suspend(rproc);
+       if (ret) {
+               dev_err(dev, "suspend failed %d\n", ret);
+               goto out;
+       }
+
+       rproc->state = RPROC_SUSPENDED;
+out:
+       mutex_unlock(&rproc->lock);
+       return ret;
+}
+
+static int __maybe_unused omap_rproc_resume(struct device *dev)
+{
+       struct platform_device *pdev = to_platform_device(dev);
+       struct rproc *rproc = platform_get_drvdata(pdev);
+       int ret = 0;
+
+       mutex_lock(&rproc->lock);
+       if (rproc->state == RPROC_OFFLINE)
+               goto out;
+
+       if (rproc->state != RPROC_SUSPENDED) {
+               ret = -EBUSY;
+               goto out;
+       }
+
+       ret = _omap_rproc_resume(rproc);
+       if (ret) {
+               dev_err(dev, "resume failed %d\n", ret);
+               goto out;
+       }
+
+       rproc->state = RPROC_RUNNING;
+out:
+       mutex_unlock(&rproc->lock);
+       return ret;
+}
+#endif /* CONFIG_PM */
+
 static const struct omap_rproc_dev_data omap4_dsp_dev_data = {
        .device_name    = "dsp",
        .fw_name        = "omap4-dsp-fw.xe64T",
@@ -754,6 +932,7 @@ static int omap_rproc_probe(struct platform_device *pdev)
        struct omap_rproc *oproc;
        struct rproc *rproc;
        const char *firmware;
+       u32 standby_addr = 0;
        int ret;
 
        if (!np) {
@@ -818,6 +997,21 @@ static int omap_rproc_probe(struct platform_device *pdev)
                        oproc->num_timers);
        }
 
+       init_completion(&oproc->pm_comp);
+
+       ret = of_property_read_u32(np, "ti,rproc-standby-info", &standby_addr);
+       if (ret || !standby_addr) {
+               ret = !standby_addr ? -EINVAL : ret;
+               goto free_rproc;
+       }
+
+       oproc->standby_addr = devm_ioremap(&pdev->dev, standby_addr,
+                                          sizeof(u32));
+       if (!oproc->standby_addr) {
+               ret = -ENOMEM;
+               goto free_rproc;
+       }
+
        ret = of_reserved_mem_device_init(&pdev->dev);
        if (ret) {
                dev_err(&pdev->dev, "device does not have specific CMA pool\n");
@@ -853,11 +1047,16 @@ static int omap_rproc_remove(struct platform_device *pdev)
        return 0;
 }
 
+static const struct dev_pm_ops omap_rproc_pm_ops = {
+       SET_SYSTEM_SLEEP_PM_OPS(omap_rproc_suspend, omap_rproc_resume)
+};
+
 static struct platform_driver omap_rproc_driver = {
        .probe = omap_rproc_probe,
        .remove = omap_rproc_remove,
        .driver = {
                .name = "omap-rproc",
+               .pm = &omap_rproc_pm_ops,
                .of_match_table = omap_rproc_of_match,
        },
 };
index 18f5226176834608e98eb00d5aa8e518120dfde6..b74d140cbbb6ca1d584353ded3d04cb3017cd70c 100644 (file)
@@ -2,7 +2,7 @@
 /*
  * Remote processor messaging
  *
- * Copyright (C) 2011 Texas Instruments, Inc.
+ * Copyright (C) 2011-2019 Texas Instruments, Inc.
  * Copyright (C) 2011 Google, Inc.
  * All rights reserved.
  */
  * @RP_MBOX_ABORT_REQUEST: a "please crash" request, used for testing the
  * recovery mechanism (to some extent).
  *
+ * @RP_MBOX_SUSPEND_AUTO: auto suspend request for the remote processor
+ *
+ * @RP_MBOX_SUSPEND_SYSTEM: system suspend request for the remote processor
+ *
+ * @RP_MBOX_SUSPEND_ACK: successful response from remote processor for a
+ * suspend request
+ *
+ * @RP_MBOX_SUSPEND_CANCEL: a cancel suspend response from a remote processor
+ * on a suspend request
+ *
  * Introduce new message definitions if any here.
  *
  * @RP_MBOX_END_MSG: Indicates end of known/defined messages from remote core
@@ -45,7 +55,11 @@ enum omap_rp_mbox_messages {
        RP_MBOX_ECHO_REQUEST    = 0xFFFFFF03,
        RP_MBOX_ECHO_REPLY      = 0xFFFFFF04,
        RP_MBOX_ABORT_REQUEST   = 0xFFFFFF05,
-       RP_MBOX_END_MSG         = 0xFFFFFF06,
+       RP_MBOX_SUSPEND_AUTO    = 0xFFFFFF10,
+       RP_MBOX_SUSPEND_SYSTEM  = 0xFFFFFF11,
+       RP_MBOX_SUSPEND_ACK     = 0xFFFFFF12,
+       RP_MBOX_SUSPEND_CANCEL  = 0xFFFFFF13,
+       RP_MBOX_END_MSG         = 0xFFFFFF14,
 };
 
 #endif /* _OMAP_RPMSG_H */