summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: e0c5136)
raw | patch | inline | side by side (parent: e0c5136)
author | Suman Anna <s-anna@ti.com> | |
Tue, 4 Dec 2018 22:07:43 +0000 (17:07 -0500) | ||
committer | Suman Anna <s-anna@ti.com> | |
Wed, 27 Feb 2019 20:35:18 +0000 (14:35 -0600) |
The AM65x SoCs have a single dual-core Arm Cortex R5F processor cluster/
subsystem (R5FSS) in the MCU voltage domain. This R5F subsystem/cluster
can be configured at boot time to be either run in a LockStep mode or in
an Asymmetric Multi Processing (AMP) fashion in Split-mode. This subsystem
has 64 KB each Tightly-Coupled Memory (TCM) internal memories for each
core split between two banks - TCMA and TCMB (further interleaved into
two banks). The subsystem does not have an MMU, but has a Region Address
Translater (RAT) module that is accessible only from the R5Fs for providing
translations between 32-bit CPU addresses into larger system bus addresses.
Add a remoteproc driver to support this subsystem to be able to load and
boot the R5F cores primarily in LockStep mode. The code also includes the
base support for Split mode. Error Recovery and Power Management features
are not currently supported. Loading support includes the internal TCMs
and DDR. RAT support is left for a future patch, and as such the reserved
memory carveout regions are all expected to be using memory regions within
the first 2 GB.
The R5F remote processors do not have an MMU, and so require fixed memory
carveout regions matching the firmware image addresses. Support for this
is provided by mandating multiple memory regions to be attached to the
remoteproc device. The first memory region will be used to serve as the
DMA pool for all dynamic allocations like the vrings and vring buffers.
The remaining memory regions are mapped into the kernel at device probe
time, and are used to provide address translations for firmware image
segments without the need for any RSC_CARVEOUT entries. Any firmware
image using memory outside of the supplied reserved memory carveout
regions will be errored out.
The R5F processors on TI K3 SoCs require a specific sequence for booting
and shutting down the processors. This sequence is also dependent on the
mode (LockStep or Split) the R5F cluster is configured for. The R5F cores
have a Memory Protection Unit (MPU) that has a default configuration that
does not allow the cores to run out of DDR out of reset. This is resolved
by using the TCMs for boot-strapping code that applies the appropriate
executable permissions on desired DDR memory. The loading into the TCMs
requires that the resets be released first with the cores in halted state.
The Power Sleep Controller (PSC) module on K3 SoCs requires that the cores
be in WFI/WFE states with no active bus transactions before the cores can
be put back into reset. Support for this is provided by using the newly
introduced .prepare() and .unprepare() ops in the remoteproc core. The
.prepare() ops is invoked before any loading, and the .unprepare() ops
is invoked after the remoteproc resource cleanup. The R5F core resets
are deasserted in .prepare() and asserted in .unprepare(), and the cores
themselves are started and halted in .start() and .stop() ops. This
ensures symmetric usage and allows the R5F cores state machine to be
maintained properly between using the sysfs 'state' variable, bind/unbind
and regular module load/unload flows.
The subsystem is represented as a single remoteproc in LockStep mode, and
as two remoteprocs in Split mode. The driver uses various TI-SCI interfaces
to talk to the System Controller (DMSC) for managing configuration, power
and reset management of these cores. IPC between the A53 cores and the R5
cores is supported through the virtio rpmsg stack using shared memory and
OMAP Mailboxes.
The driver expects the following firmware names to be used for these
cores:
am65x-mcu-r5f0_0-fw (LockStep mode and for Core0 in Split mode)
am65x-mcu-r5f0_1-fw (Core1 in Split mode)
Signed-off-by: Suman Anna <s-anna@ti.com>
subsystem (R5FSS) in the MCU voltage domain. This R5F subsystem/cluster
can be configured at boot time to be either run in a LockStep mode or in
an Asymmetric Multi Processing (AMP) fashion in Split-mode. This subsystem
has 64 KB each Tightly-Coupled Memory (TCM) internal memories for each
core split between two banks - TCMA and TCMB (further interleaved into
two banks). The subsystem does not have an MMU, but has a Region Address
Translater (RAT) module that is accessible only from the R5Fs for providing
translations between 32-bit CPU addresses into larger system bus addresses.
Add a remoteproc driver to support this subsystem to be able to load and
boot the R5F cores primarily in LockStep mode. The code also includes the
base support for Split mode. Error Recovery and Power Management features
are not currently supported. Loading support includes the internal TCMs
and DDR. RAT support is left for a future patch, and as such the reserved
memory carveout regions are all expected to be using memory regions within
the first 2 GB.
The R5F remote processors do not have an MMU, and so require fixed memory
carveout regions matching the firmware image addresses. Support for this
is provided by mandating multiple memory regions to be attached to the
remoteproc device. The first memory region will be used to serve as the
DMA pool for all dynamic allocations like the vrings and vring buffers.
The remaining memory regions are mapped into the kernel at device probe
time, and are used to provide address translations for firmware image
segments without the need for any RSC_CARVEOUT entries. Any firmware
image using memory outside of the supplied reserved memory carveout
regions will be errored out.
The R5F processors on TI K3 SoCs require a specific sequence for booting
and shutting down the processors. This sequence is also dependent on the
mode (LockStep or Split) the R5F cluster is configured for. The R5F cores
have a Memory Protection Unit (MPU) that has a default configuration that
does not allow the cores to run out of DDR out of reset. This is resolved
by using the TCMs for boot-strapping code that applies the appropriate
executable permissions on desired DDR memory. The loading into the TCMs
requires that the resets be released first with the cores in halted state.
The Power Sleep Controller (PSC) module on K3 SoCs requires that the cores
be in WFI/WFE states with no active bus transactions before the cores can
be put back into reset. Support for this is provided by using the newly
introduced .prepare() and .unprepare() ops in the remoteproc core. The
.prepare() ops is invoked before any loading, and the .unprepare() ops
is invoked after the remoteproc resource cleanup. The R5F core resets
are deasserted in .prepare() and asserted in .unprepare(), and the cores
themselves are started and halted in .start() and .stop() ops. This
ensures symmetric usage and allows the R5F cores state machine to be
maintained properly between using the sysfs 'state' variable, bind/unbind
and regular module load/unload flows.
The subsystem is represented as a single remoteproc in LockStep mode, and
as two remoteprocs in Split mode. The driver uses various TI-SCI interfaces
to talk to the System Controller (DMSC) for managing configuration, power
and reset management of these cores. IPC between the A53 cores and the R5
cores is supported through the virtio rpmsg stack using shared memory and
OMAP Mailboxes.
The driver expects the following firmware names to be used for these
cores:
am65x-mcu-r5f0_0-fw (LockStep mode and for Core0 in Split mode)
am65x-mcu-r5f0_1-fw (Core1 in Split mode)
Signed-off-by: Suman Anna <s-anna@ti.com>
drivers/remoteproc/Kconfig | patch | blob | history | |
drivers/remoteproc/Makefile | patch | blob | history | |
drivers/remoteproc/ti_k3_r5_remoteproc.c | [new file with mode: 0644] | patch | blob |
index 414f5c6215c77961702ce8cda04b8cd9baa1dc4d..4af848134c2317b8fe986923a2f61b1abe712465 100644 (file)
config ST_SLIM_REMOTEPROC
tristate
+config TI_K3_R5_REMOTEPROC
+ tristate "TI K3 R5 remoteproc support"
+ depends on ARCH_K3
+ select MAILBOX
+ select OMAP2PLUS_MBOX
+ help
+ Say y here to support TI's R5F remote processor subsystems
+ on various TI K3 family of SoCs through the remote processor
+ framework.
+
+ You want to say y here in order to offload some processing
+ tasks to these processors
+
+ It's safe to say N here if you're not interested in utilizing
+ a slave processor
+
endif # REMOTEPROC
endmenu
index d005af3c71a8cc55691b612d51f1694a9b892ca5..927cc8708699d16dada77e2b2d281a726110c383 100644 (file)
qcom_wcnss_pil-y += qcom_wcnss_iris.o
obj-$(CONFIG_ST_REMOTEPROC) += st_remoteproc.o
obj-$(CONFIG_ST_SLIM_REMOTEPROC) += st_slim_rproc.o
+obj-$(CONFIG_TI_K3_R5_REMOTEPROC) += ti_k3_r5_remoteproc.o
diff --git a/drivers/remoteproc/ti_k3_r5_remoteproc.c b/drivers/remoteproc/ti_k3_r5_remoteproc.c
--- /dev/null
@@ -0,0 +1,1344 @@
+// SPDX-License-Identifier: GPL-2.0
+/*
+ * TI K3 R5F (MCU) Remote Processor driver
+ *
+ * Copyright (C) 2017-2019 Texas Instruments Incorporated - http://www.ti.com/
+ * Suman Anna <s-anna@ti.com>
+ */
+
+#include <linux/dma-mapping.h>
+#include <linux/err.h>
+#include <linux/interrupt.h>
+#include <linux/kernel.h>
+#include <linux/mailbox_client.h>
+#include <linux/module.h>
+#include <linux/of_device.h>
+#include <linux/of_address.h>
+#include <linux/of_reserved_mem.h>
+#include <linux/platform_device.h>
+#include <linux/pm_runtime.h>
+#include <linux/remoteproc.h>
+#include <linux/omap-mailbox.h>
+#include <linux/reset.h>
+#include <linux/soc/ti/ti_sci_protocol.h>
+
+#include "omap_remoteproc.h"
+#include "remoteproc_internal.h"
+#include "ti_sci_proc.h"
+
+/* This address can either be for ATCM or BTCM with the other at address 0x0 */
+#define K3_R5_TCM_DEV_ADDR 0x41010000
+
+/* R5 TI-SCI Processor Configuration Flags */
+#define PROC_BOOT_CFG_FLAG_R5_DBG_EN 0x00000001
+#define PROC_BOOT_CFG_FLAG_R5_DBG_NIDEN 0x00000002
+#define PROC_BOOT_CFG_FLAG_R5_LOCKSTEP 0x00000100
+#define PROC_BOOT_CFG_FLAG_R5_TEINIT 0x00000200
+#define PROC_BOOT_CFG_FLAG_R5_NMFI_EN 0x00000400
+#define PROC_BOOT_CFG_FLAG_R5_TCM_RSTBASE 0x00000800
+#define PROC_BOOT_CFG_FLAG_R5_BTCM_EN 0x00001000
+#define PROC_BOOT_CFG_FLAG_R5_ATCM_EN 0x00002000
+
+/* R5 TI-SCI Processor Control Flags */
+#define PROC_BOOT_CTRL_FLAG_R5_CORE_HALT 0x00000001
+
+/* R5 TI-SCI Processor Status Flags */
+#define PROC_BOOT_STATUS_FLAG_R5_WFE 0x00000001
+#define PROC_BOOT_STATUS_FLAG_R5_WFI 0x00000002
+#define PROC_BOOT_STATUS_FLAG_R5_CLK_GATED 0x00000004
+#define PROC_BOOT_STATUS_FLAG_R5_LOCKSTEP_PERMITTED 0x00000100
+
+/**
+ * struct k3_r5_mem - internal memory structure
+ * @cpu_addr: MPU virtual address of the memory region
+ * @bus_addr: Bus address used to access the memory region
+ * @dev_addr: Device address from remoteproc view
+ * @size: Size of the memory region
+ */
+struct k3_r5_mem {
+ void __iomem *cpu_addr;
+ phys_addr_t bus_addr;
+ u32 dev_addr;
+ size_t size;
+};
+
+enum cluster_mode {
+ CLUSTER_MODE_SPLIT = 0,
+ CLUSTER_MODE_LOCKSTEP,
+};
+
+/**
+ * struct k3_r5_cluster - K3 R5F Cluster structure
+ * @dev: cached device pointer
+ * @mode: Mode to configure the Cluster - Split or LockStep
+ * @cores: list of R5 cores within the cluster
+ */
+struct k3_r5_cluster {
+ struct device *dev;
+ enum cluster_mode mode;
+ struct list_head cores;
+};
+
+/**
+ * struct k3_r5_core - K3 R5 core structure
+ * @dev: cached device pointer
+ * @rproc: rproc handle representing this core
+ * @mem: internal memory regions data
+ * @num_mems: number of internal memory regions
+ * @reset: reset control handle
+ * @tsp: TI-SCI processor control handle
+ * @ti_sci: TI-SCI handle
+ * @ti_sci_id: TI-SCI device identifier
+ * @atcm_enable: flag to control ATCM enablement
+ * @btcm_enable: flag to control BTCM enablement
+ * @loczrama: flag to dictate which TCM is at device address 0x0
+ */
+struct k3_r5_core {
+ struct list_head elem;
+ struct device *dev;
+ struct rproc *rproc;
+ struct k3_r5_mem *mem;
+ int num_mems;
+ struct reset_control *reset;
+ struct ti_sci_proc *tsp;
+ const struct ti_sci_handle *ti_sci;
+ u32 ti_sci_id;
+ u32 atcm_enable;
+ u32 btcm_enable;
+ u32 loczrama;
+};
+
+/**
+ * struct k3_r5_rproc - K3 remote processor state
+ * @dev: cached device pointer
+ * @cluster: cached pointer to parent cluster structure
+ * @mbox: mailbox channel handle
+ * @client: mailbox client to request the mailbox channel
+ * @rproc: rproc handle
+ * @core: cached pointer to r5 core structure being used
+ * @rmem: reserved memory regions data
+ * @num_rmems: number of reserved memory regions
+ */
+struct k3_r5_rproc {
+ struct device *dev;
+ struct k3_r5_cluster *cluster;
+ struct mbox_chan *mbox;
+ struct mbox_client client;
+ struct rproc *rproc;
+ struct k3_r5_core *core;
+ struct k3_r5_mem *rmem;
+ int num_rmems;
+};
+
+/**
+ * struct k3_r5_rproc_dev_data - device data for the remote processor
+ * @device_name: device name of the remote processor
+ * @fw_name: firmware name to use
+ */
+struct k3_r5_rproc_dev_data {
+ const char *device_name;
+ const char *fw_name;
+};
+
+/**
+ * k3_r5_rproc_mbox_callback() - inbound mailbox message handler
+ * @client: mailbox client pointer used for requesting the mailbox channel
+ * @data: mailbox payload
+ *
+ * This handler is invoked by the OMAP mailbox driver whenever a mailbox
+ * message is received. Usually, the mailbox payload simply contains
+ * the index of the virtqueue that is kicked by the remote processor,
+ * and we let remoteproc core handle it.
+ *
+ * In addition to virtqueue indices, we also have some out-of-band values
+ * that indicate different events. Those values are deliberately very
+ * large so they don't coincide with virtqueue indices.
+ */
+static void k3_r5_rproc_mbox_callback(struct mbox_client *client, void *data)
+{
+ struct k3_r5_rproc *kproc = container_of(client, struct k3_r5_rproc,
+ client);
+ struct device *dev = kproc->rproc->dev.parent;
+ const char *name = kproc->rproc->name;
+ u32 msg = to_omap_mbox_msg(data);
+
+ dev_dbg(dev, "mbox msg: 0x%x\n", msg);
+
+ switch (msg) {
+ case RP_MBOX_CRASH:
+ /*
+ * remoteproc detected an exception, but error recovery is not
+ * supported. So, just log this for now
+ */
+ dev_err(dev, "K3 R5F rproc %s crashed\n", name);
+ break;
+ case RP_MBOX_ECHO_REPLY:
+ dev_info(dev, "received echo reply from %s\n", name);
+ break;
+ default:
+ /* silently handle all other valid messages */
+ if (msg >= RP_MBOX_READY && msg < RP_MBOX_END_MSG)
+ return;
+ if (msg > kproc->rproc->max_notifyid) {
+ dev_dbg(dev, "dropping unknown message 0x%x", msg);
+ return;
+ }
+ /* msg contains the index of the triggered vring */
+ if (rproc_vq_interrupt(kproc->rproc, msg) == IRQ_NONE)
+ dev_dbg(dev, "no message was found in vqid %d\n", msg);
+ }
+}
+
+/* kick a virtqueue */
+static void k3_r5_rproc_kick(struct rproc *rproc, int vqid)
+{
+ struct k3_r5_rproc *kproc = rproc->priv;
+ struct device *dev = rproc->dev.parent;
+ mbox_msg_t msg = (mbox_msg_t)vqid;
+ int ret;
+
+ /* send the index of the triggered virtqueue in the mailbox payload */
+ ret = mbox_send_message(kproc->mbox, (void *)msg);
+ if (ret < 0)
+ dev_err(dev, "failed to send mailbox message, status = %d\n",
+ ret);
+}
+
+static int k3_r5_split_reset(struct k3_r5_core *core)
+{
+ int ret;
+
+ ret = reset_control_assert(core->reset);
+ if (ret) {
+ dev_err(core->dev, "local-reset assert failed, ret = %d\n",
+ ret);
+ return ret;
+ }
+
+ ret = core->ti_sci->ops.dev_ops.put_device(core->ti_sci,
+ core->ti_sci_id);
+ if (ret) {
+ dev_err(core->dev, "module-reset assert failed, ret = %d\n",
+ ret);
+ if (reset_control_deassert(core->reset))
+ dev_warn(core->dev, "local-reset deassert back failed\n");
+ }
+
+ return ret;
+}
+
+static int k3_r5_split_release(struct k3_r5_core *core)
+{
+ int ret;
+
+ ret = core->ti_sci->ops.dev_ops.get_device(core->ti_sci,
+ core->ti_sci_id);
+ if (ret) {
+ dev_err(core->dev, "module-reset deassert failed, ret = %d\n",
+ ret);
+ return ret;
+ }
+
+ ret = reset_control_deassert(core->reset);
+ if (ret) {
+ dev_err(core->dev, "local-reset deassert failed, ret = %d\n",
+ ret);
+ if (core->ti_sci->ops.dev_ops.put_device(core->ti_sci,
+ core->ti_sci_id))
+ dev_warn(core->dev, "module-reset assert back failed\n");
+ }
+
+ return ret;
+}
+
+static int k3_r5_lockstep_reset(struct k3_r5_cluster *cluster)
+{
+ struct k3_r5_core *core;
+ int ret;
+
+ /* assert local reset on all applicable cores */
+ list_for_each_entry(core, &cluster->cores, elem) {
+ ret = reset_control_assert(core->reset);
+ if (ret) {
+ dev_err(core->dev, "local-reset assert failed, ret = %d\n",
+ ret);
+ core = list_prev_entry(core, elem);
+ goto unroll_local_reset;
+ }
+ }
+
+ /* disable PSC modules on all applicable cores */
+ list_for_each_entry(core, &cluster->cores, elem) {
+ ret = core->ti_sci->ops.dev_ops.put_device(core->ti_sci,
+ core->ti_sci_id);
+ if (ret) {
+ dev_err(core->dev, "module-reset assert failed, ret = %d\n",
+ ret);
+ goto unroll_module_reset;
+ }
+ }
+
+ return 0;
+
+unroll_module_reset:
+ list_for_each_entry_continue_reverse(core, &cluster->cores, elem) {
+ if (core->ti_sci->ops.dev_ops.put_device(core->ti_sci,
+ core->ti_sci_id))
+ dev_warn(core->dev, "module-reset assert back failed\n");
+ }
+ core = list_last_entry(&cluster->cores, struct k3_r5_core, elem);
+unroll_local_reset:
+ list_for_each_entry_from_reverse(core, &cluster->cores, elem) {
+ if (reset_control_deassert(core->reset))
+ dev_warn(core->dev, "local-reset deassert back failed\n");
+ }
+
+ return ret;
+}
+
+static int k3_r5_lockstep_release(struct k3_r5_cluster *cluster)
+{
+ struct k3_r5_core *core;
+ int ret;
+
+ /* enable PSC modules on all applicable cores */
+ list_for_each_entry_reverse(core, &cluster->cores, elem) {
+ ret = core->ti_sci->ops.dev_ops.get_device(core->ti_sci,
+ core->ti_sci_id);
+ if (ret) {
+ dev_err(core->dev, "module-reset deassert failed, ret = %d\n",
+ ret);
+ core = list_next_entry(core, elem);
+ goto unroll_module_reset;
+ }
+ }
+
+ /* deassert local reset on all applicable cores */
+ list_for_each_entry_reverse(core, &cluster->cores, elem) {
+ ret = reset_control_deassert(core->reset);
+ if (ret) {
+ dev_err(core->dev, "module-reset deassert failed, ret = %d\n",
+ ret);
+ goto unroll_local_reset;
+ }
+ }
+
+ return 0;
+
+unroll_local_reset:
+ list_for_each_entry_continue(core, &cluster->cores, elem) {
+ if (reset_control_assert(core->reset))
+ dev_warn(core->dev, "local-reset assert back failed\n");
+ }
+ core = list_first_entry(&cluster->cores, struct k3_r5_core, elem);
+unroll_module_reset:
+ list_for_each_entry_from(core, &cluster->cores, elem) {
+ if (core->ti_sci->ops.dev_ops.put_device(core->ti_sci,
+ core->ti_sci_id))
+ dev_warn(core->dev, "module-reset assert back failed\n");
+ }
+
+ return ret;
+}
+
+static inline int k3_r5_core_halt(struct k3_r5_core *core)
+{
+ return ti_sci_proc_set_control(core->tsp,
+ PROC_BOOT_CTRL_FLAG_R5_CORE_HALT, 0);
+}
+
+static inline int k3_r5_core_run(struct k3_r5_core *core)
+{
+ return ti_sci_proc_set_control(core->tsp,
+ 0, PROC_BOOT_CTRL_FLAG_R5_CORE_HALT);
+}
+
+/*
+ * The R5F cores have controls for both a reset and a halt/run. The code
+ * execution from DDR requires the initial boot-strapping code to be run
+ * from the internal TCMs. This function is used to release the resets on
+ * applicable cores to allow loading into the TCMs. The .prepare() ops is
+ * invoked by remoteproc core before any firmware loading, and is followed
+ * by the .start() ops after loading to actually let the R5 cores run.
+ */
+static int k3_r5_rproc_prepare(struct rproc *rproc)
+{
+ struct k3_r5_rproc *kproc = rproc->priv;
+ struct k3_r5_cluster *cluster = kproc->cluster;
+ struct k3_r5_core *core = kproc->core;
+ struct device *dev = kproc->dev;
+ int ret;
+
+ ret = cluster->mode ? k3_r5_lockstep_release(cluster) :
+ k3_r5_split_release(core);
+ if (ret)
+ dev_err(dev, "unable to enable cores for TCM loading, ret = %d\n",
+ ret);
+
+ return ret;
+}
+
+/*
+ * This function implements the .unprepare() ops and performs the complimentary
+ * operations to that of the .prepare() ops. The function is used to assert the
+ * resets on all applicable cores for the rproc device (depending on LockStep
+ * or Split mode). This completes the second portion of powering down the R5F
+ * cores. The cores themselves are only halted in the .stop() ops, and the
+ * .unprepare() ops is invoked by the remoteproc core after the remoteproc is
+ * stopped.
+ */
+static int k3_r5_rproc_unprepare(struct rproc *rproc)
+{
+ struct k3_r5_rproc *kproc = rproc->priv;
+ struct k3_r5_cluster *cluster = kproc->cluster;
+ struct k3_r5_core *core = kproc->core;
+ struct device *dev = kproc->dev;
+ int ret;
+
+ ret = cluster->mode ? k3_r5_lockstep_reset(cluster) :
+ k3_r5_split_reset(core);
+ if (ret)
+ dev_err(dev, "unable to disable cores, ret = %d\n", ret);
+
+ return ret;
+}
+
+/*
+ * The R5F start sequence includes two different operations
+ * 1. Configure the boot vector for R5F core(s)
+ * 2. Unhalt/Run the R5F core(s)
+ *
+ * The sequence is different between LockStep and Split modes. The LockStep
+ * mode requires the boot vector to be configured only for Core0, and then
+ * unhalt both the cores to start the execution - Core1 needs to be unhalted
+ * first followed by Core0. The Split-mode requires that Core0 to be maintained
+ * always in a higher power state that Core1 (implying Core1 needs to be started
+ * always only after Core0 is started).
+ */
+static int k3_r5_rproc_start(struct rproc *rproc)
+{
+ struct k3_r5_rproc *kproc = rproc->priv;
+ struct k3_r5_cluster *cluster = kproc->cluster;
+ struct mbox_client *client = &kproc->client;
+ struct device *dev = kproc->dev;
+ struct k3_r5_core *core;
+ u32 boot_addr;
+ int ret;
+
+ client->dev = dev;
+ client->tx_done = NULL;
+ client->rx_callback = k3_r5_rproc_mbox_callback;
+ client->tx_block = false;
+ client->knows_txdone = false;
+
+ kproc->mbox = mbox_request_channel(client, 0);
+ if (IS_ERR(kproc->mbox)) {
+ ret = -EBUSY;
+ dev_err(dev, "mbox_request_channel failed: %ld\n",
+ PTR_ERR(kproc->mbox));
+ return ret;
+ }
+
+ /*
+ * Ping the remote processor, this is only for sanity-sake for now;
+ * there is no functional effect whatsoever.
+ *
+ * Note that the reply will _not_ arrive immediately: this message
+ * will wait in the mailbox fifo until the remote processor is booted.
+ */
+ ret = mbox_send_message(kproc->mbox, (void *)RP_MBOX_ECHO_REQUEST);
+ if (ret < 0) {
+ dev_err(dev, "mbox_send_message failed: %d\n", ret);
+ goto put_mbox;
+ }
+
+ boot_addr = rproc->bootaddr;
+ /* TODO: add boot_addr sanity checking */
+ dev_err(dev, "booting R5F core using boot addr = 0x%x\n", boot_addr);
+
+ /* boot vector need not be programmed for Core1 in LockStep mode */
+ core = kproc->core;
+ ret = ti_sci_proc_set_config(core->tsp, boot_addr, 0, 0);
+ if (ret)
+ goto put_mbox;
+
+ /* unhalt/run all applicable cores */
+ if (cluster->mode) {
+ list_for_each_entry_reverse(core, &cluster->cores, elem) {
+ ret = k3_r5_core_run(core);
+ if (ret)
+ goto unroll_core_run;
+ }
+ } else {
+ ret = k3_r5_core_run(core);
+ if (ret)
+ goto put_mbox;
+ }
+
+ return 0;
+
+unroll_core_run:
+ list_for_each_entry_continue(core, &cluster->cores, elem) {
+ if (k3_r5_core_halt(core))
+ dev_warn(core->dev, "core halt back failed\n");
+ }
+put_mbox:
+ mbox_free_channel(kproc->mbox);
+ return ret;
+}
+
+/*
+ * The R5F stop function includes the following operations
+ * 1. Halt R5F core(s)
+ *
+ * The sequence is different between LockStep and Split modes, and the order
+ * of cores the operations are performed are also in general reverse to that
+ * of the start function. The LockStep mode requires each operation to be
+ * performed first on Core0 followed by Core1. The Split-mode requires that
+ * Core0 to be maintained always in a higher power state that Core1 (implying
+ * Core1 needs to be stopped first before Core0).
+ *
+ * Note that the R5F halt operation in general is not effective when the R5F
+ * core is running, but is needed to make sure the core won't run after
+ * deasserting the reset the subsequent time. The asserting of reset can
+ * be done here, but is preferred to be done in the .unprepare() ops - this
+ * maintains the symmetric behavior between the .start(), .stop(), .prepare()
+ * and .unprepare() ops, and also balances them well between sysfs 'state'
+ * flow and device bind/unbind or module removal.
+ */
+static int k3_r5_rproc_stop(struct rproc *rproc)
+{
+ struct k3_r5_rproc *kproc = rproc->priv;
+ struct k3_r5_cluster *cluster = kproc->cluster;
+ struct k3_r5_core *core = kproc->core;
+ int ret;
+
+ /* halt all applicable cores */
+ if (cluster->mode) {
+ list_for_each_entry(core, &cluster->cores, elem) {
+ ret = k3_r5_core_halt(core);
+ if (ret) {
+ core = list_prev_entry(core, elem);
+ goto unroll_core_halt;
+ }
+ }
+ } else {
+ ret = k3_r5_core_halt(core);
+ if (ret)
+ goto out;
+ }
+
+ mbox_free_channel(kproc->mbox);
+
+ return 0;
+
+unroll_core_halt:
+ list_for_each_entry_from_reverse(core, &cluster->cores, elem) {
+ if (k3_r5_core_run(core))
+ dev_warn(core->dev, "core run back failed\n");
+ }
+out:
+ return ret;
+}
+
+/*
+ * Internal Memory translation helper
+ *
+ * Custom function implementing the rproc .da_to_va ops to provide address
+ * translation (device address to kernel virtual address) for internal RAMs
+ * present in a DSP or IPU device). The translated addresses can be used
+ * either by the remoteproc core for loading, or by any rpmsg bus drivers.
+ */
+static void *k3_r5_rproc_da_to_va(struct rproc *rproc, u64 da, int len,
+ u32 flags)
+{
+ struct k3_r5_rproc *kproc = rproc->priv;
+ struct k3_r5_core *core = kproc->core;
+ void __iomem *va = NULL;
+ phys_addr_t bus_addr;
+ u32 dev_addr, offset;
+ size_t size;
+ int i;
+
+ if (len <= 0)
+ return NULL;
+
+ /* handle R5-view of ATCM addresses first using address 0 */
+ size = core->mem[0].size;
+ if (da >= 0 && ((da + len) <= size)) {
+ offset = da;
+ va = core->mem[0].cpu_addr + offset;
+ return (__force void *)va;
+ }
+
+ /* handle SoC-view addresses for ATCM and BTCM */
+ for (i = 0; i < core->num_mems; i++) {
+ bus_addr = core->mem[i].bus_addr;
+ dev_addr = core->mem[i].dev_addr;
+ size = core->mem[i].size;
+
+ if (da >= bus_addr &&
+ ((da + len) <= (bus_addr + size))) {
+ offset = da - bus_addr;
+ va = core->mem[i].cpu_addr + offset;
+ return (__force void *)va;
+ }
+ }
+
+ /* handle static DDR reserved memory regions */
+ for (i = 0; i < kproc->num_rmems; i++) {
+ dev_addr = kproc->rmem[i].dev_addr;
+ size = kproc->rmem[i].size;
+
+ if (da >= dev_addr && ((da + len) <= (dev_addr + size))) {
+ offset = da - dev_addr;
+ va = kproc->rmem[i].cpu_addr + offset;
+ return (__force void *)va;
+ }
+ }
+
+ return NULL;
+}
+
+static const struct rproc_ops k3_r5_rproc_ops = {
+ .prepare = k3_r5_rproc_prepare,
+ .unprepare = k3_r5_rproc_unprepare,
+ .start = k3_r5_rproc_start,
+ .stop = k3_r5_rproc_stop,
+ .kick = k3_r5_rproc_kick,
+ .da_to_va = k3_r5_rproc_da_to_va,
+};
+
+static const char *k3_r5_rproc_get_firmware(struct device *dev)
+{
+ const struct k3_r5_rproc_dev_data *data =
+ of_device_get_match_data(dev->parent);
+
+ if (!data) {
+ dev_err(dev, "data is NULL, %s\n", dev_name(dev));
+ return ERR_PTR(-ENODEV);
+ }
+
+ for (; data && data->device_name; data++) {
+ if (!strcmp(dev_name(dev), data->device_name))
+ return data->fw_name;
+ }
+
+ return ERR_PTR(-ENODEV);
+}
+
+static int k3_r5_rproc_configure(struct k3_r5_rproc *kproc)
+{
+ struct k3_r5_cluster *cluster = kproc->cluster;
+ struct device *dev = kproc->dev;
+ struct k3_r5_core *core0, *core, *temp;
+ u32 ctrl = 0, cfg = 0, stat = 0;
+ u32 set_cfg = 0, clr_cfg = 0;
+ u64 boot_vec = 0;
+ int ret;
+
+ core0 = list_first_entry(&cluster->cores, struct k3_r5_core, elem);
+ core = cluster->mode ? core0 : kproc->core;
+
+ ret = ti_sci_proc_get_status(core->tsp, &boot_vec, &cfg, &ctrl,
+ &stat);
+ if (ret < 0)
+ return ret;
+
+ dev_dbg(dev, "boot_vector = 0x%llx, cfg = 0x%x ctrl = 0x%x stat = 0x%x\n",
+ boot_vec, cfg, ctrl, stat);
+
+ if (!(stat & PROC_BOOT_STATUS_FLAG_R5_LOCKSTEP_PERMITTED) &&
+ cluster->mode) {
+ dev_err(cluster->dev, "lockstep mode not permitted, force configuring for split-mode\n");
+ cluster->mode = 0;
+ }
+
+ /* always enable ARM mode and set boot vector to 0 */
+ boot_vec = 0x0;
+ if (core == core0) {
+ clr_cfg = PROC_BOOT_CFG_FLAG_R5_TEINIT;
+ clr_cfg |= PROC_BOOT_CFG_FLAG_R5_LOCKSTEP;
+ }
+
+ if (core->atcm_enable)
+ set_cfg |= PROC_BOOT_CFG_FLAG_R5_ATCM_EN;
+ else
+ clr_cfg |= PROC_BOOT_CFG_FLAG_R5_ATCM_EN;
+
+ if (core->btcm_enable)
+ set_cfg |= PROC_BOOT_CFG_FLAG_R5_BTCM_EN;
+ else
+ clr_cfg |= PROC_BOOT_CFG_FLAG_R5_BTCM_EN;
+
+ if (core->loczrama)
+ set_cfg |= PROC_BOOT_CFG_FLAG_R5_TCM_RSTBASE;
+ else
+ clr_cfg |= PROC_BOOT_CFG_FLAG_R5_TCM_RSTBASE;
+
+ if (cluster->mode) {
+ /*
+ * work around system firmware limitations to make sure both
+ * cores are programmed symmetrically in LockStep. LockStep
+ * and TEINIT config is only allowed with Core0.
+ */
+ list_for_each_entry(temp, &cluster->cores, elem) {
+ ret = k3_r5_core_halt(core);
+ if (ret)
+ goto out;
+
+ if (temp != core) {
+ clr_cfg &= ~PROC_BOOT_CFG_FLAG_R5_LOCKSTEP;
+ clr_cfg &= ~PROC_BOOT_CFG_FLAG_R5_TEINIT;
+ }
+ ret = ti_sci_proc_set_config(temp->tsp, boot_vec,
+ set_cfg, clr_cfg);
+ if (ret)
+ goto out;
+ }
+
+ set_cfg = PROC_BOOT_CFG_FLAG_R5_LOCKSTEP;
+ clr_cfg = 0;
+ ret = ti_sci_proc_set_config(core->tsp, boot_vec,
+ set_cfg, clr_cfg);
+ } else {
+ ret = k3_r5_core_halt(core);
+ if (ret)
+ goto out;
+
+ ret = ti_sci_proc_set_config(core->tsp, boot_vec,
+ set_cfg, clr_cfg);
+ }
+
+out:
+ return ret;
+}
+
+static int k3_r5_reserved_mem_init(struct k3_r5_rproc *kproc)
+{
+ struct device *dev = kproc->dev;
+ struct device_node *np = dev->of_node;
+ struct device_node *rmem_np;
+ struct reserved_mem *rmem;
+ int num_rmems;
+ int ret, i;
+
+ num_rmems = of_property_count_elems_of_size(np, "memory-region",
+ sizeof(phandle));
+ if (num_rmems <= 0) {
+ dev_err(dev, "device does not have reserved memory regions, ret = %d\n",
+ num_rmems);
+ return -EINVAL;
+ }
+ if (num_rmems < 2) {
+ dev_err(dev, "device needs atleast two memory regions to be defined, num = %d\n",
+ num_rmems);
+ return -EINVAL;
+ }
+
+ /* use reserved memory region 0 for vring DMA allocations */
+ ret = of_reserved_mem_device_init_by_idx(dev, np, 0);
+ if (ret) {
+ dev_err(dev, "device cannot initialize DMA pool, ret = %d\n",
+ ret);
+ return ret;
+ }
+
+ num_rmems--;
+ kproc->rmem = kcalloc(num_rmems, sizeof(*kproc->rmem), GFP_KERNEL);
+ if (!kproc->rmem) {
+ ret = -ENOMEM;
+ goto release_rmem;
+ }
+
+ /* use remaining reserved memory regions for static carveouts */
+ for (i = 0; i < num_rmems; i++) {
+ rmem_np = of_parse_phandle(np, "memory-region", i + 1);
+ if (!rmem_np) {
+ ret = -EINVAL;
+ goto unmap_rmem;
+ }
+
+ rmem = of_reserved_mem_lookup(rmem_np);
+ if (!rmem) {
+ of_node_put(rmem_np);
+ ret = -EINVAL;
+ goto unmap_rmem;
+ }
+ of_node_put(rmem_np);
+
+ kproc->rmem[i].bus_addr = rmem->base;
+ /* 64-bit address regions currently not supported */
+ kproc->rmem[i].dev_addr = (u32)rmem->base;
+ kproc->rmem[i].size = rmem->size;
+ kproc->rmem[i].cpu_addr = ioremap_wc(rmem->base, rmem->size);
+ if (!kproc->rmem[i].cpu_addr) {
+ dev_err(dev, "failed to map reserved memory#%d at %pa of size %pa\n",
+ i + 1, &rmem->base, &rmem->size);
+ ret = -ENOMEM;
+ goto unmap_rmem;
+ }
+
+ dev_dbg(dev, "reserved memory%d: bus addr %pa size 0x%zx va %pK da 0x%x\n",
+ i + 1, &kproc->rmem[i].bus_addr,
+ kproc->rmem[i].size, kproc->rmem[i].cpu_addr,
+ kproc->rmem[i].dev_addr);
+ }
+ kproc->num_rmems = num_rmems;
+
+ return 0;
+
+unmap_rmem:
+ for (i--; i >= 0; i--) {
+ if (kproc->rmem[i].cpu_addr)
+ iounmap(kproc->rmem[i].cpu_addr);
+ }
+ kfree(kproc->rmem);
+release_rmem:
+ of_reserved_mem_device_release(dev);
+ return ret;
+}
+
+static void k3_r5_reserved_mem_exit(struct k3_r5_rproc *kproc)
+{
+ int i;
+
+ for (i = 0; i < kproc->num_rmems; i++)
+ iounmap(kproc->rmem[i].cpu_addr);
+ kfree(kproc->rmem);
+
+ of_reserved_mem_device_release(kproc->dev);
+}
+
+static int k3_r5_cluster_rproc_init(struct platform_device *pdev)
+{
+ struct k3_r5_cluster *cluster = platform_get_drvdata(pdev);
+ struct device *dev = &pdev->dev;
+ struct k3_r5_rproc *kproc;
+ struct k3_r5_core *core, *core1;
+ struct device *cdev;
+ const char *fw_name;
+ struct rproc *rproc;
+ int ret;
+
+ core1 = list_last_entry(&cluster->cores, struct k3_r5_core, elem);
+ list_for_each_entry(core, &cluster->cores, elem) {
+ cdev = core->dev;
+ fw_name = k3_r5_rproc_get_firmware(cdev);
+ if (IS_ERR(fw_name)) {
+ ret = PTR_ERR(fw_name);
+ goto out;
+ }
+
+ rproc = rproc_alloc(cdev, dev_name(cdev), &k3_r5_rproc_ops,
+ fw_name, sizeof(*kproc));
+ if (!rproc) {
+ ret = -ENOMEM;
+ goto out;
+ }
+
+ /* K3 R5s have a Region Address Translator (RAT) but no MMU */
+ rproc->has_iommu = false;
+ /* error recovery is not supported at present */
+ rproc->recovery_disabled = true;
+
+ kproc = rproc->priv;
+ kproc->cluster = cluster;
+ kproc->core = core;
+ kproc->dev = cdev;
+ kproc->rproc = rproc;
+ core->rproc = rproc;
+
+ ret = k3_r5_rproc_configure(kproc);
+ if (ret) {
+ dev_err(dev, "initial configure failed, ret = %d\n",
+ ret);
+ goto err_config;
+ }
+
+ ret = k3_r5_reserved_mem_init(kproc);
+ if (ret) {
+ dev_err(dev, "reserved memory init failed, ret = %d\n",
+ ret);
+ goto err_config;
+ }
+
+ ret = rproc_add(rproc);
+ if (ret) {
+ dev_err(dev, "rproc_add failed, ret = %d\n", ret);
+ goto err_add;
+ }
+
+ /* create only one rproc in lockstep mode */
+ if (cluster->mode)
+ break;
+ }
+
+ return 0;
+
+err_split:
+ rproc_del(rproc);
+err_add:
+ k3_r5_reserved_mem_exit(kproc);
+err_config:
+ rproc_free(rproc);
+ core->rproc = NULL;
+out:
+ /* undo core0 upon any failures on core1 in split-mode */
+ if (!cluster->mode && core == core1) {
+ core = list_prev_entry(core, elem);
+ rproc = core->rproc;
+ kproc = rproc->priv;
+ goto err_split;
+ }
+ return ret;
+}
+
+static int k3_r5_cluster_rproc_exit(struct platform_device *pdev)
+{
+ struct k3_r5_cluster *cluster = platform_get_drvdata(pdev);
+ struct k3_r5_rproc *kproc;
+ struct k3_r5_core *core;
+ struct rproc *rproc;
+
+ /*
+ * lockstep mode has only one rproc associated with first core, whereas
+ * split-mode has two rprocs associated with each core, and requires
+ * that core1 be powered down first
+ */
+ core = cluster->mode ?
+ list_first_entry(&cluster->cores, struct k3_r5_core, elem) :
+ list_last_entry(&cluster->cores, struct k3_r5_core, elem);
+
+ list_for_each_entry_from_reverse(core, &cluster->cores, elem) {
+ rproc = core->rproc;
+ kproc = rproc->priv;
+
+ rproc_del(rproc);
+
+ k3_r5_reserved_mem_exit(kproc);
+
+ rproc_free(rproc);
+ core->rproc = NULL;
+ }
+
+ return 0;
+}
+
+static int k3_r5_core_of_get_internal_memories(struct platform_device *pdev,
+ struct k3_r5_core *core)
+{
+ static const char * const mem_names[] = {"atcm", "btcm"};
+ struct device *dev = &pdev->dev;
+ struct resource *res;
+ int num_mems;
+ int i, ret;
+
+ num_mems = ARRAY_SIZE(mem_names);
+ core->mem = devm_kcalloc(dev, num_mems, sizeof(*core->mem), GFP_KERNEL);
+ if (!core->mem)
+ return -ENOMEM;
+
+ for (i = 0; i < num_mems; i++) {
+ res = platform_get_resource_byname(pdev, IORESOURCE_MEM,
+ mem_names[i]);
+ core->mem[i].cpu_addr = devm_ioremap_resource(dev, res);
+ if (IS_ERR(core->mem[i].cpu_addr)) {
+ dev_err(dev, "failed to parse and map %s memory\n",
+ mem_names[i]);
+ ret = PTR_ERR(core->mem[i].cpu_addr);
+ goto fail;
+ }
+ core->mem[i].bus_addr = res->start;
+
+ /*
+ * TODO:
+ * The R5F cores can place ATCM & BTCM anywhere in its address
+ * based on the corresponding Region Registers in the System
+ * Control coprocessor. For now, place ATCM and BTCM at
+ * addresses 0 and 0x41010000 (same as the bus address on AM65x
+ * SoCs) based on loczrama setting
+ */
+ if (!strcmp(mem_names[i], "atcm")) {
+ core->mem[i].dev_addr = core->loczrama ?
+ 0 : K3_R5_TCM_DEV_ADDR;
+ } else {
+ core->mem[i].dev_addr = core->loczrama ?
+ K3_R5_TCM_DEV_ADDR : 0;
+ }
+ core->mem[i].size = resource_size(res);
+
+ dev_dbg(dev, "memory %8s: bus addr %pa size 0x%zx va %p da 0x%x\n",
+ mem_names[i], &core->mem[i].bus_addr,
+ core->mem[i].size, core->mem[i].cpu_addr,
+ core->mem[i].dev_addr);
+ }
+ core->num_mems = num_mems;
+
+ return 0;
+
+fail:
+ for (i--; i >= 0; i--) {
+ devm_release_mem_region(dev, core->mem[i].bus_addr,
+ core->mem[i].size);
+ devm_iounmap(dev, core->mem[i].cpu_addr);
+ }
+ if (core->mem)
+ devm_kfree(dev, core->mem);
+ return ret;
+}
+
+static
+struct ti_sci_proc *k3_r5_core_of_get_tsp(struct device *dev,
+ const struct ti_sci_handle *sci)
+{
+ struct ti_sci_proc *tsp;
+ u32 temp[2];
+ int ret;
+
+ ret = of_property_read_u32_array(dev->of_node, "ti,sci-proc-ids",
+ temp, 2);
+ if (ret < 0)
+ return ERR_PTR(ret);
+
+ tsp = kzalloc(sizeof(*tsp), GFP_KERNEL);
+ if (!tsp)
+ return ERR_PTR(-ENOMEM);
+
+ tsp->dev = dev;
+ tsp->sci = sci;
+ tsp->ops = &sci->ops.proc_ops;
+ tsp->proc_id = temp[0];
+ tsp->host_id = temp[1];
+
+ return tsp;
+}
+
+static int k3_r5_core_of_init(struct platform_device *pdev)
+{
+ struct device *dev = &pdev->dev;
+ struct device_node *np = dev->of_node;
+ struct k3_r5_core *core;
+ int ret, ret1;
+
+ core = devm_kzalloc(dev, sizeof(*core), GFP_KERNEL);
+ if (!core)
+ return -ENOMEM;
+
+ core->dev = dev;
+ core->atcm_enable = 0;
+ core->btcm_enable = 1;
+ core->loczrama = 1;
+
+ ret = of_property_read_u32(np, "atcm-enable", &core->atcm_enable);
+ if (ret < 0 && ret != -EINVAL) {
+ dev_err(dev, "invalid format for atcm-enable, ret = %d\n", ret);
+ goto err_of;
+ }
+
+ ret = of_property_read_u32(np, "btcm-enable", &core->btcm_enable);
+ if (ret < 0 && ret != -EINVAL) {
+ dev_err(dev, "invalid format for btcm-enable, ret = %d\n", ret);
+ goto err_of;
+ }
+
+ ret = of_property_read_u32(np, "loczrama", &core->loczrama);
+ if (ret < 0 && ret != -EINVAL) {
+ dev_err(dev, "invalid format for loczrama, ret = %d\n", ret);
+ goto err_of;
+ }
+
+ core->ti_sci = ti_sci_get_by_phandle(np, "ti,sci");
+ if (IS_ERR(core->ti_sci)) {
+ ret = PTR_ERR(core->ti_sci);
+ if (ret != -EPROBE_DEFER) {
+ dev_err(dev, "failed to get ti-sci handle, ret = %d\n",
+ ret);
+ }
+ core->ti_sci = NULL;
+ goto err_of;
+ }
+
+ ret = of_property_read_u32(np, "ti,sci-dev-id", &core->ti_sci_id);
+ if (ret) {
+ dev_err(dev, "missing 'ti,sci-dev-id' property\n");
+ goto err_sci_id;
+ }
+
+ core->reset = reset_control_get_exclusive(dev, NULL);
+ if (IS_ERR(core->reset)) {
+ ret = PTR_ERR(core->reset);
+ if (ret != -EPROBE_DEFER) {
+ dev_err(dev, "failed to get reset handle, ret = %d\n",
+ ret);
+ }
+ goto err_sci_id;
+ }
+
+ core->tsp = k3_r5_core_of_get_tsp(dev, core->ti_sci);
+ if (IS_ERR(core->tsp)) {
+ dev_err(dev, "failed to construct ti-sci proc control, ret = %d\n",
+ ret);
+ ret = PTR_ERR(core->tsp);
+ goto err_sci_proc;
+ }
+
+ ret = ti_sci_proc_request(core->tsp);
+ if (ret < 0) {
+ dev_err(dev, "ti_sci_proc_request failed, ret = %d\n", ret);
+ goto err_proc;
+ }
+
+ ret = k3_r5_core_of_get_internal_memories(pdev, core);
+ if (ret) {
+ dev_err(dev, "failed to get internal memories, ret = %d\n",
+ ret);
+ goto err_intmem;
+ }
+
+ platform_set_drvdata(pdev, core);
+
+ return 0;
+
+err_intmem:
+ ret1 = ti_sci_proc_release(core->tsp);
+ if (ret1)
+ dev_err(dev, "failed to release proc, ret1 = %d\n", ret1);
+err_proc:
+ kfree(core->tsp);
+err_sci_proc:
+ reset_control_put(core->reset);
+err_sci_id:
+ ret1 = ti_sci_put_handle(core->ti_sci);
+ if (ret1)
+ dev_err(dev, "failed to put ti_sci handle, ret = %d\n", ret1);
+err_of:
+ devm_kfree(dev, core);
+ return ret;
+}
+
+/*
+ * free the resources explicitly since driver model is not being used
+ * for the child R5F devices
+ */
+static int k3_r5_core_of_exit(struct platform_device *pdev)
+{
+ struct k3_r5_core *core = platform_get_drvdata(pdev);
+ struct device *dev = &pdev->dev;
+ int i, ret;
+
+ for (i = 0; i < core->num_mems; i++) {
+ devm_release_mem_region(dev, core->mem[i].bus_addr,
+ core->mem[i].size);
+ devm_iounmap(dev, core->mem[i].cpu_addr);
+ }
+ if (core->mem)
+ devm_kfree(dev, core->mem);
+
+ ret = ti_sci_proc_release(core->tsp);
+ if (ret)
+ dev_err(dev, "failed to release proc, ret = %d\n", ret);
+
+ kfree(core->tsp);
+ reset_control_put(core->reset);
+
+ ret = ti_sci_put_handle(core->ti_sci);
+ if (ret)
+ dev_err(dev, "failed to put ti_sci handle, ret = %d\n", ret);
+
+ platform_set_drvdata(pdev, NULL);
+ devm_kfree(dev, core);
+
+ return ret;
+}
+
+static int k3_r5_cluster_of_init(struct platform_device *pdev)
+{
+ struct k3_r5_cluster *cluster = platform_get_drvdata(pdev);
+ struct device *dev = &pdev->dev;
+ struct device_node *np = dev->of_node;
+ struct platform_device *cpdev;
+ struct device_node *child;
+ struct k3_r5_core *core, *temp;
+ int ret;
+
+ for_each_available_child_of_node(np, child) {
+ cpdev = of_find_device_by_node(child);
+ if (!cpdev) {
+ ret = -ENODEV;
+ dev_err(dev, "could not get R5 core platform device\n");
+ goto fail;
+ }
+
+ ret = k3_r5_core_of_init(cpdev);
+ if (ret) {
+ dev_err(dev, "k3_r5_core_of_init failed, ret = %d\n",
+ ret);
+ put_device(&cpdev->dev);
+ goto fail;
+ }
+
+ core = platform_get_drvdata(cpdev);
+ put_device(&cpdev->dev);
+ list_add_tail(&core->elem, &cluster->cores);
+ }
+
+ return 0;
+
+fail:
+ list_for_each_entry_safe_reverse(core, temp, &cluster->cores, elem) {
+ list_del(&core->elem);
+ cpdev = to_platform_device(core->dev);
+ if (k3_r5_core_of_exit(cpdev))
+ dev_err(dev, "k3_r5_core_of_exit cleanup failed\n");
+ }
+ return ret;
+}
+
+static int k3_r5_cluster_of_exit(struct platform_device *pdev)
+{
+ struct k3_r5_cluster *cluster = platform_get_drvdata(pdev);
+ struct device *dev = &pdev->dev;
+ struct platform_device *cpdev;
+ struct k3_r5_core *core, *temp;
+ int ret;
+
+ list_for_each_entry_safe_reverse(core, temp, &cluster->cores, elem) {
+ list_del(&core->elem);
+ cpdev = to_platform_device(core->dev);
+ ret = k3_r5_core_of_exit(cpdev);
+ if (ret) {
+ dev_err(dev, "k3_r5_core_of_exit failed, ret = %d\n",
+ ret);
+ break;
+ }
+ }
+
+ return ret;
+}
+
+static int k3_r5_probe(struct platform_device *pdev)
+{
+ struct device *dev = &pdev->dev;
+ struct device_node *np = dev->of_node;
+ struct k3_r5_cluster *cluster;
+ int ret, ret1;
+ int num_cores;
+
+ cluster = devm_kzalloc(dev, sizeof(*cluster), GFP_KERNEL);
+ if (!cluster)
+ return -ENOMEM;
+
+ cluster->dev = dev;
+ cluster->mode = CLUSTER_MODE_LOCKSTEP;
+ INIT_LIST_HEAD(&cluster->cores);
+
+ ret = of_property_read_u32(np, "lockstep-mode", &cluster->mode);
+ if (ret < 0 && ret != -EINVAL) {
+ dev_err(dev, "invalid format for lockstep-mode, ret = %d\n",
+ ret);
+ return ret;
+ }
+
+ num_cores = of_get_available_child_count(np);
+ if (num_cores != 2) {
+ dev_err(dev, "MCU cluster requires both R5F cores to be enabled, num_cores = %d\n",
+ num_cores);
+ return -ENODEV;
+ }
+
+ platform_set_drvdata(pdev, cluster);
+
+ dev_info(dev, "creating child devices for R5F cores\n");
+ ret = of_platform_populate(np, NULL, NULL, dev);
+ if (ret) {
+ dev_err(dev, "of_platform_populate failed, ret = %d\n", ret);
+ return ret;
+ }
+
+ ret = k3_r5_cluster_of_init(pdev);
+ if (ret) {
+ dev_err(dev, "k3_r5_cluster_of_init failed, ret = %d\n", ret);
+ goto fail_of;
+ }
+
+ ret = k3_r5_cluster_rproc_init(pdev);
+ if (ret) {
+ dev_err(dev, "k3_r5_cluster_rproc_init failed, ret = %d\n",
+ ret);
+ goto fail_rproc;
+ }
+
+ return 0;
+
+fail_rproc:
+ ret1 = k3_r5_cluster_of_exit(pdev);
+ if (ret1)
+ dev_err(dev, "k3_r5_cluster_of_exit failed, ret = %d\n", ret1);
+fail_of:
+ of_platform_depopulate(dev);
+ return ret;
+}
+
+static int k3_r5_remove(struct platform_device *pdev)
+{
+ struct device *dev = &pdev->dev;
+ int ret;
+
+ ret = k3_r5_cluster_rproc_exit(pdev);
+ if (ret) {
+ dev_err(dev, "k3_r5_cluster_rproc_exit failed, ret = %d\n",
+ ret);
+ goto fail;
+ }
+
+ ret = k3_r5_cluster_of_exit(pdev);
+ if (ret) {
+ dev_err(dev, "k3_r5_cluster_of_exit failed, ret = %d\n", ret);
+ goto fail;
+ }
+
+ dev_info(dev, "removing child devices for R5F cores\n");
+ of_platform_depopulate(dev);
+
+fail:
+ return ret;
+}
+
+static const struct k3_r5_rproc_dev_data am65x_r5f_dev_data[] = {
+ {
+ .device_name = "41000000.r5f",
+ .fw_name = "am65x-mcu-r5f0_0-fw",
+ },
+ {
+ .device_name = "41400000.r5f",
+ .fw_name = "am65x-mcu-r5f0_1-fw",
+ },
+ {
+ /* sentinel */
+ },
+};
+
+static const struct of_device_id k3_r5_of_match[] = {
+ {
+ .compatible = "ti,am654-r5fss",
+ .data = am65x_r5f_dev_data,
+ },
+ { /* sentinel */ },
+};
+MODULE_DEVICE_TABLE(of, k3_r5_of_match);
+
+static struct platform_driver k3_r5_rproc_driver = {
+ .probe = k3_r5_probe,
+ .remove = k3_r5_remove,
+ .driver = {
+ .name = "k3_r5_rproc",
+ .of_match_table = k3_r5_of_match,
+ },
+};
+
+module_platform_driver(k3_r5_rproc_driver);
+
+MODULE_LICENSE("GPL v2");
+MODULE_DESCRIPTION("TI K3 R5F remote processor driver");
+MODULE_AUTHOR("Suman Anna <s-anna@ti.com>");