]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/commitdiff
seccomp: Move speculation migitation control to arch code
authorThomas Gleixner <tglx@linutronix.de>
Fri, 4 May 2018 13:12:06 +0000 (15:12 +0200)
committerThomas Gleixner <tglx@linutronix.de>
Fri, 4 May 2018 22:51:44 +0000 (00:51 +0200)
The migitation control is simpler to implement in architecture code as it
avoids the extra function call to check the mode. Aside of that having an
explicit seccomp enabled mode in the architecture mitigations would require
even more workarounds.

Move it into architecture code and provide a weak function in the seccomp
code. Remove the 'which' argument as this allows the architecture to decide
which mitigations are relevant for seccomp.

Signed-off-by: Thomas Gleixner <tglx@linutronix.de>
arch/x86/kernel/cpu/bugs.c
include/linux/nospec.h
kernel/seccomp.c

index 7e0f28160e5e5239a672415193ed3d899b0da8c7..5dab4c3d26e7600c81ead42fb73f31809ea040d4 100644 (file)
@@ -569,6 +569,24 @@ static int ssb_prctl_set(struct task_struct *task, unsigned long ctrl)
        return 0;
 }
 
+int arch_prctl_spec_ctrl_set(struct task_struct *task, unsigned long which,
+                            unsigned long ctrl)
+{
+       switch (which) {
+       case PR_SPEC_STORE_BYPASS:
+               return ssb_prctl_set(task, ctrl);
+       default:
+               return -ENODEV;
+       }
+}
+
+#ifdef CONFIG_SECCOMP
+void arch_seccomp_spec_mitigate(struct task_struct *task)
+{
+       ssb_prctl_set(task, PR_SPEC_FORCE_DISABLE);
+}
+#endif
+
 static int ssb_prctl_get(struct task_struct *task)
 {
        switch (ssb_mode) {
@@ -587,17 +605,6 @@ static int ssb_prctl_get(struct task_struct *task)
        }
 }
 
-int arch_prctl_spec_ctrl_set(struct task_struct *task, unsigned long which,
-                            unsigned long ctrl)
-{
-       switch (which) {
-       case PR_SPEC_STORE_BYPASS:
-               return ssb_prctl_set(task, ctrl);
-       default:
-               return -ENODEV;
-       }
-}
-
 int arch_prctl_spec_ctrl_get(struct task_struct *task, unsigned long which)
 {
        switch (which) {
index a908c954484dab137c8e2d7448f9407076ebd584..0c5ef54fd4162830b55aa676c1ecae4ea6ac23f5 100644 (file)
@@ -62,5 +62,7 @@ static inline unsigned long array_index_mask_nospec(unsigned long index,
 int arch_prctl_spec_ctrl_get(struct task_struct *task, unsigned long which);
 int arch_prctl_spec_ctrl_set(struct task_struct *task, unsigned long which,
                             unsigned long ctrl);
+/* Speculation control for seccomp enforced mitigation */
+void arch_seccomp_spec_mitigate(struct task_struct *task);
 
 #endif /* _LINUX_NOSPEC_H */
index 53eb946120c130cdf481cc4431543317575e9edb..e691d9a6c58d1b629a390cf9e5da6c374c877873 100644 (file)
@@ -229,18 +229,7 @@ static inline bool seccomp_may_assign_mode(unsigned long seccomp_mode)
        return true;
 }
 
-/*
- * If a given speculation mitigation is opt-in (prctl()-controlled),
- * select it, by disabling speculation (enabling mitigation).
- */
-static inline void spec_mitigate(struct task_struct *task,
-                                unsigned long which)
-{
-       int state = arch_prctl_spec_ctrl_get(task, which);
-
-       if (state > 0 && (state & PR_SPEC_PRCTL))
-               arch_prctl_spec_ctrl_set(task, which, PR_SPEC_FORCE_DISABLE);
-}
+void __weak arch_seccomp_spec_mitigate(struct task_struct *task) { }
 
 static inline void seccomp_assign_mode(struct task_struct *task,
                                       unsigned long seccomp_mode,
@@ -256,7 +245,7 @@ static inline void seccomp_assign_mode(struct task_struct *task,
        smp_mb__before_atomic();
        /* Assume default seccomp processes want spec flaw mitigation. */
        if ((flags & SECCOMP_FILTER_FLAG_SPEC_ALLOW) == 0)
-               spec_mitigate(task, PR_SPEC_STORE_BYPASS);
+               arch_seccomp_spec_mitigate(task);
        set_tsk_thread_flag(task, TIF_SECCOMP);
 }