summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 4b0e7a6)
raw | patch | inline | side by side (parent: 4b0e7a6)
author | Suman Anna <s-anna@ti.com> | |
Fri, 22 Feb 2019 00:20:28 +0000 (18:20 -0600) | ||
committer | Suman Anna <s-anna@ti.com> | |
Sun, 24 Feb 2019 01:20:51 +0000 (19:20 -0600) |
The PRU remoteproc driver has been enhanced to support the optional
rpmsg stack using the virtio-ring based communication transport
between MPU and a PRU core. This provides support to any firmware
images supporting the virtio devices.
The virtio-ring signalling support is provided either through a OMAP
mailbox or through two PRU system events on OMAP-architecture based
SoCs - one event used in each direction for kicking from one processor
and receiving notification on the other processor. The virtio rpmsg
signalling is enabled only using using PRU system events for interrupts
on the Keystone-architecture based 66AK2G SoCs (it is possible to
implement using an alternate Keystone specific IPCGR registers as well).
The driver supports both signalling options, though the PRU events based
signalling is the recommended option as it avoids an external peripheral
access from the PRU side. It also provides a uniform solution across
both the OMAP, Keystone and Davinci architectures. The PRU events based
signalling takes precedence if both options are mentioned. Either of the
options would require the corresponding firmware support though. A build
dependency against MAILBOX is also added. Note that the OMAP Mailbox
IP is not present on 66AK2G and Davinci SoCs, so it is only selected
for OMAP-based SoCs.
Signed-off-by: Suman Anna <s-anna@ti.com>
rpmsg stack using the virtio-ring based communication transport
between MPU and a PRU core. This provides support to any firmware
images supporting the virtio devices.
The virtio-ring signalling support is provided either through a OMAP
mailbox or through two PRU system events on OMAP-architecture based
SoCs - one event used in each direction for kicking from one processor
and receiving notification on the other processor. The virtio rpmsg
signalling is enabled only using using PRU system events for interrupts
on the Keystone-architecture based 66AK2G SoCs (it is possible to
implement using an alternate Keystone specific IPCGR registers as well).
The driver supports both signalling options, though the PRU events based
signalling is the recommended option as it avoids an external peripheral
access from the PRU side. It also provides a uniform solution across
both the OMAP, Keystone and Davinci architectures. The PRU events based
signalling takes precedence if both options are mentioned. Either of the
options would require the corresponding firmware support though. A build
dependency against MAILBOX is also added. Note that the OMAP Mailbox
IP is not present on 66AK2G and Davinci SoCs, so it is only selected
for OMAP-based SoCs.
Signed-off-by: Suman Anna <s-anna@ti.com>
drivers/remoteproc/Kconfig | patch | blob | history | |
drivers/remoteproc/pru_rproc.c | patch | blob | history |
index 388a0a38ce9ac6aa55cf1864c06e65c16ffe45df..1919cf005e5ada2c2cb48434a35b3c553668d681 100644 (file)
tristate "TI PRU remoteproc support"
depends on TI_PRUSS
default TI_PRUSS
+ select MAILBOX
+ select OMAP2PLUS_MBOX if ARCH_OMAP2PLUS
help
Support for TI PRU remote processors present within a PRU-ICSS
subsystem via the remote processor framework.
index af53b975f7aa45e94d9699ce85f208383805fc10..eb5a3330798485bcc17dfda9723f296c0828a6ef 100644 (file)
#include <linux/bitops.h>
#include <linux/debugfs.h>
#include <linux/interrupt.h>
+#include <linux/mailbox_client.h>
#include <linux/module.h>
#include <linux/of_device.h>
+#include <linux/pruss.h>
#include <linux/pruss_driver.h>
#include <linux/remoteproc.h>
* @id: id of the PRU core within the PRUSS
* @pruss: back-reference to parent PRUSS structure
* @rproc: remoteproc pointer for this PRU core
+ * @mbox: mailbox channel handle used for vring signalling with MPU
+ * @client: mailbox client to request the mailbox channel
+ * @irq_ring: IRQ number to use for processing vring buffers
+ * @irq_kick: IRQ number to use to perform virtio kick
* @mem_regions: data for each of the PRU memory regions
* @intc_config: PRU INTC configuration data
* @iram_da: device address of Instruction RAM for this PRU
int id;
struct pruss *pruss;
struct rproc *rproc;
+ struct mbox_chan *mbox;
+ struct mbox_client client;
+ int irq_vring;
+ int irq_kick;
struct pruss_mem_region mem_regions[PRU_IOMEM_MAX];
struct pruss_intc_config intc_config;
u32 iram_da;
rproc, &pru_rproc_debug_ss_fops);
}
+/**
+ * pru_rproc_mbox_callback() - inbound mailbox message handler
+ * @client: mailbox client pointer used for requesting the mailbox channel
+ * @data: mailbox payload
+ *
+ * This handler is invoked by omap's mailbox driver whenever a mailbox
+ * message is received. Usually, the mailbox payload simply contains
+ * the index of the virtqueue that is kicked by the PRU remote processor,
+ * and we let remoteproc core handle it.
+ *
+ * In addition to virtqueue indices, we might also have some out-of-band
+ * values that indicates different events. Those values are deliberately
+ * very big so they don't coincide with virtqueue indices.
+ */
+static void pru_rproc_mbox_callback(struct mbox_client *client, void *data)
+{
+ struct pru_rproc *pru = container_of(client, struct pru_rproc, client);
+ struct device *dev = &pru->rproc->dev;
+ u32 msg = (u32)data;
+
+ dev_dbg(dev, "mbox msg: 0x%x\n", msg);
+
+ /* msg contains the index of the triggered vring */
+ if (rproc_vq_interrupt(pru->rproc, msg) == IRQ_NONE)
+ dev_dbg(dev, "no message was found in vqid %d\n", msg);
+}
+
+/**
+ * pru_rproc_vring_interrupt() - interrupt handler for processing vrings
+ * @irq: irq number associated with the PRU event MPU is listening on
+ * @data: interrupt handler data, will be a PRU rproc structure
+ *
+ * This handler is used by the PRU remoteproc driver when using PRU system
+ * events for processing the virtqueues. Unlike the mailbox IP, there is
+ * no payload associated with an interrupt, so either a unique event is
+ * used for each virtqueue kick, or a both virtqueues are processed on
+ * a single event. The latter is chosen to conserve the usable PRU system
+ * events.
+ */
+static irqreturn_t pru_rproc_vring_interrupt(int irq, void *data)
+{
+ struct pru_rproc *pru = data;
+
+ dev_dbg(&pru->rproc->dev, "got vring irq\n");
+
+ /* process incoming buffers on both the Rx and Tx vrings */
+ rproc_vq_interrupt(pru->rproc, 0);
+ rproc_vq_interrupt(pru->rproc, 1);
+
+ return IRQ_HANDLED;
+}
+
+/* kick a virtqueue */
+static void pru_rproc_kick(struct rproc *rproc, int vq_id)
+{
+ struct device *dev = &rproc->dev;
+ struct pru_rproc *pru = rproc->priv;
+ int ret;
+
+ dev_dbg(dev, "kicking vqid %d on PRU%d\n", vq_id, pru->id);
+
+ if (pru->irq_kick > 0) {
+ ret = pruss_intc_trigger(pru->irq_kick);
+ if (ret < 0)
+ dev_err(dev, "pruss_intc_trigger failed: %d\n", ret);
+ } else if (pru->mbox) {
+ /*
+ * send the index of the triggered virtqueue in the mailbox
+ * payload
+ */
+ ret = mbox_send_message(pru->mbox, (void *)vq_id);
+ if (ret < 0)
+ dev_err(dev, "mbox_send_message failed: %d\n", ret);
+ }
+}
+
/* start a PRU core */
static int pru_rproc_start(struct rproc *rproc)
{
struct device *dev = &rproc->dev;
struct pru_rproc *pru = rproc->priv;
u32 val;
+ int ret;
dev_dbg(dev, "starting PRU%d: entry-point = 0x%x\n",
pru->id, (rproc->bootaddr >> 2));
+ if (!list_empty(&pru->rproc->rvdevs)) {
+ if (!pru->mbox && (pru->irq_vring <= 0 || pru->irq_kick <= 0)) {
+ dev_err(dev, "virtio vring interrupt mechanisms are not provided\n");
+ ret = -EINVAL;
+ goto fail;
+ }
+
+ if (!pru->mbox && pru->irq_vring > 0) {
+ ret = request_threaded_irq(pru->irq_vring, NULL,
+ pru_rproc_vring_interrupt,
+ IRQF_ONESHOT, dev_name(dev),
+ pru);
+ if (ret) {
+ dev_err(dev, "failed to enable vring interrupt, ret = %d\n",
+ ret);
+ goto fail;
+ }
+ }
+ }
+
val = CTRL_CTRL_EN | ((rproc->bootaddr >> 2) << 16);
pru_control_write_reg(pru, PRU_CTRL_CTRL, val);
return 0;
+
+fail:
+ pruss_intc_unconfigure(pru->pruss, &pru->intc_config);
+ return ret;
}
/* stop/disable a PRU core */
val &= ~CTRL_CTRL_EN;
pru_control_write_reg(pru, PRU_CTRL_CTRL, val);
+ if (!list_empty(&pru->rproc->rvdevs) &&
+ !pru->mbox && pru->irq_vring > 0)
+ free_irq(pru->irq_vring, pru);
+
/* undo INTC config */
pruss_intc_unconfigure(pru->pruss, &pru->intc_config);
static struct rproc_ops pru_rproc_ops = {
.start = pru_rproc_start,
.stop = pru_rproc_stop,
+ .kick = pru_rproc_kick,
.handle_vendor_rsc = pru_rproc_handle_vendor_rsc,
.da_to_va = pru_da_to_va,
};
struct pru_rproc *pru;
const char *fw_name;
struct rproc *rproc = NULL;
+ struct mbox_client *client;
struct resource *res;
int i, ret;
const char *mem_names[PRU_IOMEM_MAX] = { "iram", "control", "debug" };
platform_set_drvdata(pdev, rproc);
+ /* get optional vring and kick interrupts for supporting virtio rpmsg */
+ pru->irq_vring = platform_get_irq_byname(pdev, "vring");
+ if (pru->irq_vring <= 0) {
+ ret = pru->irq_vring;
+ if (ret == -EPROBE_DEFER)
+ goto free_rproc;
+ dev_dbg(dev, "unable to get vring interrupt, status = %d\n",
+ ret);
+ }
+
+ pru->irq_kick = platform_get_irq_byname(pdev, "kick");
+ if (pru->irq_kick <= 0) {
+ ret = pru->irq_kick;
+ if (ret == -EPROBE_DEFER)
+ goto free_rproc;
+ dev_dbg(dev, "unable to get kick interrupt, status = %d\n",
+ ret);
+ }
+
+ /*
+ * get optional mailbox for virtio rpmsg signalling if vring and kick
+ * interrupts are not specified for OMAP architecture based SoCs
+ */
+ if (pru->irq_vring <= 0 && pru->irq_kick <= 0 &&
+ !of_device_is_compatible(np, "ti,k2g-pru")) {
+ client = &pru->client;
+ client->dev = dev;
+ client->tx_done = NULL;
+ client->rx_callback = pru_rproc_mbox_callback;
+ client->tx_block = false;
+ client->knows_txdone = false;
+ pru->mbox = mbox_request_channel(client, 0);
+ if (IS_ERR(pru->mbox)) {
+ ret = PTR_ERR(pru->mbox);
+ pru->mbox = NULL;
+ dev_dbg(dev, "unable to get mailbox channel, status = %d\n",
+ ret);
+ }
+ }
+
ret = rproc_add(pru->rproc);
if (ret) {
dev_err(dev, "rproc_add failed: %d\n", ret);
- goto free_rproc;
+ goto put_mbox;
}
pru_rproc_create_debug_entries(rproc);
return 0;
+put_mbox:
+ mbox_free_channel(pru->mbox);
free_rproc:
rproc_free(rproc);
return ret;
{
struct device *dev = &pdev->dev;
struct rproc *rproc = platform_get_drvdata(pdev);
+ struct pru_rproc *pru = rproc->priv;
dev_info(dev, "%s: removing rproc %s\n", __func__, rproc->name);
+ mbox_free_channel(pru->mbox);
+
rproc_del(rproc);
rproc_free(rproc);