summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 7cd9180)
raw | patch | inline | side by side (parent: 7cd9180)
author | Paolo Bonzini <pbonzini@redhat.com> | |
Wed, 13 Dec 2017 10:05:19 +0000 (11:05 +0100) | ||
committer | Radim Krčmář <rkrcmar@redhat.com> | |
Tue, 16 Jan 2018 15:49:44 +0000 (16:49 +0100) |
Compared to when VMCS shadowing was added to KVM, we are reading/writing
a few more fields: the PML index, the interrupt status and the preemption
timer value. The first two are because we are exposing more features
to nested guests, the preemption timer is simply because we have grown
a new optimization. Adding them to the shadow VMCS field lists reduces
the cost of a vmexit by about 1000 clock cycles for each field that exists
on bare metal.
On the other hand, the guest BNDCFGS and TSC offset are not written on
fast paths, so remove them.
Suggested-by: Jim Mattson <jmattson@google.com>
Cc: Jim Mattson <jmattson@google.com>
Cc: Wanpeng Li <wanpeng.li@hotmail.com>
Signed-off-by: Paolo Bonzini <pbonzini@redhat.com>
Signed-off-by: Radim Krčmář <rkrcmar@redhat.com>
a few more fields: the PML index, the interrupt status and the preemption
timer value. The first two are because we are exposing more features
to nested guests, the preemption timer is simply because we have grown
a new optimization. Adding them to the shadow VMCS field lists reduces
the cost of a vmexit by about 1000 clock cycles for each field that exists
on bare metal.
On the other hand, the guest BNDCFGS and TSC offset are not written on
fast paths, so remove them.
Suggested-by: Jim Mattson <jmattson@google.com>
Cc: Jim Mattson <jmattson@google.com>
Cc: Wanpeng Li <wanpeng.li@hotmail.com>
Signed-off-by: Paolo Bonzini <pbonzini@redhat.com>
Signed-off-by: Radim Krčmář <rkrcmar@redhat.com>
arch/x86/kvm/vmx.c | patch | blob | history |
diff --git a/arch/x86/kvm/vmx.c b/arch/x86/kvm/vmx.c
index 2c8749ee3221de17d3eec4167febc42b0bb36d08..7b114a293c66332f8e69e15f6a38fecfd5ad427f 100644 (file)
--- a/arch/x86/kvm/vmx.c
+++ b/arch/x86/kvm/vmx.c
GUEST_CS_LIMIT,
GUEST_CS_BASE,
GUEST_ES_BASE,
- GUEST_BNDCFGS,
+ GUEST_PML_INDEX,
+ GUEST_INTR_STATUS,
+ VMX_PREEMPTION_TIMER_VALUE,
CR0_GUEST_HOST_MASK,
CR0_READ_SHADOW,
CR4_READ_SHADOW,
- TSC_OFFSET,
EXCEPTION_BITMAP,
CPU_BASED_VM_EXEC_CONTROL,
VM_ENTRY_EXCEPTION_ERROR_CODE,
/* No checks for read only fields yet */
for (i = j = 0; i < max_shadow_read_write_fields; i++) {
+ /*
+ * PML and the preemption timer can be emulated, but the
+ * processor cannot vmwrite to fields that don't exist
+ * on bare metal.
+ */
switch (shadow_read_write_fields[i]) {
- case GUEST_BNDCFGS:
- if (!kvm_mpx_supported())
+ case GUEST_PML_INDEX:
+ if (!cpu_has_vmx_pml())
+ continue;
+ break;
+ case VMX_PREEMPTION_TIMER_VALUE:
+ if (!cpu_has_vmx_preemption_timer())
+ continue;
+ break;
+ case GUEST_INTR_STATUS:
+ if (!cpu_has_vmx_apicv())
continue;
break;
default:
!(cpu_has_vmx_invvpid_single() || cpu_has_vmx_invvpid_global()))
enable_vpid = 0;
- if (!cpu_has_vmx_shadow_vmcs())
- enable_shadow_vmcs = 0;
- if (enable_shadow_vmcs)
- init_vmcs_shadow_fields();
-
if (!cpu_has_vmx_ept() ||
!cpu_has_vmx_ept_4levels() ||
!cpu_has_vmx_ept_mt_wb() ||
kvm_x86_ops->cancel_hv_timer = NULL;
}
+ if (!cpu_has_vmx_shadow_vmcs())
+ enable_shadow_vmcs = 0;
+ if (enable_shadow_vmcs)
+ init_vmcs_shadow_fields();
+
kvm_set_posted_intr_wakeup_handler(wakeup_handler);
kvm_mce_cap_supported |= MCG_LMCE_P;