author | Greg Kroah-Hartman <gregkh@linuxfoundation.org> | |
Mon, 24 Oct 2016 09:34:22 +0000 (11:34 +0200) | ||
committer | Greg Kroah-Hartman <gregkh@linuxfoundation.org> | |
Mon, 24 Oct 2016 09:34:22 +0000 (11:34 +0200) |
Jonathan writes:
First round of IIO new device support, features and cleanups for the 4.10 cycle.
Fair number of outreachy related patches in here. Some of these may well
have already been picked up by Greg but git will sort that out for us.
Also some good staging cleanup work from other sources. Thanks Brian and Lars
in particular for this.
New device support
* ACCES 104-quad-8
- New driver for this 8 channel encoder input board. Lots of new ABI with
this one.
* AD7766
- New driver supporting AD7766, AD7766-1, AD7766-2, AD7767, AD7767-1 and
AD7767-2 24 bit ADCs.
* dmard 10
- New driver for this 3 axis accelerometer.
* Honeywell ABP pressure sensors.
- New driver covering 56 parts in this series (too many to list here!)
* HTS221
- New driver to support this relative humidiy and temperature device.
* LMP91000
- New driver for this potentiostat (form of chemical sensor). Nice example
of use of the buffered consumer interfaces and the use of a consumer
provided trigger.
* MiraMEMS DA311
- New driver for this 3 axis accelerometer.
* MiraMEMS DA280
- New driver for this 3 axis accelerometer. Follow up caught up with
vendor prefixes for these.
Staging graduations
* isl29018 light sensor
- Fixes and cleanups listed below (thanks for your hard work on this Brian!)
* sca3000
- Fixes and cleanups listed below. This was one of the small set of drivers
that went into staging when IIO was first added. Turns out it had a few
bugs and needed to be brought into the modern era! Not clear if I am
the only person who actually has one of these still wired to a board.
New features (Core)
- Add an iio_trigger_validate_own_device helper which relies on the device
and trigger having the same parent. Convenient to have this for some
of the more complex trigger / device interactions. Was hand rolled in
a few drivers already so good to bring it into the core.
- Add an iio_read_channel_offset in kernel access helper (similar to
the existing one for scale).
- IIO_ATTR_{RO, WO, RW} and IIO_DEVICE_ATTR_{RO, WO, RW} macros. These
lead some rather contrived function naming, but there is no denying they
do reduced boilerplate. I'm going to resist their introduction in
drivers 'unless' they form part of a larger set of cleanups.
- Counter channel type and index type.
New features (Drivers)
* hdc100x
- Triggered buffer support.
* mcp4725
- Device tree bindings and support.
- Voltage reference selection.
* ti-adc0832
- Triggered buffer support.
* ti-adc161s626
- Add regulator support allowing _scale and _offset values to be established
and exported.
New features (Tools)
* iio_generic_buffer
- -A option to force enable all channels rather than faulting if some are
already enabled (like -a does). Followup patches tidied this support up.
Cleanups (Core)
- Use kmalloc_array in iio_scan_mask_set.
- Take event_attrs field of iio_info structure constant
- Staging todo list updates. Most of it was long done.
- MAINTAINERS had a wrong directory listing.
Cleanups (Drivers)
* Missing i2c trivial devices entries.
* ad5592r
- Fix an endian type related sparse warnings.
* ad7150
- Constify the event attribute_group structures.
* ad7152
- Add some blank lines to improve readability.
- Sampling frequency control via chan-info element rather than hand rolled
attributes.
- add a new lock to avoid use of mlock for non state change related locking.
* ad7280
- Constify atrribute_group structure (second patch covers the event ones)
* ad7606 (Lars is driving most of the cleanup on this with some additions from
Eva)
- Fix improper setting of oversampling pins. This has been broken a very
long time in this staging driver, so not going to push this back to stable.
- Implement oversampling configuration via the chan_info mask element.
- Remove an unused int_vref_mv field.
- Remove a reundant name field from ad7606_chip_info.
- Remove default device configuration from platform_data in favour of
whatever the power on defaults are.
- Remove out of band error reporting in the kernel log as not providing
much information.
- Fix oversampling ratio by having 1 be the value for no oversampling.
- Avoid allocating buffer for each data capture.
- Factor out common code between periodic and one-shot capture.
- Move set_drvdat into common code.
- Let the common probe function return int rather than jumping through
an ERR_PTR.
- Pass struct device * into common remove to simplify code.
- Always run trigger handler only once per event (no one can remember why
it was being possibly done twice).
- Move over to the GPIO descriptor API to shorten and clarify code.
- Move the buffer code into the main file as it's not optional and is
now rather short in this driver.
- Fix the naming of the supply regulator.
- Rework regulator handling to handle errors including deferred probing.
- Tidy up a ptr_err or 0 return.
* ad7746
- Sampling frequency control via info_mask element rather than hand rolled
* ad7758
- Sampling frequency control via info_mask element rather than hand rolled
attributes.
* ad7816
- Constify the event attribute_group structure.
* adt7316
- Constify the event attribute group structures.
* ak8974
- Cleanup some sparse warnings about endian types.
* ak8975
- Cleanup some sparse warnings about endian types.
* bmi160
- Spare endian warning cleanups.
* isl29018 (towards staging graduation)
- Remove unusedvariables and defines.
- Improve consistency of error handling.
- Signed / unsigned comparison fixes.
- Use the IIO_DEVICE_ATTR_{RO, RW} macros
- Fix a race in in_illuminance_scale_available_show.
- Cleanup exit points of _read_raw
- Sanity check if in suspended state during a write_raw call as was already
done for read_raw.
- Document device tree bidnings.
- Document infrared supression controls.
- Add some newlines to improve readability and drop one that shouldn't be
there.
- Fix a poorly named functions name.
- Fix multiline coment syntax.
- Tidy up a pair or return statements by unifying them.
- Rename description in Kconfig for consistency with similar drivers.
* lidar
- cleanup power management by dropping unnecessary call.
* ltr501
- Use the claim_direct_mode helpers. Fix a race condition along the way.
* max1027
- Fix a dubious x | !y sparse warning.
- Use the new iio_trigger_validate_own_device helper.
* max440000
- Clean up some sparse warnings about endian types.
* mcp4725
- Use the regulator framework to establish the reference voltage rather than
getting it from platform data.
- Tidy up a comment typo.
- Fix a wrong PTR_ERR query (wrong regulator).
* mma7660
- Take a mma7660_nscale static.
* mma8452
- Use the new iio_trigger_validate_own_device helper.
- Use claim_direct_mode helpers - fix a race condition along the way.
* mpl3115
- Use claim_direct_mode helpers - fix a race condition along the way.
* ms65611
- Tidy up regulator error handling and clean out a static warning in the mix.
* sca3000
- Avoid a potential unitialized variable if a hardware read returns a value
that isn't actually supported (mostly warning supression).
- Fix a use before setting of the indio_dev->buffer pointer. Broken for
a very long time so not going to rush this into stable.
- Merge buffer file with core file. We used to always split these.
Sometimes it's just not worth the hassle. In this case the device's main
feature is it's hardware fifos so unlikely anyone would want to run it
without.
- Drop the sca3000_register_ring_funcs function as it's a pointless wrapper
once we have only one file.
- Fix cleaning of flag + setting of size of scan. Without this you can't
start the buffer twice and expect sensible (or any) results. Again,
broken for a long time so not heading for stable.
- Drop the custom watershed setting ABI - for now we'll just support one
value.
- Move to a hybrid hard / soft buffer design (how we've been doing it
for similar devices for a while now!)
- Cleanup some unusued variables.
- Use a fake channel to support core handling of freefall event registration.
- Cleanup the register defines.
- Fix an off by one error in axis due to IIO_NO_MOD taking up the 0 value.
Been broken since first admission of IIO to the staging tree.
- Add readback of the 3db low pass filter frequency and later writing
allowing droppign of custom measurement mode attributes as they can
be represented by the filter choices that is their main characteristic.
- Drop non standard revision attr and replace with dev_info on probe.
- Avoid a race in probe.
- Various formatting fixes.
- Kernel-docify docs that were very nearly in the write format.
* tsl2583
- Constify attribute_group structure.
* zpa2326
- Drop a redundant DEBUG ifdef.
Cleanups (Tools)
* iio_generic_buffer
- Fix the ? arguement. Previously it sort of worked as you got the help
message as a result of it not recognising the arguement.
First round of IIO new device support, features and cleanups for the 4.10 cycle.
Fair number of outreachy related patches in here. Some of these may well
have already been picked up by Greg but git will sort that out for us.
Also some good staging cleanup work from other sources. Thanks Brian and Lars
in particular for this.
New device support
* ACCES 104-quad-8
- New driver for this 8 channel encoder input board. Lots of new ABI with
this one.
* AD7766
- New driver supporting AD7766, AD7766-1, AD7766-2, AD7767, AD7767-1 and
AD7767-2 24 bit ADCs.
* dmard 10
- New driver for this 3 axis accelerometer.
* Honeywell ABP pressure sensors.
- New driver covering 56 parts in this series (too many to list here!)
* HTS221
- New driver to support this relative humidiy and temperature device.
* LMP91000
- New driver for this potentiostat (form of chemical sensor). Nice example
of use of the buffered consumer interfaces and the use of a consumer
provided trigger.
* MiraMEMS DA311
- New driver for this 3 axis accelerometer.
* MiraMEMS DA280
- New driver for this 3 axis accelerometer. Follow up caught up with
vendor prefixes for these.
Staging graduations
* isl29018 light sensor
- Fixes and cleanups listed below (thanks for your hard work on this Brian!)
* sca3000
- Fixes and cleanups listed below. This was one of the small set of drivers
that went into staging when IIO was first added. Turns out it had a few
bugs and needed to be brought into the modern era! Not clear if I am
the only person who actually has one of these still wired to a board.
New features (Core)
- Add an iio_trigger_validate_own_device helper which relies on the device
and trigger having the same parent. Convenient to have this for some
of the more complex trigger / device interactions. Was hand rolled in
a few drivers already so good to bring it into the core.
- Add an iio_read_channel_offset in kernel access helper (similar to
the existing one for scale).
- IIO_ATTR_{RO, WO, RW} and IIO_DEVICE_ATTR_{RO, WO, RW} macros. These
lead some rather contrived function naming, but there is no denying they
do reduced boilerplate. I'm going to resist their introduction in
drivers 'unless' they form part of a larger set of cleanups.
- Counter channel type and index type.
New features (Drivers)
* hdc100x
- Triggered buffer support.
* mcp4725
- Device tree bindings and support.
- Voltage reference selection.
* ti-adc0832
- Triggered buffer support.
* ti-adc161s626
- Add regulator support allowing _scale and _offset values to be established
and exported.
New features (Tools)
* iio_generic_buffer
- -A option to force enable all channels rather than faulting if some are
already enabled (like -a does). Followup patches tidied this support up.
Cleanups (Core)
- Use kmalloc_array in iio_scan_mask_set.
- Take event_attrs field of iio_info structure constant
- Staging todo list updates. Most of it was long done.
- MAINTAINERS had a wrong directory listing.
Cleanups (Drivers)
* Missing i2c trivial devices entries.
* ad5592r
- Fix an endian type related sparse warnings.
* ad7150
- Constify the event attribute_group structures.
* ad7152
- Add some blank lines to improve readability.
- Sampling frequency control via chan-info element rather than hand rolled
attributes.
- add a new lock to avoid use of mlock for non state change related locking.
* ad7280
- Constify atrribute_group structure (second patch covers the event ones)
* ad7606 (Lars is driving most of the cleanup on this with some additions from
Eva)
- Fix improper setting of oversampling pins. This has been broken a very
long time in this staging driver, so not going to push this back to stable.
- Implement oversampling configuration via the chan_info mask element.
- Remove an unused int_vref_mv field.
- Remove a reundant name field from ad7606_chip_info.
- Remove default device configuration from platform_data in favour of
whatever the power on defaults are.
- Remove out of band error reporting in the kernel log as not providing
much information.
- Fix oversampling ratio by having 1 be the value for no oversampling.
- Avoid allocating buffer for each data capture.
- Factor out common code between periodic and one-shot capture.
- Move set_drvdat into common code.
- Let the common probe function return int rather than jumping through
an ERR_PTR.
- Pass struct device * into common remove to simplify code.
- Always run trigger handler only once per event (no one can remember why
it was being possibly done twice).
- Move over to the GPIO descriptor API to shorten and clarify code.
- Move the buffer code into the main file as it's not optional and is
now rather short in this driver.
- Fix the naming of the supply regulator.
- Rework regulator handling to handle errors including deferred probing.
- Tidy up a ptr_err or 0 return.
* ad7746
- Sampling frequency control via info_mask element rather than hand rolled
* ad7758
- Sampling frequency control via info_mask element rather than hand rolled
attributes.
* ad7816
- Constify the event attribute_group structure.
* adt7316
- Constify the event attribute group structures.
* ak8974
- Cleanup some sparse warnings about endian types.
* ak8975
- Cleanup some sparse warnings about endian types.
* bmi160
- Spare endian warning cleanups.
* isl29018 (towards staging graduation)
- Remove unusedvariables and defines.
- Improve consistency of error handling.
- Signed / unsigned comparison fixes.
- Use the IIO_DEVICE_ATTR_{RO, RW} macros
- Fix a race in in_illuminance_scale_available_show.
- Cleanup exit points of _read_raw
- Sanity check if in suspended state during a write_raw call as was already
done for read_raw.
- Document device tree bidnings.
- Document infrared supression controls.
- Add some newlines to improve readability and drop one that shouldn't be
there.
- Fix a poorly named functions name.
- Fix multiline coment syntax.
- Tidy up a pair or return statements by unifying them.
- Rename description in Kconfig for consistency with similar drivers.
* lidar
- cleanup power management by dropping unnecessary call.
* ltr501
- Use the claim_direct_mode helpers. Fix a race condition along the way.
* max1027
- Fix a dubious x | !y sparse warning.
- Use the new iio_trigger_validate_own_device helper.
* max440000
- Clean up some sparse warnings about endian types.
* mcp4725
- Use the regulator framework to establish the reference voltage rather than
getting it from platform data.
- Tidy up a comment typo.
- Fix a wrong PTR_ERR query (wrong regulator).
* mma7660
- Take a mma7660_nscale static.
* mma8452
- Use the new iio_trigger_validate_own_device helper.
- Use claim_direct_mode helpers - fix a race condition along the way.
* mpl3115
- Use claim_direct_mode helpers - fix a race condition along the way.
* ms65611
- Tidy up regulator error handling and clean out a static warning in the mix.
* sca3000
- Avoid a potential unitialized variable if a hardware read returns a value
that isn't actually supported (mostly warning supression).
- Fix a use before setting of the indio_dev->buffer pointer. Broken for
a very long time so not going to rush this into stable.
- Merge buffer file with core file. We used to always split these.
Sometimes it's just not worth the hassle. In this case the device's main
feature is it's hardware fifos so unlikely anyone would want to run it
without.
- Drop the sca3000_register_ring_funcs function as it's a pointless wrapper
once we have only one file.
- Fix cleaning of flag + setting of size of scan. Without this you can't
start the buffer twice and expect sensible (or any) results. Again,
broken for a long time so not heading for stable.
- Drop the custom watershed setting ABI - for now we'll just support one
value.
- Move to a hybrid hard / soft buffer design (how we've been doing it
for similar devices for a while now!)
- Cleanup some unusued variables.
- Use a fake channel to support core handling of freefall event registration.
- Cleanup the register defines.
- Fix an off by one error in axis due to IIO_NO_MOD taking up the 0 value.
Been broken since first admission of IIO to the staging tree.
- Add readback of the 3db low pass filter frequency and later writing
allowing droppign of custom measurement mode attributes as they can
be represented by the filter choices that is their main characteristic.
- Drop non standard revision attr and replace with dev_info on probe.
- Avoid a race in probe.
- Various formatting fixes.
- Kernel-docify docs that were very nearly in the write format.
* tsl2583
- Constify attribute_group structure.
* zpa2326
- Drop a redundant DEBUG ifdef.
Cleanups (Tools)
* iio_generic_buffer
- Fix the ? arguement. Previously it sort of worked as you got the help
message as a result of it not recognising the arguement.
Simple merge
index f0a48ea78659c933839554ca879babb1b621b264,ce955f1988f269172625ed281e0692e991b1f2b7..8d04aa99187c6efec04b3dcfde9c193ca1de6cfa
lenovo Lenovo Group Ltd.
lg LG Corporation
linux Linux-specific binding
-lsi LSI Corp. (LSI Logic)
lltc Linear Technology Corporation
+lsi LSI Corp. (LSI Logic)
marvell Marvell Technology Group Ltd.
maxim Maxim Integrated Products
+ mcube mCube
meas Measurement Specialties
mediatek MediaTek Inc.
melexis Melexis N.V.
+melfas MELFAS Inc.
+ memsic MEMSIC Inc.
merrii Merrii Technology Co., Ltd.
micrel Micrel Inc.
microchip Microchip Technology Inc.
+microcrystal Micro Crystal AG
micron Micron Technology Inc.
minix MINIX Technology Ltd.
+ miramems MiraMEMS Sensing Technology Co., Ltd.
mitsubishi Mitsubishi Electric Corporation
mosaixtech Mosaix Technologies, Inc.
moxa Moxa
diff --cc MAINTAINERS
Simple merge
diff --cc drivers/iio/pressure/Kconfig
Simple merge