]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/commitdiff
remoteproc/pru: Add a PRU remoteproc driver
authorSuman Anna <s-anna@ti.com>
Fri, 15 Feb 2019 02:01:21 +0000 (20:01 -0600)
committerSuman Anna <s-anna@ti.com>
Sun, 24 Feb 2019 01:20:48 +0000 (19:20 -0600)
The Programmable Real-Time Unit Subsystem (PRUSS) consists of
dual 32-bit RISC cores (Programmable Real-Time Units, or PRUs)
for program execution. This patch adds a remoteproc platform
driver for managing the individual PRU RISC cores life cycle.

The PRU remoteproc driver uses the standard remoteproc core ELF
loader. However, the PRUs do not have a unified address space,
(has an Instruction RAM and a primary Data RAM at both 0x0) and
leverage an added .da_to_va ops to use the standard ELF loader.
This remoteproc driver does not have support for error recovery
and system suspend/resume features. Different compatibles are
used to allow providing scalability for instance-specific device
data if needed. The driver uses a default firmware-name retrieved
from device-tree, and the firmwares are expected to be present
in the standard Linux firmware search paths. They can also be
adjusted by userspace if required through the sysfs interface
provided by the remoteproc core.

The PRU remoteproc driver uses a client-driven boot methodology
- it does _not_ support auto-boot so that the PRU load and boot
is dictated by the corresponding client drivers for achieving
various usecases. This allows flexibility for the client drivers
or applications to set a firmware name (if needed) based on their
desired functionality and boot the PRU. The sysfs bind and unbind
attributes have also been suppressed so that the PRU devices cannot
be unbound and thereby shutdown a PRU from underneath a PRU client
driver.

The PRU interrupt configuration is handled within the PRUSS INTC
platform driver, and leverages the system events to interrupt
channels and host interrupts mapping configuration through a
PRU firmware resource table for now. This will be revisited and
enhanced in the future for a better interface. The mappings
are currently programmed during the booting/shutdown of the PRU.

The driver currently supports the AM335x SoC, and support for other
TI SoCs will be added in subsequent patches.

Signed-off-by: Suman Anna <s-anna@ti.com>
Signed-off-by: Andrew F. Davis <afd@ti.com>
drivers/remoteproc/Kconfig
drivers/remoteproc/Makefile
drivers/remoteproc/pru_rproc.c [new file with mode: 0644]
drivers/remoteproc/pru_rproc.h [new file with mode: 0644]

index 12fa8f26f1f0e7b6dbb167b9e5fb5e18c115b58d..388a0a38ce9ac6aa55cf1864c06e65c16ffe45df 100644 (file)
@@ -85,6 +85,18 @@ config KEYSTONE_REMOTEPROC
          It's safe to say N here if you're not interested in the Keystone
          DSPs or just want to use a bare minimum kernel.
 
+config PRU_REMOTEPROC
+       tristate "TI PRU remoteproc support"
+       depends on TI_PRUSS
+       default TI_PRUSS
+       help
+         Support for TI PRU remote processors present within a PRU-ICSS
+         subsystem via the remote processor framework.
+
+         Say Y or M here to support the Programmable Realtime Unit (PRU)
+         processors on various TI SoCs. It's safe to say N here if you're
+         not interested in the PRU or if you are unsure.
+
 config QCOM_ADSP_PIL
        tristate "Qualcomm ADSP Peripheral Image Loader"
        depends on OF && ARCH_QCOM
index 03332fa7e2ee7515d5281c175e632d4a600b3382..d005af3c71a8cc55691b612d51f1694a9b892ca5 100644 (file)
@@ -14,6 +14,7 @@ obj-$(CONFIG_OMAP_REMOTEPROC)         += omap_remoteproc.o
 obj-$(CONFIG_WKUP_M3_RPROC)            += wkup_m3_rproc.o
 obj-$(CONFIG_DA8XX_REMOTEPROC)         += da8xx_remoteproc.o
 obj-$(CONFIG_KEYSTONE_REMOTEPROC)      += keystone_remoteproc.o
+obj-$(CONFIG_PRU_REMOTEPROC)           += pru_rproc.o
 obj-$(CONFIG_QCOM_ADSP_PIL)            += qcom_adsp_pil.o
 obj-$(CONFIG_QCOM_RPROC_COMMON)                += qcom_common.o
 obj-$(CONFIG_QCOM_Q6V5_COMMON)         += qcom_q6v5.o
diff --git a/drivers/remoteproc/pru_rproc.c b/drivers/remoteproc/pru_rproc.c
new file mode 100644 (file)
index 0000000..a7adcd4
--- /dev/null
@@ -0,0 +1,488 @@
+// SPDX-License-Identifier: GPL-2.0
+/*
+ * PRU-ICSS remoteproc driver for various TI SoCs
+ *
+ * Copyright (C) 2014-2019 Texas Instruments Incorporated - http://www.ti.com/
+ *     Suman Anna <s-anna@ti.com>
+ *     Andrew F. Davis <afd@ti.com>
+ */
+
+#include <linux/bitops.h>
+#include <linux/interrupt.h>
+#include <linux/module.h>
+#include <linux/of_device.h>
+#include <linux/pruss_driver.h>
+#include <linux/remoteproc.h>
+
+#include "remoteproc_internal.h"
+#include "pru_rproc.h"
+
+/* PRU_ICSS_PRU_CTRL registers */
+#define PRU_CTRL_CTRL          0x0000
+#define PRU_CTRL_STS           0x0004
+#define PRU_CTRL_WAKEUP_EN     0x0008
+#define PRU_CTRL_CYCLE         0x000C
+#define PRU_CTRL_STALL         0x0010
+#define PRU_CTRL_CTBIR0                0x0020
+#define PRU_CTRL_CTBIR1                0x0024
+#define PRU_CTRL_CTPPR0                0x0028
+#define PRU_CTRL_CTPPR1                0x002C
+
+/* CTRL register bit-fields */
+#define CTRL_CTRL_SOFT_RST_N   BIT(0)
+#define CTRL_CTRL_EN           BIT(1)
+#define CTRL_CTRL_SLEEPING     BIT(2)
+#define CTRL_CTRL_CTR_EN       BIT(3)
+#define CTRL_CTRL_SINGLE_STEP  BIT(8)
+#define CTRL_CTRL_RUNSTATE     BIT(15)
+
+/* PRU Core IRAM address masks */
+#define PRU0_IRAM_ADDR_MASK    0x34000
+#define PRU1_IRAM_ADDR_MASK    0x38000
+
+/**
+ * enum pru_iomem - PRU core memory/register range identifiers
+ */
+enum pru_iomem {
+       PRU_IOMEM_IRAM = 0,
+       PRU_IOMEM_CTRL,
+       PRU_IOMEM_DEBUG,
+       PRU_IOMEM_MAX,
+};
+
+/**
+ * struct pru_rproc - PRU remoteproc structure
+ * @id: id of the PRU core within the PRUSS
+ * @pruss: back-reference to parent PRUSS structure
+ * @rproc: remoteproc pointer for this PRU core
+ * @mem_regions: data for each of the PRU memory regions
+ * @intc_config: PRU INTC configuration data
+ * @iram_da: device address of Instruction RAM for this PRU
+ * @pdram_da: device address of primary Data RAM for this PRU
+ * @sdram_da: device address of secondary Data RAM for this PRU
+ * @shrdram_da: device address of shared Data RAM
+ * @fw_name: name of firmware image used during loading
+ */
+struct pru_rproc {
+       int id;
+       struct pruss *pruss;
+       struct rproc *rproc;
+       struct pruss_mem_region mem_regions[PRU_IOMEM_MAX];
+       struct pruss_intc_config intc_config;
+       u32 iram_da;
+       u32 pdram_da;
+       u32 sdram_da;
+       u32 shrdram_da;
+       const char *fw_name;
+};
+
+static void *pru_d_da_to_va(struct pru_rproc *pru, u32 da, int len);
+
+static inline u32 pru_control_read_reg(struct pru_rproc *pru, unsigned int reg)
+{
+       return readl_relaxed(pru->mem_regions[PRU_IOMEM_CTRL].va + reg);
+}
+
+static inline
+void pru_control_write_reg(struct pru_rproc *pru, unsigned int reg, u32 val)
+{
+       writel_relaxed(val, pru->mem_regions[PRU_IOMEM_CTRL].va + reg);
+}
+
+static inline u32 pru_debug_read_reg(struct pru_rproc *pru, unsigned int reg)
+{
+       return readl_relaxed(pru->mem_regions[PRU_IOMEM_DEBUG].va + reg);
+}
+
+static inline
+void pru_debug_write_reg(struct pru_rproc *pru, unsigned int reg, u32 val)
+{
+       writel_relaxed(val, pru->mem_regions[PRU_IOMEM_DEBUG].va + reg);
+}
+
+/* start a PRU core */
+static int pru_rproc_start(struct rproc *rproc)
+{
+       struct device *dev = &rproc->dev;
+       struct pru_rproc *pru = rproc->priv;
+       u32 val;
+
+       dev_dbg(dev, "starting PRU%d: entry-point = 0x%x\n",
+               pru->id, (rproc->bootaddr >> 2));
+
+       val = CTRL_CTRL_EN | ((rproc->bootaddr >> 2) << 16);
+       pru_control_write_reg(pru, PRU_CTRL_CTRL, val);
+
+       return 0;
+}
+
+/* stop/disable a PRU core */
+static int pru_rproc_stop(struct rproc *rproc)
+{
+       struct device *dev = &rproc->dev;
+       struct pru_rproc *pru = rproc->priv;
+       u32 val;
+
+       dev_dbg(dev, "stopping PRU%d\n", pru->id);
+
+       val = pru_control_read_reg(pru, PRU_CTRL_CTRL);
+       val &= ~CTRL_CTRL_EN;
+       pru_control_write_reg(pru, PRU_CTRL_CTRL, val);
+
+       /* undo INTC config */
+       pruss_intc_unconfigure(pru->pruss, &pru->intc_config);
+
+       return 0;
+}
+
+/*
+ * parse the custom PRU interrupt map resource and configure the INTC
+ * appropriately
+ */
+static int pru_handle_vendor_intrmap(struct rproc *rproc,
+                                    struct fw_rsc_vendor *rsc)
+{
+       struct device *dev = rproc->dev.parent;
+       struct pru_rproc *pru = rproc->priv;
+       struct pruss *pruss = pru->pruss;
+       struct pruss_event_chnl *event_chnl_map;
+       struct fw_rsc_pruss_intrmap *intr_rsc =
+               (struct fw_rsc_pruss_intrmap *)rsc->data;
+       int i, ret;
+       s8 sys_evt, chnl, intr_no;
+
+       dev_dbg(dev, "version %d event_chnl_map_size %d event_chnl_map_addr 0x%x\n",
+               rsc->u.st.st_ver, intr_rsc->event_chnl_map_size,
+               intr_rsc->event_chnl_map_addr);
+
+       if (rsc->u.st.st_ver != 0) {
+               dev_err(dev, "only PRU interrupt resource version 0 supported\n");
+               return -EINVAL;
+       }
+
+       if (intr_rsc->event_chnl_map_size < 0 ||
+           intr_rsc->event_chnl_map_size >= MAX_PRU_SYS_EVENTS) {
+               dev_err(dev, "PRU interrupt resource has more events than present on hardware\n");
+               return -EINVAL;
+       }
+
+       /*
+        * XXX: The event_chnl_map_addr mapping is currently a pointer in device
+        * memory, evaluate if this needs to be directly in firmware file.
+        */
+       event_chnl_map = pru_d_da_to_va(pru, intr_rsc->event_chnl_map_addr,
+                                       intr_rsc->event_chnl_map_size *
+                                       sizeof(*event_chnl_map));
+       if (!event_chnl_map) {
+               dev_err(dev, "PRU interrupt resource has inadequate event_chnl_map configuration\n");
+               return -EINVAL;
+       }
+
+       /* init intc_config to defaults */
+       for (i = 0; i < ARRAY_SIZE(pru->intc_config.sysev_to_ch); i++)
+               pru->intc_config.sysev_to_ch[i] = -1;
+
+       for (i = 0; i < ARRAY_SIZE(pru->intc_config.ch_to_host); i++)
+               pru->intc_config.ch_to_host[i] = -1;
+
+       /* parse and fill in system event to interrupt channel mapping */
+       for (i = 0; i < intr_rsc->event_chnl_map_size; i++) {
+               sys_evt = event_chnl_map[i].event;
+               chnl = event_chnl_map[i].chnl;
+
+               if (sys_evt < 0 || sys_evt >= MAX_PRU_SYS_EVENTS) {
+                       dev_err(dev, "[%d] bad sys event %d\n", i, sys_evt);
+                       return -EINVAL;
+               }
+               if (chnl < 0 || chnl >= MAX_PRU_CHANNELS) {
+                       dev_err(dev, "[%d] bad channel value %d\n", i, chnl);
+                       return -EINVAL;
+               }
+
+               pru->intc_config.sysev_to_ch[sys_evt] = chnl;
+               dev_dbg(dev, "sysevt-to-ch[%d] -> %d\n", sys_evt, chnl);
+       }
+
+       /* parse and handle interrupt channel-to-host interrupt mapping */
+       for (i = 0; i < MAX_PRU_CHANNELS; i++) {
+               intr_no = intr_rsc->chnl_host_intr_map[i];
+               if (intr_no < 0) {
+                       dev_dbg(dev, "skip intr mapping for chnl %d\n", i);
+                       continue;
+               }
+
+               if (intr_no >= MAX_PRU_HOST_INT) {
+                       dev_err(dev, "bad intr mapping for chnl %d, intr_no %d\n",
+                               i, intr_no);
+                       return -EINVAL;
+               }
+
+               pru->intc_config.ch_to_host[i] = intr_no;
+               dev_dbg(dev, "chnl-to-host[%d] -> %d\n", i, intr_no);
+       }
+
+       ret = pruss_intc_configure(pruss, &pru->intc_config);
+       if (ret)
+               dev_err(dev, "failed to configure pruss intc %d\n", ret);
+
+       return ret;
+}
+
+/* PRU-specific vendor resource handler */
+static int pru_rproc_handle_vendor_rsc(struct rproc *rproc,
+                                      struct fw_rsc_vendor *rsc)
+{
+       struct device *dev = rproc->dev.parent;
+       int ret = -EINVAL;
+
+       switch (rsc->u.st.st_type) {
+       case PRUSS_RSC_INTRS:
+               ret = pru_handle_vendor_intrmap(rproc, rsc);
+               break;
+       default:
+               dev_err(dev, "%s: cannot handle unknown type %d\n", __func__,
+                       rsc->u.st.st_type);
+       }
+
+       return ret;
+}
+
+/*
+ * Convert PRU device address (data spaces only) to kernel virtual address
+ *
+ * Each PRU has access to all data memories within the PRUSS, accessible at
+ * different ranges. So, look through both its primary and secondary Data
+ * RAMs as well as any shared Data RAM to convert a PRU device address to
+ * kernel virtual address. Data RAM0 is primary Data RAM for PRU0 and Data
+ * RAM1 is primary Data RAM for PRU1.
+ */
+static void *pru_d_da_to_va(struct pru_rproc *pru, u32 da, int len)
+{
+       struct pruss_mem_region dram0, dram1, shrd_ram;
+       struct pruss *pruss = pru->pruss;
+       u32 offset;
+       void *va = NULL;
+
+       if (len <= 0)
+               return NULL;
+
+       dram0 = pruss->mem_regions[PRUSS_MEM_DRAM0];
+       dram1 = pruss->mem_regions[PRUSS_MEM_DRAM1];
+       /* PRU1 has its local RAM addresses reversed */
+       if (pru->id == 1)
+               swap(dram0, dram1);
+       shrd_ram = pruss->mem_regions[PRUSS_MEM_SHRD_RAM2];
+
+       if (da >= pru->pdram_da && da + len <= pru->pdram_da + dram0.size) {
+               offset = da - pru->pdram_da;
+               va = (__force void *)(dram0.va + offset);
+       } else if (da >= pru->sdram_da &&
+                  da + len <= pru->sdram_da + dram1.size) {
+               offset = da - pru->sdram_da;
+               va = (__force void *)(dram1.va + offset);
+       } else if (da >= pru->shrdram_da &&
+                  da + len <= pru->shrdram_da + shrd_ram.size) {
+               offset = da - pru->shrdram_da;
+               va = (__force void *)(shrd_ram.va + offset);
+       }
+
+       return va;
+}
+
+/*
+ * Convert PRU device address (instruction space) to kernel virtual address
+ *
+ * A PRU does not have an unified address space. Each PRU has its very own
+ * private Instruction RAM, and its device address is identical to that of
+ * its primary Data RAM device address.
+ */
+static void *pru_i_da_to_va(struct pru_rproc *pru, u32 da, int len)
+{
+       u32 offset;
+       void *va = NULL;
+
+       if (len <= 0)
+               return NULL;
+
+       if (da >= pru->iram_da &&
+           da + len <= pru->iram_da + pru->mem_regions[PRU_IOMEM_IRAM].size) {
+               offset = da - pru->iram_da;
+               va = (__force void *)(pru->mem_regions[PRU_IOMEM_IRAM].va +
+                                     offset);
+       }
+
+       return va;
+}
+
+/* PRU-specific address translator */
+static void *pru_da_to_va(struct rproc *rproc, u64 da, int len, u32 flags)
+{
+       struct pru_rproc *pru = rproc->priv;
+       void *va;
+       u32 exec_flag;
+
+       exec_flag = ((flags & RPROC_FLAGS_ELF_SHDR) ? flags & SHF_EXECINSTR :
+                    ((flags & RPROC_FLAGS_ELF_PHDR) ? flags & PF_X : 0));
+
+       if (exec_flag)
+               va = pru_i_da_to_va(pru, da, len);
+       else
+               va = pru_d_da_to_va(pru, da, len);
+
+       return va;
+}
+
+static struct rproc_ops pru_rproc_ops = {
+       .start                  = pru_rproc_start,
+       .stop                   = pru_rproc_stop,
+       .handle_vendor_rsc      = pru_rproc_handle_vendor_rsc,
+       .da_to_va               = pru_da_to_va,
+};
+
+/*
+ * compute PRU id based on the IRAM addresses. The PRU IRAMs are
+ * always at a particular offset within the PRUSS address space.
+ * The other alternative is to use static data for each core (not a
+ * hardware property to define it in DT), and the id can always be
+ * computated using this inherent address logic.
+ */
+static int pru_rproc_set_id(struct pru_rproc *pru)
+{
+       int ret = 0;
+       u32 mask1 = PRU0_IRAM_ADDR_MASK;
+       u32 mask2 = PRU1_IRAM_ADDR_MASK;
+
+       if ((pru->mem_regions[PRU_IOMEM_IRAM].pa & mask1) == mask1)
+               pru->id = 0;
+       else if ((pru->mem_regions[PRU_IOMEM_IRAM].pa & mask2) == mask2)
+               pru->id = 1;
+       else
+               ret = -EINVAL;
+
+       return ret;
+}
+
+static int pru_rproc_probe(struct platform_device *pdev)
+{
+       struct device *dev = &pdev->dev;
+       struct device_node *np = dev->of_node;
+       struct platform_device *ppdev = to_platform_device(dev->parent);
+       struct pru_rproc *pru;
+       const char *fw_name;
+       struct rproc *rproc = NULL;
+       struct resource *res;
+       int i, ret;
+       const char *mem_names[PRU_IOMEM_MAX] = { "iram", "control", "debug" };
+
+       if (!np) {
+               dev_err(dev, "Non-DT platform device not supported\n");
+               return -ENODEV;
+       }
+
+       ret = of_property_read_string(np, "firmware-name", &fw_name);
+       if (ret) {
+               dev_err(dev, "unable to retrieve firmware-name %d\n", ret);
+               return ret;
+       }
+
+       rproc = rproc_alloc(dev, pdev->name, &pru_rproc_ops, fw_name,
+                           sizeof(*pru));
+       if (!rproc) {
+               dev_err(dev, "rproc_alloc failed\n");
+               return -ENOMEM;
+       }
+       /* error recovery is not supported for PRUs */
+       rproc->recovery_disabled = true;
+
+       /*
+        * rproc_add will auto-boot the processor normally, but this is
+        * not desired with PRU client driven boot-flow methodology. A PRU
+        * application/client driver will boot the corresponding PRU
+        * remote-processor as part of its state machine either through
+        * the remoteproc sysfs interface or through the equivalent kernel API
+        */
+       rproc->auto_boot = false;
+
+       pru = rproc->priv;
+       pru->pruss = platform_get_drvdata(ppdev);
+       pru->rproc = rproc;
+       pru->fw_name = fw_name;
+
+       /* XXX: get this from match data if different in the future */
+       pru->iram_da = 0;
+       pru->pdram_da = 0;
+       pru->sdram_da = 0x2000;
+       pru->shrdram_da = 0x10000;
+
+       for (i = 0; i < ARRAY_SIZE(mem_names); i++) {
+               res = platform_get_resource_byname(pdev, IORESOURCE_MEM,
+                                                  mem_names[i]);
+               pru->mem_regions[i].va = devm_ioremap_resource(dev, res);
+               if (IS_ERR(pru->mem_regions[i].va)) {
+                       dev_err(dev, "failed to parse and map memory resource %d %s\n",
+                               i, mem_names[i]);
+                       ret = PTR_ERR(pru->mem_regions[i].va);
+                       goto free_rproc;
+               }
+               pru->mem_regions[i].pa = res->start;
+               pru->mem_regions[i].size = resource_size(res);
+
+               dev_dbg(dev, "memory %8s: pa %pa size 0x%zx va %p\n",
+                       mem_names[i], &pru->mem_regions[i].pa,
+                       pru->mem_regions[i].size, pru->mem_regions[i].va);
+       }
+
+       ret = pru_rproc_set_id(pru);
+       if (ret < 0)
+               goto free_rproc;
+
+       platform_set_drvdata(pdev, rproc);
+
+       ret = rproc_add(pru->rproc);
+       if (ret) {
+               dev_err(dev, "rproc_add failed: %d\n", ret);
+               goto free_rproc;
+       }
+
+       dev_info(dev, "PRU rproc node %s probed successfully\n", np->full_name);
+
+       return 0;
+
+free_rproc:
+       rproc_free(rproc);
+       return ret;
+}
+
+static int pru_rproc_remove(struct platform_device *pdev)
+{
+       struct device *dev = &pdev->dev;
+       struct rproc *rproc = platform_get_drvdata(pdev);
+
+       dev_info(dev, "%s: removing rproc %s\n", __func__, rproc->name);
+
+       rproc_del(rproc);
+       rproc_free(rproc);
+
+       return 0;
+}
+
+static const struct of_device_id pru_rproc_match[] = {
+       { .compatible = "ti,am3356-pru", },
+       {},
+};
+MODULE_DEVICE_TABLE(of, pru_rproc_match);
+
+static struct platform_driver pru_rproc_driver = {
+       .driver = {
+               .name   = "pru-rproc",
+               .of_match_table = pru_rproc_match,
+               .suppress_bind_attrs = true,
+       },
+       .probe  = pru_rproc_probe,
+       .remove = pru_rproc_remove,
+};
+module_platform_driver(pru_rproc_driver);
+
+MODULE_AUTHOR("Suman Anna <s-anna@ti.com>");
+MODULE_DESCRIPTION("PRU-ICSS Remote Processor Driver");
+MODULE_LICENSE("GPL v2");
diff --git a/drivers/remoteproc/pru_rproc.h b/drivers/remoteproc/pru_rproc.h
new file mode 100644 (file)
index 0000000..9cfe399
--- /dev/null
@@ -0,0 +1,65 @@
+/* SPDX-License-Identifier: (GPL-2.0 OR BSD-3-Clause) */
+/*
+ * PRUSS Remote Processor specific types
+ *
+ * Copyright (C) 2014-2019 Texas Instruments Incorporated - http://www.ti.com/
+ *     Suman Anna <s-anna@ti.com>
+ */
+
+#ifndef _PRU_RPROC_H_
+#define _PRU_RPROC_H_
+
+/**
+ * enum pruss_rsc_types - PRU specific resource types
+ *
+ * @PRUSS_RSC_INTRS: Resource holding information on PRU INTC configuration
+ * @PRUSS_RSC_MAX: Indicates end of known/defined PRU resource types.
+ *                This should be the last definition.
+ *
+ * Introduce new vendor resource types before PRUSS_RSC_MAX.
+ */
+enum pruss_rsc_types {
+       PRUSS_RSC_INTRS = 1,
+       PRUSS_RSC_MAX   = 2,
+};
+
+/**
+ * struct pruss_event_chnl - PRU system events _to_ channel mapping
+ * @event: number of the system event
+ * @chnl: channel number assigned to a given @event
+ *
+ * PRU system events are mapped to channels, and these channels are mapped
+ * to host interrupts. Events can be mapped to channels in a one-to-one or
+ * many-to-one ratio (multiple events per channel), and channels can be
+ * mapped to host interrupts in a one-to-one or many-to-one ratio (multiple
+ * channels per interrupt).
+ *
+ */
+struct pruss_event_chnl {
+       s8 event;
+       s8 chnl;
+};
+
+/**
+ * struct fw_rsc_pruss_intrmap - custom/vendor resource to define PRU interrupts
+ * @reserved: reserved field providing padding and alignment
+ * @chnl_host_intr_map: array of PRU channels to host interrupt mappings
+ * @event_chnl_map_size: number of event_channel mappings defined in
+ *                      @event_chnl_map_addr
+ * @event_chnl_map_addr: PRU device address of pointer to array of events to
+ *                      channel mappings (struct pruss_event_chnl elements)
+ *
+ * PRU system events are mapped to channels, and these channels are mapped
+ * to host interrupts. Events can be mapped to channels in a one-to-one or
+ * many-to-one ratio (multiple events per channel), and channels can be
+ * mapped to host interrupts in a one-to-one or many-to-one ratio (multiple
+ * channels per interrupt).
+ */
+struct fw_rsc_pruss_intrmap {
+       u16 reserved;
+       s8 chnl_host_intr_map[10];
+       u32 event_chnl_map_size;
+       u32 event_chnl_map_addr;
+};
+
+#endif /* _PRU_RPROC_H_ */