]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - rpmsg/rpmsg.git/commit
scsi: zorro_esp: Limit DMA transfers to 65536 bytes (except on Fastlane)
authorKars de Jong <jongk@linux-m68k.org>
Tue, 12 Nov 2019 17:55:23 +0000 (18:55 +0100)
committerMartin K. Petersen <martin.petersen@oracle.com>
Wed, 13 Nov 2019 03:21:34 +0000 (22:21 -0500)
commit02f7e9f351a9de95577eafdc3bd413ed1c3b589f
tree0345c194348c803ddb8854958633f88afd6c019f
parent63f565aa6e06d07bcf0cb7cfac82889c12c465a3
scsi: zorro_esp: Limit DMA transfers to 65536 bytes (except on Fastlane)

When using this driver on a Blizzard 1260, there were failures whenever DMA
transfers from the SCSI bus to memory of 65535 bytes were followed by a DMA
transfer of 1 byte. This caused the byte at offset 65535 to be overwritten
with 0xff. The Blizzard hardware can't handle single byte DMA transfers.

Besides this issue, limiting the DMA length to something that is not a
multiple of the page size is very inefficient on most file systems.

It seems this limit was chosen because the DMA transfer counter of the ESP
by default is 16 bits wide, thus limiting the length to 65535 bytes.
However, the value 0 means 65536 bytes, which is handled by the ESP and the
Blizzard just fine. It is also the default maximum used by esp_scsi when
drivers don't provide their own dma_length_limit() function.

The limit of 65536 bytes can be used by all boards except the Fastlane. The
old driver used a limit of 65532 bytes (0xfffc), which is reintroduced in
this patch.

Fixes: b7ded0e8b0d1 ("scsi: zorro_esp: Limit DMA transfers to 65535 bytes")
Link: https://lore.kernel.org/r/20191112175523.23145-1-jongk@linux-m68k.org
Signed-off-by: Kars de Jong <jongk@linux-m68k.org>
Reviewed-by: Finn Thain <fthain@telegraphics.com.au>
Signed-off-by: Martin K. Petersen <martin.petersen@oracle.com>
drivers/scsi/zorro_esp.c