lib: Add support for M4F on AM64x SoCs
[rpmsg/ti-rpmsg-char.git] / README
1 TI RPMsg Char Package
2 ======================
4 1. Introduction
5 ----------------
6 This repo contains the source code for a small rpmsg-char utility library
7 and some basic examples and/or tests exercising the API provided by the
8 ti_rpmsg_char library. The library is primarily designed to provide Linux
9 applications an easy means to open and identify rpmsg character devices
10 created by the Linux kernel rpmsg-char driver using the virtio-rpmsg-bus
11 transport back-end.
13 The library currently supports the TI K3 AM65x, J721E and J7200 SoCs, but
14 can be easily scaled to support other SoCs.
17 2. Sources
18 -----------
19 The repo is maintained as a git tree, and so the sources can simply be
20 downloaded using git.
22   git clone git://git.ti.com/rpmsg/ti-rpmsg-char.git
24 The following is the directory structure for this package:
25  - src      : Library source code and internal header files
26  - include  : Public exported headers for applications usage
27  - examples : Example source code
30 3. API
31 -------
32 The library provides only 4 basic API. Please see the documentation in
33 include/ti_rpmsg_char.h for each of the API and function arguments.
35  - rpmsg_char_init()
36  - rpmsg_char_exit()
37  - rpmsg_char_open()
38  - rpmsg_char_close()
40 Applications need only include the ti_rpmsg_char.h. All the remoteproc
41 ids to be used are defined in rproc_id.h, which is already included in
42 ti_rpmsg_char.h.
45 4. Build
46 ---------
48 4.1 Infrastructure Tools
49 The package uses the autotools infrastructure for build. The following
50 versions are used:
51     GNU autoconf : 2.69
52     GNU automake : 1.15.1
53     GNU libtool  : 2.4.6
55 The following Arm cross-compilers are used to build the library and
56 examples:
57     v8 Compiler  : gcc-arm-9.2-2019.12-x86_64-aarch64-none-linux-gnu
58     v7 Compiler  : gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf
60 4.2 Build Steps
61  1. Install the necessary autotools and compilers
62  2. Add the installed compiler bin path to your PATH variable
63       eg: export PATH=<install_path>/gcc-arm-9.2-2019.12-aarch64/bin:$PATH
64  3. Configure the autotools with necessary host and optional prefix to be
65     used to install the build libraries and executables
66       cd <ti-rpmsg-char-dir>
67       autoreconf -i
68       ./configure --host=aarch64-none-linux-gnu --prefix=<target-dir>
69  4. Build and Install Library
70       make
71       make install
72  5. Build Examples, the top-level Makefile builds only the library by
73     default
74       make -C examples
75       make -C examples install
76               or
77       cd examples
78       make
79       make install
81 4.3 Clean Steps
82   1. Use the desired generic Makefile targets
83        make clean      : Erase the files built by make
84        make distclean  : clean + Erase the files created by the configure step
85        make uninstall  : Erase the installed libraries and executables
86   2. Cleaning up examples specifically needs separate commands. It is all
87      similar to the commands in #1, but invoked with -C examples, or invoke
88      normally from within the examples folder
89        eg: make -C examples uninstall
90                      or
91            cd examples; make uninstall
92   3. Use git clean to get the repo back to a pristine state
93        git clean -dfx