[DDR] Additional checking of DDR_PHY_CTRL_1[reg_read_latency]
[sitara-dss-files/am335x-dss-files.git] / am335x-ddr-analysis.dss
index cbf929a00b6e86f45ea4de0ab85ccdff5905a2dd..07da1d0fa096d9e8e4b94b2cfc6c08afbb451383 100644 (file)
@@ -395,6 +395,17 @@ if (original_CM_PER_L3_CLKSTCTRL & 1<<2) {
        if ( (reg_val & 0x300) == (1 << 8) ) {file.write("no termination (01b)\n");}
        if ( (reg_val & 0x300) == (2 << 8) ) {file.write("full thevenin termination\n");}
        if ( (reg_val & 0x300) == (3 << 8) ) {file.write("half thevenin termination\n");}
        if ( (reg_val & 0x300) == (1 << 8) ) {file.write("no termination (01b)\n");}
        if ( (reg_val & 0x300) == (2 << 8) ) {file.write("full thevenin termination\n");}
        if ( (reg_val & 0x300) == (3 << 8) ) {file.write("half thevenin termination\n");}
+       reg_read_latency = bits32(reg_val, 4, 0);
+       if( reg_read_latency < decoded_CL+1 )
+               file.write("  * Bits 4:0 (reg_read_latency) set to " + d2d(reg_read_latency) + " -> ERROR: TOO SMALL" + newline);
+       else if (reg_read_latency == decoded_CL+1) {
+               file.write("  * Bits 4:0 (reg_read_latency) set to " + d2d(reg_read_latency) + newline);
+               file.write("    -> If PHY_INVERT_CLKOUT=0, this is an appropriate value." + newline);
+               file.write("    -> If PHY_INVERT_CLKOUT=1, this is too small." + newline);
+               file.write("    -> PHY_INVERT_CLKOUT is a write-only register, so this needs to be" + newline);
+               file.write("    -> inspected closely in the code and RatioSeed spreadsheet." + newline);
+       } else
+               file.write("  * Bits 4:0 (reg_read_latency) set to " + d2d(reg_read_latency) + " -> Ok: CL+2 is typical with PHY_INVERT_CLKOUT=1." + newline);
 
        file.write("\n");
        file.write("*********************\n");
 
        file.write("\n");
        file.write("*********************\n");