fix typo in padconf README
authorBrad Griffis <bgriffis@ti.com>
Wed, 3 Jun 2020 14:26:41 +0000 (09:26 -0500)
committerBrad Griffis <bgriffis@ti.com>
Wed, 3 Jun 2020 14:26:41 +0000 (09:26 -0500)
padconf/README

index de37b79b8219429ca6c6ad2a586c02e04ab62b82..e7808b7ad07404c1b4be4744c43a8a5362610072 100755 (executable)
@@ -54,7 +54,7 @@ The resulting output will align with what was described for the bash script.
 
 ==== am57xx-padconf-decoder.py ====
 
-This is a perl script that takes the *.rd1 file as an input, and produces
+This is a python script that takes the *.rd1 file as an input, and produces
 a *.csv file as an output.  It utilizes the xml files to decode the
 pinmuxing of the various registers.  It can be run on your host PC or even
 on the target if Python is part of the OS image (which is the case if you