remove redundant registers
add register for ABB setup and ctrl
add ABBLDO setup and ctrl registers
exit if csv creation fails
Print ID_CODE and print certain registers only if AM574x detected
decode LDOVBB_xxx_VOLTAGE_CTRL
print device ID info
relocate writing of csv header
Write decoded ABB-AVS values to csv
add helper functions for reading data and decoding registers
add helper function for bit extraction
Python script to parse AVS-ABB rd1
create shell script for collecting AVS/ABB info
add .gitignore file
fix typo in padconf README
[padconf] remove spaces after comma in csv output
[padconf] add python3 compatibility
[DDR] print ECC error registers
[DDR] additional registers and decoding for ECC
[AVS] remove unused lines
Use unix line endings for target bash scripts
Decoder of registers pertaining to AVS and ABB
Capture CM_L4PER3_CLKSTCTRL as part of CTT Dump
[boot] Check PC for dead loops
Hardware requirements
[DDR] formatting
[DDR] Add PHY_STATUS registers
[DDR] Add parsing of DPLL_DDR
Fix issue printing registers with MSB=1
DDR: Decode LISA entries
Add EXT_PHY_CONTROL_xx regs plus CTRL_SDRAM_CONFIG_EXT
Handle undefined mux modes
Add README for padconf/ directory
Python script for decoding padconf rd1 to csv
Add xml files needed by Python script
Add bash script for extracting rd1 file with Linux console
Create padconf/ directory for all related files
Rename am57xx-pinmux.dss to be more consistent
New file for dumping pinmux related registers
[AM57xx DDR] add decoding of DDR_PHY_CONTROL_1
Create am57xx-ddr.dss for checking DDR configuration
Add boot decoder for AM57xx devices
Add README file
Create AM57xx clock tree tool script
Used Sitara CTT 1.0.0.5 for outputting a valid rd1 file to
determine which addresses need to be read for which devices.
Initial testing was performed on AM572x IDK. Code is structured
to work across all AM57xx variants but will test other flavors
in the future.
Used Sitara CTT 1.0.0.5 for outputting a valid rd1 file to
determine which addresses need to be read for which devices.
Initial testing was performed on AM572x IDK. Code is structured
to work across all AM57xx variants but will test other flavors
in the future.
File name update
Specify Windows carriage returns
Initial commit