]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - .gitignore
can: d_can: Add support for Bosch D_CAN controller
[sitara-epos/sitara-epos-kernel.git] / .gitignore
1 #
2 # NOTE! Don't add files that are generated in specific
3 # subdirectories here. Add them in the ".gitignore" file
4 # in that subdirectory instead.
5 #
6 # NOTE! Please use 'git ls-files -i --exclude-standard'
7 # command after changing this file, to see if there are
8 # any tracked files which get ignored after the change.
9 #
10 # Normal rules
11 #
12 .*
13 *.o
14 *.o.*
15 *.a
16 *.s
17 *.ko
18 *.so
19 *.so.dbg
20 *.mod.c
21 *.i
22 *.lst
23 *.symtypes
24 *.order
25 modules.builtin
26 *.elf
27 *.bin
28 *.gz
29 *.bz2
30 *.lzma
31 *.xz
32 *.lzo
33 *.patch
34 *.gcno
36 #
37 # Top-level generic files
38 #
39 /tags
40 /TAGS
41 /linux
42 /vmlinux
43 /vmlinuz
44 /System.map
45 /Module.markers
46 /Module.symvers
48 #
49 # Debian directory (make deb-pkg)
50 #
51 /debian/
53 #
54 # git files that we don't want to ignore even it they are dot-files
55 #
56 !.gitignore
57 !.mailmap
59 #
60 # Generated include files
61 #
62 include/config
63 include/linux/version.h
64 include/generated
65 arch/*/include/generated
67 # stgit generated dirs
68 patches-*
70 # quilt's files
71 patches
72 series
74 # cscope files
75 cscope.*
76 ncscope.*
78 # gnu global files
79 GPATH
80 GRTAGS
81 GSYMS
82 GTAGS
84 *.orig
85 *~
86 \#*#