]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - Documentation/dmaengine.txt
video: da8xx-fb: correct suspend/resume sequence
[sitara-epos/sitara-epos-kernel.git] / Documentation / dmaengine.txt
1                         DMA Engine API Guide
2                         ====================
4                  Vinod Koul <vinod dot koul at intel.com>
6 NOTE: For DMA Engine usage in async_tx please see:
7         Documentation/crypto/async-tx-api.txt
10 Below is a guide to device driver writers on how to use the Slave-DMA API of the
11 DMA Engine. This is applicable only for slave DMA usage only.
13 The slave DMA usage consists of following steps:
14 1. Allocate a DMA slave channel
15 2. Set slave and controller specific parameters
16 3. Get a descriptor for transaction
17 4. Submit the transaction
18 5. Issue pending requests and wait for callback notification
20 1. Allocate a DMA slave channel
22    Channel allocation is slightly different in the slave DMA context,
23    client drivers typically need a channel from a particular DMA
24    controller only and even in some cases a specific channel is desired.
25    To request a channel dma_request_channel() API is used.
27    Interface:
28         struct dma_chan *dma_request_channel(dma_cap_mask_t mask,
29                         dma_filter_fn filter_fn,
30                         void *filter_param);
31    where dma_filter_fn is defined as:
32         typedef bool (*dma_filter_fn)(struct dma_chan *chan, void *filter_param);
34    The 'filter_fn' parameter is optional, but highly recommended for
35    slave and cyclic channels as they typically need to obtain a specific
36    DMA channel.
38    When the optional 'filter_fn' parameter is NULL, dma_request_channel()
39    simply returns the first channel that satisfies the capability mask.
41    Otherwise, the 'filter_fn' routine will be called once for each free
42    channel which has a capability in 'mask'.  'filter_fn' is expected to
43    return 'true' when the desired DMA channel is found.
45    A channel allocated via this interface is exclusive to the caller,
46    until dma_release_channel() is called.
48 2. Set slave and controller specific parameters
50    Next step is always to pass some specific information to the DMA
51    driver.  Most of the generic information which a slave DMA can use
52    is in struct dma_slave_config.  This allows the clients to specify
53    DMA direction, DMA addresses, bus widths, DMA burst lengths etc
54    for the peripheral.
56    If some DMA controllers have more parameters to be sent then they
57    should try to embed struct dma_slave_config in their controller
58    specific structure. That gives flexibility to client to pass more
59    parameters, if required.
61    Interface:
62         int dmaengine_slave_config(struct dma_chan *chan,
63                                   struct dma_slave_config *config)
65    Please see the dma_slave_config structure definition in dmaengine.h
66    for a detailed explaination of the struct members.  Please note
67    that the 'direction' member will be going away as it duplicates the
68    direction given in the prepare call.
70 3. Get a descriptor for transaction
72    For slave usage the various modes of slave transfers supported by the
73    DMA-engine are:
75    slave_sg     - DMA a list of scatter gather buffers from/to a peripheral
76    dma_cyclic   - Perform a cyclic DMA operation from/to a peripheral till the
77                   operation is explicitly stopped.
79    A non-NULL return of this transfer API represents a "descriptor" for
80    the given transaction.
82    Interface:
83         struct dma_async_tx_descriptor *(*chan->device->device_prep_slave_sg)(
84                 struct dma_chan *chan, struct scatterlist *sgl,
85                 unsigned int sg_len, enum dma_data_direction direction,
86                 unsigned long flags);
88         struct dma_async_tx_descriptor *(*chan->device->device_prep_dma_cyclic)(
89                 struct dma_chan *chan, dma_addr_t buf_addr, size_t buf_len,
90                 size_t period_len, enum dma_data_direction direction);
92    The peripheral driver is expected to have mapped the scatterlist for
93    the DMA operation prior to calling device_prep_slave_sg, and must
94    keep the scatterlist mapped until the DMA operation has completed.
95    The scatterlist must be mapped using the DMA struct device.  So,
96    normal setup should look like this:
98         nr_sg = dma_map_sg(chan->device->dev, sgl, sg_len);
99         if (nr_sg == 0)
100                 /* error */
102         desc = chan->device->device_prep_slave_sg(chan, sgl, nr_sg,
103                         direction, flags);
105    Once a descriptor has been obtained, the callback information can be
106    added and the descriptor must then be submitted.  Some DMA engine
107    drivers may hold a spinlock between a successful preparation and
108    submission so it is important that these two operations are closely
109    paired.
111    Note:
112         Although the async_tx API specifies that completion callback
113         routines cannot submit any new operations, this is not the
114         case for slave/cyclic DMA.
116         For slave DMA, the subsequent transaction may not be available
117         for submission prior to callback function being invoked, so
118         slave DMA callbacks are permitted to prepare and submit a new
119         transaction.
121         For cyclic DMA, a callback function may wish to terminate the
122         DMA via dmaengine_terminate_all().
124         Therefore, it is important that DMA engine drivers drop any
125         locks before calling the callback function which may cause a
126         deadlock.
128         Note that callbacks will always be invoked from the DMA
129         engines tasklet, never from interrupt context.
131 4. Submit the transaction
133    Once the descriptor has been prepared and the callback information
134    added, it must be placed on the DMA engine drivers pending queue.
136    Interface:
137         dma_cookie_t dmaengine_submit(struct dma_async_tx_descriptor *desc)
139    This returns a cookie can be used to check the progress of DMA engine
140    activity via other DMA engine calls not covered in this document.
142    dmaengine_submit() will not start the DMA operation, it merely adds
143    it to the pending queue.  For this, see step 5, dma_async_issue_pending.
145 5. Issue pending DMA requests and wait for callback notification
147    The transactions in the pending queue can be activated by calling the
148    issue_pending API. If channel is idle then the first transaction in
149    queue is started and subsequent ones queued up.
151    On completion of each DMA operation, the next in queue is started and
152    a tasklet triggered. The tasklet will then call the client driver
153    completion callback routine for notification, if set.
155    Interface:
156         void dma_async_issue_pending(struct dma_chan *chan);
158 Further APIs:
160 1. int dmaengine_terminate_all(struct dma_chan *chan)
162    This causes all activity for the DMA channel to be stopped, and may
163    discard data in the DMA FIFO which hasn't been fully transferred.
164    No callback functions will be called for any incomplete transfers.
166 2. int dmaengine_pause(struct dma_chan *chan)
168    This pauses activity on the DMA channel without data loss.
170 3. int dmaengine_resume(struct dma_chan *chan)
172    Resume a previously paused DMA channel.  It is invalid to resume a
173    channel which is not currently paused.
175 4. enum dma_status dma_async_is_tx_complete(struct dma_chan *chan,
176         dma_cookie_t cookie, dma_cookie_t *last, dma_cookie_t *used)
178    This can be used to check the status of the channel.  Please see
179    the documentation in include/linux/dmaengine.h for a more complete
180    description of this API.
182    This can be used in conjunction with dma_async_is_complete() and
183    the cookie returned from 'descriptor->submit()' to check for
184    completion of a specific DMA transaction.
186    Note:
187         Not all DMA engine drivers can return reliable information for
188         a running DMA channel.  It is recommended that DMA engine users
189         pause or stop (via dmaengine_terminate_all) the channel before
190         using this API.