1 Notes on the change from 16-bit UIDs to 32-bit UIDs:
3 - kernel code MUST take into account __kernel_uid_t and __kernel_uid32_t
4 when communicating between user and kernel space in an ioctl or data
5 structure.
7 - kernel code should use uid_t and gid_t in kernel-private structures and
8 code.
10 What's left to be done for 32-bit UIDs on all Linux architectures:
12 - Disk quotas have an interesting limitation that is not related to the
13 maximum UID/GID. They are limited by the maximum file size on the
14 underlying filesystem, because quota records are written at offsets
15 corresponding to the UID in question.
16 Further investigation is needed to see if the quota system can cope
17 properly with huge UIDs. If it can deal with 64-bit file offsets on all
18 architectures, this should not be a problem.
20 - Decide whether or not to keep backwards compatibility with the system
21 accounting file, or if we should break it as the comments suggest
22 (currently, the old 16-bit UID and GID are still written to disk, and
23 part of the former pad space is used to store separate 32-bit UID and
24 GID)
26 - Need to validate that OS emulation calls the 16-bit UID
27 compatibility syscalls, if the OS being emulated used 16-bit UIDs, or
28 uses the 32-bit UID system calls properly otherwise.
30 This affects at least:
31 iBCS on Intel
33 sparc32 emulation on sparc64
34 (need to support whatever new 32-bit UID system calls are added to
35 sparc32)
37 - Validate that all filesystems behave properly.
39 At present, 32-bit UIDs _should_ work for:
40 ext2
41 ufs
42 isofs
43 nfs
44 coda
45 udf
47 Ioctl() fixups have been made for:
48 ncpfs
49 smbfs
51 Filesystems with simple fixups to prevent 16-bit UID wraparound:
52 minix
53 sysv
54 qnx4
56 Other filesystems have not been checked yet.
58 - The ncpfs and smpfs filesystems cannot presently use 32-bit UIDs in
59 all ioctl()s. Some new ioctl()s have been added with 32-bit UIDs, but
60 more are needed. (as well as new user<->kernel data structures)
62 - The ELF core dump format only supports 16-bit UIDs on arm, i386, m68k,
63 sh, and sparc32. Fixing this is probably not that important, but would
64 require adding a new ELF section.
66 - The ioctl()s used to control the in-kernel NFS server only support
67 16-bit UIDs on arm, i386, m68k, sh, and sparc32.
69 - make sure that the UID mapping feature of AX25 networking works properly
70 (it should be safe because it's always used a 32-bit integer to
71 communicate between user and kernel)
74 Chris Wing
75 wingc@umich.edu
77 last updated: January 11, 2000