1 kernel-doc nano-HOWTO
2 =====================
4 How to format kernel-doc comments
5 ---------------------------------
7 In order to provide embedded, 'C' friendly, easy to maintain,
8 but consistent and extractable documentation of the functions and
9 data structures in the Linux kernel, the Linux kernel has adopted
10 a consistent style for documenting functions and their parameters,
11 and structures and their members.
13 The format for this documentation is called the kernel-doc format.
14 It is documented in this Documentation/kernel-doc-nano-HOWTO.txt file.
16 This style embeds the documentation within the source files, using
17 a few simple conventions. The scripts/kernel-doc perl script, some
18 SGML templates in Documentation/DocBook, and other tools understand
19 these conventions, and are used to extract this embedded documentation
20 into various documents.
22 In order to provide good documentation of kernel functions and data
23 structures, please use the following conventions to format your
24 kernel-doc comments in Linux kernel source.
26 We definitely need kernel-doc formatted documentation for functions
27 that are exported to loadable modules using EXPORT_SYMBOL.
29 We also look to provide kernel-doc formatted documentation for
30 functions externally visible to other kernel files (not marked
31 "static").
33 We also recommend providing kernel-doc formatted documentation
34 for private (file "static") routines, for consistency of kernel
35 source code layout. But this is lower priority and at the
36 discretion of the MAINTAINER of that kernel source file.
38 Data structures visible in kernel include files should also be
39 documented using kernel-doc formatted comments.
41 The opening comment mark "/**" is reserved for kernel-doc comments.
42 Only comments so marked will be considered by the kernel-doc scripts,
43 and any comment so marked must be in kernel-doc format. Do not use
44 "/**" to be begin a comment block unless the comment block contains
45 kernel-doc formatted comments. The closing comment marker for
46 kernel-doc comments can be either "*/" or "**/", but "*/" is
47 preferred in the Linux kernel tree.
49 Kernel-doc comments should be placed just before the function
50 or data structure being described.
52 Example kernel-doc function comment:
54 /**
55 * foobar() - short function description of foobar
56 * @arg1: Describe the first argument to foobar.
57 * @arg2: Describe the second argument to foobar.
58 * One can provide multiple line descriptions
59 * for arguments.
60 *
61 * A longer description, with more discussion of the function foobar()
62 * that might be useful to those using or modifying it. Begins with
63 * empty comment line, and may include additional embedded empty
64 * comment lines.
65 *
66 * The longer description can have multiple paragraphs.
67 */
69 The short description following the subject can span multiple lines
70 and ends with an @argument description, an empty line or the end of
71 the comment block.
73 The @argument descriptions must begin on the very next line following
74 this opening short function description line, with no intervening
75 empty comment lines.
77 If a function parameter is "..." (varargs), it should be listed in
78 kernel-doc notation as:
79 * @...: description
82 Example kernel-doc data structure comment.
84 /**
85 * struct blah - the basic blah structure
86 * @mem1: describe the first member of struct blah
87 * @mem2: describe the second member of struct blah,
88 * perhaps with more lines and words.
89 *
90 * Longer description of this structure.
91 */
93 The kernel-doc function comments describe each parameter to the
94 function, in order, with the @name lines.
96 The kernel-doc data structure comments describe each structure member
97 in the data structure, with the @name lines.
99 The longer description formatting is "reflowed", losing your line
100 breaks. So presenting carefully formatted lists within these
101 descriptions won't work so well; derived documentation will lose
102 the formatting.
104 See the section below "How to add extractable documentation to your
105 source files" for more details and notes on how to format kernel-doc
106 comments.
108 Components of the kernel-doc system
109 -----------------------------------
111 Many places in the source tree have extractable documentation in the
112 form of block comments above functions. The components of this system
113 are:
115 - scripts/kernel-doc
117 This is a perl script that hunts for the block comments and can mark
118 them up directly into DocBook, man, text, and HTML. (No, not
119 texinfo.)
121 - Documentation/DocBook/*.tmpl
123 These are SGML template files, which are normal SGML files with
124 special place-holders for where the extracted documentation should
125 go.
127 - scripts/basic/docproc.c
129 This is a program for converting SGML template files into SGML
130 files. When a file is referenced it is searched for symbols
131 exported (EXPORT_SYMBOL), to be able to distinguish between internal
132 and external functions.
133 It invokes kernel-doc, giving it the list of functions that
134 are to be documented.
135 Additionally it is used to scan the SGML template files to locate
136 all the files referenced herein. This is used to generate dependency
137 information as used by make.
139 - Makefile
141 The targets 'sgmldocs', 'psdocs', 'pdfdocs', and 'htmldocs' are used
142 to build DocBook files, PostScript files, PDF files, and html files
143 in Documentation/DocBook.
145 - Documentation/DocBook/Makefile
147 This is where C files are associated with SGML templates.
150 How to extract the documentation
151 --------------------------------
153 If you just want to read the ready-made books on the various
154 subsystems (see Documentation/DocBook/*.tmpl), just type 'make
155 psdocs', or 'make pdfdocs', or 'make htmldocs', depending on your
156 preference. If you would rather read a different format, you can type
157 'make sgmldocs' and then use DocBook tools to convert
158 Documentation/DocBook/*.sgml to a format of your choice (for example,
159 'db2html ...' if 'make htmldocs' was not defined).
161 If you want to see man pages instead, you can do this:
163 $ cd linux
164 $ scripts/kernel-doc -man $(find -name '*.c') | split-man.pl /tmp/man
165 $ scripts/kernel-doc -man $(find -name '*.h') | split-man.pl /tmp/man
167 Here is split-man.pl:
169 -->
170 #!/usr/bin/perl
172 if ($#ARGV < 0) {
173 die "where do I put the results?\n";
174 }
176 mkdir $ARGV[0],0777;
177 $state = 0;
178 while (<STDIN>) {
179 if (/^\.TH \"[^\"]*\" 9 \"([^\"]*)\"/) {
180 if ($state == 1) { close OUT }
181 $state = 1;
182 $fn = "$ARGV[0]/$1.9";
183 print STDERR "Creating $fn\n";
184 open OUT, ">$fn" or die "can't open $fn: $!\n";
185 print OUT $_;
186 } elsif ($state != 0) {
187 print OUT $_;
188 }
189 }
191 close OUT;
192 <--
194 If you just want to view the documentation for one function in one
195 file, you can do this:
197 $ scripts/kernel-doc -man -function fn file | nroff -man | less
199 or this:
201 $ scripts/kernel-doc -text -function fn file
204 How to add extractable documentation to your source files
205 ---------------------------------------------------------
207 The format of the block comment is like this:
209 /**
210 * function_name(:)? (- short description)?
211 (* @parameterx(space)*: (description of parameter x)?)*
212 (* a blank line)?
213 * (Description:)? (Description of function)?
214 * (section header: (section description)? )*
215 (*)?*/
217 All "description" text can span multiple lines, although the
218 function_name & its short description are traditionally on a single line.
219 Description text may also contain blank lines (i.e., lines that contain
220 only a "*").
222 "section header:" names must be unique per function (or struct,
223 union, typedef, enum).
225 Avoid putting a spurious blank line after the function name, or else the
226 description will be repeated!
228 All descriptive text is further processed, scanning for the following special
229 patterns, which are highlighted appropriately.
231 'funcname()' - function
232 '$ENVVAR' - environment variable
233 '&struct_name' - name of a structure (up to two words including 'struct')
234 '@parameter' - name of a parameter
235 '%CONST' - name of a constant.
237 NOTE 1: The multi-line descriptive text you provide does *not* recognize
238 line breaks, so if you try to format some text nicely, as in:
240 Return codes
241 0 - cool
242 1 - invalid arg
243 2 - out of memory
245 this will all run together and produce:
247 Return codes 0 - cool 1 - invalid arg 2 - out of memory
249 NOTE 2: If the descriptive text you provide has lines that begin with
250 some phrase followed by a colon, each of those phrases will be taken as
251 a new section heading, which means you should similarly try to avoid text
252 like:
254 Return codes:
255 0: cool
256 1: invalid arg
257 2: out of memory
259 every line of which would start a new section. Again, probably not
260 what you were after.
262 Take a look around the source tree for examples.
265 kernel-doc for structs, unions, enums, and typedefs
266 ---------------------------------------------------
268 Beside functions you can also write documentation for structs, unions,
269 enums and typedefs. Instead of the function name you must write the name
270 of the declaration; the struct/union/enum/typedef must always precede
271 the name. Nesting of declarations is not supported.
272 Use the argument mechanism to document members or constants.
274 Inside a struct description, you can use the "private:" and "public:"
275 comment tags. Structure fields that are inside a "private:" area
276 are not listed in the generated output documentation. The "private:"
277 and "public:" tags must begin immediately following a "/*" comment
278 marker. They may optionally include comments between the ":" and the
279 ending "*/" marker.
281 Example:
283 /**
284 * struct my_struct - short description
285 * @a: first member
286 * @b: second member
287 *
288 * Longer description
289 */
290 struct my_struct {
291 int a;
292 int b;
293 /* private: internal use only */
294 int c;
295 };
298 Including documentation blocks in source files
299 ----------------------------------------------
301 To facilitate having source code and comments close together, you can
302 include kernel-doc documentation blocks that are free-form comments
303 instead of being kernel-doc for functions, structures, unions,
304 enums, or typedefs. This could be used for something like a
305 theory of operation for a driver or library code, for example.
307 This is done by using a DOC: section keyword with a section title. E.g.:
309 /**
310 * DOC: Theory of Operation
311 *
312 * The whizbang foobar is a dilly of a gizmo. It can do whatever you
313 * want it to do, at any time. It reads your mind. Here's how it works.
314 *
315 * foo bar splat
316 *
317 * The only drawback to this gizmo is that is can sometimes damage
318 * hardware, software, or its subject(s).
319 */
321 DOC: sections are used in SGML templates files as indicated below.
324 How to make new SGML template files
325 -----------------------------------
327 SGML template files (*.tmpl) are like normal SGML files, except that
328 they can contain escape sequences where extracted documentation should
329 be inserted.
331 !E<filename> is replaced by the documentation, in <filename>, for
332 functions that are exported using EXPORT_SYMBOL: the function list is
333 collected from files listed in Documentation/DocBook/Makefile.
335 !I<filename> is replaced by the documentation for functions that are
336 _not_ exported using EXPORT_SYMBOL.
338 !D<filename> is used to name additional files to search for functions
339 exported using EXPORT_SYMBOL.
341 !F<filename> <function [functions...]> is replaced by the
342 documentation, in <filename>, for the functions listed.
344 !P<filename> <section title> is replaced by the contents of the DOC:
345 section titled <section title> from <filename>.
346 Spaces are allowed in <section title>; do not quote the <section title>.
348 !C<filename> is replaced by nothing, but makes the tools check that
349 all DOC: sections and documented functions, symbols, etc. are used.
350 This makes sense to use when you use !F/!P only and want to verify
351 that all documentation is included.
353 Tim.
354 */ <twaugh@redhat.com>