1 GETTING STARTED WITH KMEMCHECK
2 ==============================
4 Vegard Nossum <vegardno@ifi.uio.no>
7 Contents
8 ========
9 0. Introduction
10 1. Downloading
11 2. Configuring and compiling
12 3. How to use
13 3.1. Booting
14 3.2. Run-time enable/disable
15 3.3. Debugging
16 3.4. Annotating false positives
17 4. Reporting errors
18 5. Technical description
21 0. Introduction
22 ===============
24 kmemcheck is a debugging feature for the Linux Kernel. More specifically, it
25 is a dynamic checker that detects and warns about some uses of uninitialized
26 memory.
28 Userspace programmers might be familiar with Valgrind's memcheck. The main
29 difference between memcheck and kmemcheck is that memcheck works for userspace
30 programs only, and kmemcheck works for the kernel only. The implementations
31 are of course vastly different. Because of this, kmemcheck is not as accurate
32 as memcheck, but it turns out to be good enough in practice to discover real
33 programmer errors that the compiler is not able to find through static
34 analysis.
36 Enabling kmemcheck on a kernel will probably slow it down to the extent that
37 the machine will not be usable for normal workloads such as e.g. an
38 interactive desktop. kmemcheck will also cause the kernel to use about twice
39 as much memory as normal. For this reason, kmemcheck is strictly a debugging
40 feature.
43 1. Downloading
44 ==============
46 As of version 2.6.31-rc1, kmemcheck is included in the mainline kernel.
49 2. Configuring and compiling
50 ============================
52 kmemcheck only works for the x86 (both 32- and 64-bit) platform. A number of
53 configuration variables must have specific settings in order for the kmemcheck
54 menu to even appear in "menuconfig". These are:
56 o CONFIG_CC_OPTIMIZE_FOR_SIZE=n
58 This option is located under "General setup" / "Optimize for size".
60 Without this, gcc will use certain optimizations that usually lead to
61 false positive warnings from kmemcheck. An example of this is a 16-bit
62 field in a struct, where gcc may load 32 bits, then discard the upper
63 16 bits. kmemcheck sees only the 32-bit load, and may trigger a
64 warning for the upper 16 bits (if they're uninitialized).
66 o CONFIG_SLAB=y or CONFIG_SLUB=y
68 This option is located under "General setup" / "Choose SLAB
69 allocator".
71 o CONFIG_FUNCTION_TRACER=n
73 This option is located under "Kernel hacking" / "Tracers" / "Kernel
74 Function Tracer"
76 When function tracing is compiled in, gcc emits a call to another
77 function at the beginning of every function. This means that when the
78 page fault handler is called, the ftrace framework will be called
79 before kmemcheck has had a chance to handle the fault. If ftrace then
80 modifies memory that was tracked by kmemcheck, the result is an
81 endless recursive page fault.
83 o CONFIG_DEBUG_PAGEALLOC=n
85 This option is located under "Kernel hacking" / "Debug page memory
86 allocations".
88 In addition, I highly recommend turning on CONFIG_DEBUG_INFO=y. This is also
89 located under "Kernel hacking". With this, you will be able to get line number
90 information from the kmemcheck warnings, which is extremely valuable in
91 debugging a problem. This option is not mandatory, however, because it slows
92 down the compilation process and produces a much bigger kernel image.
94 Now the kmemcheck menu should be visible (under "Kernel hacking" / "kmemcheck:
95 trap use of uninitialized memory"). Here follows a description of the
96 kmemcheck configuration variables:
98 o CONFIG_KMEMCHECK
100 This must be enabled in order to use kmemcheck at all...
102 o CONFIG_KMEMCHECK_[DISABLED | ENABLED | ONESHOT]_BY_DEFAULT
104 This option controls the status of kmemcheck at boot-time. "Enabled"
105 will enable kmemcheck right from the start, "disabled" will boot the
106 kernel as normal (but with the kmemcheck code compiled in, so it can
107 be enabled at run-time after the kernel has booted), and "one-shot" is
108 a special mode which will turn kmemcheck off automatically after
109 detecting the first use of uninitialized memory.
111 If you are using kmemcheck to actively debug a problem, then you
112 probably want to choose "enabled" here.
114 The one-shot mode is mostly useful in automated test setups because it
115 can prevent floods of warnings and increase the chances of the machine
116 surviving in case something is really wrong. In other cases, the one-
117 shot mode could actually be counter-productive because it would turn
118 itself off at the very first error -- in the case of a false positive
119 too -- and this would come in the way of debugging the specific
120 problem you were interested in.
122 If you would like to use your kernel as normal, but with a chance to
123 enable kmemcheck in case of some problem, it might be a good idea to
124 choose "disabled" here. When kmemcheck is disabled, most of the run-
125 time overhead is not incurred, and the kernel will be almost as fast
126 as normal.
128 o CONFIG_KMEMCHECK_QUEUE_SIZE
130 Select the maximum number of error reports to store in an internal
131 (fixed-size) buffer. Since errors can occur virtually anywhere and in
132 any context, we need a temporary storage area which is guaranteed not
133 to generate any other page faults when accessed. The queue will be
134 emptied as soon as a tasklet may be scheduled. If the queue is full,
135 new error reports will be lost.
137 The default value of 64 is probably fine. If some code produces more
138 than 64 errors within an irqs-off section, then the code is likely to
139 produce many, many more, too, and these additional reports seldom give
140 any more information (the first report is usually the most valuable
141 anyway).
143 This number might have to be adjusted if you are not using serial
144 console or similar to capture the kernel log. If you are using the
145 "dmesg" command to save the log, then getting a lot of kmemcheck
146 warnings might overflow the kernel log itself, and the earlier reports
147 will get lost in that way instead. Try setting this to 10 or so on
148 such a setup.
150 o CONFIG_KMEMCHECK_SHADOW_COPY_SHIFT
152 Select the number of shadow bytes to save along with each entry of the
153 error-report queue. These bytes indicate what parts of an allocation
154 are initialized, uninitialized, etc. and will be displayed when an
155 error is detected to help the debugging of a particular problem.
157 The number entered here is actually the logarithm of the number of
158 bytes that will be saved. So if you pick for example 5 here, kmemcheck
159 will save 2^5 = 32 bytes.
161 The default value should be fine for debugging most problems. It also
162 fits nicely within 80 columns.
164 o CONFIG_KMEMCHECK_PARTIAL_OK
166 This option (when enabled) works around certain GCC optimizations that
167 produce 32-bit reads from 16-bit variables where the upper 16 bits are
168 thrown away afterwards.
170 The default value (enabled) is recommended. This may of course hide
171 some real errors, but disabling it would probably produce a lot of
172 false positives.
174 o CONFIG_KMEMCHECK_BITOPS_OK
176 This option silences warnings that would be generated for bit-field
177 accesses where not all the bits are initialized at the same time. This
178 may also hide some real bugs.
180 This option is probably obsolete, or it should be replaced with
181 the kmemcheck-/bitfield-annotations for the code in question. The
182 default value is therefore fine.
184 Now compile the kernel as usual.
187 3. How to use
188 =============
190 3.1. Booting
191 ============
193 First some information about the command-line options. There is only one
194 option specific to kmemcheck, and this is called "kmemcheck". It can be used
195 to override the default mode as chosen by the CONFIG_KMEMCHECK_*_BY_DEFAULT
196 option. Its possible settings are:
198 o kmemcheck=0 (disabled)
199 o kmemcheck=1 (enabled)
200 o kmemcheck=2 (one-shot mode)
202 If SLUB debugging has been enabled in the kernel, it may take precedence over
203 kmemcheck in such a way that the slab caches which are under SLUB debugging
204 will not be tracked by kmemcheck. In order to ensure that this doesn't happen
205 (even though it shouldn't by default), use SLUB's boot option "slub_debug",
206 like this: slub_debug=-
208 In fact, this option may also be used for fine-grained control over SLUB vs.
209 kmemcheck. For example, if the command line includes "kmemcheck=1
210 slub_debug=,dentry", then SLUB debugging will be used only for the "dentry"
211 slab cache, and with kmemcheck tracking all the other caches. This is advanced
212 usage, however, and is not generally recommended.
215 3.2. Run-time enable/disable
216 ============================
218 When the kernel has booted, it is possible to enable or disable kmemcheck at
219 run-time. WARNING: This feature is still experimental and may cause false
220 positive warnings to appear. Therefore, try not to use this. If you find that
221 it doesn't work properly (e.g. you see an unreasonable amount of warnings), I
222 will be happy to take bug reports.
224 Use the file /proc/sys/kernel/kmemcheck for this purpose, e.g.:
226 $ echo 0 > /proc/sys/kernel/kmemcheck # disables kmemcheck
228 The numbers are the same as for the kmemcheck= command-line option.
231 3.3. Debugging
232 ==============
234 A typical report will look something like this:
236 WARNING: kmemcheck: Caught 32-bit read from uninitialized memory (ffff88003e4a2024)
237 80000000000000000000000000000000000000000088ffff0000000000000000
238 i i i i u u u u i i i i i i i i u u u u u u u u u u u u u u u u
239 ^
241 Pid: 1856, comm: ntpdate Not tainted 2.6.29-rc5 #264 945P-A
242 RIP: 0010:[<ffffffff8104ede8>] [<ffffffff8104ede8>] __dequeue_signal+0xc8/0x190
243 RSP: 0018:ffff88003cdf7d98 EFLAGS: 00210002
244 RAX: 0000000000000030 RBX: ffff88003d4ea968 RCX: 0000000000000009
245 RDX: ffff88003e5d6018 RSI: ffff88003e5d6024 RDI: ffff88003cdf7e84
246 RBP: ffff88003cdf7db8 R08: ffff88003e5d6000 R09: 0000000000000000
247 R10: 0000000000000080 R11: 0000000000000000 R12: 000000000000000e
248 R13: ffff88003cdf7e78 R14: ffff88003d530710 R15: ffff88003d5a98c8
249 FS: 0000000000000000(0000) GS:ffff880001982000(0063) knlGS:00000
250 CS: 0010 DS: 002b ES: 002b CR0: 0000000080050033
251 CR2: ffff88003f806ea0 CR3: 000000003c036000 CR4: 00000000000006a0
252 DR0: 0000000000000000 DR1: 0000000000000000 DR2: 0000000000000000
253 DR3: 0000000000000000 DR6: 00000000ffff4ff0 DR7: 0000000000000400
254 [<ffffffff8104f04e>] dequeue_signal+0x8e/0x170
255 [<ffffffff81050bd8>] get_signal_to_deliver+0x98/0x390
256 [<ffffffff8100b87d>] do_notify_resume+0xad/0x7d0
257 [<ffffffff8100c7b5>] int_signal+0x12/0x17
258 [<ffffffffffffffff>] 0xffffffffffffffff
260 The single most valuable information in this report is the RIP (or EIP on 32-
261 bit) value. This will help us pinpoint exactly which instruction that caused
262 the warning.
264 If your kernel was compiled with CONFIG_DEBUG_INFO=y, then all we have to do
265 is give this address to the addr2line program, like this:
267 $ addr2line -e vmlinux -i ffffffff8104ede8
268 arch/x86/include/asm/string_64.h:12
269 include/asm-generic/siginfo.h:287
270 kernel/signal.c:380
271 kernel/signal.c:410
273 The "-e vmlinux" tells addr2line which file to look in. IMPORTANT: This must
274 be the vmlinux of the kernel that produced the warning in the first place! If
275 not, the line number information will almost certainly be wrong.
277 The "-i" tells addr2line to also print the line numbers of inlined functions.
278 In this case, the flag was very important, because otherwise, it would only
279 have printed the first line, which is just a call to memcpy(), which could be
280 called from a thousand places in the kernel, and is therefore not very useful.
281 These inlined functions would not show up in the stack trace above, simply
282 because the kernel doesn't load the extra debugging information. This
283 technique can of course be used with ordinary kernel oopses as well.
285 In this case, it's the caller of memcpy() that is interesting, and it can be
286 found in include/asm-generic/siginfo.h, line 287:
288 281 static inline void copy_siginfo(struct siginfo *to, struct siginfo *from)
289 282 {
290 283 if (from->si_code < 0)
291 284 memcpy(to, from, sizeof(*to));
292 285 else
293 286 /* _sigchld is currently the largest know union member */
294 287 memcpy(to, from, __ARCH_SI_PREAMBLE_SIZE + sizeof(from->_sifields._sigchld));
295 288 }
297 Since this was a read (kmemcheck usually warns about reads only, though it can
298 warn about writes to unallocated or freed memory as well), it was probably the
299 "from" argument which contained some uninitialized bytes. Following the chain
300 of calls, we move upwards to see where "from" was allocated or initialized,
301 kernel/signal.c, line 380:
303 359 static void collect_signal(int sig, struct sigpending *list, siginfo_t *info)
304 360 {
305 ...
306 367 list_for_each_entry(q, &list->list, list) {
307 368 if (q->info.si_signo == sig) {
308 369 if (first)
309 370 goto still_pending;
310 371 first = q;
311 ...
312 377 if (first) {
313 378 still_pending:
314 379 list_del_init(&first->list);
315 380 copy_siginfo(info, &first->info);
316 381 __sigqueue_free(first);
317 ...
318 392 }
319 393 }
321 Here, it is &first->info that is being passed on to copy_siginfo(). The
322 variable "first" was found on a list -- passed in as the second argument to
323 collect_signal(). We continue our journey through the stack, to figure out
324 where the item on "list" was allocated or initialized. We move to line 410:
326 395 static int __dequeue_signal(struct sigpending *pending, sigset_t *mask,
327 396 siginfo_t *info)
328 397 {
329 ...
330 410 collect_signal(sig, pending, info);
331 ...
332 414 }
334 Now we need to follow the "pending" pointer, since that is being passed on to
335 collect_signal() as "list". At this point, we've run out of lines from the
336 "addr2line" output. Not to worry, we just paste the next addresses from the
337 kmemcheck stack dump, i.e.:
339 [<ffffffff8104f04e>] dequeue_signal+0x8e/0x170
340 [<ffffffff81050bd8>] get_signal_to_deliver+0x98/0x390
341 [<ffffffff8100b87d>] do_notify_resume+0xad/0x7d0
342 [<ffffffff8100c7b5>] int_signal+0x12/0x17
344 $ addr2line -e vmlinux -i ffffffff8104f04e ffffffff81050bd8 \
345 ffffffff8100b87d ffffffff8100c7b5
346 kernel/signal.c:446
347 kernel/signal.c:1806
348 arch/x86/kernel/signal.c:805
349 arch/x86/kernel/signal.c:871
350 arch/x86/kernel/entry_64.S:694
352 Remember that since these addresses were found on the stack and not as the
353 RIP value, they actually point to the _next_ instruction (they are return
354 addresses). This becomes obvious when we look at the code for line 446:
356 422 int dequeue_signal(struct task_struct *tsk, sigset_t *mask, siginfo_t *info)
357 423 {
358 ...
359 431 signr = __dequeue_signal(&tsk->signal->shared_pending,
360 432 mask, info);
361 433 /*
362 434 * itimer signal ?
363 435 *
364 436 * itimers are process shared and we restart periodic
365 437 * itimers in the signal delivery path to prevent DoS
366 438 * attacks in the high resolution timer case. This is
367 439 * compliant with the old way of self restarting
368 440 * itimers, as the SIGALRM is a legacy signal and only
369 441 * queued once. Changing the restart behaviour to
370 442 * restart the timer in the signal dequeue path is
371 443 * reducing the timer noise on heavy loaded !highres
372 444 * systems too.
373 445 */
374 446 if (unlikely(signr == SIGALRM)) {
375 ...
376 489 }
378 So instead of looking at 446, we should be looking at 431, which is the line
379 that executes just before 446. Here we see that what we are looking for is
380 &tsk->signal->shared_pending.
382 Our next task is now to figure out which function that puts items on this
383 "shared_pending" list. A crude, but efficient tool, is git grep:
385 $ git grep -n 'shared_pending' kernel/
386 ...
387 kernel/signal.c:828: pending = group ? &t->signal->shared_pending : &t->pending;
388 kernel/signal.c:1339: pending = group ? &t->signal->shared_pending : &t->pending;
389 ...
391 There were more results, but none of them were related to list operations,
392 and these were the only assignments. We inspect the line numbers more closely
393 and find that this is indeed where items are being added to the list:
395 816 static int send_signal(int sig, struct siginfo *info, struct task_struct *t,
396 817 int group)
397 818 {
398 ...
399 828 pending = group ? &t->signal->shared_pending : &t->pending;
400 ...
401 851 q = __sigqueue_alloc(t, GFP_ATOMIC, (sig < SIGRTMIN &&
402 852 (is_si_special(info) ||
403 853 info->si_code >= 0)));
404 854 if (q) {
405 855 list_add_tail(&q->list, &pending->list);
406 ...
407 890 }
409 and:
411 1309 int send_sigqueue(struct sigqueue *q, struct task_struct *t, int group)
412 1310 {
413 ....
414 1339 pending = group ? &t->signal->shared_pending : &t->pending;
415 1340 list_add_tail(&q->list, &pending->list);
416 ....
417 1347 }
419 In the first case, the list element we are looking for, "q", is being returned
420 from the function __sigqueue_alloc(), which looks like an allocation function.
421 Let's take a look at it:
423 187 static struct sigqueue *__sigqueue_alloc(struct task_struct *t, gfp_t flags,
424 188 int override_rlimit)
425 189 {
426 190 struct sigqueue *q = NULL;
427 191 struct user_struct *user;
428 192
429 193 /*
430 194 * We won't get problems with the target's UID changing under us
431 195 * because changing it requires RCU be used, and if t != current, the
432 196 * caller must be holding the RCU readlock (by way of a spinlock) and
433 197 * we use RCU protection here
434 198 */
435 199 user = get_uid(__task_cred(t)->user);
436 200 atomic_inc(&user->sigpending);
437 201 if (override_rlimit ||
438 202 atomic_read(&user->sigpending) <=
439 203 t->signal->rlim[RLIMIT_SIGPENDING].rlim_cur)
440 204 q = kmem_cache_alloc(sigqueue_cachep, flags);
441 205 if (unlikely(q == NULL)) {
442 206 atomic_dec(&user->sigpending);
443 207 free_uid(user);
444 208 } else {
445 209 INIT_LIST_HEAD(&q->list);
446 210 q->flags = 0;
447 211 q->user = user;
448 212 }
449 213
450 214 return q;
451 215 }
453 We see that this function initializes q->list, q->flags, and q->user. It seems
454 that now is the time to look at the definition of "struct sigqueue", e.g.:
456 14 struct sigqueue {
457 15 struct list_head list;
458 16 int flags;
459 17 siginfo_t info;
460 18 struct user_struct *user;
461 19 };
463 And, you might remember, it was a memcpy() on &first->info that caused the
464 warning, so this makes perfect sense. It also seems reasonable to assume that
465 it is the caller of __sigqueue_alloc() that has the responsibility of filling
466 out (initializing) this member.
468 But just which fields of the struct were uninitialized? Let's look at
469 kmemcheck's report again:
471 WARNING: kmemcheck: Caught 32-bit read from uninitialized memory (ffff88003e4a2024)
472 80000000000000000000000000000000000000000088ffff0000000000000000
473 i i i i u u u u i i i i i i i i u u u u u u u u u u u u u u u u
474 ^
476 These first two lines are the memory dump of the memory object itself, and the
477 shadow bytemap, respectively. The memory object itself is in this case
478 &first->info. Just beware that the start of this dump is NOT the start of the
479 object itself! The position of the caret (^) corresponds with the address of
480 the read (ffff88003e4a2024).
482 The shadow bytemap dump legend is as follows:
484 i - initialized
485 u - uninitialized
486 a - unallocated (memory has been allocated by the slab layer, but has not
487 yet been handed off to anybody)
488 f - freed (memory has been allocated by the slab layer, but has been freed
489 by the previous owner)
491 In order to figure out where (relative to the start of the object) the
492 uninitialized memory was located, we have to look at the disassembly. For
493 that, we'll need the RIP address again:
495 RIP: 0010:[<ffffffff8104ede8>] [<ffffffff8104ede8>] __dequeue_signal+0xc8/0x190
497 $ objdump -d --no-show-raw-insn vmlinux | grep -C 8 ffffffff8104ede8:
498 ffffffff8104edc8: mov %r8,0x8(%r8)
499 ffffffff8104edcc: test %r10d,%r10d
500 ffffffff8104edcf: js ffffffff8104ee88 <__dequeue_signal+0x168>
501 ffffffff8104edd5: mov %rax,%rdx
502 ffffffff8104edd8: mov $0xc,%ecx
503 ffffffff8104eddd: mov %r13,%rdi
504 ffffffff8104ede0: mov $0x30,%eax
505 ffffffff8104ede5: mov %rdx,%rsi
506 ffffffff8104ede8: rep movsl %ds:(%rsi),%es:(%rdi)
507 ffffffff8104edea: test $0x2,%al
508 ffffffff8104edec: je ffffffff8104edf0 <__dequeue_signal+0xd0>
509 ffffffff8104edee: movsw %ds:(%rsi),%es:(%rdi)
510 ffffffff8104edf0: test $0x1,%al
511 ffffffff8104edf2: je ffffffff8104edf5 <__dequeue_signal+0xd5>
512 ffffffff8104edf4: movsb %ds:(%rsi),%es:(%rdi)
513 ffffffff8104edf5: mov %r8,%rdi
514 ffffffff8104edf8: callq ffffffff8104de60 <__sigqueue_free>
516 As expected, it's the "rep movsl" instruction from the memcpy() that causes
517 the warning. We know about REP MOVSL that it uses the register RCX to count
518 the number of remaining iterations. By taking a look at the register dump
519 again (from the kmemcheck report), we can figure out how many bytes were left
520 to copy:
522 RAX: 0000000000000030 RBX: ffff88003d4ea968 RCX: 0000000000000009
524 By looking at the disassembly, we also see that %ecx is being loaded with the
525 value $0xc just before (ffffffff8104edd8), so we are very lucky. Keep in mind
526 that this is the number of iterations, not bytes. And since this is a "long"
527 operation, we need to multiply by 4 to get the number of bytes. So this means
528 that the uninitialized value was encountered at 4 * (0xc - 0x9) = 12 bytes
529 from the start of the object.
531 We can now try to figure out which field of the "struct siginfo" that was not
532 initialized. This is the beginning of the struct:
534 40 typedef struct siginfo {
535 41 int si_signo;
536 42 int si_errno;
537 43 int si_code;
538 44
539 45 union {
540 ..
541 92 } _sifields;
542 93 } siginfo_t;
544 On 64-bit, the int is 4 bytes long, so it must the the union member that has
545 not been initialized. We can verify this using gdb:
547 $ gdb vmlinux
548 ...
549 (gdb) p &((struct siginfo *) 0)->_sifields
550 $1 = (union {...} *) 0x10
552 Actually, it seems that the union member is located at offset 0x10 -- which
553 means that gcc has inserted 4 bytes of padding between the members si_code
554 and _sifields. We can now get a fuller picture of the memory dump:
556 _----------------------------=> si_code
557 / _--------------------=> (padding)
558 | / _------------=> _sifields(._kill._pid)
559 | | / _----=> _sifields(._kill._uid)
560 | | | /
561 -------|-------|-------|-------|
562 80000000000000000000000000000000000000000088ffff0000000000000000
563 i i i i u u u u i i i i i i i i u u u u u u u u u u u u u u u u
565 This allows us to realize another important fact: si_code contains the value
566 0x80. Remember that x86 is little endian, so the first 4 bytes "80000000" are
567 really the number 0x00000080. With a bit of research, we find that this is
568 actually the constant SI_KERNEL defined in include/asm-generic/siginfo.h:
570 144 #define SI_KERNEL 0x80 /* sent by the kernel from somewhere */
572 This macro is used in exactly one place in the x86 kernel: In send_signal()
573 in kernel/signal.c:
575 816 static int send_signal(int sig, struct siginfo *info, struct task_struct *t,
576 817 int group)
577 818 {
578 ...
579 828 pending = group ? &t->signal->shared_pending : &t->pending;
580 ...
581 851 q = __sigqueue_alloc(t, GFP_ATOMIC, (sig < SIGRTMIN &&
582 852 (is_si_special(info) ||
583 853 info->si_code >= 0)));
584 854 if (q) {
585 855 list_add_tail(&q->list, &pending->list);
586 856 switch ((unsigned long) info) {
587 ...
588 865 case (unsigned long) SEND_SIG_PRIV:
589 866 q->info.si_signo = sig;
590 867 q->info.si_errno = 0;
591 868 q->info.si_code = SI_KERNEL;
592 869 q->info.si_pid = 0;
593 870 q->info.si_uid = 0;
594 871 break;
595 ...
596 890 }
598 Not only does this match with the .si_code member, it also matches the place
599 we found earlier when looking for where siginfo_t objects are enqueued on the
600 "shared_pending" list.
602 So to sum up: It seems that it is the padding introduced by the compiler
603 between two struct fields that is uninitialized, and this gets reported when
604 we do a memcpy() on the struct. This means that we have identified a false
605 positive warning.
607 Normally, kmemcheck will not report uninitialized accesses in memcpy() calls
608 when both the source and destination addresses are tracked. (Instead, we copy
609 the shadow bytemap as well). In this case, the destination address clearly
610 was not tracked. We can dig a little deeper into the stack trace from above:
612 arch/x86/kernel/signal.c:805
613 arch/x86/kernel/signal.c:871
614 arch/x86/kernel/entry_64.S:694
616 And we clearly see that the destination siginfo object is located on the
617 stack:
619 782 static void do_signal(struct pt_regs *regs)
620 783 {
621 784 struct k_sigaction ka;
622 785 siginfo_t info;
623 ...
624 804 signr = get_signal_to_deliver(&info, &ka, regs, NULL);
625 ...
626 854 }
628 And this &info is what eventually gets passed to copy_siginfo() as the
629 destination argument.
631 Now, even though we didn't find an actual error here, the example is still a
632 good one, because it shows how one would go about to find out what the report
633 was all about.
636 3.4. Annotating false positives
637 ===============================
639 There are a few different ways to make annotations in the source code that
640 will keep kmemcheck from checking and reporting certain allocations. Here
641 they are:
643 o __GFP_NOTRACK_FALSE_POSITIVE
645 This flag can be passed to kmalloc() or kmem_cache_alloc() (therefore
646 also to other functions that end up calling one of these) to indicate
647 that the allocation should not be tracked because it would lead to
648 a false positive report. This is a "big hammer" way of silencing
649 kmemcheck; after all, even if the false positive pertains to
650 particular field in a struct, for example, we will now lose the
651 ability to find (real) errors in other parts of the same struct.
653 Example:
655 /* No warnings will ever trigger on accessing any part of x */
656 x = kmalloc(sizeof *x, GFP_KERNEL | __GFP_NOTRACK_FALSE_POSITIVE);
658 o kmemcheck_bitfield_begin(name)/kmemcheck_bitfield_end(name) and
659 kmemcheck_annotate_bitfield(ptr, name)
661 The first two of these three macros can be used inside struct
662 definitions to signal, respectively, the beginning and end of a
663 bitfield. Additionally, this will assign the bitfield a name, which
664 is given as an argument to the macros.
666 Having used these markers, one can later use
667 kmemcheck_annotate_bitfield() at the point of allocation, to indicate
668 which parts of the allocation is part of a bitfield.
670 Example:
672 struct foo {
673 int x;
675 kmemcheck_bitfield_begin(flags);
676 int flag_a:1;
677 int flag_b:1;
678 kmemcheck_bitfield_end(flags);
680 int y;
681 };
683 struct foo *x = kmalloc(sizeof *x);
685 /* No warnings will trigger on accessing the bitfield of x */
686 kmemcheck_annotate_bitfield(x, flags);
688 Note that kmemcheck_annotate_bitfield() can be used even before the
689 return value of kmalloc() is checked -- in other words, passing NULL
690 as the first argument is legal (and will do nothing).
693 4. Reporting errors
694 ===================
696 As we have seen, kmemcheck will produce false positive reports. Therefore, it
697 is not very wise to blindly post kmemcheck warnings to mailing lists and
698 maintainers. Instead, I encourage maintainers and developers to find errors
699 in their own code. If you get a warning, you can try to work around it, try
700 to figure out if it's a real error or not, or simply ignore it. Most
701 developers know their own code and will quickly and efficiently determine the
702 root cause of a kmemcheck report. This is therefore also the most efficient
703 way to work with kmemcheck.
705 That said, we (the kmemcheck maintainers) will always be on the lookout for
706 false positives that we can annotate and silence. So whatever you find,
707 please drop us a note privately! Kernel configs and steps to reproduce (if
708 available) are of course a great help too.
710 Happy hacking!
713 5. Technical description
714 ========================
716 kmemcheck works by marking memory pages non-present. This means that whenever
717 somebody attempts to access the page, a page fault is generated. The page
718 fault handler notices that the page was in fact only hidden, and so it calls
719 on the kmemcheck code to make further investigations.
721 When the investigations are completed, kmemcheck "shows" the page by marking
722 it present (as it would be under normal circumstances). This way, the
723 interrupted code can continue as usual.
725 But after the instruction has been executed, we should hide the page again, so
726 that we can catch the next access too! Now kmemcheck makes use of a debugging
727 feature of the processor, namely single-stepping. When the processor has
728 finished the one instruction that generated the memory access, a debug
729 exception is raised. From here, we simply hide the page again and continue
730 execution, this time with the single-stepping feature turned off.
732 kmemcheck requires some assistance from the memory allocator in order to work.
733 The memory allocator needs to
735 1. Tell kmemcheck about newly allocated pages and pages that are about to
736 be freed. This allows kmemcheck to set up and tear down the shadow memory
737 for the pages in question. The shadow memory stores the status of each
738 byte in the allocation proper, e.g. whether it is initialized or
739 uninitialized.
741 2. Tell kmemcheck which parts of memory should be marked uninitialized.
742 There are actually a few more states, such as "not yet allocated" and
743 "recently freed".
745 If a slab cache is set up using the SLAB_NOTRACK flag, it will never return
746 memory that can take page faults because of kmemcheck.
748 If a slab cache is NOT set up using the SLAB_NOTRACK flag, callers can still
749 request memory with the __GFP_NOTRACK or __GFP_NOTRACK_FALSE_POSITIVE flags.
750 This does not prevent the page faults from occurring, however, but marks the
751 object in question as being initialized so that no warnings will ever be
752 produced for this object.
754 Currently, the SLAB and SLUB allocators are supported by kmemcheck.