]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - Documentation/kref.txt
arm:omap:am33xx: Reverting gigabit disabling support
[sitara-epos/sitara-epos-kernel.git] / Documentation / kref.txt
2 krefs allow you to add reference counters to your objects.  If you
3 have objects that are used in multiple places and passed around, and
4 you don't have refcounts, your code is almost certainly broken.  If
5 you want refcounts, krefs are the way to go.
7 To use a kref, add one to your data structures like:
9 struct my_data
10 {
11         .
12         .
13         struct kref refcount;
14         .
15         .
16 };
18 The kref can occur anywhere within the data structure.
20 You must initialize the kref after you allocate it.  To do this, call
21 kref_init as so:
23      struct my_data *data;
25      data = kmalloc(sizeof(*data), GFP_KERNEL);
26      if (!data)
27             return -ENOMEM;
28      kref_init(&data->refcount);
30 This sets the refcount in the kref to 1.
32 Once you have an initialized kref, you must follow the following
33 rules:
35 1) If you make a non-temporary copy of a pointer, especially if
36    it can be passed to another thread of execution, you must
37    increment the refcount with kref_get() before passing it off:
38        kref_get(&data->refcount);
39    If you already have a valid pointer to a kref-ed structure (the
40    refcount cannot go to zero) you may do this without a lock.
42 2) When you are done with a pointer, you must call kref_put():
43        kref_put(&data->refcount, data_release);
44    If this is the last reference to the pointer, the release
45    routine will be called.  If the code never tries to get
46    a valid pointer to a kref-ed structure without already
47    holding a valid pointer, it is safe to do this without
48    a lock.
50 3) If the code attempts to gain a reference to a kref-ed structure
51    without already holding a valid pointer, it must serialize access
52    where a kref_put() cannot occur during the kref_get(), and the
53    structure must remain valid during the kref_get().
55 For example, if you allocate some data and then pass it to another
56 thread to process:
58 void data_release(struct kref *ref)
59 {
60         struct my_data *data = container_of(ref, struct my_data, refcount);
61         kfree(data);
62 }
64 void more_data_handling(void *cb_data)
65 {
66         struct my_data *data = cb_data;
67         .
68         . do stuff with data here
69         .
70         kref_put(&data->refcount, data_release);
71 }
73 int my_data_handler(void)
74 {
75         int rv = 0;
76         struct my_data *data;
77         struct task_struct *task;
78         data = kmalloc(sizeof(*data), GFP_KERNEL);
79         if (!data)
80                 return -ENOMEM;
81         kref_init(&data->refcount);
83         kref_get(&data->refcount);
84         task = kthread_run(more_data_handling, data, "more_data_handling");
85         if (task == ERR_PTR(-ENOMEM)) {
86                 rv = -ENOMEM;
87                 goto out;
88         }
90         .
91         . do stuff with data here
92         .
93  out:
94         kref_put(&data->refcount, data_release);
95         return rv;
96 }
98 This way, it doesn't matter what order the two threads handle the
99 data, the kref_put() handles knowing when the data is not referenced
100 any more and releasing it.  The kref_get() does not require a lock,
101 since we already have a valid pointer that we own a refcount for.  The
102 put needs no lock because nothing tries to get the data without
103 already holding a pointer.
105 Note that the "before" in rule 1 is very important.  You should never
106 do something like:
108         task = kthread_run(more_data_handling, data, "more_data_handling");
109         if (task == ERR_PTR(-ENOMEM)) {
110                 rv = -ENOMEM;
111                 goto out;
112         } else
113                 /* BAD BAD BAD - get is after the handoff */
114                 kref_get(&data->refcount);
116 Don't assume you know what you are doing and use the above construct.
117 First of all, you may not know what you are doing.  Second, you may
118 know what you are doing (there are some situations where locking is
119 involved where the above may be legal) but someone else who doesn't
120 know what they are doing may change the code or copy the code.  It's
121 bad style.  Don't do it.
123 There are some situations where you can optimize the gets and puts.
124 For instance, if you are done with an object and enqueuing it for
125 something else or passing it off to something else, there is no reason
126 to do a get then a put:
128         /* Silly extra get and put */
129         kref_get(&obj->ref);
130         enqueue(obj);
131         kref_put(&obj->ref, obj_cleanup);
133 Just do the enqueue.  A comment about this is always welcome:
135         enqueue(obj);
136         /* We are done with obj, so we pass our refcount off
137            to the queue.  DON'T TOUCH obj AFTER HERE! */
139 The last rule (rule 3) is the nastiest one to handle.  Say, for
140 instance, you have a list of items that are each kref-ed, and you wish
141 to get the first one.  You can't just pull the first item off the list
142 and kref_get() it.  That violates rule 3 because you are not already
143 holding a valid pointer.  You must add a mutex (or some other lock).
144 For instance:
146 static DEFINE_MUTEX(mutex);
147 static LIST_HEAD(q);
148 struct my_data
150         struct kref      refcount;
151         struct list_head link;
152 };
154 static struct my_data *get_entry()
156         struct my_data *entry = NULL;
157         mutex_lock(&mutex);
158         if (!list_empty(&q)) {
159                 entry = container_of(q.next, struct my_data, link);
160                 kref_get(&entry->refcount);
161         }
162         mutex_unlock(&mutex);
163         return entry;
166 static void release_entry(struct kref *ref)
168         struct my_data *entry = container_of(ref, struct my_data, refcount);
170         list_del(&entry->link);
171         kfree(entry);
174 static void put_entry(struct my_data *entry)
176         mutex_lock(&mutex);
177         kref_put(&entry->refcount, release_entry);
178         mutex_unlock(&mutex);
181 The kref_put() return value is useful if you do not want to hold the
182 lock during the whole release operation.  Say you didn't want to call
183 kfree() with the lock held in the example above (since it is kind of
184 pointless to do so).  You could use kref_put() as follows:
186 static void release_entry(struct kref *ref)
188         /* All work is done after the return from kref_put(). */
191 static void put_entry(struct my_data *entry)
193         mutex_lock(&mutex);
194         if (kref_put(&entry->refcount, release_entry)) {
195                 list_del(&entry->link);
196                 mutex_unlock(&mutex);
197                 kfree(entry);
198         } else
199                 mutex_unlock(&mutex);
202 This is really more useful if you have to call other routines as part
203 of the free operations that could take a long time or might claim the
204 same lock.  Note that doing everything in the release routine is still
205 preferred as it is a little neater.
208 Corey Minyard <minyard@acm.org>
210 A lot of this was lifted from Greg Kroah-Hartman's 2004 OLS paper and
211 presentation on krefs, which can be found at:
212   http://www.kroah.com/linux/talks/ols_2004_kref_paper/Reprint-Kroah-Hartman-OLS2004.pdf
213 and:
214   http://www.kroah.com/linux/talks/ols_2004_kref_talk/