]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - Documentation/mono.txt
video: da8xx-fb: correct suspend/resume sequence
[sitara-epos/sitara-epos-kernel.git] / Documentation / mono.txt
1                Mono(tm) Binary Kernel Support for Linux
2                -----------------------------------------
4 To configure Linux to automatically execute Mono-based .NET binaries
5 (in the form of .exe files) without the need to use the mono CLR
6 wrapper, you can use the BINFMT_MISC kernel support.
8 This will allow you to execute Mono-based .NET binaries just like any
9 other program after you have done the following:
11 1) You MUST FIRST install the Mono CLR support, either by downloading
12    a binary package, a source tarball or by installing from CVS. Binary
13    packages for several distributions can be found at:
15         http://go-mono.com/download.html
17    Instructions for compiling Mono can be found at:
19         http://www.go-mono.com/compiling.html
21    Once the Mono CLR support has been installed, just check that
22    /usr/bin/mono (which could be located elsewhere, for example
23    /usr/local/bin/mono) is working.
25 2) You have to compile BINFMT_MISC either as a module or into
26    the kernel (CONFIG_BINFMT_MISC) and set it up properly.
27    If you choose to compile it as a module, you will have
28    to insert it manually with modprobe/insmod, as kmod
29    cannot be easily supported with binfmt_misc. 
30    Read the file 'binfmt_misc.txt' in this directory to know
31    more about the configuration process.
33 3) Add the following entries to /etc/rc.local or similar script
34    to be run at system startup:
36 # Insert BINFMT_MISC module into the kernel
37 if [ ! -e /proc/sys/fs/binfmt_misc/register ]; then
38         /sbin/modprobe binfmt_misc
39         # Some distributions, like Fedora Core, perform
40         # the following command automatically when the
41         # binfmt_misc module is loaded into the kernel.
42         # Thus, it is possible that the following line
43         # is not needed at all. Look at /etc/modprobe.conf
44         # to check whether this is applicable or not.
45         mount -t binfmt_misc none /proc/sys/fs/binfmt_misc
46 fi
48 # Register support for .NET CLR binaries
49 if [ -e /proc/sys/fs/binfmt_misc/register ]; then
50         # Replace /usr/bin/mono with the correct pathname to
51         # the Mono CLR runtime (usually /usr/local/bin/mono
52         # when compiling from sources or CVS).
53         echo ':CLR:M::MZ::/usr/bin/mono:' > /proc/sys/fs/binfmt_misc/register
54 else
55         echo "No binfmt_misc support"
56         exit 1
57 fi
59 4) Check that .exe binaries can be ran without the need of a
60    wrapper script, simply by launching the .exe file directly
61    from a command prompt, for example:
63         /usr/bin/xsd.exe
65    NOTE: If this fails with a permission denied error, check
66          that the .exe file has execute permissions.