1 =============================
2 NO-MMU MEMORY MAPPING SUPPORT
3 =============================
5 The kernel has limited support for memory mapping under no-MMU conditions, such
6 as are used in uClinux environments. From the userspace point of view, memory
7 mapping is made use of in conjunction with the mmap() system call, the shmat()
8 call and the execve() system call. From the kernel's point of view, execve()
9 mapping is actually performed by the binfmt drivers, which call back into the
10 mmap() routines to do the actual work.
12 Memory mapping behaviour also involves the way fork(), vfork(), clone() and
13 ptrace() work. Under uClinux there is no fork(), and clone() must be supplied
14 the CLONE_VM flag.
16 The behaviour is similar between the MMU and no-MMU cases, but not identical;
17 and it's also much more restricted in the latter case:
19 (*) Anonymous mapping, MAP_PRIVATE
21 In the MMU case: VM regions backed by arbitrary pages; copy-on-write
22 across fork.
24 In the no-MMU case: VM regions backed by arbitrary contiguous runs of
25 pages.
27 (*) Anonymous mapping, MAP_SHARED
29 These behave very much like private mappings, except that they're
30 shared across fork() or clone() without CLONE_VM in the MMU case. Since
31 the no-MMU case doesn't support these, behaviour is identical to
32 MAP_PRIVATE there.
34 (*) File, MAP_PRIVATE, PROT_READ / PROT_EXEC, !PROT_WRITE
36 In the MMU case: VM regions backed by pages read from file; changes to
37 the underlying file are reflected in the mapping; copied across fork.
39 In the no-MMU case:
41 - If one exists, the kernel will re-use an existing mapping to the
42 same segment of the same file if that has compatible permissions,
43 even if this was created by another process.
45 - If possible, the file mapping will be directly on the backing device
46 if the backing device has the BDI_CAP_MAP_DIRECT capability and
47 appropriate mapping protection capabilities. Ramfs, romfs, cramfs
48 and mtd might all permit this.
50 - If the backing device device can't or won't permit direct sharing,
51 but does have the BDI_CAP_MAP_COPY capability, then a copy of the
52 appropriate bit of the file will be read into a contiguous bit of
53 memory and any extraneous space beyond the EOF will be cleared
55 - Writes to the file do not affect the mapping; writes to the mapping
56 are visible in other processes (no MMU protection), but should not
57 happen.
59 (*) File, MAP_PRIVATE, PROT_READ / PROT_EXEC, PROT_WRITE
61 In the MMU case: like the non-PROT_WRITE case, except that the pages in
62 question get copied before the write actually happens. From that point
63 on writes to the file underneath that page no longer get reflected into
64 the mapping's backing pages. The page is then backed by swap instead.
66 In the no-MMU case: works much like the non-PROT_WRITE case, except
67 that a copy is always taken and never shared.
69 (*) Regular file / blockdev, MAP_SHARED, PROT_READ / PROT_EXEC / PROT_WRITE
71 In the MMU case: VM regions backed by pages read from file; changes to
72 pages written back to file; writes to file reflected into pages backing
73 mapping; shared across fork.
75 In the no-MMU case: not supported.
77 (*) Memory backed regular file, MAP_SHARED, PROT_READ / PROT_EXEC / PROT_WRITE
79 In the MMU case: As for ordinary regular files.
81 In the no-MMU case: The filesystem providing the memory-backed file
82 (such as ramfs or tmpfs) may choose to honour an open, truncate, mmap
83 sequence by providing a contiguous sequence of pages to map. In that
84 case, a shared-writable memory mapping will be possible. It will work
85 as for the MMU case. If the filesystem does not provide any such
86 support, then the mapping request will be denied.
88 (*) Memory backed blockdev, MAP_SHARED, PROT_READ / PROT_EXEC / PROT_WRITE
90 In the MMU case: As for ordinary regular files.
92 In the no-MMU case: As for memory backed regular files, but the
93 blockdev must be able to provide a contiguous run of pages without
94 truncate being called. The ramdisk driver could do this if it allocated
95 all its memory as a contiguous array upfront.
97 (*) Memory backed chardev, MAP_SHARED, PROT_READ / PROT_EXEC / PROT_WRITE
99 In the MMU case: As for ordinary regular files.
101 In the no-MMU case: The character device driver may choose to honour
102 the mmap() by providing direct access to the underlying device if it
103 provides memory or quasi-memory that can be accessed directly. Examples
104 of such are frame buffers and flash devices. If the driver does not
105 provide any such support, then the mapping request will be denied.
108 ============================
109 FURTHER NOTES ON NO-MMU MMAP
110 ============================
112 (*) A request for a private mapping of a file may return a buffer that is not
113 page-aligned. This is because XIP may take place, and the data may not be
114 paged aligned in the backing store.
116 (*) A request for an anonymous mapping will always be page aligned. If
117 possible the size of the request should be a power of two otherwise some
118 of the space may be wasted as the kernel must allocate a power-of-2
119 granule but will only discard the excess if appropriately configured as
120 this has an effect on fragmentation.
122 (*) The memory allocated by a request for an anonymous mapping will normally
123 be cleared by the kernel before being returned in accordance with the
124 Linux man pages (ver 2.22 or later).
126 In the MMU case this can be achieved with reasonable performance as
127 regions are backed by virtual pages, with the contents only being mapped
128 to cleared physical pages when a write happens on that specific page
129 (prior to which, the pages are effectively mapped to the global zero page
130 from which reads can take place). This spreads out the time it takes to
131 initialize the contents of a page - depending on the write-usage of the
132 mapping.
134 In the no-MMU case, however, anonymous mappings are backed by physical
135 pages, and the entire map is cleared at allocation time. This can cause
136 significant delays during a userspace malloc() as the C library does an
137 anonymous mapping and the kernel then does a memset for the entire map.
139 However, for memory that isn't required to be precleared - such as that
140 returned by malloc() - mmap() can take a MAP_UNINITIALIZED flag to
141 indicate to the kernel that it shouldn't bother clearing the memory before
142 returning it. Note that CONFIG_MMAP_ALLOW_UNINITIALIZED must be enabled
143 to permit this, otherwise the flag will be ignored.
145 uClibc uses this to speed up malloc(), and the ELF-FDPIC binfmt uses this
146 to allocate the brk and stack region.
148 (*) A list of all the private copy and anonymous mappings on the system is
149 visible through /proc/maps in no-MMU mode.
151 (*) A list of all the mappings in use by a process is visible through
152 /proc/<pid>/maps in no-MMU mode.
154 (*) Supplying MAP_FIXED or a requesting a particular mapping address will
155 result in an error.
157 (*) Files mapped privately usually have to have a read method provided by the
158 driver or filesystem so that the contents can be read into the memory
159 allocated if mmap() chooses not to map the backing device directly. An
160 error will result if they don't. This is most likely to be encountered
161 with character device files, pipes, fifos and sockets.
164 ==========================
165 INTERPROCESS SHARED MEMORY
166 ==========================
168 Both SYSV IPC SHM shared memory and POSIX shared memory is supported in NOMMU
169 mode. The former through the usual mechanism, the latter through files created
170 on ramfs or tmpfs mounts.
173 =======
174 FUTEXES
175 =======
177 Futexes are supported in NOMMU mode if the arch supports them. An error will
178 be given if an address passed to the futex system call lies outside the
179 mappings made by a process or if the mapping in which the address lies does not
180 support futexes (such as an I/O chardev mapping).
183 =============
184 NO-MMU MREMAP
185 =============
187 The mremap() function is partially supported. It may change the size of a
188 mapping, and may move it[*] if MREMAP_MAYMOVE is specified and if the new size
189 of the mapping exceeds the size of the slab object currently occupied by the
190 memory to which the mapping refers, or if a smaller slab object could be used.
192 MREMAP_FIXED is not supported, though it is ignored if there's no change of
193 address and the object does not need to be moved.
195 Shared mappings may not be moved. Shareable mappings may not be moved either,
196 even if they are not currently shared.
198 The mremap() function must be given an exact match for base address and size of
199 a previously mapped object. It may not be used to create holes in existing
200 mappings, move parts of existing mappings or resize parts of mappings. It must
201 act on a complete mapping.
203 [*] Not currently supported.
206 ============================================
207 PROVIDING SHAREABLE CHARACTER DEVICE SUPPORT
208 ============================================
210 To provide shareable character device support, a driver must provide a
211 file->f_op->get_unmapped_area() operation. The mmap() routines will call this
212 to get a proposed address for the mapping. This may return an error if it
213 doesn't wish to honour the mapping because it's too long, at a weird offset,
214 under some unsupported combination of flags or whatever.
216 The driver should also provide backing device information with capabilities set
217 to indicate the permitted types of mapping on such devices. The default is
218 assumed to be readable and writable, not executable, and only shareable
219 directly (can't be copied).
221 The file->f_op->mmap() operation will be called to actually inaugurate the
222 mapping. It can be rejected at that point. Returning the ENOSYS error will
223 cause the mapping to be copied instead if BDI_CAP_MAP_COPY is specified.
225 The vm_ops->close() routine will be invoked when the last mapping on a chardev
226 is removed. An existing mapping will be shared, partially or not, if possible
227 without notifying the driver.
229 It is permitted also for the file->f_op->get_unmapped_area() operation to
230 return -ENOSYS. This will be taken to mean that this operation just doesn't
231 want to handle it, despite the fact it's got an operation. For instance, it
232 might try directing the call to a secondary driver which turns out not to
233 implement it. Such is the case for the framebuffer driver which attempts to
234 direct the call to the device-specific driver. Under such circumstances, the
235 mapping request will be rejected if BDI_CAP_MAP_COPY is not specified, and a
236 copy mapped otherwise.
238 IMPORTANT NOTE:
240 Some types of device may present a different appearance to anyone
241 looking at them in certain modes. Flash chips can be like this; for
242 instance if they're in programming or erase mode, you might see the
243 status reflected in the mapping, instead of the data.
245 In such a case, care must be taken lest userspace see a shared or a
246 private mapping showing such information when the driver is busy
247 controlling the device. Remember especially: private executable
248 mappings may still be mapped directly off the device under some
249 circumstances!
252 ==============================================
253 PROVIDING SHAREABLE MEMORY-BACKED FILE SUPPORT
254 ==============================================
256 Provision of shared mappings on memory backed files is similar to the provision
257 of support for shared mapped character devices. The main difference is that the
258 filesystem providing the service will probably allocate a contiguous collection
259 of pages and permit mappings to be made on that.
261 It is recommended that a truncate operation applied to such a file that
262 increases the file size, if that file is empty, be taken as a request to gather
263 enough pages to honour a mapping. This is required to support POSIX shared
264 memory.
266 Memory backed devices are indicated by the mapping's backing device info having
267 the memory_backed flag set.
270 ========================================
271 PROVIDING SHAREABLE BLOCK DEVICE SUPPORT
272 ========================================
274 Provision of shared mappings on block device files is exactly the same as for
275 character devices. If there isn't a real device underneath, then the driver
276 should allocate sufficient contiguous memory to honour any supported mapping.
279 =================================
280 ADJUSTING PAGE TRIMMING BEHAVIOUR
281 =================================
283 NOMMU mmap automatically rounds up to the nearest power-of-2 number of pages
284 when performing an allocation. This can have adverse effects on memory
285 fragmentation, and as such, is left configurable. The default behaviour is to
286 aggressively trim allocations and discard any excess pages back in to the page
287 allocator. In order to retain finer-grained control over fragmentation, this
288 behaviour can either be disabled completely, or bumped up to a higher page
289 watermark where trimming begins.
291 Page trimming behaviour is configurable via the sysctl `vm.nr_trim_pages'.