]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - Documentation/stable_kernel_rules.txt
arm:omap:am33xx: Reverting gigabit disabling support
[sitara-epos/sitara-epos-kernel.git] / Documentation / stable_kernel_rules.txt
1 Everything you ever wanted to know about Linux 2.6 -stable releases.
3 Rules on what kind of patches are accepted, and which ones are not, into the
4 "-stable" tree:
6  - It must be obviously correct and tested.
7  - It cannot be bigger than 100 lines, with context.
8  - It must fix only one thing.
9  - It must fix a real bug that bothers people (not a, "This could be a
10    problem..." type thing).
11  - It must fix a problem that causes a build error (but not for things
12    marked CONFIG_BROKEN), an oops, a hang, data corruption, a real
13    security issue, or some "oh, that's not good" issue.  In short, something
14    critical.
15  - New device IDs and quirks are also accepted.
16  - No "theoretical race condition" issues, unless an explanation of how the
17    race can be exploited is also provided.
18  - It cannot contain any "trivial" fixes in it (spelling changes,
19    whitespace cleanups, etc).
20  - It must follow the Documentation/SubmittingPatches rules.
21  - It or an equivalent fix must already exist in Linus' tree (upstream).
24 Procedure for submitting patches to the -stable tree:
26  - Send the patch, after verifying that it follows the above rules, to
27    stable@vger.kernel.org.  You must note the upstream commit ID in the
28    changelog of your submission.
29  - To have the patch automatically included in the stable tree, add the tag
30      Cc: stable@vger.kernel.org
31    in the sign-off area. Once the patch is merged it will be applied to
32    the stable tree without anything else needing to be done by the author
33    or subsystem maintainer.
34  - If the patch requires other patches as prerequisites which can be
35    cherry-picked than this can be specified in the following format in
36    the sign-off area:
38      Cc: <stable@vger.kernel.org> # .32.x: a1f84a3: sched: Check for idle
39      Cc: <stable@vger.kernel.org> # .32.x: 1b9508f: sched: Rate-limit newidle
40      Cc: <stable@vger.kernel.org> # .32.x: fd21073: sched: Fix affinity logic
41      Cc: <stable@vger.kernel.org> # .32.x
42     Signed-off-by: Ingo Molnar <mingo@elte.hu>
44    The tag sequence has the meaning of:
45      git cherry-pick a1f84a3
46      git cherry-pick 1b9508f
47      git cherry-pick fd21073
48      git cherry-pick <this commit>
50  - The sender will receive an ACK when the patch has been accepted into the
51    queue, or a NAK if the patch is rejected.  This response might take a few
52    days, according to the developer's schedules.
53  - If accepted, the patch will be added to the -stable queue, for review by
54    other developers and by the relevant subsystem maintainer.
55  - Security patches should not be sent to this alias, but instead to the
56    documented security@kernel.org address.
59 Review cycle:
61  - When the -stable maintainers decide for a review cycle, the patches will be
62    sent to the review committee, and the maintainer of the affected area of
63    the patch (unless the submitter is the maintainer of the area) and CC: to
64    the linux-kernel mailing list.
65  - The review committee has 48 hours in which to ACK or NAK the patch.
66  - If the patch is rejected by a member of the committee, or linux-kernel
67    members object to the patch, bringing up issues that the maintainers and
68    members did not realize, the patch will be dropped from the queue.
69  - At the end of the review cycle, the ACKed patches will be added to the
70    latest -stable release, and a new -stable release will happen.
71  - Security patches will be accepted into the -stable tree directly from the
72    security kernel team, and not go through the normal review cycle.
73    Contact the kernel security team for more details on this procedure.
76 Review committee:
78  - This is made up of a number of kernel developers who have volunteered for
79    this task, and a few that haven't.