]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - README
eCAP:PWM: Add device driver support for eCAP module
[sitara-epos/sitara-epos-kernel.git] / README
1         Linux kernel release 3.x <http://kernel.org/>
3 These are the release notes for Linux version 3.  Read them carefully,
4 as they tell you what this is all about, explain how to install the
5 kernel, and what to do if something goes wrong. 
7 WHAT IS LINUX?
9   Linux is a clone of the operating system Unix, written from scratch by
10   Linus Torvalds with assistance from a loosely-knit team of hackers across
11   the Net. It aims towards POSIX and Single UNIX Specification compliance.
13   It has all the features you would expect in a modern fully-fledged Unix,
14   including true multitasking, virtual memory, shared libraries, demand
15   loading, shared copy-on-write executables, proper memory management,
16   and multistack networking including IPv4 and IPv6.
18   It is distributed under the GNU General Public License - see the
19   accompanying COPYING file for more details. 
21 ON WHAT HARDWARE DOES IT RUN?
23   Although originally developed first for 32-bit x86-based PCs (386 or higher),
24   today Linux also runs on (at least) the Compaq Alpha AXP, Sun SPARC and
25   UltraSPARC, Motorola 68000, PowerPC, PowerPC64, ARM, Hitachi SuperH, Cell,
26   IBM S/390, MIPS, HP PA-RISC, Intel IA-64, DEC VAX, AMD x86-64, AXIS CRIS,
27   Xtensa, Tilera TILE, AVR32 and Renesas M32R architectures.
29   Linux is easily portable to most general-purpose 32- or 64-bit architectures
30   as long as they have a paged memory management unit (PMMU) and a port of the
31   GNU C compiler (gcc) (part of The GNU Compiler Collection, GCC). Linux has
32   also been ported to a number of architectures without a PMMU, although
33   functionality is then obviously somewhat limited.
34   Linux has also been ported to itself. You can now run the kernel as a
35   userspace application - this is called UserMode Linux (UML).
37 DOCUMENTATION:
39  - There is a lot of documentation available both in electronic form on
40    the Internet and in books, both Linux-specific and pertaining to
41    general UNIX questions.  I'd recommend looking into the documentation
42    subdirectories on any Linux FTP site for the LDP (Linux Documentation
43    Project) books.  This README is not meant to be documentation on the
44    system: there are much better sources available.
46  - There are various README files in the Documentation/ subdirectory:
47    these typically contain kernel-specific installation notes for some 
48    drivers for example. See Documentation/00-INDEX for a list of what
49    is contained in each file.  Please read the Changes file, as it
50    contains information about the problems, which may result by upgrading
51    your kernel.
53  - The Documentation/DocBook/ subdirectory contains several guides for
54    kernel developers and users.  These guides can be rendered in a
55    number of formats:  PostScript (.ps), PDF, HTML, & man-pages, among others.
56    After installation, "make psdocs", "make pdfdocs", "make htmldocs",
57    or "make mandocs" will render the documentation in the requested format.
59 INSTALLING the kernel source:
61  - If you install the full sources, put the kernel tarball in a
62    directory where you have permissions (eg. your home directory) and
63    unpack it:
65                 gzip -cd linux-3.X.tar.gz | tar xvf -
67    or
68                 bzip2 -dc linux-3.X.tar.bz2 | tar xvf -
71    Replace "XX" with the version number of the latest kernel.
73    Do NOT use the /usr/src/linux area! This area has a (usually
74    incomplete) set of kernel headers that are used by the library header
75    files.  They should match the library, and not get messed up by
76    whatever the kernel-du-jour happens to be.
78  - You can also upgrade between 3.x releases by patching.  Patches are
79    distributed in the traditional gzip and the newer bzip2 format.  To
80    install by patching, get all the newer patch files, enter the
81    top level directory of the kernel source (linux-3.x) and execute:
83                 gzip -cd ../patch-3.x.gz | patch -p1
85    or
86                 bzip2 -dc ../patch-3.x.bz2 | patch -p1
88    (repeat xx for all versions bigger than the version of your current
89    source tree, _in_order_) and you should be ok.  You may want to remove
90    the backup files (xxx~ or xxx.orig), and make sure that there are no
91    failed patches (xxx# or xxx.rej). If there are, either you or me has
92    made a mistake.
94    Unlike patches for the 3.x kernels, patches for the 3.x.y kernels
95    (also known as the -stable kernels) are not incremental but instead apply
96    directly to the base 3.x kernel.  Please read
97    Documentation/applying-patches.txt for more information.
99    Alternatively, the script patch-kernel can be used to automate this
100    process.  It determines the current kernel version and applies any
101    patches found.
103                 linux/scripts/patch-kernel linux
105    The first argument in the command above is the location of the
106    kernel source.  Patches are applied from the current directory, but
107    an alternative directory can be specified as the second argument.
109  - If you are upgrading between releases using the stable series patches
110    (for example, patch-3.x.y), note that these "dot-releases" are
111    not incremental and must be applied to the 3.x base tree. For
112    example, if your base kernel is 3.0 and you want to apply the
113    3.0.3 patch, you do not and indeed must not first apply the
114    3.0.1 and 3.0.2 patches. Similarly, if you are running kernel
115    version 3.0.2 and want to jump to 3.0.3, you must first
116    reverse the 3.0.2 patch (that is, patch -R) _before_ applying
117    the 3.0.3 patch.
118    You can read more on this in Documentation/applying-patches.txt
120  - Make sure you have no stale .o files and dependencies lying around:
122                 cd linux
123                 make mrproper
125    You should now have the sources correctly installed.
127 SOFTWARE REQUIREMENTS
129    Compiling and running the 3.x kernels requires up-to-date
130    versions of various software packages.  Consult
131    Documentation/Changes for the minimum version numbers required
132    and how to get updates for these packages.  Beware that using
133    excessively old versions of these packages can cause indirect
134    errors that are very difficult to track down, so don't assume that
135    you can just update packages when obvious problems arise during
136    build or operation.
138 BUILD directory for the kernel:
140    When compiling the kernel all output files will per default be
141    stored together with the kernel source code.
142    Using the option "make O=output/dir" allow you to specify an alternate
143    place for the output files (including .config).
144    Example:
145      kernel source code:        /usr/src/linux-3.N
146      build directory:           /home/name/build/kernel
148    To configure and build the kernel use:
149    cd /usr/src/linux-3.N
150    make O=/home/name/build/kernel menuconfig
151    make O=/home/name/build/kernel
152    sudo make O=/home/name/build/kernel modules_install install
154    Please note: If the 'O=output/dir' option is used then it must be
155    used for all invocations of make.
157 CONFIGURING the kernel:
159    Do not skip this step even if you are only upgrading one minor
160    version.  New configuration options are added in each release, and
161    odd problems will turn up if the configuration files are not set up
162    as expected.  If you want to carry your existing configuration to a
163    new version with minimal work, use "make oldconfig", which will
164    only ask you for the answers to new questions.
166  - Alternate configuration commands are:
167         "make config"      Plain text interface.
168         "make menuconfig"  Text based color menus, radiolists & dialogs.
169         "make nconfig"     Enhanced text based color menus.
170         "make xconfig"     X windows (Qt) based configuration tool.
171         "make gconfig"     X windows (Gtk) based configuration tool.
172         "make oldconfig"   Default all questions based on the contents of
173                            your existing ./.config file and asking about
174                            new config symbols.
175         "make silentoldconfig"
176                            Like above, but avoids cluttering the screen
177                            with questions already answered.
178                            Additionally updates the dependencies.
179         "make defconfig"   Create a ./.config file by using the default
180                            symbol values from either arch/$ARCH/defconfig
181                            or arch/$ARCH/configs/${PLATFORM}_defconfig,
182                            depending on the architecture.
183         "make ${PLATFORM}_defconfig"
184                           Create a ./.config file by using the default
185                           symbol values from
186                           arch/$ARCH/configs/${PLATFORM}_defconfig.
187                           Use "make help" to get a list of all available
188                           platforms of your architecture.
189         "make allyesconfig"
190                            Create a ./.config file by setting symbol
191                            values to 'y' as much as possible.
192         "make allmodconfig"
193                            Create a ./.config file by setting symbol
194                            values to 'm' as much as possible.
195         "make allnoconfig" Create a ./.config file by setting symbol
196                            values to 'n' as much as possible.
197         "make randconfig"  Create a ./.config file by setting symbol
198                            values to random values.
200    You can find more information on using the Linux kernel config tools
201    in Documentation/kbuild/kconfig.txt.
203         NOTES on "make config":
204         - having unnecessary drivers will make the kernel bigger, and can
205           under some circumstances lead to problems: probing for a
206           nonexistent controller card may confuse your other controllers
207         - compiling the kernel with "Processor type" set higher than 386
208           will result in a kernel that does NOT work on a 386.  The
209           kernel will detect this on bootup, and give up.
210         - A kernel with math-emulation compiled in will still use the
211           coprocessor if one is present: the math emulation will just
212           never get used in that case.  The kernel will be slightly larger,
213           but will work on different machines regardless of whether they
214           have a math coprocessor or not. 
215         - the "kernel hacking" configuration details usually result in a
216           bigger or slower kernel (or both), and can even make the kernel
217           less stable by configuring some routines to actively try to
218           break bad code to find kernel problems (kmalloc()).  Thus you
219           should probably answer 'n' to the questions for
220           "development", "experimental", or "debugging" features.
222 COMPILING the kernel:
224  - Make sure you have at least gcc 3.2 available.
225    For more information, refer to Documentation/Changes.
227    Please note that you can still run a.out user programs with this kernel.
229  - Do a "make" to create a compressed kernel image. It is also
230    possible to do "make install" if you have lilo installed to suit the
231    kernel makefiles, but you may want to check your particular lilo setup first.
233    To do the actual install you have to be root, but none of the normal
234    build should require that. Don't take the name of root in vain.
236  - If you configured any of the parts of the kernel as `modules', you
237    will also have to do "make modules_install".
239  - Verbose kernel compile/build output:
241    Normally the kernel build system runs in a fairly quiet mode (but not
242    totally silent).  However, sometimes you or other kernel developers need
243    to see compile, link, or other commands exactly as they are executed.
244    For this, use "verbose" build mode.  This is done by inserting
245    "V=1" in the "make" command.  E.g.:
247         make V=1 all
249    To have the build system also tell the reason for the rebuild of each
250    target, use "V=2".  The default is "V=0".
252  - Keep a backup kernel handy in case something goes wrong.  This is 
253    especially true for the development releases, since each new release
254    contains new code which has not been debugged.  Make sure you keep a
255    backup of the modules corresponding to that kernel, as well.  If you
256    are installing a new kernel with the same version number as your
257    working kernel, make a backup of your modules directory before you
258    do a "make modules_install".
259    Alternatively, before compiling, use the kernel config option
260    "LOCALVERSION" to append a unique suffix to the regular kernel version.
261    LOCALVERSION can be set in the "General Setup" menu.
263  - In order to boot your new kernel, you'll need to copy the kernel
264    image (e.g. .../linux/arch/i386/boot/bzImage after compilation)
265    to the place where your regular bootable kernel is found. 
267  - Booting a kernel directly from a floppy without the assistance of a
268    bootloader such as LILO, is no longer supported.
270    If you boot Linux from the hard drive, chances are you use LILO which
271    uses the kernel image as specified in the file /etc/lilo.conf.  The
272    kernel image file is usually /vmlinuz, /boot/vmlinuz, /bzImage or
273    /boot/bzImage.  To use the new kernel, save a copy of the old image
274    and copy the new image over the old one.  Then, you MUST RERUN LILO
275    to update the loading map!! If you don't, you won't be able to boot
276    the new kernel image.
278    Reinstalling LILO is usually a matter of running /sbin/lilo. 
279    You may wish to edit /etc/lilo.conf to specify an entry for your
280    old kernel image (say, /vmlinux.old) in case the new one does not
281    work.  See the LILO docs for more information. 
283    After reinstalling LILO, you should be all set.  Shutdown the system,
284    reboot, and enjoy!
286    If you ever need to change the default root device, video mode,
287    ramdisk size, etc.  in the kernel image, use the 'rdev' program (or
288    alternatively the LILO boot options when appropriate).  No need to
289    recompile the kernel to change these parameters. 
291  - Reboot with the new kernel and enjoy. 
293 IF SOMETHING GOES WRONG:
295  - If you have problems that seem to be due to kernel bugs, please check
296    the file MAINTAINERS to see if there is a particular person associated
297    with the part of the kernel that you are having trouble with. If there
298    isn't anyone listed there, then the second best thing is to mail
299    them to me (torvalds@linux-foundation.org), and possibly to any other
300    relevant mailing-list or to the newsgroup.
302  - In all bug-reports, *please* tell what kernel you are talking about,
303    how to duplicate the problem, and what your setup is (use your common
304    sense).  If the problem is new, tell me so, and if the problem is
305    old, please try to tell me when you first noticed it.
307  - If the bug results in a message like
309         unable to handle kernel paging request at address C0000010
310         Oops: 0002
311         EIP:   0010:XXXXXXXX
312         eax: xxxxxxxx   ebx: xxxxxxxx   ecx: xxxxxxxx   edx: xxxxxxxx
313         esi: xxxxxxxx   edi: xxxxxxxx   ebp: xxxxxxxx
314         ds: xxxx  es: xxxx  fs: xxxx  gs: xxxx
315         Pid: xx, process nr: xx
316         xx xx xx xx xx xx xx xx xx xx
318    or similar kernel debugging information on your screen or in your
319    system log, please duplicate it *exactly*.  The dump may look
320    incomprehensible to you, but it does contain information that may
321    help debugging the problem.  The text above the dump is also
322    important: it tells something about why the kernel dumped code (in
323    the above example it's due to a bad kernel pointer). More information
324    on making sense of the dump is in Documentation/oops-tracing.txt
326  - If you compiled the kernel with CONFIG_KALLSYMS you can send the dump
327    as is, otherwise you will have to use the "ksymoops" program to make
328    sense of the dump (but compiling with CONFIG_KALLSYMS is usually preferred).
329    This utility can be downloaded from
330    ftp://ftp.<country>.kernel.org/pub/linux/utils/kernel/ksymoops/ .
331    Alternately you can do the dump lookup by hand:
333  - In debugging dumps like the above, it helps enormously if you can
334    look up what the EIP value means.  The hex value as such doesn't help
335    me or anybody else very much: it will depend on your particular
336    kernel setup.  What you should do is take the hex value from the EIP
337    line (ignore the "0010:"), and look it up in the kernel namelist to
338    see which kernel function contains the offending address.
340    To find out the kernel function name, you'll need to find the system
341    binary associated with the kernel that exhibited the symptom.  This is
342    the file 'linux/vmlinux'.  To extract the namelist and match it against
343    the EIP from the kernel crash, do:
345                 nm vmlinux | sort | less
347    This will give you a list of kernel addresses sorted in ascending
348    order, from which it is simple to find the function that contains the
349    offending address.  Note that the address given by the kernel
350    debugging messages will not necessarily match exactly with the
351    function addresses (in fact, that is very unlikely), so you can't
352    just 'grep' the list: the list will, however, give you the starting
353    point of each kernel function, so by looking for the function that
354    has a starting address lower than the one you are searching for but
355    is followed by a function with a higher address you will find the one
356    you want.  In fact, it may be a good idea to include a bit of
357    "context" in your problem report, giving a few lines around the
358    interesting one. 
360    If you for some reason cannot do the above (you have a pre-compiled
361    kernel image or similar), telling me as much about your setup as
362    possible will help.  Please read the REPORTING-BUGS document for details.
364  - Alternately, you can use gdb on a running kernel. (read-only; i.e. you
365    cannot change values or set break points.) To do this, first compile the
366    kernel with -g; edit arch/i386/Makefile appropriately, then do a "make
367    clean". You'll also need to enable CONFIG_PROC_FS (via "make config").
369    After you've rebooted with the new kernel, do "gdb vmlinux /proc/kcore".
370    You can now use all the usual gdb commands. The command to look up the
371    point where your system crashed is "l *0xXXXXXXXX". (Replace the XXXes
372    with the EIP value.)
374    gdb'ing a non-running kernel currently fails because gdb (wrongly)
375    disregards the starting offset for which the kernel is compiled.