1 menu "Kernel hacking"
3 source "lib/Kconfig.debug"
5 config STRICT_DEVMEM
6 bool "Filter access to /dev/mem"
7 depends on MMU
8 ---help---
9 If this option is disabled, you allow userspace (root) access to all
10 of memory, including kernel and userspace memory. Accidental
11 access to this is obviously disastrous, but specific access can
12 be used by people debugging the kernel.
14 If this option is switched on, the /dev/mem file only allows
15 userspace access to memory mapped peripherals.
17 If in doubt, say Y.
19 # RMK wants arm kernels compiled with frame pointers or stack unwinding.
20 # If you know what you are doing and are willing to live without stack
21 # traces, you can get a slightly smaller kernel by setting this option to
22 # n, but then RMK will have to kill you ;).
23 config FRAME_POINTER
24 bool
25 depends on !THUMB2_KERNEL
26 default y if !ARM_UNWIND || FUNCTION_GRAPH_TRACER
27 help
28 If you say N here, the resulting kernel will be slightly smaller and
29 faster. However, if neither FRAME_POINTER nor ARM_UNWIND are enabled,
30 when a problem occurs with the kernel, the information that is
31 reported is severely limited.
33 config ARM_UNWIND
34 bool "Enable stack unwinding support (EXPERIMENTAL)"
35 depends on AEABI && EXPERIMENTAL
36 default y
37 help
38 This option enables stack unwinding support in the kernel
39 using the information automatically generated by the
40 compiler. The resulting kernel image is slightly bigger but
41 the performance is not affected. Currently, this feature
42 only works with EABI compilers. If unsure say Y.
44 config OLD_MCOUNT
45 bool
46 depends on FUNCTION_TRACER && FRAME_POINTER
47 default y
49 config DEBUG_USER
50 bool "Verbose user fault messages"
51 help
52 When a user program crashes due to an exception, the kernel can
53 print a brief message explaining what the problem was. This is
54 sometimes helpful for debugging but serves no purpose on a
55 production system. Most people should say N here.
57 In addition, you need to pass user_debug=N on the kernel command
58 line to enable this feature. N consists of the sum of:
60 1 - undefined instruction events
61 2 - system calls
62 4 - invalid data aborts
63 8 - SIGSEGV faults
64 16 - SIGBUS faults
66 # These options are only for real kernel hackers who want to get their hands dirty.
67 config DEBUG_LL
68 bool "Kernel low-level debugging functions (read help!)"
69 depends on DEBUG_KERNEL
70 help
71 Say Y here to include definitions of printascii, printch, printhex
72 in the kernel. This is helpful if you are debugging code that
73 executes before the console is initialized.
75 Note that selecting this option will limit the kernel to a single
76 UART definition, as specified below. Attempting to boot the kernel
77 image on a different platform *will not work*, so this option should
78 not be enabled for kernels that are intended to be portable.
80 choice
81 prompt "Kernel low-level debugging port"
82 depends on DEBUG_LL
84 config DEBUG_LL_UART_NONE
85 bool "No low-level debugging UART"
86 help
87 Say Y here if your platform doesn't provide a UART option
88 below. This relies on your platform choosing the right UART
89 definition internally in order for low-level debugging to
90 work.
92 config DEBUG_ICEDCC
93 bool "Kernel low-level debugging via EmbeddedICE DCC channel"
94 help
95 Say Y here if you want the debug print routines to direct
96 their output to the EmbeddedICE macrocell's DCC channel using
97 co-processor 14. This is known to work on the ARM9 style ICE
98 channel and on the XScale with the PEEDI.
100 Note that the system will appear to hang during boot if there
101 is nothing connected to read from the DCC.
103 config DEBUG_FOOTBRIDGE_COM1
104 bool "Kernel low-level debugging messages via footbridge 8250 at PCI COM1"
105 depends on FOOTBRIDGE
106 help
107 Say Y here if you want the debug print routines to direct
108 their output to the 8250 at PCI COM1.
110 config DEBUG_DC21285_PORT
111 bool "Kernel low-level debugging messages via footbridge serial port"
112 depends on FOOTBRIDGE
113 help
114 Say Y here if you want the debug print routines to direct
115 their output to the serial port in the DC21285 (Footbridge).
117 config DEBUG_CLPS711X_UART1
118 bool "Kernel low-level debugging messages via UART1"
119 depends on ARCH_CLPS711X
120 help
121 Say Y here if you want the debug print routines to direct
122 their output to the first serial port on these devices.
124 config DEBUG_CLPS711X_UART2
125 bool "Kernel low-level debugging messages via UART2"
126 depends on ARCH_CLPS711X
127 help
128 Say Y here if you want the debug print routines to direct
129 their output to the second serial port on these devices.
131 config DEBUG_HIGHBANK_UART
132 bool "Kernel low-level debugging messages via Highbank UART"
133 depends on ARCH_HIGHBANK
134 help
135 Say Y here if you want the debug print routines to direct
136 their output to the UART on Highbank based devices.
138 config DEBUG_IMX1_UART
139 bool "i.MX1 Debug UART"
140 depends on SOC_IMX1
141 help
142 Say Y here if you want kernel low-level debugging support
143 on i.MX1.
145 config DEBUG_IMX23_UART
146 bool "i.MX23 Debug UART"
147 depends on SOC_IMX23
148 help
149 Say Y here if you want kernel low-level debugging support
150 on i.MX23.
152 config DEBUG_IMX25_UART
153 bool "i.MX25 Debug UART"
154 depends on SOC_IMX25
155 help
156 Say Y here if you want kernel low-level debugging support
157 on i.MX25.
159 config DEBUG_IMX21_IMX27_UART
160 bool "i.MX21 and i.MX27 Debug UART"
161 depends on SOC_IMX21 || SOC_IMX27
162 help
163 Say Y here if you want kernel low-level debugging support
164 on i.MX21 or i.MX27.
166 config DEBUG_IMX28_UART
167 bool "i.MX28 Debug UART"
168 depends on SOC_IMX28
169 help
170 Say Y here if you want kernel low-level debugging support
171 on i.MX28.
173 config DEBUG_IMX31_IMX35_UART
174 bool "i.MX31 and i.MX35 Debug UART"
175 depends on SOC_IMX31 || SOC_IMX35
176 help
177 Say Y here if you want kernel low-level debugging support
178 on i.MX31 or i.MX35.
180 config DEBUG_IMX51_UART
181 bool "i.MX51 Debug UART"
182 depends on SOC_IMX51
183 help
184 Say Y here if you want kernel low-level debugging support
185 on i.MX51.
187 config DEBUG_IMX50_IMX53_UART
188 bool "i.MX50 and i.MX53 Debug UART"
189 depends on SOC_IMX50 || SOC_IMX53
190 help
191 Say Y here if you want kernel low-level debugging support
192 on i.MX50 or i.MX53.
194 config DEBUG_IMX6Q_UART
195 bool "i.MX6Q Debug UART"
196 depends on SOC_IMX6Q
197 help
198 Say Y here if you want kernel low-level debugging support
199 on i.MX6Q.
201 config DEBUG_S3C_UART0
202 depends on PLAT_SAMSUNG
203 bool "Use S3C UART 0 for low-level debug"
204 help
205 Say Y here if you want the debug print routines to direct
206 their output to UART 0. The port must have been initialised
207 by the boot-loader before use.
209 The uncompressor code port configuration is now handled
210 by CONFIG_S3C_LOWLEVEL_UART_PORT.
212 config DEBUG_S3C_UART1
213 depends on PLAT_SAMSUNG
214 bool "Use S3C UART 1 for low-level debug"
215 help
216 Say Y here if you want the debug print routines to direct
217 their output to UART 1. The port must have been initialised
218 by the boot-loader before use.
220 The uncompressor code port configuration is now handled
221 by CONFIG_S3C_LOWLEVEL_UART_PORT.
223 config DEBUG_S3C_UART2
224 depends on PLAT_SAMSUNG
225 bool "Use S3C UART 2 for low-level debug"
226 help
227 Say Y here if you want the debug print routines to direct
228 their output to UART 2. The port must have been initialised
229 by the boot-loader before use.
231 The uncompressor code port configuration is now handled
232 by CONFIG_S3C_LOWLEVEL_UART_PORT.
234 config DEBUG_REALVIEW_STD_PORT
235 bool "RealView Default UART"
236 depends on ARCH_REALVIEW
237 help
238 Say Y here if you want the debug print routines to direct
239 their output to the serial port on RealView EB, PB11MP, PBA8
240 and PBX platforms.
242 config DEBUG_REALVIEW_PB1176_PORT
243 bool "RealView PB1176 UART"
244 depends on MACH_REALVIEW_PB1176
245 help
246 Say Y here if you want the debug print routines to direct
247 their output to the standard serial port on the RealView
248 PB1176 platform.
250 endchoice
252 config EARLY_PRINTK
253 bool "Early printk"
254 depends on DEBUG_LL
255 help
256 Say Y here if you want to have an early console using the
257 kernel low-level debugging functions. Add earlyprintk to your
258 kernel parameters to enable this console.
260 config OC_ETM
261 bool "On-chip ETM and ETB"
262 depends on ARM_AMBA
263 help
264 Enables the on-chip embedded trace macrocell and embedded trace
265 buffer driver that will allow you to collect traces of the
266 kernel code.
268 config ARM_KPROBES_TEST
269 tristate "Kprobes test module"
270 depends on KPROBES && MODULES
271 help
272 Perform tests of kprobes API and instruction set simulation.
274 endmenu