]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - arch/arm/Kconfig.debug
Merge branch 'kconfig' of git://git.kernel.org/pub/scm/linux/kernel/git/mmarek/kbuild
[sitara-epos/sitara-epos-kernel.git] / arch / arm / Kconfig.debug
1 menu "Kernel hacking"
3 source "lib/Kconfig.debug"
5 config STRICT_DEVMEM
6         bool "Filter access to /dev/mem"
7         depends on MMU
8         ---help---
9           If this option is disabled, you allow userspace (root) access to all
10           of memory, including kernel and userspace memory. Accidental
11           access to this is obviously disastrous, but specific access can
12           be used by people debugging the kernel.
14           If this option is switched on, the /dev/mem file only allows
15           userspace access to memory mapped peripherals.
17           If in doubt, say Y.
19 # RMK wants arm kernels compiled with frame pointers or stack unwinding.
20 # If you know what you are doing and are willing to live without stack
21 # traces, you can get a slightly smaller kernel by setting this option to
22 # n, but then RMK will have to kill you ;).
23 config FRAME_POINTER
24         bool
25         depends on !THUMB2_KERNEL
26         default y if !ARM_UNWIND || FUNCTION_GRAPH_TRACER
27         help
28           If you say N here, the resulting kernel will be slightly smaller and
29           faster. However, if neither FRAME_POINTER nor ARM_UNWIND are enabled,
30           when a problem occurs with the kernel, the information that is
31           reported is severely limited.
33 config ARM_UNWIND
34         bool "Enable stack unwinding support (EXPERIMENTAL)"
35         depends on AEABI && EXPERIMENTAL
36         default y
37         help
38           This option enables stack unwinding support in the kernel
39           using the information automatically generated by the
40           compiler. The resulting kernel image is slightly bigger but
41           the performance is not affected. Currently, this feature
42           only works with EABI compilers. If unsure say Y.
44 config OLD_MCOUNT
45         bool
46         depends on FUNCTION_TRACER && FRAME_POINTER
47         default y
49 config DEBUG_USER
50         bool "Verbose user fault messages"
51         help
52           When a user program crashes due to an exception, the kernel can
53           print a brief message explaining what the problem was. This is
54           sometimes helpful for debugging but serves no purpose on a
55           production system. Most people should say N here.
57           In addition, you need to pass user_debug=N on the kernel command
58           line to enable this feature.  N consists of the sum of:
60               1 - undefined instruction events
61               2 - system calls
62               4 - invalid data aborts
63               8 - SIGSEGV faults
64              16 - SIGBUS faults
66 # These options are only for real kernel hackers who want to get their hands dirty.
67 config DEBUG_LL
68         bool "Kernel low-level debugging functions (read help!)"
69         depends on DEBUG_KERNEL
70         help
71           Say Y here to include definitions of printascii, printch, printhex
72           in the kernel.  This is helpful if you are debugging code that
73           executes before the console is initialized.
75           Note that selecting this option will limit the kernel to a single
76           UART definition, as specified below. Attempting to boot the kernel
77           image on a different platform *will not work*, so this option should
78           not be enabled for kernels that are intended to be portable.
80 choice
81         prompt "Kernel low-level debugging port"
82         depends on DEBUG_LL
84         config DEBUG_LL_UART_NONE
85                 bool "No low-level debugging UART"
86                 help
87                   Say Y here if your platform doesn't provide a UART option
88                   below. This relies on your platform choosing the right UART
89                   definition internally in order for low-level debugging to
90                   work.
92         config DEBUG_ICEDCC
93                 bool "Kernel low-level debugging via EmbeddedICE DCC channel"
94                 help
95                   Say Y here if you want the debug print routines to direct
96                   their output to the EmbeddedICE macrocell's DCC channel using
97                   co-processor 14. This is known to work on the ARM9 style ICE
98                   channel and on the XScale with the PEEDI.
100                   Note that the system will appear to hang during boot if there
101                   is nothing connected to read from the DCC.
103         config DEBUG_FOOTBRIDGE_COM1
104                 bool "Kernel low-level debugging messages via footbridge 8250 at PCI COM1"
105                 depends on FOOTBRIDGE
106                 help
107                   Say Y here if you want the debug print routines to direct
108                   their output to the 8250 at PCI COM1.
110         config DEBUG_DC21285_PORT
111                 bool "Kernel low-level debugging messages via footbridge serial port"
112                 depends on FOOTBRIDGE
113                 help
114                   Say Y here if you want the debug print routines to direct
115                   their output to the serial port in the DC21285 (Footbridge).
117         config DEBUG_CLPS711X_UART1
118                 bool "Kernel low-level debugging messages via UART1"
119                 depends on ARCH_CLPS711X
120                 help
121                   Say Y here if you want the debug print routines to direct
122                   their output to the first serial port on these devices.
124         config DEBUG_CLPS711X_UART2
125                 bool "Kernel low-level debugging messages via UART2"
126                 depends on ARCH_CLPS711X
127                 help
128                   Say Y here if you want the debug print routines to direct
129                   their output to the second serial port on these devices.
131         config DEBUG_HIGHBANK_UART
132                 bool "Kernel low-level debugging messages via Highbank UART"
133                 depends on ARCH_HIGHBANK
134                 help
135                   Say Y here if you want the debug print routines to direct
136                   their output to the UART on Highbank based devices.
138         config DEBUG_IMX1_UART
139                 bool "i.MX1 Debug UART"
140                 depends on SOC_IMX1
141                 help
142                   Say Y here if you want kernel low-level debugging support
143                   on i.MX1.
145         config DEBUG_IMX23_UART
146                 bool "i.MX23 Debug UART"
147                 depends on SOC_IMX23
148                 help
149                   Say Y here if you want kernel low-level debugging support
150                   on i.MX23.
152         config DEBUG_IMX25_UART
153                 bool "i.MX25 Debug UART"
154                 depends on SOC_IMX25
155                 help
156                   Say Y here if you want kernel low-level debugging support
157                   on i.MX25.
159         config DEBUG_IMX21_IMX27_UART
160                 bool "i.MX21 and i.MX27 Debug UART"
161                 depends on SOC_IMX21 || SOC_IMX27
162                 help
163                   Say Y here if you want kernel low-level debugging support
164                   on i.MX21 or i.MX27.
166         config DEBUG_IMX28_UART
167                 bool "i.MX28 Debug UART"
168                 depends on SOC_IMX28
169                 help
170                   Say Y here if you want kernel low-level debugging support
171                   on i.MX28.
173         config DEBUG_IMX31_IMX35_UART
174                 bool "i.MX31 and i.MX35 Debug UART"
175                 depends on SOC_IMX31 || SOC_IMX35
176                 help
177                   Say Y here if you want kernel low-level debugging support
178                   on i.MX31 or i.MX35.
180         config DEBUG_IMX51_UART
181                 bool "i.MX51 Debug UART"
182                 depends on SOC_IMX51
183                 help
184                   Say Y here if you want kernel low-level debugging support
185                   on i.MX51.
187         config DEBUG_IMX50_IMX53_UART
188                 bool "i.MX50 and i.MX53 Debug UART"
189                 depends on SOC_IMX50 || SOC_IMX53
190                 help
191                   Say Y here if you want kernel low-level debugging support
192                   on i.MX50 or i.MX53.
194         config DEBUG_IMX6Q_UART
195                 bool "i.MX6Q Debug UART"
196                 depends on SOC_IMX6Q
197                 help
198                   Say Y here if you want kernel low-level debugging support
199                   on i.MX6Q.
201         config DEBUG_S3C_UART0
202                 depends on PLAT_SAMSUNG
203                 bool "Use S3C UART 0 for low-level debug"
204                 help
205                   Say Y here if you want the debug print routines to direct
206                   their output to UART 0. The port must have been initialised
207                   by the boot-loader before use.
209                   The uncompressor code port configuration is now handled
210                   by CONFIG_S3C_LOWLEVEL_UART_PORT.
212         config DEBUG_S3C_UART1
213                 depends on PLAT_SAMSUNG
214                 bool "Use S3C UART 1 for low-level debug"
215                 help
216                   Say Y here if you want the debug print routines to direct
217                   their output to UART 1. The port must have been initialised
218                   by the boot-loader before use.
220                   The uncompressor code port configuration is now handled
221                   by CONFIG_S3C_LOWLEVEL_UART_PORT.
223         config DEBUG_S3C_UART2
224                 depends on PLAT_SAMSUNG
225                 bool "Use S3C UART 2 for low-level debug"
226                 help
227                   Say Y here if you want the debug print routines to direct
228                   their output to UART 2. The port must have been initialised
229                   by the boot-loader before use.
231                   The uncompressor code port configuration is now handled
232                   by CONFIG_S3C_LOWLEVEL_UART_PORT.
234         config DEBUG_REALVIEW_STD_PORT
235                 bool "RealView Default UART"
236                 depends on ARCH_REALVIEW
237                 help
238                   Say Y here if you want the debug print routines to direct
239                   their output to the serial port on RealView EB, PB11MP, PBA8
240                   and PBX platforms.
242         config DEBUG_REALVIEW_PB1176_PORT
243                 bool "RealView PB1176 UART"
244                 depends on MACH_REALVIEW_PB1176
245                 help
246                   Say Y here if you want the debug print routines to direct
247                   their output to the standard serial port on the RealView
248                   PB1176 platform.
250 endchoice
252 config EARLY_PRINTK
253         bool "Early printk"
254         depends on DEBUG_LL
255         help
256           Say Y here if you want to have an early console using the
257           kernel low-level debugging functions. Add earlyprintk to your
258           kernel parameters to enable this console.
260 config OC_ETM
261         bool "On-chip ETM and ETB"
262         depends on ARM_AMBA
263         help
264           Enables the on-chip embedded trace macrocell and embedded trace
265           buffer driver that will allow you to collect traces of the
266           kernel code.
268 config ARM_KPROBES_TEST
269         tristate "Kprobes test module"
270         depends on KPROBES && MODULES
271         help
272           Perform tests of kprobes API and instruction set simulation.
274 endmenu