]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - arch/arm/configs/pcontrol_g20_defconfig
arm:omap:am33xx: Enable cpuidle in the defconfig
[sitara-epos/sitara-epos-kernel.git] / arch / arm / configs / pcontrol_g20_defconfig
1 CONFIG_EXPERIMENTAL=y
2 CONFIG_CROSS_COMPILE="/opt/arm-2010q1/bin/arm-none-linux-gnueabi-"
3 # CONFIG_LOCALVERSION_AUTO is not set
4 # CONFIG_SWAP is not set
5 CONFIG_SYSVIPC=y
6 CONFIG_POSIX_MQUEUE=y
7 CONFIG_TREE_PREEMPT_RCU=y
8 CONFIG_IKCONFIG=y
9 CONFIG_IKCONFIG_PROC=y
10 CONFIG_LOG_BUF_SHIFT=14
11 CONFIG_NAMESPACES=y
12 CONFIG_BLK_DEV_INITRD=y
13 CONFIG_EXPERT=y
14 # CONFIG_SYSCTL_SYSCALL is not set
15 # CONFIG_KALLSYMS is not set
16 # CONFIG_VM_EVENT_COUNTERS is not set
17 # CONFIG_COMPAT_BRK is not set
18 CONFIG_SLAB=y
19 CONFIG_MODULES=y
20 CONFIG_MODULE_UNLOAD=y
21 # CONFIG_LBDAF is not set
22 # CONFIG_BLK_DEV_BSG is not set
23 CONFIG_DEFAULT_DEADLINE=y
24 CONFIG_ARCH_AT91=y
25 CONFIG_ARCH_AT91SAM9G20=y
26 CONFIG_MACH_PCONTROL_G20=y
27 CONFIG_AT91_PROGRAMMABLE_CLOCKS=y
28 CONFIG_NO_HZ=y
29 CONFIG_HIGH_RES_TIMERS=y
30 CONFIG_PREEMPT=y
31 CONFIG_AEABI=y
32 # CONFIG_OABI_COMPAT is not set
33 CONFIG_ZBOOT_ROM_TEXT=0x0
34 CONFIG_ZBOOT_ROM_BSS=0x0
35 CONFIG_CMDLINE="console=ttyS0,115200 mem=128M mtdparts=atmel_nand:128k(bootstrap)ro,256k(uboot)ro,128k(env1)ro,128k(env2)ro,2M(linux),-(root) root=/dev/mmcblk0p1 rootwait rw"
36 CONFIG_VFP=y
37 CONFIG_BINFMT_MISC=y
38 CONFIG_NET=y
39 CONFIG_PACKET=y
40 CONFIG_UNIX=y
41 CONFIG_INET=y
42 # CONFIG_INET_XFRM_MODE_TRANSPORT is not set
43 # CONFIG_INET_XFRM_MODE_TUNNEL is not set
44 # CONFIG_INET_XFRM_MODE_BEET is not set
45 # CONFIG_INET_LRO is not set
46 # CONFIG_IPV6 is not set
47 CONFIG_VLAN_8021Q=y
48 # CONFIG_WIRELESS is not set
49 CONFIG_UEVENT_HELPER_PATH="/sbin/hotplug"
50 # CONFIG_FW_LOADER is not set
51 CONFIG_MTD=y
52 CONFIG_MTD_PARTITIONS=y
53 CONFIG_MTD_CMDLINE_PARTS=y
54 CONFIG_MTD_CHAR=y
55 CONFIG_MTD_BLOCK=y
56 CONFIG_MTD_COMPLEX_MAPPINGS=y
57 CONFIG_MTD_PHRAM=m
58 CONFIG_MTD_NAND=y
59 CONFIG_MTD_NAND_ATMEL=y
60 CONFIG_BLK_DEV_LOOP=y
61 CONFIG_BLK_DEV_RAM=y
62 CONFIG_BLK_DEV_RAM_SIZE=8192
63 CONFIG_ATMEL_TCLIB=y
64 CONFIG_EEPROM_AT24=m
65 CONFIG_SCSI=m
66 # CONFIG_SCSI_PROC_FS is not set
67 CONFIG_BLK_DEV_SD=m
68 CONFIG_SCSI_MULTI_LUN=y
69 # CONFIG_SCSI_LOWLEVEL is not set
70 CONFIG_NETDEVICES=y
71 CONFIG_MACVLAN=m
72 CONFIG_TUN=m
73 CONFIG_SMSC_PHY=m
74 CONFIG_BROADCOM_PHY=m
75 CONFIG_NET_ETHERNET=y
76 CONFIG_MII=y
77 CONFIG_MACB=y
78 CONFIG_SMSC911X=m
79 # CONFIG_NETDEV_1000 is not set
80 # CONFIG_NETDEV_10000 is not set
81 # CONFIG_WLAN is not set
82 CONFIG_PPP=m
83 CONFIG_PPP_ASYNC=m
84 CONFIG_PPP_DEFLATE=m
85 CONFIG_PPP_MPPE=m
86 CONFIG_INPUT_POLLDEV=y
87 CONFIG_INPUT_SPARSEKMAP=y
88 # CONFIG_INPUT_MOUSEDEV is not set
89 CONFIG_INPUT_EVDEV=m
90 CONFIG_INPUT_EVBUG=m
91 # CONFIG_KEYBOARD_ATKBD is not set
92 CONFIG_KEYBOARD_GPIO=m
93 CONFIG_KEYBOARD_MATRIX=m
94 # CONFIG_INPUT_MOUSE is not set
95 CONFIG_INPUT_TOUCHSCREEN=y
96 CONFIG_INPUT_MISC=y
97 CONFIG_INPUT_UINPUT=m
98 CONFIG_INPUT_GPIO_ROTARY_ENCODER=m
99 # CONFIG_SERIO is not set
100 # CONFIG_DEVKMEM is not set
101 CONFIG_SERIAL_ATMEL=y
102 CONFIG_SERIAL_ATMEL_CONSOLE=y
103 CONFIG_SERIAL_MAX3100=m
104 # CONFIG_LEGACY_PTYS is not set
105 # CONFIG_HW_RANDOM is not set
106 CONFIG_R3964=m
107 CONFIG_I2C=m
108 CONFIG_I2C_CHARDEV=m
109 # CONFIG_I2C_HELPER_AUTO is not set
110 CONFIG_I2C_GPIO=m
111 CONFIG_SPI=y
112 CONFIG_SPI_ATMEL=m
113 CONFIG_SPI_SPIDEV=m
114 CONFIG_GPIO_SYSFS=y
115 CONFIG_W1=m
116 CONFIG_W1_MASTER_GPIO=m
117 CONFIG_W1_SLAVE_DS2431=m
118 # CONFIG_HWMON is not set
119 CONFIG_WATCHDOG=y
120 CONFIG_AT91SAM9X_WATCHDOG=y
121 # CONFIG_MFD_SUPPORT is not set
122 # CONFIG_HID_SUPPORT is not set
123 CONFIG_USB=y
124 # CONFIG_USB_DEVICE_CLASS is not set
125 CONFIG_USB_OHCI_HCD=y
126 CONFIG_USB_STORAGE=m
127 CONFIG_USB_LIBUSUAL=y
128 CONFIG_USB_SERIAL=m
129 CONFIG_USB_SERIAL_GENERIC=y
130 CONFIG_USB_SERIAL_FTDI_SIO=m
131 CONFIG_USB_SERIAL_PL2303=m
132 CONFIG_USB_GADGET=y
133 CONFIG_USB_ZERO=m
134 CONFIG_USB_ETH=m
135 CONFIG_USB_FILE_STORAGE=m
136 CONFIG_USB_G_SERIAL=m
137 CONFIG_USB_G_HID=m
138 CONFIG_MMC=y
139 CONFIG_MMC_UNSAFE_RESUME=y
140 CONFIG_MMC_ATMELMCI=y
141 CONFIG_NEW_LEDS=y
142 CONFIG_LEDS_CLASS=y
143 CONFIG_LEDS_GPIO=y
144 CONFIG_LEDS_TRIGGERS=y
145 CONFIG_LEDS_TRIGGER_TIMER=y
146 CONFIG_LEDS_TRIGGER_HEARTBEAT=y
147 CONFIG_LEDS_TRIGGER_DEFAULT_ON=y
148 CONFIG_RTC_CLASS=y
149 CONFIG_RTC_DRV_AT91SAM9=y
150 CONFIG_AUXDISPLAY=y
151 CONFIG_UIO=y
152 CONFIG_UIO_PDRV=y
153 CONFIG_STAGING=y
154 # CONFIG_STAGING_EXCLUDE_BUILD is not set
155 CONFIG_IIO=y
156 CONFIG_EXT2_FS=y
157 CONFIG_EXT3_FS=y
158 # CONFIG_EXT3_FS_XATTR is not set
159 CONFIG_VFAT_FS=y
160 CONFIG_TMPFS=y
161 CONFIG_JFFS2_FS=y
162 CONFIG_NFS_FS=y
163 CONFIG_NFS_V3=y
164 CONFIG_NFS_V4=y
165 CONFIG_PARTITION_ADVANCED=y
166 CONFIG_NLS_CODEPAGE_437=y
167 CONFIG_NLS_CODEPAGE_850=y
168 CONFIG_NLS_ISO8859_1=y
169 CONFIG_NLS_ISO8859_15=y
170 CONFIG_NLS_UTF8=y
171 # CONFIG_RCU_CPU_STALL_DETECTOR is not set
172 CONFIG_CRYPTO=y
173 CONFIG_CRYPTO_ANSI_CPRNG=y
174 # CONFIG_CRYPTO_HW is not set
175 CONFIG_CRC_CCITT=y