]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - arch/arm/configs/stamp9g20_defconfig
arm:omap:am33xx: Enable cpuidle in the defconfig
[sitara-epos/sitara-epos-kernel.git] / arch / arm / configs / stamp9g20_defconfig
1 CONFIG_EXPERIMENTAL=y
2 # CONFIG_LOCALVERSION_AUTO is not set
3 # CONFIG_SWAP is not set
4 CONFIG_SYSVIPC=y
5 CONFIG_TREE_PREEMPT_RCU=y
6 CONFIG_LOG_BUF_SHIFT=14
7 CONFIG_BLK_DEV_INITRD=y
8 CONFIG_SLAB=y
9 CONFIG_MODULES=y
10 CONFIG_MODULE_UNLOAD=y
11 # CONFIG_LBDAF is not set
12 # CONFIG_BLK_DEV_BSG is not set
13 # CONFIG_IOSCHED_DEADLINE is not set
14 CONFIG_ARCH_AT91=y
15 CONFIG_ARCH_AT91SAM9G20=y
16 CONFIG_MACH_PORTUXG20=y
17 CONFIG_MACH_STAMP9G20=y
18 CONFIG_AT91_PROGRAMMABLE_CLOCKS=y
19 CONFIG_AT91_SLOW_CLOCK=y
20 CONFIG_NO_HZ=y
21 CONFIG_HIGH_RES_TIMERS=y
22 CONFIG_PREEMPT=y
23 CONFIG_AEABI=y
24 # CONFIG_OABI_COMPAT is not set
25 CONFIG_ZBOOT_ROM_TEXT=0x0
26 CONFIG_ZBOOT_ROM_BSS=0x0
27 CONFIG_CMDLINE="mem=64M console=ttyS0,115200 initrd=0x21100000,3145728 root=/dev/ram0 rw"
28 CONFIG_KEXEC=y
29 CONFIG_CPU_IDLE=y
30 CONFIG_PM=y
31 CONFIG_NET=y
32 CONFIG_PACKET=y
33 CONFIG_UNIX=y
34 CONFIG_INET=y
35 # CONFIG_INET_XFRM_MODE_TRANSPORT is not set
36 # CONFIG_INET_XFRM_MODE_TUNNEL is not set
37 # CONFIG_INET_XFRM_MODE_BEET is not set
38 # CONFIG_INET_LRO is not set
39 # CONFIG_IPV6 is not set
40 # CONFIG_WIRELESS is not set
41 CONFIG_UEVENT_HELPER_PATH="/sbin/hotplug"
42 CONFIG_MTD=y
43 CONFIG_MTD_CONCAT=y
44 CONFIG_MTD_PARTITIONS=y
45 CONFIG_MTD_CMDLINE_PARTS=y
46 CONFIG_MTD_CHAR=y
47 CONFIG_MTD_BLOCK=y
48 CONFIG_MTD_DATAFLASH=y
49 CONFIG_MTD_NAND=y
50 CONFIG_MTD_NAND_ATMEL=y
51 CONFIG_BLK_DEV_LOOP=y
52 CONFIG_BLK_DEV_RAM=y
53 CONFIG_BLK_DEV_RAM_SIZE=8192
54 # CONFIG_MISC_DEVICES is not set
55 CONFIG_SCSI=y
56 CONFIG_BLK_DEV_SD=y
57 CONFIG_SCSI_MULTI_LUN=y
58 # CONFIG_SCSI_LOWLEVEL is not set
59 CONFIG_NETDEVICES=y
60 CONFIG_NET_ETHERNET=y
61 CONFIG_MACB=y
62 # CONFIG_NETDEV_1000 is not set
63 # CONFIG_NETDEV_10000 is not set
64 # CONFIG_WLAN is not set
65 # CONFIG_INPUT_MOUSEDEV_PSAUX is not set
66 CONFIG_INPUT_MOUSEDEV_SCREEN_X=320
67 CONFIG_INPUT_MOUSEDEV_SCREEN_Y=240
68 # CONFIG_INPUT_KEYBOARD is not set
69 # CONFIG_INPUT_MOUSE is not set
70 # CONFIG_SERIO is not set
71 CONFIG_SERIAL_ATMEL=y
72 CONFIG_SERIAL_ATMEL_CONSOLE=y
73 # CONFIG_LEGACY_PTYS is not set
74 # CONFIG_HW_RANDOM is not set
75 CONFIG_I2C=y
76 CONFIG_I2C_CHARDEV=y
77 CONFIG_I2C_GPIO=y
78 CONFIG_SPI=y
79 CONFIG_SPI_ATMEL=y
80 CONFIG_SPI_SPIDEV=y
81 CONFIG_GPIO_SYSFS=y
82 CONFIG_W1=y
83 CONFIG_W1_MASTER_GPIO=y
84 CONFIG_W1_SLAVE_THERM=y
85 CONFIG_W1_SLAVE_DS2431=y
86 # CONFIG_HWMON is not set
87 CONFIG_WATCHDOG=y
88 CONFIG_AT91SAM9X_WATCHDOG=y
89 # CONFIG_VGA_CONSOLE is not set
90 # CONFIG_HID_SUPPORT is not set
91 CONFIG_USB=y
92 CONFIG_USB_DEVICEFS=y
93 # CONFIG_USB_DEVICE_CLASS is not set
94 CONFIG_USB_MON=y
95 CONFIG_USB_OHCI_HCD=y
96 CONFIG_USB_STORAGE=y
97 CONFIG_USB_GADGET=m
98 CONFIG_USB_ZERO=m
99 CONFIG_USB_ETH=m
100 CONFIG_USB_FILE_STORAGE=m
101 CONFIG_USB_G_SERIAL=m
102 CONFIG_MMC=y
103 # CONFIG_MMC_AT91 is not set
104 CONFIG_MMC_ATMELMCI=y
105 CONFIG_NEW_LEDS=y
106 CONFIG_LEDS_CLASS=y
107 CONFIG_LEDS_GPIO=y
108 CONFIG_LEDS_TRIGGERS=y
109 CONFIG_LEDS_TRIGGER_TIMER=y
110 CONFIG_LEDS_TRIGGER_HEARTBEAT=y
111 CONFIG_LEDS_TRIGGER_DEFAULT_ON=y
112 CONFIG_RTC_CLASS=y
113 CONFIG_RTC_DRV_AT91SAM9=y
114 CONFIG_EXT2_FS=y
115 CONFIG_EXT3_FS=y
116 CONFIG_INOTIFY=y
117 CONFIG_VFAT_FS=y
118 CONFIG_TMPFS=y
119 CONFIG_JFFS2_FS=y
120 CONFIG_JFFS2_SUMMARY=y
121 CONFIG_NFS_FS=y
122 CONFIG_NFS_V3=y
123 CONFIG_NLS_CODEPAGE_437=y
124 CONFIG_NLS_CODEPAGE_850=y
125 CONFIG_NLS_ISO8859_1=y
126 CONFIG_NLS_ISO8859_15=y
127 CONFIG_NLS_UTF8=y
128 # CONFIG_RCU_CPU_STALL_DETECTOR is not set
129 # CONFIG_ARM_UNWIND is not set