1 /*
2 * OMAP2xxx DVFS virtual clock functions
3 *
4 * Copyright (C) 2005-2008 Texas Instruments, Inc.
5 * Copyright (C) 2004-2010 Nokia Corporation
6 *
7 * Contacts:
8 * Richard Woodruff <r-woodruff2@ti.com>
9 * Paul Walmsley
10 *
11 * Based on earlier work by Tuukka Tikkanen, Tony Lindgren,
12 * Gordon McNutt and RidgeRun, Inc.
13 *
14 * This program is free software; you can redistribute it and/or modify
15 * it under the terms of the GNU General Public License version 2 as
16 * published by the Free Software Foundation.
17 *
18 * XXX Some of this code should be replaceable by the upcoming OPP layer
19 * code. However, some notion of "rate set" is probably still necessary
20 * for OMAP2xxx at least. Rate sets should be generalized so they can be
21 * used for any OMAP chip, not just OMAP2xxx. In particular, Richard Woodruff
22 * has in the past expressed a preference to use rate sets for OPP changes,
23 * rather than dynamically recalculating the clock tree, so if someone wants
24 * this badly enough to write the code to handle it, we should support it
25 * as an option.
26 */
27 #undef DEBUG
29 #include <linux/kernel.h>
30 #include <linux/errno.h>
31 #include <linux/clk.h>
32 #include <linux/io.h>
33 #include <linux/cpufreq.h>
34 #include <linux/slab.h>
36 #include <plat/clock.h>
37 #include <plat/sram.h>
38 #include <plat/sdrc.h>
40 #include "clock.h"
41 #include "clock2xxx.h"
42 #include "opp2xxx.h"
43 #include "cm2xxx_3xxx.h"
44 #include "cm-regbits-24xx.h"
46 const struct prcm_config *curr_prcm_set;
47 const struct prcm_config *rate_table;
49 /**
50 * omap2_table_mpu_recalc - just return the MPU speed
51 * @clk: virt_prcm_set struct clk
52 *
53 * Set virt_prcm_set's rate to the mpu_speed field of the current PRCM set.
54 */
55 unsigned long omap2_table_mpu_recalc(struct clk *clk)
56 {
57 return curr_prcm_set->mpu_speed;
58 }
60 /*
61 * Look for a rate equal or less than the target rate given a configuration set.
62 *
63 * What's not entirely clear is "which" field represents the key field.
64 * Some might argue L3-DDR, others ARM, others IVA. This code is simple and
65 * just uses the ARM rates.
66 */
67 long omap2_round_to_table_rate(struct clk *clk, unsigned long rate)
68 {
69 const struct prcm_config *ptr;
70 long highest_rate;
72 highest_rate = -EINVAL;
74 for (ptr = rate_table; ptr->mpu_speed; ptr++) {
75 if (!(ptr->flags & cpu_mask))
76 continue;
77 if (ptr->xtal_speed != sclk->rate)
78 continue;
80 highest_rate = ptr->mpu_speed;
82 /* Can check only after xtal frequency check */
83 if (ptr->mpu_speed <= rate)
84 break;
85 }
86 return highest_rate;
87 }
89 /* Sets basic clocks based on the specified rate */
90 int omap2_select_table_rate(struct clk *clk, unsigned long rate)
91 {
92 u32 cur_rate, done_rate, bypass = 0, tmp;
93 const struct prcm_config *prcm;
94 unsigned long found_speed = 0;
95 unsigned long flags;
97 for (prcm = rate_table; prcm->mpu_speed; prcm++) {
98 if (!(prcm->flags & cpu_mask))
99 continue;
101 if (prcm->xtal_speed != sclk->rate)
102 continue;
104 if (prcm->mpu_speed <= rate) {
105 found_speed = prcm->mpu_speed;
106 break;
107 }
108 }
110 if (!found_speed) {
111 printk(KERN_INFO "Could not set MPU rate to %luMHz\n",
112 rate / 1000000);
113 return -EINVAL;
114 }
116 curr_prcm_set = prcm;
117 cur_rate = omap2xxx_clk_get_core_rate(dclk);
119 if (prcm->dpll_speed == cur_rate / 2) {
120 omap2xxx_sdrc_reprogram(CORE_CLK_SRC_DPLL, 1);
121 } else if (prcm->dpll_speed == cur_rate * 2) {
122 omap2xxx_sdrc_reprogram(CORE_CLK_SRC_DPLL_X2, 1);
123 } else if (prcm->dpll_speed != cur_rate) {
124 local_irq_save(flags);
126 if (prcm->dpll_speed == prcm->xtal_speed)
127 bypass = 1;
129 if ((prcm->cm_clksel2_pll & OMAP24XX_CORE_CLK_SRC_MASK) ==
130 CORE_CLK_SRC_DPLL_X2)
131 done_rate = CORE_CLK_SRC_DPLL_X2;
132 else
133 done_rate = CORE_CLK_SRC_DPLL;
135 /* MPU divider */
136 omap2_cm_write_mod_reg(prcm->cm_clksel_mpu, MPU_MOD, CM_CLKSEL);
138 /* dsp + iva1 div(2420), iva2.1(2430) */
139 omap2_cm_write_mod_reg(prcm->cm_clksel_dsp,
140 OMAP24XX_DSP_MOD, CM_CLKSEL);
142 omap2_cm_write_mod_reg(prcm->cm_clksel_gfx, GFX_MOD, CM_CLKSEL);
144 /* Major subsystem dividers */
145 tmp = omap2_cm_read_mod_reg(CORE_MOD, CM_CLKSEL1) & OMAP24XX_CLKSEL_DSS2_MASK;
146 omap2_cm_write_mod_reg(prcm->cm_clksel1_core | tmp, CORE_MOD,
147 CM_CLKSEL1);
149 if (cpu_is_omap2430())
150 omap2_cm_write_mod_reg(prcm->cm_clksel_mdm,
151 OMAP2430_MDM_MOD, CM_CLKSEL);
153 /* x2 to enter omap2xxx_sdrc_init_params() */
154 omap2xxx_sdrc_reprogram(CORE_CLK_SRC_DPLL_X2, 1);
156 omap2_set_prcm(prcm->cm_clksel1_pll, prcm->base_sdrc_rfr,
157 bypass);
159 omap2xxx_sdrc_init_params(omap2xxx_sdrc_dll_is_unlocked());
160 omap2xxx_sdrc_reprogram(done_rate, 0);
162 local_irq_restore(flags);
163 }
165 return 0;
166 }
168 #ifdef CONFIG_CPU_FREQ
169 /*
170 * Walk PRCM rate table and fillout cpufreq freq_table
171 * XXX This should be replaced by an OPP layer in the near future
172 */
173 static struct cpufreq_frequency_table *freq_table;
175 void omap2_clk_init_cpufreq_table(struct cpufreq_frequency_table **table)
176 {
177 const struct prcm_config *prcm;
178 int i = 0;
179 int tbl_sz = 0;
181 if (!cpu_is_omap24xx())
182 return;
184 for (prcm = rate_table; prcm->mpu_speed; prcm++) {
185 if (!(prcm->flags & cpu_mask))
186 continue;
187 if (prcm->xtal_speed != sclk->rate)
188 continue;
190 /* don't put bypass rates in table */
191 if (prcm->dpll_speed == prcm->xtal_speed)
192 continue;
194 tbl_sz++;
195 }
197 /*
198 * XXX Ensure that we're doing what CPUFreq expects for this error
199 * case and the following one
200 */
201 if (tbl_sz == 0) {
202 pr_warning("%s: no matching entries in rate_table\n",
203 __func__);
204 return;
205 }
207 /* Include the CPUFREQ_TABLE_END terminator entry */
208 tbl_sz++;
210 freq_table = kzalloc(sizeof(struct cpufreq_frequency_table) * tbl_sz,
211 GFP_ATOMIC);
212 if (!freq_table) {
213 pr_err("%s: could not kzalloc frequency table\n", __func__);
214 return;
215 }
217 for (prcm = rate_table; prcm->mpu_speed; prcm++) {
218 if (!(prcm->flags & cpu_mask))
219 continue;
220 if (prcm->xtal_speed != sclk->rate)
221 continue;
223 /* don't put bypass rates in table */
224 if (prcm->dpll_speed == prcm->xtal_speed)
225 continue;
227 freq_table[i].index = i;
228 freq_table[i].frequency = prcm->mpu_speed / 1000;
229 i++;
230 }
232 freq_table[i].index = i;
233 freq_table[i].frequency = CPUFREQ_TABLE_END;
235 *table = &freq_table[0];
236 }
238 void omap2_clk_exit_cpufreq_table(struct cpufreq_frequency_table **table)
239 {
240 if (!cpu_is_omap24xx())
241 return;
243 kfree(freq_table);
244 }
246 #endif