]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - arch/arm/mach-omap2/clockdomain.c
Merge branch 'master' of git://git.kernel.org/pub/scm/linux/kernel/git/linville/wirel...
[sitara-epos/sitara-epos-kernel.git] / arch / arm / mach-omap2 / clockdomain.c
1 /*
2  * OMAP2/3/4 clockdomain framework functions
3  *
4  * Copyright (C) 2008-2010 Texas Instruments, Inc.
5  * Copyright (C) 2008-2010 Nokia Corporation
6  *
7  * Written by Paul Walmsley and Jouni Högander
8  * Added OMAP4 specific support by Abhijit Pagare <abhijitpagare@ti.com>
9  *
10  * This program is free software; you can redistribute it and/or modify
11  * it under the terms of the GNU General Public License version 2 as
12  * published by the Free Software Foundation.
13  */
14 #undef DEBUG
16 #include <linux/kernel.h>
17 #include <linux/device.h>
18 #include <linux/list.h>
19 #include <linux/errno.h>
20 #include <linux/delay.h>
21 #include <linux/clk.h>
22 #include <linux/limits.h>
23 #include <linux/err.h>
25 #include <linux/io.h>
27 #include <linux/bitops.h>
29 #include <plat/clock.h>
30 #include "clockdomain.h"
32 /* clkdm_list contains all registered struct clockdomains */
33 static LIST_HEAD(clkdm_list);
35 /* array of clockdomain deps to be added/removed when clkdm in hwsup mode */
36 static struct clkdm_autodep *autodeps;
38 static struct clkdm_ops *arch_clkdm;
40 /* Private functions */
42 static struct clockdomain *_clkdm_lookup(const char *name)
43 {
44         struct clockdomain *clkdm, *temp_clkdm;
46         if (!name)
47                 return NULL;
49         clkdm = NULL;
51         list_for_each_entry(temp_clkdm, &clkdm_list, node) {
52                 if (!strcmp(name, temp_clkdm->name)) {
53                         clkdm = temp_clkdm;
54                         break;
55                 }
56         }
58         return clkdm;
59 }
61 /**
62  * _clkdm_register - register a clockdomain
63  * @clkdm: struct clockdomain * to register
64  *
65  * Adds a clockdomain to the internal clockdomain list.
66  * Returns -EINVAL if given a null pointer, -EEXIST if a clockdomain is
67  * already registered by the provided name, or 0 upon success.
68  */
69 static int _clkdm_register(struct clockdomain *clkdm)
70 {
71         struct powerdomain *pwrdm;
73         if (!clkdm || !clkdm->name)
74                 return -EINVAL;
76         if (!omap_chip_is(clkdm->omap_chip))
77                 return -EINVAL;
79         pwrdm = pwrdm_lookup(clkdm->pwrdm.name);
80         if (!pwrdm) {
81                 pr_err("clockdomain: %s: powerdomain %s does not exist\n",
82                         clkdm->name, clkdm->pwrdm.name);
83                 return -EINVAL;
84         }
85         clkdm->pwrdm.ptr = pwrdm;
87         /* Verify that the clockdomain is not already registered */
88         if (_clkdm_lookup(clkdm->name))
89                 return -EEXIST;
91         list_add(&clkdm->node, &clkdm_list);
93         pwrdm_add_clkdm(pwrdm, clkdm);
95         pr_debug("clockdomain: registered %s\n", clkdm->name);
97         return 0;
98 }
100 /* _clkdm_deps_lookup - look up the specified clockdomain in a clkdm list */
101 static struct clkdm_dep *_clkdm_deps_lookup(struct clockdomain *clkdm,
102                                             struct clkdm_dep *deps)
104         struct clkdm_dep *cd;
106         if (!clkdm || !deps || !omap_chip_is(clkdm->omap_chip))
107                 return ERR_PTR(-EINVAL);
109         for (cd = deps; cd->clkdm_name; cd++) {
110                 if (!omap_chip_is(cd->omap_chip))
111                         continue;
113                 if (!cd->clkdm && cd->clkdm_name)
114                         cd->clkdm = _clkdm_lookup(cd->clkdm_name);
116                 if (cd->clkdm == clkdm)
117                         break;
118         }
120         if (!cd->clkdm_name)
121                 return ERR_PTR(-ENOENT);
123         return cd;
126 /*
127  * _autodep_lookup - resolve autodep clkdm names to clkdm pointers; store
128  * @autodep: struct clkdm_autodep * to resolve
129  *
130  * Resolve autodep clockdomain names to clockdomain pointers via
131  * clkdm_lookup() and store the pointers in the autodep structure.  An
132  * "autodep" is a clockdomain sleep/wakeup dependency that is
133  * automatically added and removed whenever clocks in the associated
134  * clockdomain are enabled or disabled (respectively) when the
135  * clockdomain is in hardware-supervised mode.  Meant to be called
136  * once at clockdomain layer initialization, since these should remain
137  * fixed for a particular architecture.  No return value.
138  *
139  * XXX autodeps are deprecated and should be removed at the earliest
140  * opportunity
141  */
142 static void _autodep_lookup(struct clkdm_autodep *autodep)
144         struct clockdomain *clkdm;
146         if (!autodep)
147                 return;
149         if (!omap_chip_is(autodep->omap_chip))
150                 return;
152         clkdm = clkdm_lookup(autodep->clkdm.name);
153         if (!clkdm) {
154                 pr_err("clockdomain: autodeps: clockdomain %s does not exist\n",
155                          autodep->clkdm.name);
156                 clkdm = ERR_PTR(-ENOENT);
157         }
158         autodep->clkdm.ptr = clkdm;
161 /*
162  * _clkdm_add_autodeps - add auto sleepdeps/wkdeps to clkdm upon clock enable
163  * @clkdm: struct clockdomain *
164  *
165  * Add the "autodep" sleep & wakeup dependencies to clockdomain 'clkdm'
166  * in hardware-supervised mode.  Meant to be called from clock framework
167  * when a clock inside clockdomain 'clkdm' is enabled.  No return value.
168  *
169  * XXX autodeps are deprecated and should be removed at the earliest
170  * opportunity
171  */
172 void _clkdm_add_autodeps(struct clockdomain *clkdm)
174         struct clkdm_autodep *autodep;
176         if (!autodeps || clkdm->flags & CLKDM_NO_AUTODEPS)
177                 return;
179         for (autodep = autodeps; autodep->clkdm.ptr; autodep++) {
180                 if (IS_ERR(autodep->clkdm.ptr))
181                         continue;
183                 if (!omap_chip_is(autodep->omap_chip))
184                         continue;
186                 pr_debug("clockdomain: adding %s sleepdep/wkdep for "
187                          "clkdm %s\n", autodep->clkdm.ptr->name,
188                          clkdm->name);
190                 clkdm_add_sleepdep(clkdm, autodep->clkdm.ptr);
191                 clkdm_add_wkdep(clkdm, autodep->clkdm.ptr);
192         }
195 /*
196  * _clkdm_add_autodeps - remove auto sleepdeps/wkdeps from clkdm
197  * @clkdm: struct clockdomain *
198  *
199  * Remove the "autodep" sleep & wakeup dependencies from clockdomain 'clkdm'
200  * in hardware-supervised mode.  Meant to be called from clock framework
201  * when a clock inside clockdomain 'clkdm' is disabled.  No return value.
202  *
203  * XXX autodeps are deprecated and should be removed at the earliest
204  * opportunity
205  */
206 void _clkdm_del_autodeps(struct clockdomain *clkdm)
208         struct clkdm_autodep *autodep;
210         if (!autodeps || clkdm->flags & CLKDM_NO_AUTODEPS)
211                 return;
213         for (autodep = autodeps; autodep->clkdm.ptr; autodep++) {
214                 if (IS_ERR(autodep->clkdm.ptr))
215                         continue;
217                 if (!omap_chip_is(autodep->omap_chip))
218                         continue;
220                 pr_debug("clockdomain: removing %s sleepdep/wkdep for "
221                          "clkdm %s\n", autodep->clkdm.ptr->name,
222                          clkdm->name);
224                 clkdm_del_sleepdep(clkdm, autodep->clkdm.ptr);
225                 clkdm_del_wkdep(clkdm, autodep->clkdm.ptr);
226         }
229 /**
230  * _resolve_clkdm_deps() - resolve clkdm_names in @clkdm_deps to clkdms
231  * @clkdm: clockdomain that we are resolving dependencies for
232  * @clkdm_deps: ptr to array of struct clkdm_deps to resolve
233  *
234  * Iterates through @clkdm_deps, looking up the struct clockdomain named by
235  * clkdm_name and storing the clockdomain pointer in the struct clkdm_dep.
236  * No return value.
237  */
238 static void _resolve_clkdm_deps(struct clockdomain *clkdm,
239                                 struct clkdm_dep *clkdm_deps)
241         struct clkdm_dep *cd;
243         for (cd = clkdm_deps; cd && cd->clkdm_name; cd++) {
244                 if (!omap_chip_is(cd->omap_chip))
245                         continue;
246                 if (cd->clkdm)
247                         continue;
248                 cd->clkdm = _clkdm_lookup(cd->clkdm_name);
250                 WARN(!cd->clkdm, "clockdomain: %s: could not find clkdm %s while resolving dependencies - should never happen",
251                      clkdm->name, cd->clkdm_name);
252         }
255 /* Public functions */
257 /**
258  * clkdm_init - set up the clockdomain layer
259  * @clkdms: optional pointer to an array of clockdomains to register
260  * @init_autodeps: optional pointer to an array of autodeps to register
261  * @custom_funcs: func pointers for arch specific implementations
262  *
263  * Set up internal state.  If a pointer to an array of clockdomains
264  * @clkdms was supplied, loop through the list of clockdomains,
265  * register all that are available on the current platform. Similarly,
266  * if a pointer to an array of clockdomain autodependencies
267  * @init_autodeps was provided, register those.  No return value.
268  */
269 void clkdm_init(struct clockdomain **clkdms,
270                 struct clkdm_autodep *init_autodeps,
271                 struct clkdm_ops *custom_funcs)
273         struct clockdomain **c = NULL;
274         struct clockdomain *clkdm;
275         struct clkdm_autodep *autodep = NULL;
277         if (!custom_funcs)
278                 WARN(1, "No custom clkdm functions registered\n");
279         else
280                 arch_clkdm = custom_funcs;
282         if (clkdms)
283                 for (c = clkdms; *c; c++)
284                         _clkdm_register(*c);
286         autodeps = init_autodeps;
287         if (autodeps)
288                 for (autodep = autodeps; autodep->clkdm.ptr; autodep++)
289                         _autodep_lookup(autodep);
291         /*
292          * Put all clockdomains into software-supervised mode; PM code
293          * should later enable hardware-supervised mode as appropriate
294          */
295         list_for_each_entry(clkdm, &clkdm_list, node) {
296                 if (clkdm->flags & CLKDM_CAN_FORCE_WAKEUP)
297                         clkdm_wakeup(clkdm);
298                 else if (clkdm->flags & CLKDM_CAN_DISABLE_AUTO)
299                         clkdm_deny_idle(clkdm);
301                 _resolve_clkdm_deps(clkdm, clkdm->wkdep_srcs);
302                 clkdm_clear_all_wkdeps(clkdm);
304                 _resolve_clkdm_deps(clkdm, clkdm->sleepdep_srcs);
305                 clkdm_clear_all_sleepdeps(clkdm);
306         }
309 /**
310  * clkdm_lookup - look up a clockdomain by name, return a pointer
311  * @name: name of clockdomain
312  *
313  * Find a registered clockdomain by its name @name.  Returns a pointer
314  * to the struct clockdomain if found, or NULL otherwise.
315  */
316 struct clockdomain *clkdm_lookup(const char *name)
318         struct clockdomain *clkdm, *temp_clkdm;
320         if (!name)
321                 return NULL;
323         clkdm = NULL;
325         list_for_each_entry(temp_clkdm, &clkdm_list, node) {
326                 if (!strcmp(name, temp_clkdm->name)) {
327                         clkdm = temp_clkdm;
328                         break;
329                 }
330         }
332         return clkdm;
335 /**
336  * clkdm_for_each - call function on each registered clockdomain
337  * @fn: callback function *
338  *
339  * Call the supplied function @fn for each registered clockdomain.
340  * The callback function @fn can return anything but 0 to bail
341  * out early from the iterator.  The callback function is called with
342  * the clkdm_mutex held, so no clockdomain structure manipulation
343  * functions should be called from the callback, although hardware
344  * clockdomain control functions are fine.  Returns the last return
345  * value of the callback function, which should be 0 for success or
346  * anything else to indicate failure; or -EINVAL if the function pointer
347  * is null.
348  */
349 int clkdm_for_each(int (*fn)(struct clockdomain *clkdm, void *user),
350                         void *user)
352         struct clockdomain *clkdm;
353         int ret = 0;
355         if (!fn)
356                 return -EINVAL;
358         list_for_each_entry(clkdm, &clkdm_list, node) {
359                 ret = (*fn)(clkdm, user);
360                 if (ret)
361                         break;
362         }
364         return ret;
368 /**
369  * clkdm_get_pwrdm - return a ptr to the pwrdm that this clkdm resides in
370  * @clkdm: struct clockdomain *
371  *
372  * Return a pointer to the struct powerdomain that the specified clockdomain
373  * @clkdm exists in, or returns NULL if @clkdm is NULL.
374  */
375 struct powerdomain *clkdm_get_pwrdm(struct clockdomain *clkdm)
377         if (!clkdm)
378                 return NULL;
380         return clkdm->pwrdm.ptr;
384 /* Hardware clockdomain control */
386 /**
387  * clkdm_add_wkdep - add a wakeup dependency from clkdm2 to clkdm1
388  * @clkdm1: wake this struct clockdomain * up (dependent)
389  * @clkdm2: when this struct clockdomain * wakes up (source)
390  *
391  * When the clockdomain represented by @clkdm2 wakes up, wake up
392  * @clkdm1. Implemented in hardware on the OMAP, this feature is
393  * designed to reduce wakeup latency of the dependent clockdomain @clkdm1.
394  * Returns -EINVAL if presented with invalid clockdomain pointers,
395  * -ENOENT if @clkdm2 cannot wake up clkdm1 in hardware, or 0 upon
396  * success.
397  */
398 int clkdm_add_wkdep(struct clockdomain *clkdm1, struct clockdomain *clkdm2)
400         struct clkdm_dep *cd;
401         int ret = 0;
403         if (!clkdm1 || !clkdm2)
404                 return -EINVAL;
406         cd = _clkdm_deps_lookup(clkdm2, clkdm1->wkdep_srcs);
407         if (IS_ERR(cd))
408                 ret = PTR_ERR(cd);
410         if (!arch_clkdm || !arch_clkdm->clkdm_add_wkdep)
411                 ret = -EINVAL;
413         if (ret) {
414                 pr_debug("clockdomain: hardware cannot set/clear wake up of "
415                          "%s when %s wakes up\n", clkdm1->name, clkdm2->name);
416                 return ret;
417         }
419         if (atomic_inc_return(&cd->wkdep_usecount) == 1) {
420                 pr_debug("clockdomain: hardware will wake up %s when %s wakes "
421                          "up\n", clkdm1->name, clkdm2->name);
423                 ret = arch_clkdm->clkdm_add_wkdep(clkdm1, clkdm2);
424         }
426         return ret;
429 /**
430  * clkdm_del_wkdep - remove a wakeup dependency from clkdm2 to clkdm1
431  * @clkdm1: wake this struct clockdomain * up (dependent)
432  * @clkdm2: when this struct clockdomain * wakes up (source)
433  *
434  * Remove a wakeup dependency causing @clkdm1 to wake up when @clkdm2
435  * wakes up.  Returns -EINVAL if presented with invalid clockdomain
436  * pointers, -ENOENT if @clkdm2 cannot wake up clkdm1 in hardware, or
437  * 0 upon success.
438  */
439 int clkdm_del_wkdep(struct clockdomain *clkdm1, struct clockdomain *clkdm2)
441         struct clkdm_dep *cd;
442         int ret = 0;
444         if (!clkdm1 || !clkdm2)
445                 return -EINVAL;
447         cd = _clkdm_deps_lookup(clkdm2, clkdm1->wkdep_srcs);
448         if (IS_ERR(cd))
449                 ret = PTR_ERR(cd);
451         if (!arch_clkdm || !arch_clkdm->clkdm_del_wkdep)
452                 ret = -EINVAL;
454         if (ret) {
455                 pr_debug("clockdomain: hardware cannot set/clear wake up of "
456                          "%s when %s wakes up\n", clkdm1->name, clkdm2->name);
457                 return ret;
458         }
460         if (atomic_dec_return(&cd->wkdep_usecount) == 0) {
461                 pr_debug("clockdomain: hardware will no longer wake up %s "
462                          "after %s wakes up\n", clkdm1->name, clkdm2->name);
464                 ret = arch_clkdm->clkdm_del_wkdep(clkdm1, clkdm2);
465         }
467         return ret;
470 /**
471  * clkdm_read_wkdep - read wakeup dependency state from clkdm2 to clkdm1
472  * @clkdm1: wake this struct clockdomain * up (dependent)
473  * @clkdm2: when this struct clockdomain * wakes up (source)
474  *
475  * Return 1 if a hardware wakeup dependency exists wherein @clkdm1 will be
476  * awoken when @clkdm2 wakes up; 0 if dependency is not set; -EINVAL
477  * if either clockdomain pointer is invalid; or -ENOENT if the hardware
478  * is incapable.
479  *
480  * REVISIT: Currently this function only represents software-controllable
481  * wakeup dependencies.  Wakeup dependencies fixed in hardware are not
482  * yet handled here.
483  */
484 int clkdm_read_wkdep(struct clockdomain *clkdm1, struct clockdomain *clkdm2)
486         struct clkdm_dep *cd;
487         int ret = 0;
489         if (!clkdm1 || !clkdm2)
490                 return -EINVAL;
492         cd = _clkdm_deps_lookup(clkdm2, clkdm1->wkdep_srcs);
493         if (IS_ERR(cd))
494                 ret = PTR_ERR(cd);
496         if (!arch_clkdm || !arch_clkdm->clkdm_read_wkdep)
497                 ret = -EINVAL;
499         if (ret) {
500                 pr_debug("clockdomain: hardware cannot set/clear wake up of "
501                          "%s when %s wakes up\n", clkdm1->name, clkdm2->name);
502                 return ret;
503         }
505         /* XXX It's faster to return the atomic wkdep_usecount */
506         return arch_clkdm->clkdm_read_wkdep(clkdm1, clkdm2);
509 /**
510  * clkdm_clear_all_wkdeps - remove all wakeup dependencies from target clkdm
511  * @clkdm: struct clockdomain * to remove all wakeup dependencies from
512  *
513  * Remove all inter-clockdomain wakeup dependencies that could cause
514  * @clkdm to wake.  Intended to be used during boot to initialize the
515  * PRCM to a known state, after all clockdomains are put into swsup idle
516  * and woken up.  Returns -EINVAL if @clkdm pointer is invalid, or
517  * 0 upon success.
518  */
519 int clkdm_clear_all_wkdeps(struct clockdomain *clkdm)
521         if (!clkdm)
522                 return -EINVAL;
524         if (!arch_clkdm || !arch_clkdm->clkdm_clear_all_wkdeps)
525                 return -EINVAL;
527         return arch_clkdm->clkdm_clear_all_wkdeps(clkdm);
530 /**
531  * clkdm_add_sleepdep - add a sleep dependency from clkdm2 to clkdm1
532  * @clkdm1: prevent this struct clockdomain * from sleeping (dependent)
533  * @clkdm2: when this struct clockdomain * is active (source)
534  *
535  * Prevent @clkdm1 from automatically going inactive (and then to
536  * retention or off) if @clkdm2 is active.  Returns -EINVAL if
537  * presented with invalid clockdomain pointers or called on a machine
538  * that does not support software-configurable hardware sleep
539  * dependencies, -ENOENT if the specified dependency cannot be set in
540  * hardware, or 0 upon success.
541  */
542 int clkdm_add_sleepdep(struct clockdomain *clkdm1, struct clockdomain *clkdm2)
544         struct clkdm_dep *cd;
545         int ret = 0;
547         if (!clkdm1 || !clkdm2)
548                 return -EINVAL;
550         cd = _clkdm_deps_lookup(clkdm2, clkdm1->sleepdep_srcs);
551         if (IS_ERR(cd))
552                 ret = PTR_ERR(cd);
554         if (!arch_clkdm || !arch_clkdm->clkdm_add_sleepdep)
555                 ret = -EINVAL;
557         if (ret) {
558                 pr_debug("clockdomain: hardware cannot set/clear sleep "
559                          "dependency affecting %s from %s\n", clkdm1->name,
560                          clkdm2->name);
561                 return ret;
562         }
564         if (atomic_inc_return(&cd->sleepdep_usecount) == 1) {
565                 pr_debug("clockdomain: will prevent %s from sleeping if %s "
566                          "is active\n", clkdm1->name, clkdm2->name);
568                 ret = arch_clkdm->clkdm_add_sleepdep(clkdm1, clkdm2);
569         }
571         return ret;
574 /**
575  * clkdm_del_sleepdep - remove a sleep dependency from clkdm2 to clkdm1
576  * @clkdm1: prevent this struct clockdomain * from sleeping (dependent)
577  * @clkdm2: when this struct clockdomain * is active (source)
578  *
579  * Allow @clkdm1 to automatically go inactive (and then to retention or
580  * off), independent of the activity state of @clkdm2.  Returns -EINVAL
581  * if presented with invalid clockdomain pointers or called on a machine
582  * that does not support software-configurable hardware sleep dependencies,
583  * -ENOENT if the specified dependency cannot be cleared in hardware, or
584  * 0 upon success.
585  */
586 int clkdm_del_sleepdep(struct clockdomain *clkdm1, struct clockdomain *clkdm2)
588         struct clkdm_dep *cd;
589         int ret = 0;
591         if (!clkdm1 || !clkdm2)
592                 return -EINVAL;
594         cd = _clkdm_deps_lookup(clkdm2, clkdm1->sleepdep_srcs);
595         if (IS_ERR(cd))
596                 ret = PTR_ERR(cd);
598         if (!arch_clkdm || !arch_clkdm->clkdm_del_sleepdep)
599                 ret = -EINVAL;
601         if (ret) {
602                 pr_debug("clockdomain: hardware cannot set/clear sleep "
603                          "dependency affecting %s from %s\n", clkdm1->name,
604                          clkdm2->name);
605                 return ret;
606         }
608         if (atomic_dec_return(&cd->sleepdep_usecount) == 0) {
609                 pr_debug("clockdomain: will no longer prevent %s from "
610                          "sleeping if %s is active\n", clkdm1->name,
611                          clkdm2->name);
613                 ret = arch_clkdm->clkdm_del_sleepdep(clkdm1, clkdm2);
614         }
616         return ret;
619 /**
620  * clkdm_read_sleepdep - read sleep dependency state from clkdm2 to clkdm1
621  * @clkdm1: prevent this struct clockdomain * from sleeping (dependent)
622  * @clkdm2: when this struct clockdomain * is active (source)
623  *
624  * Return 1 if a hardware sleep dependency exists wherein @clkdm1 will
625  * not be allowed to automatically go inactive if @clkdm2 is active;
626  * 0 if @clkdm1's automatic power state inactivity transition is independent
627  * of @clkdm2's; -EINVAL if either clockdomain pointer is invalid or called
628  * on a machine that does not support software-configurable hardware sleep
629  * dependencies; or -ENOENT if the hardware is incapable.
630  *
631  * REVISIT: Currently this function only represents software-controllable
632  * sleep dependencies.  Sleep dependencies fixed in hardware are not
633  * yet handled here.
634  */
635 int clkdm_read_sleepdep(struct clockdomain *clkdm1, struct clockdomain *clkdm2)
637         struct clkdm_dep *cd;
638         int ret = 0;
640         if (!clkdm1 || !clkdm2)
641                 return -EINVAL;
643         cd = _clkdm_deps_lookup(clkdm2, clkdm1->sleepdep_srcs);
644         if (IS_ERR(cd))
645                 ret = PTR_ERR(cd);
647         if (!arch_clkdm || !arch_clkdm->clkdm_read_sleepdep)
648                 ret = -EINVAL;
650         if (ret) {
651                 pr_debug("clockdomain: hardware cannot set/clear sleep "
652                          "dependency affecting %s from %s\n", clkdm1->name,
653                          clkdm2->name);
654                 return ret;
655         }
657         /* XXX It's faster to return the atomic sleepdep_usecount */
658         return arch_clkdm->clkdm_read_sleepdep(clkdm1, clkdm2);
661 /**
662  * clkdm_clear_all_sleepdeps - remove all sleep dependencies from target clkdm
663  * @clkdm: struct clockdomain * to remove all sleep dependencies from
664  *
665  * Remove all inter-clockdomain sleep dependencies that could prevent
666  * @clkdm from idling.  Intended to be used during boot to initialize the
667  * PRCM to a known state, after all clockdomains are put into swsup idle
668  * and woken up.  Returns -EINVAL if @clkdm pointer is invalid, or
669  * 0 upon success.
670  */
671 int clkdm_clear_all_sleepdeps(struct clockdomain *clkdm)
673         if (!clkdm)
674                 return -EINVAL;
676         if (!arch_clkdm || !arch_clkdm->clkdm_clear_all_sleepdeps)
677                 return -EINVAL;
679         return arch_clkdm->clkdm_clear_all_sleepdeps(clkdm);
682 /**
683  * clkdm_sleep - force clockdomain sleep transition
684  * @clkdm: struct clockdomain *
685  *
686  * Instruct the CM to force a sleep transition on the specified
687  * clockdomain @clkdm.  Returns -EINVAL if @clkdm is NULL or if
688  * clockdomain does not support software-initiated sleep; 0 upon
689  * success.
690  */
691 int clkdm_sleep(struct clockdomain *clkdm)
693         if (!clkdm)
694                 return -EINVAL;
696         if (!(clkdm->flags & CLKDM_CAN_FORCE_SLEEP)) {
697                 pr_debug("clockdomain: %s does not support forcing "
698                          "sleep via software\n", clkdm->name);
699                 return -EINVAL;
700         }
702         if (!arch_clkdm || !arch_clkdm->clkdm_sleep)
703                 return -EINVAL;
705         pr_debug("clockdomain: forcing sleep on %s\n", clkdm->name);
707         return arch_clkdm->clkdm_sleep(clkdm);
710 /**
711  * clkdm_wakeup - force clockdomain wakeup transition
712  * @clkdm: struct clockdomain *
713  *
714  * Instruct the CM to force a wakeup transition on the specified
715  * clockdomain @clkdm.  Returns -EINVAL if @clkdm is NULL or if the
716  * clockdomain does not support software-controlled wakeup; 0 upon
717  * success.
718  */
719 int clkdm_wakeup(struct clockdomain *clkdm)
721         if (!clkdm)
722                 return -EINVAL;
724         if (!(clkdm->flags & CLKDM_CAN_FORCE_WAKEUP)) {
725                 pr_debug("clockdomain: %s does not support forcing "
726                          "wakeup via software\n", clkdm->name);
727                 return -EINVAL;
728         }
730         if (!arch_clkdm || !arch_clkdm->clkdm_wakeup)
731                 return -EINVAL;
733         pr_debug("clockdomain: forcing wakeup on %s\n", clkdm->name);
735         return arch_clkdm->clkdm_wakeup(clkdm);
738 /**
739  * clkdm_allow_idle - enable hwsup idle transitions for clkdm
740  * @clkdm: struct clockdomain *
741  *
742  * Allow the hardware to automatically switch the clockdomain @clkdm into
743  * active or idle states, as needed by downstream clocks.  If the
744  * clockdomain has any downstream clocks enabled in the clock
745  * framework, wkdep/sleepdep autodependencies are added; this is so
746  * device drivers can read and write to the device.  No return value.
747  */
748 void clkdm_allow_idle(struct clockdomain *clkdm)
750         if (!clkdm)
751                 return;
753         if (!(clkdm->flags & CLKDM_CAN_ENABLE_AUTO)) {
754                 pr_debug("clock: automatic idle transitions cannot be enabled "
755                          "on clockdomain %s\n", clkdm->name);
756                 return;
757         }
759         if (!arch_clkdm || !arch_clkdm->clkdm_allow_idle)
760                 return;
762         pr_debug("clockdomain: enabling automatic idle transitions for %s\n",
763                  clkdm->name);
765         arch_clkdm->clkdm_allow_idle(clkdm);
766         pwrdm_clkdm_state_switch(clkdm);
769 /**
770  * clkdm_deny_idle - disable hwsup idle transitions for clkdm
771  * @clkdm: struct clockdomain *
772  *
773  * Prevent the hardware from automatically switching the clockdomain
774  * @clkdm into inactive or idle states.  If the clockdomain has
775  * downstream clocks enabled in the clock framework, wkdep/sleepdep
776  * autodependencies are removed.  No return value.
777  */
778 void clkdm_deny_idle(struct clockdomain *clkdm)
780         if (!clkdm)
781                 return;
783         if (!(clkdm->flags & CLKDM_CAN_DISABLE_AUTO)) {
784                 pr_debug("clockdomain: automatic idle transitions cannot be "
785                          "disabled on %s\n", clkdm->name);
786                 return;
787         }
789         if (!arch_clkdm || !arch_clkdm->clkdm_deny_idle)
790                 return;
792         pr_debug("clockdomain: disabling automatic idle transitions for %s\n",
793                  clkdm->name);
795         arch_clkdm->clkdm_deny_idle(clkdm);
799 /* Clockdomain-to-clock framework interface code */
801 /**
802  * clkdm_clk_enable - add an enabled downstream clock to this clkdm
803  * @clkdm: struct clockdomain *
804  * @clk: struct clk * of the enabled downstream clock
805  *
806  * Increment the usecount of the clockdomain @clkdm and ensure that it
807  * is awake before @clk is enabled.  Intended to be called by
808  * clk_enable() code.  If the clockdomain is in software-supervised
809  * idle mode, force the clockdomain to wake.  If the clockdomain is in
810  * hardware-supervised idle mode, add clkdm-pwrdm autodependencies, to
811  * ensure that devices in the clockdomain can be read from/written to
812  * by on-chip processors.  Returns -EINVAL if passed null pointers;
813  * returns 0 upon success or if the clockdomain is in hwsup idle mode.
814  */
815 int clkdm_clk_enable(struct clockdomain *clkdm, struct clk *clk)
817         /*
818          * XXX Rewrite this code to maintain a list of enabled
819          * downstream clocks for debugging purposes?
820          */
822         if (!clkdm || !clk)
823                 return -EINVAL;
825         if (!arch_clkdm || !arch_clkdm->clkdm_clk_enable)
826                 return -EINVAL;
828         if (atomic_inc_return(&clkdm->usecount) > 1)
829                 return 0;
831         /* Clockdomain now has one enabled downstream clock */
833         pr_debug("clockdomain: clkdm %s: clk %s now enabled\n", clkdm->name,
834                  clk->name);
836         arch_clkdm->clkdm_clk_enable(clkdm);
837         pwrdm_wait_transition(clkdm->pwrdm.ptr);
838         pwrdm_clkdm_state_switch(clkdm);
840         return 0;
843 /**
844  * clkdm_clk_disable - remove an enabled downstream clock from this clkdm
845  * @clkdm: struct clockdomain *
846  * @clk: struct clk * of the disabled downstream clock
847  *
848  * Decrement the usecount of this clockdomain @clkdm when @clk is
849  * disabled.  Intended to be called by clk_disable() code.  If the
850  * clockdomain usecount goes to 0, put the clockdomain to sleep
851  * (software-supervised mode) or remove the clkdm autodependencies
852  * (hardware-supervised mode).  Returns -EINVAL if passed null
853  * pointers; -ERANGE if the @clkdm usecount underflows and debugging
854  * is enabled; or returns 0 upon success or if the clockdomain is in
855  * hwsup idle mode.
856  */
857 int clkdm_clk_disable(struct clockdomain *clkdm, struct clk *clk)
859         /*
860          * XXX Rewrite this code to maintain a list of enabled
861          * downstream clocks for debugging purposes?
862          */
864         if (!clkdm || !clk)
865                 return -EINVAL;
867         if (!arch_clkdm || !arch_clkdm->clkdm_clk_disable)
868                 return -EINVAL;
870 #ifdef DEBUG
871         if (atomic_read(&clkdm->usecount) == 0) {
872                 WARN_ON(1); /* underflow */
873                 return -ERANGE;
874         }
875 #endif
877         if (atomic_dec_return(&clkdm->usecount) > 0)
878                 return 0;
880         /* All downstream clocks of this clockdomain are now disabled */
882         pr_debug("clockdomain: clkdm %s: clk %s now disabled\n", clkdm->name,
883                  clk->name);
885         arch_clkdm->clkdm_clk_disable(clkdm);
886         pwrdm_clkdm_state_switch(clkdm);
888         return 0;