ARM: OMAP3+: dpll: Configure autoidle mode only if its supported
[sitara-epos/sitara-epos-kernel.git] / arch / arm / mach-omap2 / dpll3xxx.c
1 /*
2  * OMAP3/4 - specific DPLL control functions
3  *
4  * Copyright (C) 2009-2010 Texas Instruments, Inc.
5  * Copyright (C) 2009-2010 Nokia Corporation
6  *
7  * Written by Paul Walmsley
8  * Testing and integration fixes by Jouni Högander
9  *
10  * 36xx support added by Vishwanath BS, Richard Woodruff, and Nishanth
11  * Menon
12  *
13  * Parts of this code are based on code written by
14  * Richard Woodruff, Tony Lindgren, Tuukka Tikkanen, Karthik Dasu
15  *
16  * This program is free software; you can redistribute it and/or modify
17  * it under the terms of the GNU General Public License version 2 as
18  * published by the Free Software Foundation.
19  */
21 #include <linux/kernel.h>
22 #include <linux/device.h>
23 #include <linux/list.h>
24 #include <linux/errno.h>
25 #include <linux/delay.h>
26 #include <linux/clk.h>
27 #include <linux/io.h>
28 #include <linux/bitops.h>
29 #include <linux/clkdev.h>
31 #include <plat/cpu.h>
32 #include <plat/clock.h>
34 #include "clock.h"
35 #include "cm2xxx_3xxx.h"
36 #include "cm-regbits-34xx.h"
38 /* CM_AUTOIDLE_PLL*.AUTO_* bit values */
39 #define DPLL_AUTOIDLE_DISABLE                   0x0
40 #define DPLL_AUTOIDLE_LOW_POWER_STOP            0x1
42 #define MAX_DPLL_WAIT_TRIES             1000000
44 /* Private functions */
46 /* _omap3_dpll_write_clken - write clken_bits arg to a DPLL's enable bits */
47 static void _omap3_dpll_write_clken(struct clk *clk, u8 clken_bits)
48 {
49         const struct dpll_data *dd;
50         u32 v;
52         dd = clk->dpll_data;
54         v = __raw_readl(dd->control_reg);
55         v &= ~dd->enable_mask;
56         v |= clken_bits << __ffs(dd->enable_mask);
57         __raw_writel(v, dd->control_reg);
58 }
60 /* _omap3_wait_dpll_status: wait for a DPLL to enter a specific state */
61 static int _omap3_wait_dpll_status(struct clk *clk, u8 state)
62 {
63         const struct dpll_data *dd;
64         int i = 0;
65         int ret = -EINVAL;
67         dd = clk->dpll_data;
69         state <<= __ffs(dd->idlest_mask);
71         while (((__raw_readl(dd->idlest_reg) & dd->idlest_mask) != state) &&
72                i < MAX_DPLL_WAIT_TRIES) {
73                 i++;
74                 udelay(1);
75         }
77         if (i == MAX_DPLL_WAIT_TRIES) {
78                 printk(KERN_ERR "clock: %s failed transition to '%s'\n",
79                        clk->name, (state) ? "locked" : "bypassed");
80         } else {
81                 pr_debug("clock: %s transition to '%s' in %d loops\n",
82                          clk->name, (state) ? "locked" : "bypassed", i);
84                 ret = 0;
85         }
87         return ret;
88 }
90 /* From 3430 TRM ES2 4.7.6.2 */
91 static u16 _omap3_dpll_compute_freqsel(struct clk *clk, u8 n)
92 {
93         unsigned long fint;
94         u16 f = 0;
96         fint = clk->dpll_data->clk_ref->rate / n;
98         pr_debug("clock: fint is %lu\n", fint);
100         if (fint >= 750000 && fint <= 1000000)
101                 f = 0x3;
102         else if (fint > 1000000 && fint <= 1250000)
103                 f = 0x4;
104         else if (fint > 1250000 && fint <= 1500000)
105                 f = 0x5;
106         else if (fint > 1500000 && fint <= 1750000)
107                 f = 0x6;
108         else if (fint > 1750000 && fint <= 2100000)
109                 f = 0x7;
110         else if (fint > 7500000 && fint <= 10000000)
111                 f = 0xB;
112         else if (fint > 10000000 && fint <= 12500000)
113                 f = 0xC;
114         else if (fint > 12500000 && fint <= 15000000)
115                 f = 0xD;
116         else if (fint > 15000000 && fint <= 17500000)
117                 f = 0xE;
118         else if (fint > 17500000 && fint <= 21000000)
119                 f = 0xF;
120         else
121                 pr_debug("clock: unknown freqsel setting for %d\n", n);
123         return f;
126 /*
127  * _omap3_noncore_dpll_lock - instruct a DPLL to lock and wait for readiness
128  * @clk: pointer to a DPLL struct clk
129  *
130  * Instructs a non-CORE DPLL to lock.  Waits for the DPLL to report
131  * readiness before returning.  Will save and restore the DPLL's
132  * autoidle state across the enable, per the CDP code.  If the DPLL
133  * locked successfully, return 0; if the DPLL did not lock in the time
134  * allotted, or DPLL3 was passed in, return -EINVAL.
135  */
136 static int _omap3_noncore_dpll_lock(struct clk *clk)
138         u8 ai;
139         int r;
141         pr_debug("clock: locking DPLL %s\n", clk->name);
143         ai = omap3_dpll_autoidle_read(clk);
145         if (ai)
146                 omap3_dpll_deny_idle(clk);
148         _omap3_dpll_write_clken(clk, DPLL_LOCKED);
150         r = _omap3_wait_dpll_status(clk, 1);
152         if (ai)
153                 omap3_dpll_allow_idle(clk);
155         return r;
158 /*
159  * _omap3_noncore_dpll_bypass - instruct a DPLL to bypass and wait for readiness
160  * @clk: pointer to a DPLL struct clk
161  *
162  * Instructs a non-CORE DPLL to enter low-power bypass mode.  In
163  * bypass mode, the DPLL's rate is set equal to its parent clock's
164  * rate.  Waits for the DPLL to report readiness before returning.
165  * Will save and restore the DPLL's autoidle state across the enable,
166  * per the CDP code.  If the DPLL entered bypass mode successfully,
167  * return 0; if the DPLL did not enter bypass in the time allotted, or
168  * DPLL3 was passed in, or the DPLL does not support low-power bypass,
169  * return -EINVAL.
170  */
171 static int _omap3_noncore_dpll_bypass(struct clk *clk)
173         int r;
174         u8 ai;
176         if (!(clk->dpll_data->modes & (1 << DPLL_LOW_POWER_BYPASS)))
177                 return -EINVAL;
179         pr_debug("clock: configuring DPLL %s for low-power bypass\n",
180                  clk->name);
182         ai = omap3_dpll_autoidle_read(clk);
184         _omap3_dpll_write_clken(clk, DPLL_LOW_POWER_BYPASS);
186         r = _omap3_wait_dpll_status(clk, 0);
188         if (ai)
189                 omap3_dpll_allow_idle(clk);
191         return r;
194 /*
195  * _omap3_noncore_dpll_stop - instruct a DPLL to stop
196  * @clk: pointer to a DPLL struct clk
197  *
198  * Instructs a non-CORE DPLL to enter low-power stop. Will save and
199  * restore the DPLL's autoidle state across the stop, per the CDP
200  * code.  If DPLL3 was passed in, or the DPLL does not support
201  * low-power stop, return -EINVAL; otherwise, return 0.
202  */
203 static int _omap3_noncore_dpll_stop(struct clk *clk)
205         u8 ai;
207         if (!(clk->dpll_data->modes & (1 << DPLL_LOW_POWER_STOP)))
208                 return -EINVAL;
210         pr_debug("clock: stopping DPLL %s\n", clk->name);
212         ai = omap3_dpll_autoidle_read(clk);
214         _omap3_dpll_write_clken(clk, DPLL_LOW_POWER_STOP);
216         if (ai)
217                 omap3_dpll_allow_idle(clk);
219         return 0;
222 /**
223  * _lookup_dco - Lookup DCO used by j-type DPLL
224  * @clk: pointer to a DPLL struct clk
225  * @dco: digital control oscillator selector
226  * @m: DPLL multiplier to set
227  * @n: DPLL divider to set
228  *
229  * See 36xx TRM section 3.5.3.3.3.2 "Type B DPLL (Low-Jitter)"
230  *
231  * XXX This code is not needed for 3430/AM35xx; can it be optimized
232  * out in non-multi-OMAP builds for those chips?
233  */
234 static void _lookup_dco(struct clk *clk, u8 *dco, u16 m, u8 n)
236         unsigned long fint, clkinp; /* watch out for overflow */
238         clkinp = clk->parent->rate;
239         fint = (clkinp / n) * m;
241         if (fint < 1000000000)
242                 *dco = 2;
243         else
244                 *dco = 4;
247 /**
248  * _lookup_sddiv - Calculate sigma delta divider for j-type DPLL
249  * @clk: pointer to a DPLL struct clk
250  * @sd_div: target sigma-delta divider
251  * @m: DPLL multiplier to set
252  * @n: DPLL divider to set
253  *
254  * See 36xx TRM section 3.5.3.3.3.2 "Type B DPLL (Low-Jitter)"
255  *
256  * XXX This code is not needed for 3430/AM35xx; can it be optimized
257  * out in non-multi-OMAP builds for those chips?
258  */
259 static void _lookup_sddiv(struct clk *clk, u8 *sd_div, u16 m, u8 n)
261         unsigned long clkinp, sd; /* watch out for overflow */
262         int mod1, mod2;
264         clkinp = clk->parent->rate;
266         /*
267          * target sigma-delta to near 250MHz
268          * sd = ceil[(m/(n+1)) * (clkinp_MHz / 250)]
269          */
270         clkinp /= 100000; /* shift from MHz to 10*Hz for 38.4 and 19.2 */
271         mod1 = (clkinp * m) % (250 * n);
272         sd = (clkinp * m) / (250 * n);
273         mod2 = sd % 10;
274         sd /= 10;
276         if (mod1 || mod2)
277                 sd++;
278         *sd_div = sd;
281 /*
282  * _omap3_noncore_dpll_program - set non-core DPLL M,N values directly
283  * @clk: struct clk * of DPLL to set
284  * @m: DPLL multiplier to set
285  * @n: DPLL divider to set
286  * @freqsel: FREQSEL value to set
287  *
288  * Program the DPLL with the supplied M, N values, and wait for the DPLL to
289  * lock..  Returns -EINVAL upon error, or 0 upon success.
290  */
291 static int omap3_noncore_dpll_program(struct clk *clk, u16 m, u8 n, u16 freqsel)
293         struct dpll_data *dd = clk->dpll_data;
294         u8 dco, sd_div;
295         u32 v;
297         /* 3430 ES2 TRM: 4.7.6.9 DPLL Programming Sequence */
298         _omap3_noncore_dpll_bypass(clk);
300         /*
301          * Set jitter correction. No jitter correction for OMAP4, 3630
302          * and AM33XX since freqsel field is no longer present
303          */
304         if (!cpu_is_omap44xx() && !cpu_is_omap3630() && !cpu_is_am33xx()) {
305                 v = __raw_readl(dd->control_reg);
306                 v &= ~dd->freqsel_mask;
307                 v |= freqsel << __ffs(dd->freqsel_mask);
308                 __raw_writel(v, dd->control_reg);
309         }
311         /* Set DPLL multiplier, divider */
312         v = __raw_readl(dd->mult_div1_reg);
313         v &= ~(dd->mult_mask | dd->div1_mask);
314         v |= m << __ffs(dd->mult_mask);
315         v |= (n - 1) << __ffs(dd->div1_mask);
317         /* Configure dco and sd_div for dplls that have these fields */
318         if (dd->dco_mask) {
319                 _lookup_dco(clk, &dco, m, n);
320                 v &= ~(dd->dco_mask);
321                 v |= dco << __ffs(dd->dco_mask);
322         }
323         if (dd->sddiv_mask) {
324                 _lookup_sddiv(clk, &sd_div, m, n);
325                 v &= ~(dd->sddiv_mask);
326                 v |= sd_div << __ffs(dd->sddiv_mask);
327         }
329         __raw_writel(v, dd->mult_div1_reg);
331         /* We let the clock framework set the other output dividers later */
333         /* REVISIT: Set ramp-up delay? */
335         _omap3_noncore_dpll_lock(clk);
337         return 0;
340 /* Public functions */
342 /**
343  * omap3_dpll_recalc - recalculate DPLL rate
344  * @clk: DPLL struct clk
345  *
346  * Recalculate and propagate the DPLL rate.
347  */
348 unsigned long omap3_dpll_recalc(struct clk *clk)
350         return omap2_get_dpll_rate(clk);
353 /* Non-CORE DPLL (e.g., DPLLs that do not control SDRC) clock functions */
355 /**
356  * omap3_noncore_dpll_enable - instruct a DPLL to enter bypass or lock mode
357  * @clk: pointer to a DPLL struct clk
358  *
359  * Instructs a non-CORE DPLL to enable, e.g., to enter bypass or lock.
360  * The choice of modes depends on the DPLL's programmed rate: if it is
361  * the same as the DPLL's parent clock, it will enter bypass;
362  * otherwise, it will enter lock.  This code will wait for the DPLL to
363  * indicate readiness before returning, unless the DPLL takes too long
364  * to enter the target state.  Intended to be used as the struct clk's
365  * enable function.  If DPLL3 was passed in, or the DPLL does not
366  * support low-power stop, or if the DPLL took too long to enter
367  * bypass or lock, return -EINVAL; otherwise, return 0.
368  */
369 int omap3_noncore_dpll_enable(struct clk *clk)
371         int r;
372         struct dpll_data *dd;
374         dd = clk->dpll_data;
375         if (!dd)
376                 return -EINVAL;
378         if (clk->rate == dd->clk_bypass->rate) {
379                 WARN_ON(clk->parent != dd->clk_bypass);
380                 r = _omap3_noncore_dpll_bypass(clk);
381         } else {
382                 WARN_ON(clk->parent != dd->clk_ref);
383                 r = _omap3_noncore_dpll_lock(clk);
384         }
385         /*
386          *FIXME: this is dubious - if clk->rate has changed, what about
387          * propagating?
388          */
389         if (!r)
390                 clk->rate = (clk->recalc) ? clk->recalc(clk) :
391                         omap2_get_dpll_rate(clk);
393         return r;
396 /**
397  * omap3_noncore_dpll_disable - instruct a DPLL to enter low-power stop
398  * @clk: pointer to a DPLL struct clk
399  *
400  * Instructs a non-CORE DPLL to enter low-power stop.  This function is
401  * intended for use in struct clkops.  No return value.
402  */
403 void omap3_noncore_dpll_disable(struct clk *clk)
405         _omap3_noncore_dpll_stop(clk);
409 /* Non-CORE DPLL rate set code */
411 /**
412  * omap3_noncore_dpll_set_rate - set non-core DPLL rate
413  * @clk: struct clk * of DPLL to set
414  * @rate: rounded target rate
415  *
416  * Set the DPLL CLKOUT to the target rate.  If the DPLL can enter
417  * low-power bypass, and the target rate is the bypass source clock
418  * rate, then configure the DPLL for bypass.  Otherwise, round the
419  * target rate if it hasn't been done already, then program and lock
420  * the DPLL.  Returns -EINVAL upon error, or 0 upon success.
421  */
422 int omap3_noncore_dpll_set_rate(struct clk *clk, unsigned long rate)
424         struct clk *new_parent = NULL;
425         unsigned long hw_rate;
426         u16 freqsel = 0;
427         struct dpll_data *dd;
428         int ret;
430         if (!clk || !rate)
431                 return -EINVAL;
433         dd = clk->dpll_data;
434         if (!dd)
435                 return -EINVAL;
437         hw_rate = (clk->recalc) ? clk->recalc(clk) : omap2_get_dpll_rate(clk);
438         if (rate == hw_rate)
439                 return 0;
441         /*
442          * Ensure both the bypass and ref clocks are enabled prior to
443          * doing anything; we need the bypass clock running to reprogram
444          * the DPLL.
445          */
446         omap2_clk_enable(dd->clk_bypass);
447         omap2_clk_enable(dd->clk_ref);
449         if (dd->clk_bypass->rate == rate &&
450             (clk->dpll_data->modes & (1 << DPLL_LOW_POWER_BYPASS))) {
451                 pr_debug("clock: %s: set rate: entering bypass.\n", clk->name);
453                 ret = _omap3_noncore_dpll_bypass(clk);
454                 if (!ret)
455                         new_parent = dd->clk_bypass;
456         } else {
457                 if (dd->last_rounded_rate != rate)
458                         rate = clk->round_rate(clk, rate);
460                 if (dd->last_rounded_rate == 0)
461                         return -EINVAL;
463                 /* No freqsel on OMAP4, OMAP3630 and AM33XX */
464                 if (!cpu_is_omap44xx() && !cpu_is_omap3630() &&
465                         !cpu_is_am33xx()) {
466                         freqsel = _omap3_dpll_compute_freqsel(clk,
467                                                 dd->last_rounded_n);
468                         if (!freqsel)
469                                 WARN_ON(1);
470                 }
472                 pr_debug("clock: %s: set rate: locking rate to %lu.\n",
473                          clk->name, rate);
475                 ret = omap3_noncore_dpll_program(clk, dd->last_rounded_m,
476                                                  dd->last_rounded_n, freqsel);
477                 if (!ret)
478                         new_parent = dd->clk_ref;
479         }
480         if (!ret) {
481                 /*
482                  * Switch the parent clock in the hierarchy, and make sure
483                  * that the new parent's usecount is correct.  Note: we
484                  * enable the new parent before disabling the old to avoid
485                  * any unnecessary hardware disable->enable transitions.
486                  */
487                 if (clk->usecount) {
488                         omap2_clk_enable(new_parent);
489                         omap2_clk_disable(clk->parent);
490                 }
491                 clk_reparent(clk, new_parent);
492                 clk->rate = rate;
493         }
494         omap2_clk_disable(dd->clk_ref);
495         omap2_clk_disable(dd->clk_bypass);
497         return 0;
500 /* DPLL autoidle read/set code */
502 /**
503  * omap3_dpll_autoidle_read - read a DPLL's autoidle bits
504  * @clk: struct clk * of the DPLL to read
505  *
506  * Return the DPLL's autoidle bits, shifted down to bit 0.  Returns
507  * -EINVAL if passed a null pointer or if the struct clk does not
508  * appear to refer to a DPLL.
509  */
510 u32 omap3_dpll_autoidle_read(struct clk *clk)
512         const struct dpll_data *dd;
513         u32 v;
515         if (!clk || !clk->dpll_data)
516                 return -EINVAL;
518         dd = clk->dpll_data;
520         if (!dd->autoidle_reg)
521                 return -EINVAL;
523         v = __raw_readl(dd->autoidle_reg);
524         v &= dd->autoidle_mask;
525         v >>= __ffs(dd->autoidle_mask);
527         return v;
530 /**
531  * omap3_dpll_allow_idle - enable DPLL autoidle bits
532  * @clk: struct clk * of the DPLL to operate on
533  *
534  * Enable DPLL automatic idle control.  This automatic idle mode
535  * switching takes effect only when the DPLL is locked, at least on
536  * OMAP3430.  The DPLL will enter low-power stop when its downstream
537  * clocks are gated.  No return value.
538  */
539 void omap3_dpll_allow_idle(struct clk *clk)
541         const struct dpll_data *dd;
542         u32 v;
544         if (!clk || !clk->dpll_data)
545                 return;
547         dd = clk->dpll_data;
549         if (!dd->autoidle_reg) {
550                 pr_debug("clock: DPLL %s: autoidle not supported\n",
551                         clk->name);
552                 return;
553         }
555         /*
556          * REVISIT: CORE DPLL can optionally enter low-power bypass
557          * by writing 0x5 instead of 0x1.  Add some mechanism to
558          * optionally enter this mode.
559          */
560         v = __raw_readl(dd->autoidle_reg);
561         v &= ~dd->autoidle_mask;
562         v |= DPLL_AUTOIDLE_LOW_POWER_STOP << __ffs(dd->autoidle_mask);
563         __raw_writel(v, dd->autoidle_reg);
567 /**
568  * omap3_dpll_deny_idle - prevent DPLL from automatically idling
569  * @clk: struct clk * of the DPLL to operate on
570  *
571  * Disable DPLL automatic idle control.  No return value.
572  */
573 void omap3_dpll_deny_idle(struct clk *clk)
575         const struct dpll_data *dd;
576         u32 v;
578         if (!clk || !clk->dpll_data)
579                 return;
581         dd = clk->dpll_data;
583         if (!dd->autoidle_reg) {
584                 pr_debug("clock: DPLL %s: autoidle not supported\n",
585                         clk->name);
586                 return;
587         }
589         v = __raw_readl(dd->autoidle_reg);
590         v &= ~dd->autoidle_mask;
591         v |= DPLL_AUTOIDLE_DISABLE << __ffs(dd->autoidle_mask);
592         __raw_writel(v, dd->autoidle_reg);
596 /* Clock control for DPLL outputs */
598 /**
599  * omap3_clkoutx2_recalc - recalculate DPLL X2 output virtual clock rate
600  * @clk: DPLL output struct clk
601  *
602  * Using parent clock DPLL data, look up DPLL state.  If locked, set our
603  * rate to the dpll_clk * 2; otherwise, just use dpll_clk.
604  */
605 unsigned long omap3_clkoutx2_recalc(struct clk *clk)
607         const struct dpll_data *dd;
608         unsigned long rate;
609         u32 v;
610         struct clk *pclk;
612         /* Walk up the parents of clk, looking for a DPLL */
613         pclk = clk->parent;
614         while (pclk && !pclk->dpll_data)
615                 pclk = pclk->parent;
617         /* clk does not have a DPLL as a parent? */
618         WARN_ON(!pclk);
620         dd = pclk->dpll_data;
622         WARN_ON(!dd->enable_mask);
624         v = __raw_readl(dd->control_reg) & dd->enable_mask;
625         v >>= __ffs(dd->enable_mask);
626         if ((v != OMAP3XXX_EN_DPLL_LOCKED) || (dd->flags & DPLL_J_TYPE))
627                 rate = clk->parent->rate;
628         else
629                 rate = clk->parent->rate * 2;
630         return rate;