]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - arch/arm/mach-omap2/dpll3xxx.c
Merge branch 'msm-fix' of git://codeaurora.org/quic/kernel/davidb/linux-msm into...
[sitara-epos/sitara-epos-kernel.git] / arch / arm / mach-omap2 / dpll3xxx.c
1 /*
2  * OMAP3/4 - specific DPLL control functions
3  *
4  * Copyright (C) 2009-2010 Texas Instruments, Inc.
5  * Copyright (C) 2009-2010 Nokia Corporation
6  *
7  * Written by Paul Walmsley
8  * Testing and integration fixes by Jouni Högander
9  *
10  * 36xx support added by Vishwanath BS, Richard Woodruff, and Nishanth
11  * Menon
12  *
13  * Parts of this code are based on code written by
14  * Richard Woodruff, Tony Lindgren, Tuukka Tikkanen, Karthik Dasu
15  *
16  * This program is free software; you can redistribute it and/or modify
17  * it under the terms of the GNU General Public License version 2 as
18  * published by the Free Software Foundation.
19  */
21 #include <linux/kernel.h>
22 #include <linux/device.h>
23 #include <linux/list.h>
24 #include <linux/errno.h>
25 #include <linux/delay.h>
26 #include <linux/clk.h>
27 #include <linux/io.h>
28 #include <linux/bitops.h>
29 #include <linux/clkdev.h>
31 #include <plat/cpu.h>
32 #include <plat/clock.h>
34 #include "clock.h"
35 #include "cm2xxx_3xxx.h"
36 #include "cm-regbits-34xx.h"
38 /* CM_AUTOIDLE_PLL*.AUTO_* bit values */
39 #define DPLL_AUTOIDLE_DISABLE                   0x0
40 #define DPLL_AUTOIDLE_LOW_POWER_STOP            0x1
42 #define MAX_DPLL_WAIT_TRIES             1000000
44 /* Private functions */
46 /* _omap3_dpll_write_clken - write clken_bits arg to a DPLL's enable bits */
47 static void _omap3_dpll_write_clken(struct clk *clk, u8 clken_bits)
48 {
49         const struct dpll_data *dd;
50         u32 v;
52         dd = clk->dpll_data;
54         v = __raw_readl(dd->control_reg);
55         v &= ~dd->enable_mask;
56         v |= clken_bits << __ffs(dd->enable_mask);
57         __raw_writel(v, dd->control_reg);
58 }
60 /* _omap3_wait_dpll_status: wait for a DPLL to enter a specific state */
61 static int _omap3_wait_dpll_status(struct clk *clk, u8 state)
62 {
63         const struct dpll_data *dd;
64         int i = 0;
65         int ret = -EINVAL;
67         dd = clk->dpll_data;
69         state <<= __ffs(dd->idlest_mask);
71         while (((__raw_readl(dd->idlest_reg) & dd->idlest_mask) != state) &&
72                i < MAX_DPLL_WAIT_TRIES) {
73                 i++;
74                 udelay(1);
75         }
77         if (i == MAX_DPLL_WAIT_TRIES) {
78                 printk(KERN_ERR "clock: %s failed transition to '%s'\n",
79                        clk->name, (state) ? "locked" : "bypassed");
80         } else {
81                 pr_debug("clock: %s transition to '%s' in %d loops\n",
82                          clk->name, (state) ? "locked" : "bypassed", i);
84                 ret = 0;
85         }
87         return ret;
88 }
90 /* From 3430 TRM ES2 4.7.6.2 */
91 static u16 _omap3_dpll_compute_freqsel(struct clk *clk, u8 n)
92 {
93         unsigned long fint;
94         u16 f = 0;
96         fint = clk->dpll_data->clk_ref->rate / n;
98         pr_debug("clock: fint is %lu\n", fint);
100         if (fint >= 750000 && fint <= 1000000)
101                 f = 0x3;
102         else if (fint > 1000000 && fint <= 1250000)
103                 f = 0x4;
104         else if (fint > 1250000 && fint <= 1500000)
105                 f = 0x5;
106         else if (fint > 1500000 && fint <= 1750000)
107                 f = 0x6;
108         else if (fint > 1750000 && fint <= 2100000)
109                 f = 0x7;
110         else if (fint > 7500000 && fint <= 10000000)
111                 f = 0xB;
112         else if (fint > 10000000 && fint <= 12500000)
113                 f = 0xC;
114         else if (fint > 12500000 && fint <= 15000000)
115                 f = 0xD;
116         else if (fint > 15000000 && fint <= 17500000)
117                 f = 0xE;
118         else if (fint > 17500000 && fint <= 21000000)
119                 f = 0xF;
120         else
121                 pr_debug("clock: unknown freqsel setting for %d\n", n);
123         return f;
126 /*
127  * _omap3_noncore_dpll_lock - instruct a DPLL to lock and wait for readiness
128  * @clk: pointer to a DPLL struct clk
129  *
130  * Instructs a non-CORE DPLL to lock.  Waits for the DPLL to report
131  * readiness before returning.  Will save and restore the DPLL's
132  * autoidle state across the enable, per the CDP code.  If the DPLL
133  * locked successfully, return 0; if the DPLL did not lock in the time
134  * allotted, or DPLL3 was passed in, return -EINVAL.
135  */
136 static int _omap3_noncore_dpll_lock(struct clk *clk)
138         u8 ai;
139         int r;
141         pr_debug("clock: locking DPLL %s\n", clk->name);
143         ai = omap3_dpll_autoidle_read(clk);
145         omap3_dpll_deny_idle(clk);
147         _omap3_dpll_write_clken(clk, DPLL_LOCKED);
149         r = _omap3_wait_dpll_status(clk, 1);
151         if (ai)
152                 omap3_dpll_allow_idle(clk);
154         return r;
157 /*
158  * _omap3_noncore_dpll_bypass - instruct a DPLL to bypass and wait for readiness
159  * @clk: pointer to a DPLL struct clk
160  *
161  * Instructs a non-CORE DPLL to enter low-power bypass mode.  In
162  * bypass mode, the DPLL's rate is set equal to its parent clock's
163  * rate.  Waits for the DPLL to report readiness before returning.
164  * Will save and restore the DPLL's autoidle state across the enable,
165  * per the CDP code.  If the DPLL entered bypass mode successfully,
166  * return 0; if the DPLL did not enter bypass in the time allotted, or
167  * DPLL3 was passed in, or the DPLL does not support low-power bypass,
168  * return -EINVAL.
169  */
170 static int _omap3_noncore_dpll_bypass(struct clk *clk)
172         int r;
173         u8 ai;
175         if (!(clk->dpll_data->modes & (1 << DPLL_LOW_POWER_BYPASS)))
176                 return -EINVAL;
178         pr_debug("clock: configuring DPLL %s for low-power bypass\n",
179                  clk->name);
181         ai = omap3_dpll_autoidle_read(clk);
183         _omap3_dpll_write_clken(clk, DPLL_LOW_POWER_BYPASS);
185         r = _omap3_wait_dpll_status(clk, 0);
187         if (ai)
188                 omap3_dpll_allow_idle(clk);
189         else
190                 omap3_dpll_deny_idle(clk);
192         return r;
195 /*
196  * _omap3_noncore_dpll_stop - instruct a DPLL to stop
197  * @clk: pointer to a DPLL struct clk
198  *
199  * Instructs a non-CORE DPLL to enter low-power stop. Will save and
200  * restore the DPLL's autoidle state across the stop, per the CDP
201  * code.  If DPLL3 was passed in, or the DPLL does not support
202  * low-power stop, return -EINVAL; otherwise, return 0.
203  */
204 static int _omap3_noncore_dpll_stop(struct clk *clk)
206         u8 ai;
208         if (!(clk->dpll_data->modes & (1 << DPLL_LOW_POWER_STOP)))
209                 return -EINVAL;
211         pr_debug("clock: stopping DPLL %s\n", clk->name);
213         ai = omap3_dpll_autoidle_read(clk);
215         _omap3_dpll_write_clken(clk, DPLL_LOW_POWER_STOP);
217         if (ai)
218                 omap3_dpll_allow_idle(clk);
219         else
220                 omap3_dpll_deny_idle(clk);
222         return 0;
225 /**
226  * _lookup_dco - Lookup DCO used by j-type DPLL
227  * @clk: pointer to a DPLL struct clk
228  * @dco: digital control oscillator selector
229  * @m: DPLL multiplier to set
230  * @n: DPLL divider to set
231  *
232  * See 36xx TRM section 3.5.3.3.3.2 "Type B DPLL (Low-Jitter)"
233  *
234  * XXX This code is not needed for 3430/AM35xx; can it be optimized
235  * out in non-multi-OMAP builds for those chips?
236  */
237 static void _lookup_dco(struct clk *clk, u8 *dco, u16 m, u8 n)
239         unsigned long fint, clkinp; /* watch out for overflow */
241         clkinp = clk->parent->rate;
242         fint = (clkinp / n) * m;
244         if (fint < 1000000000)
245                 *dco = 2;
246         else
247                 *dco = 4;
250 /**
251  * _lookup_sddiv - Calculate sigma delta divider for j-type DPLL
252  * @clk: pointer to a DPLL struct clk
253  * @sd_div: target sigma-delta divider
254  * @m: DPLL multiplier to set
255  * @n: DPLL divider to set
256  *
257  * See 36xx TRM section 3.5.3.3.3.2 "Type B DPLL (Low-Jitter)"
258  *
259  * XXX This code is not needed for 3430/AM35xx; can it be optimized
260  * out in non-multi-OMAP builds for those chips?
261  */
262 static void _lookup_sddiv(struct clk *clk, u8 *sd_div, u16 m, u8 n)
264         unsigned long clkinp, sd; /* watch out for overflow */
265         int mod1, mod2;
267         clkinp = clk->parent->rate;
269         /*
270          * target sigma-delta to near 250MHz
271          * sd = ceil[(m/(n+1)) * (clkinp_MHz / 250)]
272          */
273         clkinp /= 100000; /* shift from MHz to 10*Hz for 38.4 and 19.2 */
274         mod1 = (clkinp * m) % (250 * n);
275         sd = (clkinp * m) / (250 * n);
276         mod2 = sd % 10;
277         sd /= 10;
279         if (mod1 || mod2)
280                 sd++;
281         *sd_div = sd;
284 /*
285  * _omap3_noncore_dpll_program - set non-core DPLL M,N values directly
286  * @clk: struct clk * of DPLL to set
287  * @m: DPLL multiplier to set
288  * @n: DPLL divider to set
289  * @freqsel: FREQSEL value to set
290  *
291  * Program the DPLL with the supplied M, N values, and wait for the DPLL to
292  * lock..  Returns -EINVAL upon error, or 0 upon success.
293  */
294 static int omap3_noncore_dpll_program(struct clk *clk, u16 m, u8 n, u16 freqsel)
296         struct dpll_data *dd = clk->dpll_data;
297         u8 dco, sd_div;
298         u32 v;
300         /* 3430 ES2 TRM: 4.7.6.9 DPLL Programming Sequence */
301         _omap3_noncore_dpll_bypass(clk);
303         /*
304          * Set jitter correction. No jitter correction for OMAP4 and 3630
305          * since freqsel field is no longer present
306          */
307         if (!cpu_is_omap44xx() && !cpu_is_omap3630()) {
308                 v = __raw_readl(dd->control_reg);
309                 v &= ~dd->freqsel_mask;
310                 v |= freqsel << __ffs(dd->freqsel_mask);
311                 __raw_writel(v, dd->control_reg);
312         }
314         /* Set DPLL multiplier, divider */
315         v = __raw_readl(dd->mult_div1_reg);
316         v &= ~(dd->mult_mask | dd->div1_mask);
317         v |= m << __ffs(dd->mult_mask);
318         v |= (n - 1) << __ffs(dd->div1_mask);
320         /* Configure dco and sd_div for dplls that have these fields */
321         if (dd->dco_mask) {
322                 _lookup_dco(clk, &dco, m, n);
323                 v &= ~(dd->dco_mask);
324                 v |= dco << __ffs(dd->dco_mask);
325         }
326         if (dd->sddiv_mask) {
327                 _lookup_sddiv(clk, &sd_div, m, n);
328                 v &= ~(dd->sddiv_mask);
329                 v |= sd_div << __ffs(dd->sddiv_mask);
330         }
332         __raw_writel(v, dd->mult_div1_reg);
334         /* We let the clock framework set the other output dividers later */
336         /* REVISIT: Set ramp-up delay? */
338         _omap3_noncore_dpll_lock(clk);
340         return 0;
343 /* Public functions */
345 /**
346  * omap3_dpll_recalc - recalculate DPLL rate
347  * @clk: DPLL struct clk
348  *
349  * Recalculate and propagate the DPLL rate.
350  */
351 unsigned long omap3_dpll_recalc(struct clk *clk)
353         return omap2_get_dpll_rate(clk);
356 /* Non-CORE DPLL (e.g., DPLLs that do not control SDRC) clock functions */
358 /**
359  * omap3_noncore_dpll_enable - instruct a DPLL to enter bypass or lock mode
360  * @clk: pointer to a DPLL struct clk
361  *
362  * Instructs a non-CORE DPLL to enable, e.g., to enter bypass or lock.
363  * The choice of modes depends on the DPLL's programmed rate: if it is
364  * the same as the DPLL's parent clock, it will enter bypass;
365  * otherwise, it will enter lock.  This code will wait for the DPLL to
366  * indicate readiness before returning, unless the DPLL takes too long
367  * to enter the target state.  Intended to be used as the struct clk's
368  * enable function.  If DPLL3 was passed in, or the DPLL does not
369  * support low-power stop, or if the DPLL took too long to enter
370  * bypass or lock, return -EINVAL; otherwise, return 0.
371  */
372 int omap3_noncore_dpll_enable(struct clk *clk)
374         int r;
375         struct dpll_data *dd;
377         dd = clk->dpll_data;
378         if (!dd)
379                 return -EINVAL;
381         if (clk->rate == dd->clk_bypass->rate) {
382                 WARN_ON(clk->parent != dd->clk_bypass);
383                 r = _omap3_noncore_dpll_bypass(clk);
384         } else {
385                 WARN_ON(clk->parent != dd->clk_ref);
386                 r = _omap3_noncore_dpll_lock(clk);
387         }
388         /*
389          *FIXME: this is dubious - if clk->rate has changed, what about
390          * propagating?
391          */
392         if (!r)
393                 clk->rate = (clk->recalc) ? clk->recalc(clk) :
394                         omap2_get_dpll_rate(clk);
396         return r;
399 /**
400  * omap3_noncore_dpll_disable - instruct a DPLL to enter low-power stop
401  * @clk: pointer to a DPLL struct clk
402  *
403  * Instructs a non-CORE DPLL to enter low-power stop.  This function is
404  * intended for use in struct clkops.  No return value.
405  */
406 void omap3_noncore_dpll_disable(struct clk *clk)
408         _omap3_noncore_dpll_stop(clk);
412 /* Non-CORE DPLL rate set code */
414 /**
415  * omap3_noncore_dpll_set_rate - set non-core DPLL rate
416  * @clk: struct clk * of DPLL to set
417  * @rate: rounded target rate
418  *
419  * Set the DPLL CLKOUT to the target rate.  If the DPLL can enter
420  * low-power bypass, and the target rate is the bypass source clock
421  * rate, then configure the DPLL for bypass.  Otherwise, round the
422  * target rate if it hasn't been done already, then program and lock
423  * the DPLL.  Returns -EINVAL upon error, or 0 upon success.
424  */
425 int omap3_noncore_dpll_set_rate(struct clk *clk, unsigned long rate)
427         struct clk *new_parent = NULL;
428         unsigned long hw_rate;
429         u16 freqsel = 0;
430         struct dpll_data *dd;
431         int ret;
433         if (!clk || !rate)
434                 return -EINVAL;
436         dd = clk->dpll_data;
437         if (!dd)
438                 return -EINVAL;
440         hw_rate = (clk->recalc) ? clk->recalc(clk) : omap2_get_dpll_rate(clk);
441         if (rate == hw_rate)
442                 return 0;
444         /*
445          * Ensure both the bypass and ref clocks are enabled prior to
446          * doing anything; we need the bypass clock running to reprogram
447          * the DPLL.
448          */
449         omap2_clk_enable(dd->clk_bypass);
450         omap2_clk_enable(dd->clk_ref);
452         if (dd->clk_bypass->rate == rate &&
453             (clk->dpll_data->modes & (1 << DPLL_LOW_POWER_BYPASS))) {
454                 pr_debug("clock: %s: set rate: entering bypass.\n", clk->name);
456                 ret = _omap3_noncore_dpll_bypass(clk);
457                 if (!ret)
458                         new_parent = dd->clk_bypass;
459         } else {
460                 if (dd->last_rounded_rate != rate)
461                         rate = clk->round_rate(clk, rate);
463                 if (dd->last_rounded_rate == 0)
464                         return -EINVAL;
466                 /* No freqsel on OMAP4 and OMAP3630 */
467                 if (!cpu_is_omap44xx() && !cpu_is_omap3630()) {
468                         freqsel = _omap3_dpll_compute_freqsel(clk,
469                                                 dd->last_rounded_n);
470                         if (!freqsel)
471                                 WARN_ON(1);
472                 }
474                 pr_debug("clock: %s: set rate: locking rate to %lu.\n",
475                          clk->name, rate);
477                 ret = omap3_noncore_dpll_program(clk, dd->last_rounded_m,
478                                                  dd->last_rounded_n, freqsel);
479                 if (!ret)
480                         new_parent = dd->clk_ref;
481         }
482         if (!ret) {
483                 /*
484                  * Switch the parent clock in the hierarchy, and make sure
485                  * that the new parent's usecount is correct.  Note: we
486                  * enable the new parent before disabling the old to avoid
487                  * any unnecessary hardware disable->enable transitions.
488                  */
489                 if (clk->usecount) {
490                         omap2_clk_enable(new_parent);
491                         omap2_clk_disable(clk->parent);
492                 }
493                 clk_reparent(clk, new_parent);
494                 clk->rate = rate;
495         }
496         omap2_clk_disable(dd->clk_ref);
497         omap2_clk_disable(dd->clk_bypass);
499         return 0;
502 /* DPLL autoidle read/set code */
504 /**
505  * omap3_dpll_autoidle_read - read a DPLL's autoidle bits
506  * @clk: struct clk * of the DPLL to read
507  *
508  * Return the DPLL's autoidle bits, shifted down to bit 0.  Returns
509  * -EINVAL if passed a null pointer or if the struct clk does not
510  * appear to refer to a DPLL.
511  */
512 u32 omap3_dpll_autoidle_read(struct clk *clk)
514         const struct dpll_data *dd;
515         u32 v;
517         if (!clk || !clk->dpll_data)
518                 return -EINVAL;
520         dd = clk->dpll_data;
522         v = __raw_readl(dd->autoidle_reg);
523         v &= dd->autoidle_mask;
524         v >>= __ffs(dd->autoidle_mask);
526         return v;
529 /**
530  * omap3_dpll_allow_idle - enable DPLL autoidle bits
531  * @clk: struct clk * of the DPLL to operate on
532  *
533  * Enable DPLL automatic idle control.  This automatic idle mode
534  * switching takes effect only when the DPLL is locked, at least on
535  * OMAP3430.  The DPLL will enter low-power stop when its downstream
536  * clocks are gated.  No return value.
537  */
538 void omap3_dpll_allow_idle(struct clk *clk)
540         const struct dpll_data *dd;
541         u32 v;
543         if (!clk || !clk->dpll_data)
544                 return;
546         dd = clk->dpll_data;
548         /*
549          * REVISIT: CORE DPLL can optionally enter low-power bypass
550          * by writing 0x5 instead of 0x1.  Add some mechanism to
551          * optionally enter this mode.
552          */
553         v = __raw_readl(dd->autoidle_reg);
554         v &= ~dd->autoidle_mask;
555         v |= DPLL_AUTOIDLE_LOW_POWER_STOP << __ffs(dd->autoidle_mask);
556         __raw_writel(v, dd->autoidle_reg);
559 /**
560  * omap3_dpll_deny_idle - prevent DPLL from automatically idling
561  * @clk: struct clk * of the DPLL to operate on
562  *
563  * Disable DPLL automatic idle control.  No return value.
564  */
565 void omap3_dpll_deny_idle(struct clk *clk)
567         const struct dpll_data *dd;
568         u32 v;
570         if (!clk || !clk->dpll_data)
571                 return;
573         dd = clk->dpll_data;
575         v = __raw_readl(dd->autoidle_reg);
576         v &= ~dd->autoidle_mask;
577         v |= DPLL_AUTOIDLE_DISABLE << __ffs(dd->autoidle_mask);
578         __raw_writel(v, dd->autoidle_reg);
582 /* Clock control for DPLL outputs */
584 /**
585  * omap3_clkoutx2_recalc - recalculate DPLL X2 output virtual clock rate
586  * @clk: DPLL output struct clk
587  *
588  * Using parent clock DPLL data, look up DPLL state.  If locked, set our
589  * rate to the dpll_clk * 2; otherwise, just use dpll_clk.
590  */
591 unsigned long omap3_clkoutx2_recalc(struct clk *clk)
593         const struct dpll_data *dd;
594         unsigned long rate;
595         u32 v;
596         struct clk *pclk;
598         /* Walk up the parents of clk, looking for a DPLL */
599         pclk = clk->parent;
600         while (pclk && !pclk->dpll_data)
601                 pclk = pclk->parent;
603         /* clk does not have a DPLL as a parent? */
604         WARN_ON(!pclk);
606         dd = pclk->dpll_data;
608         WARN_ON(!dd->enable_mask);
610         v = __raw_readl(dd->control_reg) & dd->enable_mask;
611         v >>= __ffs(dd->enable_mask);
612         if ((v != OMAP3XXX_EN_DPLL_LOCKED) || (dd->flags & DPLL_J_TYPE))
613                 rate = clk->parent->rate;
614         else
615                 rate = clk->parent->rate * 2;
616         return rate;