ARM: OMAP: AM33XX: Basic suspend resume support
[sitara-epos/sitara-epos-kernel.git] / arch / arm / mach-omap2 / pm33xx.c
1 /*
2  * AM33XX Power Management Routines
3  *
4  * Copyright (C) 2012 Texas Instruments Incorporated - http://www.ti.com/
5  *
6  * This program is free software; you can redistribute it and/or
7  * modify it under the terms of the GNU General Public License as
8  * published by the Free Software Foundation version 2.
9  *
10  * This program is distributed "as is" WITHOUT ANY WARRANTY of any
11  * kind, whether express or implied; without even the implied warranty
12  * of MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
13  * GNU General Public License for more details.
14  */
16 #include <linux/kernel.h>
17 #include <linux/init.h>
18 #include <linux/clk.h>
19 #include <linux/console.h>
20 #include <linux/err.h>
21 #include <linux/firmware.h>
22 #include <linux/io.h>
23 #include <linux/platform_device.h>
24 #include <linux/sched.h>
25 #include <linux/suspend.h>
27 #include <plat/prcm.h>
28 #include <plat/mailbox.h>
29 #include <plat/sram.h>
30 #include <plat/omap_hwmod.h>
31 #include <plat/omap_device.h>
33 #include <asm/suspend.h>
34 #include <asm/proc-fns.h>
35 #include <asm/sizes.h>
37 #include "pm.h"
39 static int m3_state;
40 static struct device *mpu_dev;
41 struct omap_mbox *m3_mbox;
42 void __iomem *ipc_regs;
43 void __iomem *m3_eoi;
44 void __iomem *m3_code;
46 bool enable_deep_sleep = true;
48 struct a8_wkup_m3_ipc_data {
49         int resume_addr;
50         int sleep_mode;
51         int ipc_data1;
52         int ipc_data2;
53 } am33xx_lp_ipc;
55 static int am33xx_set_low_power_state(struct a8_wkup_m3_ipc_data *);
56 void (*am33xx_do_wfi_sram)(void);
58 #define DS_RESUME_ADDR  0x40300010
59 #define DS_MODE         0x5
60 #define DS_IPC_DEFAULT  0xffffffff
62 #define A8_M3_IPC_REGS  0x44E11328
63 #define M3_TXEV_EOI     0x44E11324
65 #ifdef CONFIG_SUSPEND
66 static suspend_state_t suspend_state = PM_SUSPEND_ON;
68 static int am33xx_do_sram_idle(long unsigned int state)
69 {
70         am33xx_do_wfi_sram();
71         return 0;
72 }
74 static inline bool is_suspending(void)
75 {
76         return (suspend_state != PM_SUSPEND_ON) && console_suspend_enabled;
77 }
79 static int am33xx_pm_suspend(void)
80 {
81         int ret = 0;
83         /* Block console output in case it is on one of the OMAP UARTs */
84         if (!is_suspending()) {
85                 if (!console_trylock()) {
86                         ret = -EAGAIN;
87                         goto err;
88                 }
89         }
91         ret = cpu_suspend(0, am33xx_do_sram_idle);
92         if (ret)
93                 pr_err("Could not suspend\n");
94         else
95                 goto done;
97 err:
98         pr_err("Console still active\n");
99 done:
100         return ret;
103 static int am33xx_pm_enter(suspend_state_t unused)
105         int ret = 0;
107         switch (suspend_state) {
108         case PM_SUSPEND_STANDBY:
109         case PM_SUSPEND_MEM:
110                 ret = am33xx_pm_suspend();
111                 break;
112         default:
113                 ret = -EINVAL;
114         }
116         return ret;
119 static int am33xx_pm_begin(suspend_state_t state)
121         int ret = 0;
123         am33xx_lp_ipc.resume_addr = DS_RESUME_ADDR;
124         am33xx_lp_ipc.sleep_mode  = DS_MODE;
125         am33xx_lp_ipc.ipc_data1   = DS_IPC_DEFAULT;
126         am33xx_lp_ipc.ipc_data2   = DS_IPC_DEFAULT;
128         am33xx_set_low_power_state(&am33xx_lp_ipc);
130         ret = omap_mbox_msg_send(m3_mbox, 0xABCDABCD);
131         if (!ret) {
132                 pr_info("Message sent\n");
133                 omap_mbox_msg_rx_flush(m3_mbox);
134         }
136         omap_mbox_disable_irq(m3_mbox, IRQ_RX);
138         disable_hlt();
139         suspend_state = state;
141         return ret;
144 static void am33xx_pm_end(void)
146         suspend_state = PM_SUSPEND_ON;
148         if (!is_suspending())
149                 console_unlock();
151         omap_mbox_enable_irq(m3_mbox, IRQ_RX);
152         return;
155 static const struct platform_suspend_ops am33xx_pm_ops = {
156         .begin          = am33xx_pm_begin,
157         .end            = am33xx_pm_end,
158         .enter          = am33xx_pm_enter,
159         .valid          = suspend_valid_only_mem,
160 };
161 #endif /* CONFIG_SUSPEND */
163 /*
164  * Push the minimal suspend-resume code to SRAM
165  */
166 void am33xx_push_sram_idle(void)
168         am33xx_do_wfi_sram = omap_sram_push(am33xx_do_wfi, am33xx_do_wfi_sz);
171 int am33xx_set_low_power_state(struct a8_wkup_m3_ipc_data *data)
173         __raw_writel(data->resume_addr, ipc_regs);
174         __raw_writel(data->sleep_mode, ipc_regs + 0x4);
175         __raw_writel(data->ipc_data1, ipc_regs + 0x8);
176         __raw_writel(data->ipc_data2, ipc_regs + 0xc);
178         return 0;
181 /*
182  * Dummy notifier for the mailbox
183  * TODO: Can this be completely removed?
184  */
185 int wkup_m3_mbox_msg(struct notifier_block *self, unsigned long len, void *msg)
187         return 0;
190 static struct notifier_block wkup_m3_mbox_notifier = {
191         .notifier_call = wkup_m3_mbox_msg,
192 };
194 /* Interrupt from M3 to A8 */
195 static irqreturn_t wkup_m3_txev_handler(int irq, void *unused)
197         m3_state++;
199         if (m3_eoi) {
200                 __raw_writel(0x1, m3_eoi);
201                 __raw_writel(0x0, m3_eoi);
202                 return IRQ_HANDLED;
203         } else {
204                 pr_err("%s unexpected interrupt. "
205                 "Something is seriously wrong\n", __func__);
206                 return IRQ_NONE;
207         }
210 /* Initiliaze WKUP_M3, load the binary blob and let it run */
211 static int wkup_m3_init(void)
213         struct clk *m3_clk;
214         struct omap_hwmod *wkup_m3_oh;
215         const struct firmware *firmware;
216         int ret = 0;
218         wkup_m3_oh = omap_hwmod_lookup("wkup_m3");
220         if (!wkup_m3_oh) {
221                 pr_err("%s: could not find omap_hwmod\n", __func__);
222                 ret = -ENODEV;
223                 goto exit;
224         }
226         ipc_regs = ioremap(A8_M3_IPC_REGS, 0x4*8);
227         if (!ipc_regs) {
228                 pr_err("Could not ioremap the IPC area\b");
229                 ret = -ENOMEM;
230                 goto exit;
231         }
233         m3_eoi = ioremap(M3_TXEV_EOI, 0x4);
234         if (!m3_eoi) {
235                 pr_err("Could not ioremap the EOI register\n");
236                 ret = -ENOMEM;
237                 goto err1;
238         }
240         /* Reserve the MBOX for sending messages to M3 */
241         m3_mbox = omap_mbox_get("wkup_m3", &wkup_m3_mbox_notifier);
242         if (IS_ERR(m3_mbox)) {
243                 pr_err("Could not reserve mailbox for A8->M3 IPC\n");
244                 ret = -ENODEV;
245                 goto err2;
246         }
248         /* Enable access to the M3 code and data area from A8 */
249         m3_clk = clk_get(NULL, "wkup_m3_fck");
250         if (IS_ERR(m3_clk)) {
251                 pr_err("%s failed to enable WKUP_M3 clock\n", __func__);
252                 goto err3;
253         }
255         if (clk_enable(m3_clk)) {
256                 pr_err("%s WKUP_M3: clock enable Failed\n", __func__);
257                 goto err4;
258         }
260         m3_code = ioremap(0x44D00000, SZ_16K);
261         if (!m3_code) {
262                 pr_err("%s Could not ioremap M3 code space\n", __func__);
263                 ret = -ENOMEM;
264                 goto err5;
265         }
267         /* Now try to load the firware */
268         ret = request_firmware(&firmware, "cm3-firmware.bin", mpu_dev);
269         if (ret < 0) {
270                 dev_err(mpu_dev, "request_firmware failed\n");
271                 goto err6;
272         } else {
273                 memcpy(m3_code, firmware->data, firmware->size);
274                 pr_info("Copied the M3 firmware to UMEM\n");
275         }
277         ret = omap_hwmod_deassert_hardreset(wkup_m3_oh, "wkup_m3");
278         if (ret) {
279                 pr_err("Could not deassert the reset for WKUP_M3\n");
280                 goto err6;
281         }
283         ret = request_irq(AM33XX_IRQ_M3_M3SP_TXEV, wkup_m3_txev_handler,
284                           IRQF_DISABLED, "wkup_m3_txev", NULL);
285         if (ret)
286                 pr_err("%s request_irq failed for 0x%x\n", __func__,
287                         AM33XX_IRQ_M3_M3SP_TXEV);
288         else
289                 return 0;
291 err6:
292         release_firmware(firmware);
293         iounmap(m3_code);
294 err5:
295         clk_disable(m3_clk);
296 err4:
297         clk_put(m3_clk);
298 err3:
299         omap_mbox_put(m3_mbox, &wkup_m3_mbox_notifier);
300 err2:
301         iounmap(m3_eoi);
302 err1:
303         iounmap(ipc_regs);
304 exit:
305         return ret;
309 static int __init am33xx_pm_init(void)
311         int ret;
313         if (!cpu_is_am33xx())
314                 return -ENODEV;
316         pr_info("Power Management for AM33XX family\n");
318         mpu_dev = omap_device_get_by_hwmod_name("mpu");
320         if (!mpu_dev) {
321                 pr_warning("%s: unable to get the mpu device\n", __func__);
322                 return -EINVAL;
323         }
325         ret = wkup_m3_init();
327         if (ret) {
328                 pr_err("Could not initialise WKUP_M3."
329                         "Power management will be compromised\n");
330                 enable_deep_sleep = false;
331         }
333 #ifdef CONFIG_SUSPEND
334         if (enable_deep_sleep)
335                 suspend_set_ops(&am33xx_pm_ops);
336 #endif /* CONFIG_SUSPEND */
338         return ret;
340 late_initcall(am33xx_pm_init);