]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - arch/arm/mach-omap2/powerdomain.h
ARM: OMAP: AM33XX: Update the suspend code for DS1
[sitara-epos/sitara-epos-kernel.git] / arch / arm / mach-omap2 / powerdomain.h
1 /*
2  * OMAP2/3/4 powerdomain control
3  *
4  * Copyright (C) 2007-2008, 2010 Texas Instruments, Inc.
5  * Copyright (C) 2007-2011 Nokia Corporation
6  *
7  * Paul Walmsley
8  *
9  * This program is free software; you can redistribute it and/or modify
10  * it under the terms of the GNU General Public License version 2 as
11  * published by the Free Software Foundation.
12  *
13  * XXX This should be moved to the mach-omap2/ directory at the earliest
14  * opportunity.
15  */
17 #ifndef __ARCH_ARM_MACH_OMAP2_POWERDOMAIN_H
18 #define __ARCH_ARM_MACH_OMAP2_POWERDOMAIN_H
20 #include <linux/types.h>
21 #include <linux/list.h>
23 #include <linux/atomic.h>
25 #include <plat/cpu.h>
27 #include "voltage.h"
29 /* Powerdomain basic power states */
30 #define PWRDM_POWER_OFF         0x0
31 #define PWRDM_POWER_RET         0x1
32 #define PWRDM_POWER_INACTIVE    0x2
33 #define PWRDM_POWER_ON          0x3
35 #define PWRDM_MAX_PWRSTS        4
37 /* Powerdomain allowable state bitfields */
38 #define PWRSTS_ON               (1 << PWRDM_POWER_ON)
39 #define PWRSTS_INACTIVE         (1 << PWRDM_POWER_INACTIVE)
40 #define PWRSTS_RET              (1 << PWRDM_POWER_RET)
41 #define PWRSTS_OFF              (1 << PWRDM_POWER_OFF)
43 #define PWRSTS_OFF_ON           (PWRSTS_OFF | PWRSTS_ON)
44 #define PWRSTS_OFF_RET          (PWRSTS_OFF | PWRSTS_RET)
45 #define PWRSTS_RET_ON           (PWRSTS_RET | PWRSTS_ON)
46 #define PWRSTS_OFF_RET_ON       (PWRSTS_OFF_RET | PWRSTS_ON)
49 /* Powerdomain flags */
50 #define PWRDM_HAS_HDWR_SAR      (1 << 0) /* hardware save-and-restore support */
51 #define PWRDM_HAS_MPU_QUIRK     (1 << 1) /* MPU pwr domain has MEM bank 0 bits
52                                           * in MEM bank 1 position. This is
53                                           * true for OMAP3430
54                                           */
55 #define PWRDM_HAS_LOWPOWERSTATECHANGE   (1 << 2) /*
56                                                   * support to transition from a
57                                                   * sleep state to a lower sleep
58                                                   * state without waking up the
59                                                   * powerdomain
60                                                   */
62 /*
63  * Number of memory banks that are power-controllable.  On OMAP4430, the
64  * maximum is 5.
65  */
66 #define PWRDM_MAX_MEM_BANKS     5
68 /*
69  * Maximum number of clockdomains that can be associated with a powerdomain.
70  * CORE powerdomain on AM33XX is the worst case
71  */
72 #define PWRDM_MAX_CLKDMS        11
74 /* XXX A completely arbitrary number. What is reasonable here? */
75 #define PWRDM_TRANSITION_BAILOUT 100000
77 struct clockdomain;
78 struct powerdomain;
80 /**
81  * struct powerdomain - OMAP powerdomain
82  * @name: Powerdomain name
83  * @voltdm: voltagedomain containing this powerdomain
84  * @prcm_offs: the address offset from CM_BASE/PRM_BASE
85  * @prcm_partition: (OMAP4 only) the PRCM partition ID containing @prcm_offs
86  * @pwrsts: Possible powerdomain power states
87  * @pwrsts_logic_ret: Possible logic power states when pwrdm in RETENTION
88  * @flags: Powerdomain flags
89  * @banks: Number of software-controllable memory banks in this powerdomain
90  * @pwrsts_mem_ret: Possible memory bank pwrstates when pwrdm in RETENTION
91  * @pwrsts_mem_on: Possible memory bank pwrstates when pwrdm in ON
92  * @pwrdm_clkdms: Clockdomains in this powerdomain
93  * @node: list_head linking all powerdomains
94  * @voltdm_node: list_head linking all powerdomains in a voltagedomain
95  * @state:
96  * @state_counter:
97  * @timer:
98  * @state_timer:
99  *
100  * @prcm_partition possible values are defined in mach-omap2/prcm44xx.h.
101  */
102 struct powerdomain {
103         const char *name;
104         union {
105                 const char *name;
106                 struct voltagedomain *ptr;
107         } voltdm;
108         const s16 prcm_offs;
109         const u8 pwrsts;
110         const u8 pwrsts_logic_ret;
111         const u8 flags;
112         const u8 banks;
113         const u8 pwrsts_mem_ret[PWRDM_MAX_MEM_BANKS];
114         const u8 pwrsts_mem_on[PWRDM_MAX_MEM_BANKS];
115         const u8 prcm_partition;
116         struct clockdomain *pwrdm_clkdms[PWRDM_MAX_CLKDMS];
117         struct list_head node;
118         struct list_head voltdm_node;
119         int state;
120         unsigned state_counter[PWRDM_MAX_PWRSTS];
121         unsigned ret_logic_off_counter;
122         unsigned ret_mem_off_counter[PWRDM_MAX_MEM_BANKS];
124 #ifdef CONFIG_PM_DEBUG
125         s64 timer;
126         s64 state_timer[PWRDM_MAX_PWRSTS];
127 #endif
128 };
130 /**
131  * struct pwrdm_ops - Arch specific function implementations
132  * @pwrdm_set_next_pwrst: Set the target power state for a pd
133  * @pwrdm_read_next_pwrst: Read the target power state set for a pd
134  * @pwrdm_read_pwrst: Read the current power state of a pd
135  * @pwrdm_read_prev_pwrst: Read the prev power state entered by the pd
136  * @pwrdm_set_logic_retst: Set the logic state in RET for a pd
137  * @pwrdm_set_mem_onst: Set the Memory state in ON for a pd
138  * @pwrdm_set_mem_retst: Set the Memory state in RET for a pd
139  * @pwrdm_read_logic_pwrst: Read the current logic state of a pd
140  * @pwrdm_read_prev_logic_pwrst: Read the previous logic state entered by a pd
141  * @pwrdm_read_logic_retst: Read the logic state in RET for a pd
142  * @pwrdm_read_mem_pwrst: Read the current memory state of a pd
143  * @pwrdm_read_prev_mem_pwrst: Read the previous memory state entered by a pd
144  * @pwrdm_read_mem_retst: Read the memory state in RET for a pd
145  * @pwrdm_clear_all_prev_pwrst: Clear all previous power states logged for a pd
146  * @pwrdm_enable_hdwr_sar: Enable Hardware Save-Restore feature for the pd
147  * @pwrdm_disable_hdwr_sar: Disable Hardware Save-Restore feature for a pd
148  * @pwrdm_set_lowpwrstchange: Enable pd transitions from a shallow to deep sleep
149  * @pwrdm_wait_transition: Wait for a pd state transition to complete
150  */
151 struct pwrdm_ops {
152         int     (*pwrdm_set_next_pwrst)(struct powerdomain *pwrdm, u8 pwrst);
153         int     (*pwrdm_read_next_pwrst)(struct powerdomain *pwrdm);
154         int     (*pwrdm_read_pwrst)(struct powerdomain *pwrdm);
155         int     (*pwrdm_read_prev_pwrst)(struct powerdomain *pwrdm);
156         int     (*pwrdm_set_logic_retst)(struct powerdomain *pwrdm, u8 pwrst);
157         int     (*pwrdm_set_mem_onst)(struct powerdomain *pwrdm, u8 bank, u8 pwrst);
158         int     (*pwrdm_set_mem_retst)(struct powerdomain *pwrdm, u8 bank, u8 pwrst);
159         int     (*pwrdm_read_logic_pwrst)(struct powerdomain *pwrdm);
160         int     (*pwrdm_read_prev_logic_pwrst)(struct powerdomain *pwrdm);
161         int     (*pwrdm_read_logic_retst)(struct powerdomain *pwrdm);
162         int     (*pwrdm_read_mem_pwrst)(struct powerdomain *pwrdm, u8 bank);
163         int     (*pwrdm_read_prev_mem_pwrst)(struct powerdomain *pwrdm, u8 bank);
164         int     (*pwrdm_read_mem_retst)(struct powerdomain *pwrdm, u8 bank);
165         int     (*pwrdm_clear_all_prev_pwrst)(struct powerdomain *pwrdm);
166         int     (*pwrdm_enable_hdwr_sar)(struct powerdomain *pwrdm);
167         int     (*pwrdm_disable_hdwr_sar)(struct powerdomain *pwrdm);
168         int     (*pwrdm_set_lowpwrstchange)(struct powerdomain *pwrdm);
169         int     (*pwrdm_wait_transition)(struct powerdomain *pwrdm);
170 };
172 int pwrdm_register_platform_funcs(struct pwrdm_ops *custom_funcs);
173 int pwrdm_register_pwrdms(struct powerdomain **pwrdm_list);
174 int pwrdm_complete_init(void);
176 struct powerdomain *pwrdm_lookup(const char *name);
178 int pwrdm_for_each(int (*fn)(struct powerdomain *pwrdm, void *user),
179                         void *user);
180 int pwrdm_for_each_nolock(int (*fn)(struct powerdomain *pwrdm, void *user),
181                         void *user);
183 int pwrdm_add_clkdm(struct powerdomain *pwrdm, struct clockdomain *clkdm);
184 int pwrdm_del_clkdm(struct powerdomain *pwrdm, struct clockdomain *clkdm);
185 int pwrdm_for_each_clkdm(struct powerdomain *pwrdm,
186                          int (*fn)(struct powerdomain *pwrdm,
187                                    struct clockdomain *clkdm));
188 struct voltagedomain *pwrdm_get_voltdm(struct powerdomain *pwrdm);
190 int pwrdm_get_mem_bank_count(struct powerdomain *pwrdm);
192 int pwrdm_set_next_pwrst(struct powerdomain *pwrdm, u8 pwrst);
193 int pwrdm_read_next_pwrst(struct powerdomain *pwrdm);
194 int pwrdm_read_pwrst(struct powerdomain *pwrdm);
195 int pwrdm_read_prev_pwrst(struct powerdomain *pwrdm);
196 int pwrdm_clear_all_prev_pwrst(struct powerdomain *pwrdm);
198 int pwrdm_set_logic_retst(struct powerdomain *pwrdm, u8 pwrst);
199 int pwrdm_set_mem_onst(struct powerdomain *pwrdm, u8 bank, u8 pwrst);
200 int pwrdm_set_mem_retst(struct powerdomain *pwrdm, u8 bank, u8 pwrst);
202 int pwrdm_read_logic_pwrst(struct powerdomain *pwrdm);
203 int pwrdm_read_prev_logic_pwrst(struct powerdomain *pwrdm);
204 int pwrdm_read_logic_retst(struct powerdomain *pwrdm);
205 int pwrdm_read_mem_pwrst(struct powerdomain *pwrdm, u8 bank);
206 int pwrdm_read_prev_mem_pwrst(struct powerdomain *pwrdm, u8 bank);
207 int pwrdm_read_mem_retst(struct powerdomain *pwrdm, u8 bank);
209 int pwrdm_enable_hdwr_sar(struct powerdomain *pwrdm);
210 int pwrdm_disable_hdwr_sar(struct powerdomain *pwrdm);
211 bool pwrdm_has_hdwr_sar(struct powerdomain *pwrdm);
213 int pwrdm_wait_transition(struct powerdomain *pwrdm);
215 int pwrdm_state_switch(struct powerdomain *pwrdm);
216 int pwrdm_clkdm_state_switch(struct clockdomain *clkdm);
217 int pwrdm_pre_transition(void);
218 int pwrdm_post_transition(void);
219 int pwrdm_set_lowpwrstchange(struct powerdomain *pwrdm);
220 int pwrdm_get_context_loss_count(struct powerdomain *pwrdm);
221 bool pwrdm_can_ever_lose_context(struct powerdomain *pwrdm);
223 extern void omap242x_powerdomains_init(void);
224 extern void omap243x_powerdomains_init(void);
225 extern void omap3xxx_powerdomains_init(void);
226 extern void am33xx_powerdomains_init(void);
227 extern void omap44xx_powerdomains_init(void);
229 extern struct pwrdm_ops omap2_pwrdm_operations;
230 extern struct pwrdm_ops omap3_pwrdm_operations;
231 extern struct pwrdm_ops am33xx_pwrdm_operations;
232 extern struct pwrdm_ops omap4_pwrdm_operations;
234 /* Common Internal functions used across OMAP rev's */
235 extern u32 omap2_pwrdm_get_mem_bank_onstate_mask(u8 bank);
236 extern u32 omap2_pwrdm_get_mem_bank_retst_mask(u8 bank);
237 extern u32 omap2_pwrdm_get_mem_bank_stst_mask(u8 bank);
239 extern struct powerdomain wkup_omap2_pwrdm;
240 extern struct powerdomain gfx_omap2_pwrdm;
243 #endif