1 /*
2 * OMAP2+ common Power & Reset Management (PRM) IP block functions
3 *
4 * Copyright (C) 2011 Texas Instruments, Inc.
5 * Tero Kristo <t-kristo@ti.com>
6 *
7 * This program is free software; you can redistribute it and/or modify
8 * it under the terms of the GNU General Public License version 2 as
9 * published by the Free Software Foundation.
10 *
11 *
12 * For historical purposes, the API used to configure the PRM
13 * interrupt handler refers to it as the "PRCM interrupt." The
14 * underlying registers are located in the PRM on OMAP3/4.
15 *
16 * XXX This code should eventually be moved to a PRM driver.
17 */
19 #include <linux/kernel.h>
20 #include <linux/module.h>
21 #include <linux/init.h>
22 #include <linux/io.h>
23 #include <linux/irq.h>
24 #include <linux/interrupt.h>
25 #include <linux/slab.h>
27 #include <mach/system.h>
28 #include <plat/common.h>
29 #include <plat/prcm.h>
30 #include <plat/irqs.h>
32 #include "prm2xxx_3xxx.h"
33 #include "prm44xx.h"
35 /*
36 * OMAP_PRCM_MAX_NR_PENDING_REG: maximum number of PRM_IRQ*_MPU regs
37 * XXX this is technically not needed, since
38 * omap_prcm_register_chain_handler() could allocate this based on the
39 * actual amount of memory needed for the SoC
40 */
41 #define OMAP_PRCM_MAX_NR_PENDING_REG 2
43 /*
44 * prcm_irq_chips: an array of all of the "generic IRQ chips" in use
45 * by the PRCM interrupt handler code. There will be one 'chip' per
46 * PRM_{IRQSTATUS,IRQENABLE}_MPU register pair. (So OMAP3 will have
47 * one "chip" and OMAP4 will have two.)
48 */
49 static struct irq_chip_generic **prcm_irq_chips;
51 /*
52 * prcm_irq_setup: the PRCM IRQ parameters for the hardware the code
53 * is currently running on. Defined and passed by initialization code
54 * that calls omap_prcm_register_chain_handler().
55 */
56 static struct omap_prcm_irq_setup *prcm_irq_setup;
58 /* Private functions */
60 /*
61 * Move priority events from events to priority_events array
62 */
63 static void omap_prcm_events_filter_priority(unsigned long *events,
64 unsigned long *priority_events)
65 {
66 int i;
68 for (i = 0; i < prcm_irq_setup->nr_regs; i++) {
69 priority_events[i] =
70 events[i] & prcm_irq_setup->priority_mask[i];
71 events[i] ^= priority_events[i];
72 }
73 }
75 /*
76 * PRCM Interrupt Handler
77 *
78 * This is a common handler for the OMAP PRCM interrupts. Pending
79 * interrupts are detected by a call to prcm_pending_events and
80 * dispatched accordingly. Clearing of the wakeup events should be
81 * done by the SoC specific individual handlers.
82 */
83 static void omap_prcm_irq_handler(unsigned int irq, struct irq_desc *desc)
84 {
85 unsigned long pending[OMAP_PRCM_MAX_NR_PENDING_REG];
86 unsigned long priority_pending[OMAP_PRCM_MAX_NR_PENDING_REG];
87 struct irq_chip *chip = irq_desc_get_chip(desc);
88 unsigned int virtirq;
89 int nr_irqs = prcm_irq_setup->nr_regs * 32;
91 /*
92 * If we are suspended, mask all interrupts from PRCM level,
93 * this does not ack them, and they will be pending until we
94 * re-enable the interrupts, at which point the
95 * omap_prcm_irq_handler will be executed again. The
96 * _save_and_clear_irqen() function must ensure that the PRM
97 * write to disable all IRQs has reached the PRM before
98 * returning, or spurious PRCM interrupts may occur during
99 * suspend.
100 */
101 if (prcm_irq_setup->suspended) {
102 prcm_irq_setup->save_and_clear_irqen(prcm_irq_setup->saved_mask);
103 prcm_irq_setup->suspend_save_flag = true;
104 }
106 /*
107 * Loop until all pending irqs are handled, since
108 * generic_handle_irq() can cause new irqs to come
109 */
110 while (!prcm_irq_setup->suspended) {
111 prcm_irq_setup->read_pending_irqs(pending);
113 /* No bit set, then all IRQs are handled */
114 if (find_first_bit(pending, nr_irqs) >= nr_irqs)
115 break;
117 omap_prcm_events_filter_priority(pending, priority_pending);
119 /*
120 * Loop on all currently pending irqs so that new irqs
121 * cannot starve previously pending irqs
122 */
124 /* Serve priority events first */
125 for_each_set_bit(virtirq, priority_pending, nr_irqs)
126 generic_handle_irq(prcm_irq_setup->base_irq + virtirq);
128 /* Serve normal events next */
129 for_each_set_bit(virtirq, pending, nr_irqs)
130 generic_handle_irq(prcm_irq_setup->base_irq + virtirq);
131 }
132 if (chip->irq_ack)
133 chip->irq_ack(&desc->irq_data);
134 if (chip->irq_eoi)
135 chip->irq_eoi(&desc->irq_data);
136 chip->irq_unmask(&desc->irq_data);
138 prcm_irq_setup->ocp_barrier(); /* avoid spurious IRQs */
139 }
141 /* Public functions */
143 /**
144 * omap_prcm_event_to_irq - given a PRCM event name, returns the
145 * corresponding IRQ on which the handler should be registered
146 * @name: name of the PRCM interrupt bit to look up - see struct omap_prcm_irq
147 *
148 * Returns the Linux internal IRQ ID corresponding to @name upon success,
149 * or -ENOENT upon failure.
150 */
151 int omap_prcm_event_to_irq(const char *name)
152 {
153 int i;
155 if (!prcm_irq_setup || !name)
156 return -ENOENT;
158 for (i = 0; i < prcm_irq_setup->nr_irqs; i++)
159 if (!strcmp(prcm_irq_setup->irqs[i].name, name))
160 return prcm_irq_setup->base_irq +
161 prcm_irq_setup->irqs[i].offset;
163 return -ENOENT;
164 }
166 /**
167 * omap_prcm_irq_cleanup - reverses memory allocated and other steps
168 * done by omap_prcm_register_chain_handler()
169 *
170 * No return value.
171 */
172 void omap_prcm_irq_cleanup(void)
173 {
174 int i;
176 if (!prcm_irq_setup) {
177 pr_err("PRCM: IRQ handler not initialized; cannot cleanup\n");
178 return;
179 }
181 if (prcm_irq_chips) {
182 for (i = 0; i < prcm_irq_setup->nr_regs; i++) {
183 if (prcm_irq_chips[i])
184 irq_remove_generic_chip(prcm_irq_chips[i],
185 0xffffffff, 0, 0);
186 prcm_irq_chips[i] = NULL;
187 }
188 kfree(prcm_irq_chips);
189 prcm_irq_chips = NULL;
190 }
192 kfree(prcm_irq_setup->saved_mask);
193 prcm_irq_setup->saved_mask = NULL;
195 kfree(prcm_irq_setup->priority_mask);
196 prcm_irq_setup->priority_mask = NULL;
198 irq_set_chained_handler(prcm_irq_setup->irq, NULL);
200 if (prcm_irq_setup->base_irq > 0)
201 irq_free_descs(prcm_irq_setup->base_irq,
202 prcm_irq_setup->nr_regs * 32);
203 prcm_irq_setup->base_irq = 0;
204 }
206 void omap_prcm_irq_prepare(void)
207 {
208 prcm_irq_setup->suspended = true;
209 }
211 void omap_prcm_irq_complete(void)
212 {
213 prcm_irq_setup->suspended = false;
215 /* If we have not saved the masks, do not attempt to restore */
216 if (!prcm_irq_setup->suspend_save_flag)
217 return;
219 prcm_irq_setup->suspend_save_flag = false;
221 /*
222 * Re-enable all masked PRCM irq sources, this causes the PRCM
223 * interrupt to fire immediately if the events were masked
224 * previously in the chain handler
225 */
226 prcm_irq_setup->restore_irqen(prcm_irq_setup->saved_mask);
227 }
229 /**
230 * omap_prcm_register_chain_handler - initializes the prcm chained interrupt
231 * handler based on provided parameters
232 * @irq_setup: hardware data about the underlying PRM/PRCM
233 *
234 * Set up the PRCM chained interrupt handler on the PRCM IRQ. Sets up
235 * one generic IRQ chip per PRM interrupt status/enable register pair.
236 * Returns 0 upon success, -EINVAL if called twice or if invalid
237 * arguments are passed, or -ENOMEM on any other error.
238 */
239 int omap_prcm_register_chain_handler(struct omap_prcm_irq_setup *irq_setup)
240 {
241 int nr_regs = irq_setup->nr_regs;
242 u32 mask[OMAP_PRCM_MAX_NR_PENDING_REG];
243 int offset, i;
244 struct irq_chip_generic *gc;
245 struct irq_chip_type *ct;
247 if (!irq_setup)
248 return -EINVAL;
250 if (prcm_irq_setup) {
251 pr_err("PRCM: already initialized; won't reinitialize\n");
252 return -EINVAL;
253 }
255 if (nr_regs > OMAP_PRCM_MAX_NR_PENDING_REG) {
256 pr_err("PRCM: nr_regs too large\n");
257 return -EINVAL;
258 }
260 prcm_irq_setup = irq_setup;
262 prcm_irq_chips = kzalloc(sizeof(void *) * nr_regs, GFP_KERNEL);
263 prcm_irq_setup->saved_mask = kzalloc(sizeof(u32) * nr_regs, GFP_KERNEL);
264 prcm_irq_setup->priority_mask = kzalloc(sizeof(u32) * nr_regs,
265 GFP_KERNEL);
267 if (!prcm_irq_chips || !prcm_irq_setup->saved_mask ||
268 !prcm_irq_setup->priority_mask) {
269 pr_err("PRCM: kzalloc failed\n");
270 goto err;
271 }
273 memset(mask, 0, sizeof(mask));
275 for (i = 0; i < irq_setup->nr_irqs; i++) {
276 offset = irq_setup->irqs[i].offset;
277 mask[offset >> 5] |= 1 << (offset & 0x1f);
278 if (irq_setup->irqs[i].priority)
279 irq_setup->priority_mask[offset >> 5] |=
280 1 << (offset & 0x1f);
281 }
283 irq_set_chained_handler(irq_setup->irq, omap_prcm_irq_handler);
285 irq_setup->base_irq = irq_alloc_descs(-1, 0, irq_setup->nr_regs * 32,
286 0);
288 if (irq_setup->base_irq < 0) {
289 pr_err("PRCM: failed to allocate irq descs: %d\n",
290 irq_setup->base_irq);
291 goto err;
292 }
294 for (i = 0; i <= irq_setup->nr_regs; i++) {
295 gc = irq_alloc_generic_chip("PRCM", 1,
296 irq_setup->base_irq + i * 32, prm_base,
297 handle_level_irq);
299 if (!gc) {
300 pr_err("PRCM: failed to allocate generic chip\n");
301 goto err;
302 }
303 ct = gc->chip_types;
304 ct->chip.irq_ack = irq_gc_ack_set_bit;
305 ct->chip.irq_mask = irq_gc_mask_clr_bit;
306 ct->chip.irq_unmask = irq_gc_mask_set_bit;
308 ct->regs.ack = irq_setup->ack + i * 4;
309 ct->regs.mask = irq_setup->mask + i * 4;
311 irq_setup_generic_chip(gc, mask[i], 0, IRQ_NOREQUEST, 0);
312 prcm_irq_chips[i] = gc;
313 }
315 return 0;
317 err:
318 omap_prcm_irq_cleanup();
319 return -ENOMEM;
320 }