]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - arch/arm/mach-omap2/prm_common.c
arm:omap:am33xx: register edma platform
[sitara-epos/sitara-epos-kernel.git] / arch / arm / mach-omap2 / prm_common.c
1 /*
2  * OMAP2+ common Power & Reset Management (PRM) IP block functions
3  *
4  * Copyright (C) 2011 Texas Instruments, Inc.
5  * Tero Kristo <t-kristo@ti.com>
6  *
7  * This program is free software; you can redistribute it and/or modify
8  * it under the terms of the GNU General Public License version 2 as
9  * published by the Free Software Foundation.
10  *
11  *
12  * For historical purposes, the API used to configure the PRM
13  * interrupt handler refers to it as the "PRCM interrupt."  The
14  * underlying registers are located in the PRM on OMAP3/4.
15  *
16  * XXX This code should eventually be moved to a PRM driver.
17  */
19 #include <linux/kernel.h>
20 #include <linux/module.h>
21 #include <linux/init.h>
22 #include <linux/io.h>
23 #include <linux/irq.h>
24 #include <linux/interrupt.h>
25 #include <linux/slab.h>
27 #include <mach/system.h>
28 #include <plat/common.h>
29 #include <plat/prcm.h>
30 #include <plat/irqs.h>
32 #include "prm2xxx_3xxx.h"
33 #include "prm44xx.h"
35 /*
36  * OMAP_PRCM_MAX_NR_PENDING_REG: maximum number of PRM_IRQ*_MPU regs
37  * XXX this is technically not needed, since
38  * omap_prcm_register_chain_handler() could allocate this based on the
39  * actual amount of memory needed for the SoC
40  */
41 #define OMAP_PRCM_MAX_NR_PENDING_REG            2
43 /*
44  * prcm_irq_chips: an array of all of the "generic IRQ chips" in use
45  * by the PRCM interrupt handler code.  There will be one 'chip' per
46  * PRM_{IRQSTATUS,IRQENABLE}_MPU register pair.  (So OMAP3 will have
47  * one "chip" and OMAP4 will have two.)
48  */
49 static struct irq_chip_generic **prcm_irq_chips;
51 /*
52  * prcm_irq_setup: the PRCM IRQ parameters for the hardware the code
53  * is currently running on.  Defined and passed by initialization code
54  * that calls omap_prcm_register_chain_handler().
55  */
56 static struct omap_prcm_irq_setup *prcm_irq_setup;
58 /* Private functions */
60 /*
61  * Move priority events from events to priority_events array
62  */
63 static void omap_prcm_events_filter_priority(unsigned long *events,
64         unsigned long *priority_events)
65 {
66         int i;
68         for (i = 0; i < prcm_irq_setup->nr_regs; i++) {
69                 priority_events[i] =
70                         events[i] & prcm_irq_setup->priority_mask[i];
71                 events[i] ^= priority_events[i];
72         }
73 }
75 /*
76  * PRCM Interrupt Handler
77  *
78  * This is a common handler for the OMAP PRCM interrupts. Pending
79  * interrupts are detected by a call to prcm_pending_events and
80  * dispatched accordingly. Clearing of the wakeup events should be
81  * done by the SoC specific individual handlers.
82  */
83 static void omap_prcm_irq_handler(unsigned int irq, struct irq_desc *desc)
84 {
85         unsigned long pending[OMAP_PRCM_MAX_NR_PENDING_REG];
86         unsigned long priority_pending[OMAP_PRCM_MAX_NR_PENDING_REG];
87         struct irq_chip *chip = irq_desc_get_chip(desc);
88         unsigned int virtirq;
89         int nr_irqs = prcm_irq_setup->nr_regs * 32;
91         /*
92          * If we are suspended, mask all interrupts from PRCM level,
93          * this does not ack them, and they will be pending until we
94          * re-enable the interrupts, at which point the
95          * omap_prcm_irq_handler will be executed again.  The
96          * _save_and_clear_irqen() function must ensure that the PRM
97          * write to disable all IRQs has reached the PRM before
98          * returning, or spurious PRCM interrupts may occur during
99          * suspend.
100          */
101         if (prcm_irq_setup->suspended) {
102                 prcm_irq_setup->save_and_clear_irqen(prcm_irq_setup->saved_mask);
103                 prcm_irq_setup->suspend_save_flag = true;
104         }
106         /*
107          * Loop until all pending irqs are handled, since
108          * generic_handle_irq() can cause new irqs to come
109          */
110         while (!prcm_irq_setup->suspended) {
111                 prcm_irq_setup->read_pending_irqs(pending);
113                 /* No bit set, then all IRQs are handled */
114                 if (find_first_bit(pending, nr_irqs) >= nr_irqs)
115                         break;
117                 omap_prcm_events_filter_priority(pending, priority_pending);
119                 /*
120                  * Loop on all currently pending irqs so that new irqs
121                  * cannot starve previously pending irqs
122                  */
124                 /* Serve priority events first */
125                 for_each_set_bit(virtirq, priority_pending, nr_irqs)
126                         generic_handle_irq(prcm_irq_setup->base_irq + virtirq);
128                 /* Serve normal events next */
129                 for_each_set_bit(virtirq, pending, nr_irqs)
130                         generic_handle_irq(prcm_irq_setup->base_irq + virtirq);
131         }
132         if (chip->irq_ack)
133                 chip->irq_ack(&desc->irq_data);
134         if (chip->irq_eoi)
135                 chip->irq_eoi(&desc->irq_data);
136         chip->irq_unmask(&desc->irq_data);
138         prcm_irq_setup->ocp_barrier(); /* avoid spurious IRQs */
141 /* Public functions */
143 /**
144  * omap_prcm_event_to_irq - given a PRCM event name, returns the
145  * corresponding IRQ on which the handler should be registered
146  * @name: name of the PRCM interrupt bit to look up - see struct omap_prcm_irq
147  *
148  * Returns the Linux internal IRQ ID corresponding to @name upon success,
149  * or -ENOENT upon failure.
150  */
151 int omap_prcm_event_to_irq(const char *name)
153         int i;
155         if (!prcm_irq_setup || !name)
156                 return -ENOENT;
158         for (i = 0; i < prcm_irq_setup->nr_irqs; i++)
159                 if (!strcmp(prcm_irq_setup->irqs[i].name, name))
160                         return prcm_irq_setup->base_irq +
161                                 prcm_irq_setup->irqs[i].offset;
163         return -ENOENT;
166 /**
167  * omap_prcm_irq_cleanup - reverses memory allocated and other steps
168  * done by omap_prcm_register_chain_handler()
169  *
170  * No return value.
171  */
172 void omap_prcm_irq_cleanup(void)
174         int i;
176         if (!prcm_irq_setup) {
177                 pr_err("PRCM: IRQ handler not initialized; cannot cleanup\n");
178                 return;
179         }
181         if (prcm_irq_chips) {
182                 for (i = 0; i < prcm_irq_setup->nr_regs; i++) {
183                         if (prcm_irq_chips[i])
184                                 irq_remove_generic_chip(prcm_irq_chips[i],
185                                         0xffffffff, 0, 0);
186                         prcm_irq_chips[i] = NULL;
187                 }
188                 kfree(prcm_irq_chips);
189                 prcm_irq_chips = NULL;
190         }
192         kfree(prcm_irq_setup->saved_mask);
193         prcm_irq_setup->saved_mask = NULL;
195         kfree(prcm_irq_setup->priority_mask);
196         prcm_irq_setup->priority_mask = NULL;
198         irq_set_chained_handler(prcm_irq_setup->irq, NULL);
200         if (prcm_irq_setup->base_irq > 0)
201                 irq_free_descs(prcm_irq_setup->base_irq,
202                         prcm_irq_setup->nr_regs * 32);
203         prcm_irq_setup->base_irq = 0;
206 void omap_prcm_irq_prepare(void)
208         prcm_irq_setup->suspended = true;
211 void omap_prcm_irq_complete(void)
213         prcm_irq_setup->suspended = false;
215         /* If we have not saved the masks, do not attempt to restore */
216         if (!prcm_irq_setup->suspend_save_flag)
217                 return;
219         prcm_irq_setup->suspend_save_flag = false;
221         /*
222          * Re-enable all masked PRCM irq sources, this causes the PRCM
223          * interrupt to fire immediately if the events were masked
224          * previously in the chain handler
225          */
226         prcm_irq_setup->restore_irqen(prcm_irq_setup->saved_mask);
229 /**
230  * omap_prcm_register_chain_handler - initializes the prcm chained interrupt
231  * handler based on provided parameters
232  * @irq_setup: hardware data about the underlying PRM/PRCM
233  *
234  * Set up the PRCM chained interrupt handler on the PRCM IRQ.  Sets up
235  * one generic IRQ chip per PRM interrupt status/enable register pair.
236  * Returns 0 upon success, -EINVAL if called twice or if invalid
237  * arguments are passed, or -ENOMEM on any other error.
238  */
239 int omap_prcm_register_chain_handler(struct omap_prcm_irq_setup *irq_setup)
241         int nr_regs = irq_setup->nr_regs;
242         u32 mask[OMAP_PRCM_MAX_NR_PENDING_REG];
243         int offset, i;
244         struct irq_chip_generic *gc;
245         struct irq_chip_type *ct;
247         if (!irq_setup)
248                 return -EINVAL;
250         if (prcm_irq_setup) {
251                 pr_err("PRCM: already initialized; won't reinitialize\n");
252                 return -EINVAL;
253         }
255         if (nr_regs > OMAP_PRCM_MAX_NR_PENDING_REG) {
256                 pr_err("PRCM: nr_regs too large\n");
257                 return -EINVAL;
258         }
260         prcm_irq_setup = irq_setup;
262         prcm_irq_chips = kzalloc(sizeof(void *) * nr_regs, GFP_KERNEL);
263         prcm_irq_setup->saved_mask = kzalloc(sizeof(u32) * nr_regs, GFP_KERNEL);
264         prcm_irq_setup->priority_mask = kzalloc(sizeof(u32) * nr_regs,
265                 GFP_KERNEL);
267         if (!prcm_irq_chips || !prcm_irq_setup->saved_mask ||
268             !prcm_irq_setup->priority_mask) {
269                 pr_err("PRCM: kzalloc failed\n");
270                 goto err;
271         }
273         memset(mask, 0, sizeof(mask));
275         for (i = 0; i < irq_setup->nr_irqs; i++) {
276                 offset = irq_setup->irqs[i].offset;
277                 mask[offset >> 5] |= 1 << (offset & 0x1f);
278                 if (irq_setup->irqs[i].priority)
279                         irq_setup->priority_mask[offset >> 5] |=
280                                 1 << (offset & 0x1f);
281         }
283         irq_set_chained_handler(irq_setup->irq, omap_prcm_irq_handler);
285         irq_setup->base_irq = irq_alloc_descs(-1, 0, irq_setup->nr_regs * 32,
286                 0);
288         if (irq_setup->base_irq < 0) {
289                 pr_err("PRCM: failed to allocate irq descs: %d\n",
290                         irq_setup->base_irq);
291                 goto err;
292         }
294         for (i = 0; i <= irq_setup->nr_regs; i++) {
295                 gc = irq_alloc_generic_chip("PRCM", 1,
296                         irq_setup->base_irq + i * 32, prm_base,
297                         handle_level_irq);
299                 if (!gc) {
300                         pr_err("PRCM: failed to allocate generic chip\n");
301                         goto err;
302                 }
303                 ct = gc->chip_types;
304                 ct->chip.irq_ack = irq_gc_ack_set_bit;
305                 ct->chip.irq_mask = irq_gc_mask_clr_bit;
306                 ct->chip.irq_unmask = irq_gc_mask_set_bit;
308                 ct->regs.ack = irq_setup->ack + i * 4;
309                 ct->regs.mask = irq_setup->mask + i * 4;
311                 irq_setup_generic_chip(gc, mask[i], 0, IRQ_NOREQUEST, 0);
312                 prcm_irq_chips[i] = gc;
313         }
315         return 0;
317 err:
318         omap_prcm_irq_cleanup();
319         return -ENOMEM;