]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - arch/arm/mach-omap2/sdrc2xxx.c
arm:omap:am33xx: Register HSMMC Platform on AM335x EVM
[sitara-epos/sitara-epos-kernel.git] / arch / arm / mach-omap2 / sdrc2xxx.c
1 /*
2  * linux/arch/arm/mach-omap2/sdrc2xxx.c
3  *
4  * SDRAM timing related functions for OMAP2xxx
5  *
6  * Copyright (C) 2005, 2008 Texas Instruments Inc.
7  * Copyright (C) 2005, 2008 Nokia Corporation
8  *
9  * Tony Lindgren <tony@atomide.com>
10  * Paul Walmsley
11  * Richard Woodruff <r-woodruff2@ti.com>
12  *
13  * This program is free software; you can redistribute it and/or modify
14  * it under the terms of the GNU General Public License version 2 as
15  * published by the Free Software Foundation.
16  */
18 #include <linux/module.h>
19 #include <linux/kernel.h>
20 #include <linux/device.h>
21 #include <linux/list.h>
22 #include <linux/errno.h>
23 #include <linux/delay.h>
24 #include <linux/clk.h>
25 #include <linux/io.h>
27 #include "common.h"
28 #include <plat/clock.h>
29 #include <plat/sram.h>
31 #include "prm2xxx_3xxx.h"
32 #include "clock.h"
33 #include <plat/sdrc.h>
34 #include "sdrc.h"
36 /* Memory timing, DLL mode flags */
37 #define M_DDR           1
38 #define M_LOCK_CTRL     (1 << 2)
39 #define M_UNLOCK        0
40 #define M_LOCK          1
43 static struct memory_timings mem_timings;
44 static u32 curr_perf_level = CORE_CLK_SRC_DPLL_X2;
46 static u32 omap2xxx_sdrc_get_slow_dll_ctrl(void)
47 {
48         return mem_timings.slow_dll_ctrl;
49 }
51 static u32 omap2xxx_sdrc_get_fast_dll_ctrl(void)
52 {
53         return mem_timings.fast_dll_ctrl;
54 }
56 static u32 omap2xxx_sdrc_get_type(void)
57 {
58         return mem_timings.m_type;
59 }
61 /*
62  * Check the DLL lock state, and return tue if running in unlock mode.
63  * This is needed to compensate for the shifted DLL value in unlock mode.
64  */
65 u32 omap2xxx_sdrc_dll_is_unlocked(void)
66 {
67         /* dlla and dllb are a set */
68         u32 dll_state = sdrc_read_reg(SDRC_DLLA_CTRL);
70         if ((dll_state & (1 << 2)) == (1 << 2))
71                 return 1;
72         else
73                 return 0;
74 }
76 /*
77  * 'level' is the value to store to CM_CLKSEL2_PLL.CORE_CLK_SRC.
78  * Practical values are CORE_CLK_SRC_DPLL (for CORE_CLK = DPLL_CLK) or
79  * CORE_CLK_SRC_DPLL_X2 (for CORE_CLK = * DPLL_CLK * 2)
80  *
81  * Used by the clock framework during CORE DPLL changes
82  */
83 u32 omap2xxx_sdrc_reprogram(u32 level, u32 force)
84 {
85         u32 dll_ctrl, m_type;
86         u32 prev = curr_perf_level;
87         unsigned long flags;
89         if ((curr_perf_level == level) && !force)
90                 return prev;
92         if (level == CORE_CLK_SRC_DPLL)
93                 dll_ctrl = omap2xxx_sdrc_get_slow_dll_ctrl();
94         else if (level == CORE_CLK_SRC_DPLL_X2)
95                 dll_ctrl = omap2xxx_sdrc_get_fast_dll_ctrl();
96         else
97                 return prev;
99         m_type = omap2xxx_sdrc_get_type();
101         local_irq_save(flags);
102         /*
103          * XXX These calls should be abstracted out through a
104          * prm2xxx.c function
105          */
106         if (cpu_is_omap2420())
107                 __raw_writel(0xffff, OMAP2420_PRCM_VOLTSETUP);
108         else
109                 __raw_writel(0xffff, OMAP2430_PRCM_VOLTSETUP);
110         omap2_sram_reprogram_sdrc(level, dll_ctrl, m_type);
111         curr_perf_level = level;
112         local_irq_restore(flags);
114         return prev;
117 /* Used by the clock framework during CORE DPLL changes */
118 void omap2xxx_sdrc_init_params(u32 force_lock_to_unlock_mode)
120         unsigned long dll_cnt;
121         u32 fast_dll = 0;
123         /* DDR = 1, SDR = 0 */
124         mem_timings.m_type = !((sdrc_read_reg(SDRC_MR_0) & 0x3) == 0x1);
126         /* 2422 es2.05 and beyond has a single SIP DDR instead of 2 like others.
127          * In the case of 2422, its ok to use CS1 instead of CS0.
128          */
129         if (cpu_is_omap2422())
130                 mem_timings.base_cs = 1;
131         else
132                 mem_timings.base_cs = 0;
134         if (mem_timings.m_type != M_DDR)
135                 return;
137         /* With DDR we need to determine the low frequency DLL value */
138         if (((mem_timings.fast_dll_ctrl & (1 << 2)) == M_LOCK_CTRL))
139                 mem_timings.dll_mode = M_UNLOCK;
140         else
141                 mem_timings.dll_mode = M_LOCK;
143         if (mem_timings.base_cs == 0) {
144                 fast_dll = sdrc_read_reg(SDRC_DLLA_CTRL);
145                 dll_cnt = sdrc_read_reg(SDRC_DLLA_STATUS) & 0xff00;
146         } else {
147                 fast_dll = sdrc_read_reg(SDRC_DLLB_CTRL);
148                 dll_cnt = sdrc_read_reg(SDRC_DLLB_STATUS) & 0xff00;
149         }
150         if (force_lock_to_unlock_mode) {
151                 fast_dll &= ~0xff00;
152                 fast_dll |= dll_cnt;            /* Current lock mode */
153         }
154         /* set fast timings with DLL filter disabled */
155         mem_timings.fast_dll_ctrl = (fast_dll | (3 << 8));
157         /* No disruptions, DDR will be offline & C-ABI not followed */
158         omap2_sram_ddr_init(&mem_timings.slow_dll_ctrl,
159                             mem_timings.fast_dll_ctrl,
160                             mem_timings.base_cs,
161                             force_lock_to_unlock_mode);
162         mem_timings.slow_dll_ctrl &= 0xff00;    /* Keep lock value */
164         /* Turn status into unlock ctrl */
165         mem_timings.slow_dll_ctrl |=
166                 ((mem_timings.fast_dll_ctrl & 0xF) | (1 << 2));
168         /* 90 degree phase for anything below 133Mhz + disable DLL filter */
169         mem_timings.slow_dll_ctrl |= ((1 << 1) | (3 << 8));