]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - arch/arm/mach-omap2/vc.c
arm:omap:am33xx: Register HSMMC Platform on AM335x EVM
[sitara-epos/sitara-epos-kernel.git] / arch / arm / mach-omap2 / vc.c
1 /*
2  * OMAP Voltage Controller (VC) interface
3  *
4  * Copyright (C) 2011 Texas Instruments, Inc.
5  *
6  * This file is licensed under the terms of the GNU General Public
7  * License version 2. This program is licensed "as is" without any
8  * warranty of any kind, whether express or implied.
9  */
10 #include <linux/kernel.h>
11 #include <linux/delay.h>
12 #include <linux/init.h>
14 #include <plat/cpu.h>
16 #include "voltage.h"
17 #include "vc.h"
18 #include "prm-regbits-34xx.h"
19 #include "prm-regbits-44xx.h"
20 #include "prm44xx.h"
22 /**
23  * struct omap_vc_channel_cfg - describe the cfg_channel bitfield
24  * @sa: bit for slave address
25  * @rav: bit for voltage configuration register
26  * @rac: bit for command configuration register
27  * @racen: enable bit for RAC
28  * @cmd: bit for command value set selection
29  *
30  * Channel configuration bits, common for OMAP3+
31  * OMAP3 register: PRM_VC_CH_CONF
32  * OMAP4 register: PRM_VC_CFG_CHANNEL
33  * OMAP5 register: PRM_VC_SMPS_<voltdm>_CONFIG
34  */
35 struct omap_vc_channel_cfg {
36         u8 sa;
37         u8 rav;
38         u8 rac;
39         u8 racen;
40         u8 cmd;
41 };
43 static struct omap_vc_channel_cfg vc_default_channel_cfg = {
44         .sa    = BIT(0),
45         .rav   = BIT(1),
46         .rac   = BIT(2),
47         .racen = BIT(3),
48         .cmd   = BIT(4),
49 };
51 /*
52  * On OMAP3+, all VC channels have the above default bitfield
53  * configuration, except the OMAP4 MPU channel.  This appears
54  * to be a freak accident as every other VC channel has the
55  * default configuration, thus creating a mutant channel config.
56  */
57 static struct omap_vc_channel_cfg vc_mutant_channel_cfg = {
58         .sa    = BIT(0),
59         .rav   = BIT(2),
60         .rac   = BIT(3),
61         .racen = BIT(4),
62         .cmd   = BIT(1),
63 };
65 static struct omap_vc_channel_cfg *vc_cfg_bits;
66 #define CFG_CHANNEL_MASK 0x1f
68 /**
69  * omap_vc_config_channel - configure VC channel to PMIC mappings
70  * @voltdm: pointer to voltagdomain defining the desired VC channel
71  *
72  * Configures the VC channel to PMIC mappings for the following
73  * PMIC settings
74  * - i2c slave address (SA)
75  * - voltage configuration address (RAV)
76  * - command configuration address (RAC) and enable bit (RACEN)
77  * - command values for ON, ONLP, RET and OFF (CMD)
78  *
79  * This function currently only allows flexible configuration of the
80  * non-default channel.  Starting with OMAP4, there are more than 2
81  * channels, with one defined as the default (on OMAP4, it's MPU.)
82  * Only the non-default channel can be configured.
83  */
84 static int omap_vc_config_channel(struct voltagedomain *voltdm)
85 {
86         struct omap_vc_channel *vc = voltdm->vc;
88         /*
89          * For default channel, the only configurable bit is RACEN.
90          * All others must stay at zero (see function comment above.)
91          */
92         if (vc->flags & OMAP_VC_CHANNEL_DEFAULT)
93                 vc->cfg_channel &= vc_cfg_bits->racen;
95         voltdm->rmw(CFG_CHANNEL_MASK << vc->cfg_channel_sa_shift,
96                     vc->cfg_channel << vc->cfg_channel_sa_shift,
97                     vc->cfg_channel_reg);
99         return 0;
102 /* Voltage scale and accessory APIs */
103 int omap_vc_pre_scale(struct voltagedomain *voltdm,
104                       unsigned long target_volt,
105                       u8 *target_vsel, u8 *current_vsel)
107         struct omap_vc_channel *vc = voltdm->vc;
108         u32 vc_cmdval;
110         /* Check if sufficient pmic info is available for this vdd */
111         if (!voltdm->pmic) {
112                 pr_err("%s: Insufficient pmic info to scale the vdd_%s\n",
113                         __func__, voltdm->name);
114                 return -EINVAL;
115         }
117         if (!voltdm->pmic->uv_to_vsel) {
118                 pr_err("%s: PMIC function to convert voltage in uV to"
119                         "vsel not registered. Hence unable to scale voltage"
120                         "for vdd_%s\n", __func__, voltdm->name);
121                 return -ENODATA;
122         }
124         if (!voltdm->read || !voltdm->write) {
125                 pr_err("%s: No read/write API for accessing vdd_%s regs\n",
126                         __func__, voltdm->name);
127                 return -EINVAL;
128         }
130         *target_vsel = voltdm->pmic->uv_to_vsel(target_volt);
131         *current_vsel = voltdm->pmic->uv_to_vsel(voltdm->nominal_volt);
133         /* Setting the ON voltage to the new target voltage */
134         vc_cmdval = voltdm->read(vc->cmdval_reg);
135         vc_cmdval &= ~vc->common->cmd_on_mask;
136         vc_cmdval |= (*target_vsel << vc->common->cmd_on_shift);
137         voltdm->write(vc_cmdval, vc->cmdval_reg);
139         omap_vp_update_errorgain(voltdm, target_volt);
141         return 0;
144 void omap_vc_post_scale(struct voltagedomain *voltdm,
145                         unsigned long target_volt,
146                         u8 target_vsel, u8 current_vsel)
148         u32 smps_steps = 0, smps_delay = 0;
150         smps_steps = abs(target_vsel - current_vsel);
151         /* SMPS slew rate / step size. 2us added as buffer. */
152         smps_delay = ((smps_steps * voltdm->pmic->step_size) /
153                         voltdm->pmic->slew_rate) + 2;
154         udelay(smps_delay);
157 /* vc_bypass_scale - VC bypass method of voltage scaling */
158 int omap_vc_bypass_scale(struct voltagedomain *voltdm,
159                          unsigned long target_volt)
161         struct omap_vc_channel *vc = voltdm->vc;
162         u32 loop_cnt = 0, retries_cnt = 0;
163         u32 vc_valid, vc_bypass_val_reg, vc_bypass_value;
164         u8 target_vsel, current_vsel;
165         int ret;
167         ret = omap_vc_pre_scale(voltdm, target_volt, &target_vsel, &current_vsel);
168         if (ret)
169                 return ret;
171         vc_valid = vc->common->valid;
172         vc_bypass_val_reg = vc->common->bypass_val_reg;
173         vc_bypass_value = (target_vsel << vc->common->data_shift) |
174                 (vc->volt_reg_addr << vc->common->regaddr_shift) |
175                 (vc->i2c_slave_addr << vc->common->slaveaddr_shift);
177         voltdm->write(vc_bypass_value, vc_bypass_val_reg);
178         voltdm->write(vc_bypass_value | vc_valid, vc_bypass_val_reg);
180         vc_bypass_value = voltdm->read(vc_bypass_val_reg);
181         /*
182          * Loop till the bypass command is acknowledged from the SMPS.
183          * NOTE: This is legacy code. The loop count and retry count needs
184          * to be revisited.
185          */
186         while (!(vc_bypass_value & vc_valid)) {
187                 loop_cnt++;
189                 if (retries_cnt > 10) {
190                         pr_warning("%s: Retry count exceeded\n", __func__);
191                         return -ETIMEDOUT;
192                 }
194                 if (loop_cnt > 50) {
195                         retries_cnt++;
196                         loop_cnt = 0;
197                         udelay(10);
198                 }
199                 vc_bypass_value = voltdm->read(vc_bypass_val_reg);
200         }
202         omap_vc_post_scale(voltdm, target_volt, target_vsel, current_vsel);
203         return 0;
206 static void __init omap3_vfsm_init(struct voltagedomain *voltdm)
208         /*
209          * Voltage Manager FSM parameters init
210          * XXX This data should be passed in from the board file
211          */
212         voltdm->write(OMAP3_CLKSETUP, OMAP3_PRM_CLKSETUP_OFFSET);
213         voltdm->write(OMAP3_VOLTOFFSET, OMAP3_PRM_VOLTOFFSET_OFFSET);
214         voltdm->write(OMAP3_VOLTSETUP2, OMAP3_PRM_VOLTSETUP2_OFFSET);
217 static void __init omap3_vc_init_channel(struct voltagedomain *voltdm)
219         static bool is_initialized;
221         if (is_initialized)
222                 return;
224         omap3_vfsm_init(voltdm);
226         is_initialized = true;
230 /* OMAP4 specific voltage init functions */
231 static void __init omap4_vc_init_channel(struct voltagedomain *voltdm)
233         static bool is_initialized;
234         u32 vc_val;
236         if (is_initialized)
237                 return;
239         /* XXX These are magic numbers and do not belong! */
240         vc_val = (0x60 << OMAP4430_SCLL_SHIFT | 0x26 << OMAP4430_SCLH_SHIFT);
241         voltdm->write(vc_val, OMAP4_PRM_VC_CFG_I2C_CLK_OFFSET);
243         is_initialized = true;
246 /**
247  * omap_vc_i2c_init - initialize I2C interface to PMIC
248  * @voltdm: voltage domain containing VC data
249  *
250  * Use PMIC supplied seetings for I2C high-speed mode and
251  * master code (if set) and program the VC I2C configuration
252  * register.
253  *
254  * The VC I2C configuration is common to all VC channels,
255  * so this function only configures I2C for the first VC
256  * channel registers.  All other VC channels will use the
257  * same configuration.
258  */
259 static void __init omap_vc_i2c_init(struct voltagedomain *voltdm)
261         struct omap_vc_channel *vc = voltdm->vc;
262         static bool initialized;
263         static bool i2c_high_speed;
264         u8 mcode;
266         if (initialized) {
267                 if (voltdm->pmic->i2c_high_speed != i2c_high_speed)
268                         pr_warn("%s: I2C config for all channels must match.",
269                                 __func__);
270                 return;
271         }
273         i2c_high_speed = voltdm->pmic->i2c_high_speed;
274         if (i2c_high_speed)
275                 voltdm->rmw(vc->common->i2c_cfg_hsen_mask,
276                             vc->common->i2c_cfg_hsen_mask,
277                             vc->common->i2c_cfg_reg);
279         mcode = voltdm->pmic->i2c_mcode;
280         if (mcode)
281                 voltdm->rmw(vc->common->i2c_mcode_mask,
282                             mcode << __ffs(vc->common->i2c_mcode_mask),
283                             vc->common->i2c_cfg_reg);
285         initialized = true;
288 void __init omap_vc_init_channel(struct voltagedomain *voltdm)
290         struct omap_vc_channel *vc = voltdm->vc;
291         u8 on_vsel, onlp_vsel, ret_vsel, off_vsel;
292         u32 val;
294         if (!voltdm->pmic || !voltdm->pmic->uv_to_vsel) {
295                 pr_err("%s: missing PMIC for vdd_%s.\n",
296                        __func__, voltdm->name);
297                 return;
298         }
300         if (!voltdm->read || !voltdm->write) {
301                 pr_err("%s: No read/write API for accessing vdd_%s regs\n",
302                         __func__, voltdm->name);
303                 return;
304         }
306         vc->cfg_channel = 0;
307         if (vc->flags & OMAP_VC_CHANNEL_CFG_MUTANT)
308                 vc_cfg_bits = &vc_mutant_channel_cfg;
309         else
310                 vc_cfg_bits = &vc_default_channel_cfg;
312         /* get PMIC/board specific settings */
313         vc->i2c_slave_addr = voltdm->pmic->i2c_slave_addr;
314         vc->volt_reg_addr = voltdm->pmic->volt_reg_addr;
315         vc->cmd_reg_addr = voltdm->pmic->cmd_reg_addr;
316         vc->setup_time = voltdm->pmic->volt_setup_time;
318         /* Configure the i2c slave address for this VC */
319         voltdm->rmw(vc->smps_sa_mask,
320                     vc->i2c_slave_addr << __ffs(vc->smps_sa_mask),
321                     vc->smps_sa_reg);
322         vc->cfg_channel |= vc_cfg_bits->sa;
324         /*
325          * Configure the PMIC register addresses.
326          */
327         voltdm->rmw(vc->smps_volra_mask,
328                     vc->volt_reg_addr << __ffs(vc->smps_volra_mask),
329                     vc->smps_volra_reg);
330         vc->cfg_channel |= vc_cfg_bits->rav;
332         if (vc->cmd_reg_addr) {
333                 voltdm->rmw(vc->smps_cmdra_mask,
334                             vc->cmd_reg_addr << __ffs(vc->smps_cmdra_mask),
335                             vc->smps_cmdra_reg);
336                 vc->cfg_channel |= vc_cfg_bits->rac | vc_cfg_bits->racen;
337         }
339         /* Set up the on, inactive, retention and off voltage */
340         on_vsel = voltdm->pmic->uv_to_vsel(voltdm->pmic->on_volt);
341         onlp_vsel = voltdm->pmic->uv_to_vsel(voltdm->pmic->onlp_volt);
342         ret_vsel = voltdm->pmic->uv_to_vsel(voltdm->pmic->ret_volt);
343         off_vsel = voltdm->pmic->uv_to_vsel(voltdm->pmic->off_volt);
344         val = ((on_vsel << vc->common->cmd_on_shift) |
345                (onlp_vsel << vc->common->cmd_onlp_shift) |
346                (ret_vsel << vc->common->cmd_ret_shift) |
347                (off_vsel << vc->common->cmd_off_shift));
348         voltdm->write(val, vc->cmdval_reg);
349         vc->cfg_channel |= vc_cfg_bits->cmd;
351         /* Channel configuration */
352         omap_vc_config_channel(voltdm);
354         /* Configure the setup times */
355         voltdm->rmw(voltdm->vfsm->voltsetup_mask,
356                     vc->setup_time << __ffs(voltdm->vfsm->voltsetup_mask),
357                     voltdm->vfsm->voltsetup_reg);
359         omap_vc_i2c_init(voltdm);
361         if (cpu_is_omap34xx())
362                 omap3_vc_init_channel(voltdm);
363         else if (cpu_is_omap44xx())
364                 omap4_vc_init_channel(voltdm);