ARM: OMAP2+: hwmod: Add an API to handle master standby mode
[sitara-epos/sitara-epos-kernel.git] / arch / arm / plat-omap / include / plat / omap_hwmod.h
1 /*
2  * omap_hwmod macros, structures
3  *
4  * Copyright (C) 2009-2011 Nokia Corporation
5  * Copyright (C) 2011 Texas Instruments, Inc.
6  * Paul Walmsley
7  *
8  * Created in collaboration with (alphabetical order): BenoĆ®t Cousson,
9  * Kevin Hilman, Tony Lindgren, Rajendra Nayak, Vikram Pandita, Sakari
10  * Poussa, Anand Sawant, Santosh Shilimkar, Richard Woodruff
11  *
12  * This program is free software; you can redistribute it and/or modify
13  * it under the terms of the GNU General Public License version 2 as
14  * published by the Free Software Foundation.
15  *
16  * These headers and macros are used to define OMAP on-chip module
17  * data and their integration with other OMAP modules and Linux.
18  * Copious documentation and references can also be found in the
19  * omap_hwmod code, in arch/arm/mach-omap2/omap_hwmod.c (as of this
20  * writing).
21  *
22  * To do:
23  * - add interconnect error log structures
24  * - add pinmuxing
25  * - init_conn_id_bit (CONNID_BIT_VECTOR)
26  * - implement default hwmod SMS/SDRC flags?
27  * - move Linux-specific data ("non-ROM data") out
28  *
29  */
30 #ifndef __ARCH_ARM_PLAT_OMAP_INCLUDE_MACH_OMAP_HWMOD_H
31 #define __ARCH_ARM_PLAT_OMAP_INCLUDE_MACH_OMAP_HWMOD_H
33 #include <linux/kernel.h>
34 #include <linux/init.h>
35 #include <linux/list.h>
36 #include <linux/ioport.h>
37 #include <linux/spinlock.h>
38 #include <plat/cpu.h>
40 struct omap_device;
42 extern struct omap_hwmod_sysc_fields omap_hwmod_sysc_type1;
43 extern struct omap_hwmod_sysc_fields omap_hwmod_sysc_type2;
45 /*
46  * OCP SYSCONFIG bit shifts/masks TYPE1. These are for IPs compliant
47  * with the original PRCM protocol defined for OMAP2420
48  */
49 #define SYSC_TYPE1_MIDLEMODE_SHIFT      12
50 #define SYSC_TYPE1_MIDLEMODE_MASK       (0x3 << SYSC_MIDLEMODE_SHIFT)
51 #define SYSC_TYPE1_CLOCKACTIVITY_SHIFT  8
52 #define SYSC_TYPE1_CLOCKACTIVITY_MASK   (0x3 << SYSC_CLOCKACTIVITY_SHIFT)
53 #define SYSC_TYPE1_SIDLEMODE_SHIFT      3
54 #define SYSC_TYPE1_SIDLEMODE_MASK       (0x3 << SYSC_SIDLEMODE_SHIFT)
55 #define SYSC_TYPE1_ENAWAKEUP_SHIFT      2
56 #define SYSC_TYPE1_ENAWAKEUP_MASK       (1 << SYSC_ENAWAKEUP_SHIFT)
57 #define SYSC_TYPE1_SOFTRESET_SHIFT      1
58 #define SYSC_TYPE1_SOFTRESET_MASK       (1 << SYSC_SOFTRESET_SHIFT)
59 #define SYSC_TYPE1_AUTOIDLE_SHIFT       0
60 #define SYSC_TYPE1_AUTOIDLE_MASK        (1 << SYSC_AUTOIDLE_SHIFT)
62 /*
63  * OCP SYSCONFIG bit shifts/masks TYPE2. These are for IPs compliant
64  * with the new PRCM protocol defined for new OMAP4 IPs.
65  */
66 #define SYSC_TYPE2_SOFTRESET_SHIFT      0
67 #define SYSC_TYPE2_SOFTRESET_MASK       (1 << SYSC_TYPE2_SOFTRESET_SHIFT)
68 #define SYSC_TYPE2_SIDLEMODE_SHIFT      2
69 #define SYSC_TYPE2_SIDLEMODE_MASK       (0x3 << SYSC_TYPE2_SIDLEMODE_SHIFT)
70 #define SYSC_TYPE2_MIDLEMODE_SHIFT      4
71 #define SYSC_TYPE2_MIDLEMODE_MASK       (0x3 << SYSC_TYPE2_MIDLEMODE_SHIFT)
73 /* OCP SYSSTATUS bit shifts/masks */
74 #define SYSS_RESETDONE_SHIFT            0
75 #define SYSS_RESETDONE_MASK             (1 << SYSS_RESETDONE_SHIFT)
77 /* Master standby/slave idle mode flags */
78 #define HWMOD_IDLEMODE_FORCE            (1 << 0)
79 #define HWMOD_IDLEMODE_NO               (1 << 1)
80 #define HWMOD_IDLEMODE_SMART            (1 << 2)
81 #define HWMOD_IDLEMODE_SMART_WKUP       (1 << 3)
83 /* modulemode control type (SW or HW) */
84 #define MODULEMODE_HWCTRL               1
85 #define MODULEMODE_SWCTRL               2
88 /**
89  * struct omap_hwmod_mux_info - hwmod specific mux configuration
90  * @pads:              array of omap_device_pad entries
91  * @nr_pads:           number of omap_device_pad entries
92  *
93  * Note that this is currently built during init as needed.
94  */
95 struct omap_hwmod_mux_info {
96         int                             nr_pads;
97         struct omap_device_pad          *pads;
98         int                             nr_pads_dynamic;
99         struct omap_device_pad          **pads_dynamic;
100         int                             *irqs;
101         bool                            enabled;
102 };
104 /**
105  * struct omap_hwmod_irq_info - MPU IRQs used by the hwmod
106  * @name: name of the IRQ channel (module local name)
107  * @irq: IRQ channel ID (should be non-negative except -1 = terminator)
108  *
109  * @name should be something short, e.g., "tx" or "rx".  It is for use
110  * by platform_get_resource_byname().  It is defined locally to the
111  * hwmod.
112  */
113 struct omap_hwmod_irq_info {
114         const char      *name;
115         s16             irq;
116 };
118 /**
119  * struct omap_hwmod_dma_info - DMA channels used by the hwmod
120  * @name: name of the DMA channel (module local name)
121  * @dma_req: DMA request ID (should be non-negative except -1 = terminator)
122  *
123  * @name should be something short, e.g., "tx" or "rx".  It is for use
124  * by platform_get_resource_byname().  It is defined locally to the
125  * hwmod.
126  */
127 struct omap_hwmod_dma_info {
128         const char      *name;
129         s16             dma_req;
130 };
132 /**
133  * struct omap_hwmod_rst_info - IPs reset lines use by hwmod
134  * @name: name of the reset line (module local name)
135  * @rst_shift: Offset of the reset bit
136  * @st_shift: Offset of the reset status bit (OMAP2/3 only)
137  *
138  * @name should be something short, e.g., "cpu0" or "rst". It is defined
139  * locally to the hwmod.
140  */
141 struct omap_hwmod_rst_info {
142         const char      *name;
143         u8              rst_shift;
144         u8              st_shift;
145 };
147 /**
148  * struct omap_hwmod_opt_clk - optional clocks used by this hwmod
149  * @role: "sys", "32k", "tv", etc -- for use in clk_get()
150  * @clk: opt clock: OMAP clock name
151  * @_clk: pointer to the struct clk (filled in at runtime)
152  *
153  * The module's interface clock and main functional clock should not
154  * be added as optional clocks.
155  */
156 struct omap_hwmod_opt_clk {
157         const char      *role;
158         const char      *clk;
159         struct clk      *_clk;
160 };
163 /* omap_hwmod_omap2_firewall.flags bits */
164 #define OMAP_FIREWALL_L3                (1 << 0)
165 #define OMAP_FIREWALL_L4                (1 << 1)
167 /**
168  * struct omap_hwmod_omap2_firewall - OMAP2/3 device firewall data
169  * @l3_perm_bit: bit shift for L3_PM_*_PERMISSION_*
170  * @l4_fw_region: L4 firewall region ID
171  * @l4_prot_group: L4 protection group ID
172  * @flags: (see omap_hwmod_omap2_firewall.flags macros above)
173  */
174 struct omap_hwmod_omap2_firewall {
175         u8 l3_perm_bit;
176         u8 l4_fw_region;
177         u8 l4_prot_group;
178         u8 flags;
179 };
182 /*
183  * omap_hwmod_addr_space.flags bits
184  *
185  * ADDR_MAP_ON_INIT: Map this address space during omap_hwmod init.
186  * ADDR_TYPE_RT: Address space contains module register target data.
187  */
188 #define ADDR_MAP_ON_INIT        (1 << 0)        /* XXX does not belong */
189 #define ADDR_TYPE_RT            (1 << 1)
191 /**
192  * struct omap_hwmod_addr_space - address space handled by the hwmod
193  * @name: name of the address space
194  * @pa_start: starting physical address
195  * @pa_end: ending physical address
196  * @flags: (see omap_hwmod_addr_space.flags macros above)
197  *
198  * Address space doesn't necessarily follow physical interconnect
199  * structure.  GPMC is one example.
200  */
201 struct omap_hwmod_addr_space {
202         const char *name;
203         u32 pa_start;
204         u32 pa_end;
205         u8 flags;
206 };
209 /*
210  * omap_hwmod_ocp_if.user bits: these indicate the initiators that use this
211  * interface to interact with the hwmod.  Used to add sleep dependencies
212  * when the module is enabled or disabled.
213  */
214 #define OCP_USER_MPU                    (1 << 0)
215 #define OCP_USER_SDMA                   (1 << 1)
217 /* omap_hwmod_ocp_if.flags bits */
218 #define OCPIF_SWSUP_IDLE                (1 << 0)
219 #define OCPIF_CAN_BURST                 (1 << 1)
221 /**
222  * struct omap_hwmod_ocp_if - OCP interface data
223  * @master: struct omap_hwmod that initiates OCP transactions on this link
224  * @slave: struct omap_hwmod that responds to OCP transactions on this link
225  * @addr: address space associated with this link
226  * @clk: interface clock: OMAP clock name
227  * @_clk: pointer to the interface struct clk (filled in at runtime)
228  * @fw: interface firewall data
229  * @width: OCP data width
230  * @user: initiators using this interface (see OCP_USER_* macros above)
231  * @flags: OCP interface flags (see OCPIF_* macros above)
232  *
233  * It may also be useful to add a tag_cnt field for OCP2.x devices.
234  *
235  * Parameter names beginning with an underscore are managed internally by
236  * the omap_hwmod code and should not be set during initialization.
237  */
238 struct omap_hwmod_ocp_if {
239         struct omap_hwmod               *master;
240         struct omap_hwmod               *slave;
241         struct omap_hwmod_addr_space    *addr;
242         const char                      *clk;
243         struct clk                      *_clk;
244         union {
245                 struct omap_hwmod_omap2_firewall omap2;
246         }                               fw;
247         u8                              width;
248         u8                              user;
249         u8                              flags;
250 };
253 /* Macros for use in struct omap_hwmod_sysconfig */
255 /* Flags for use in omap_hwmod_sysconfig.idlemodes */
256 #define MASTER_STANDBY_SHIFT    4
257 #define SLAVE_IDLE_SHIFT        0
258 #define SIDLE_FORCE             (HWMOD_IDLEMODE_FORCE << SLAVE_IDLE_SHIFT)
259 #define SIDLE_NO                (HWMOD_IDLEMODE_NO << SLAVE_IDLE_SHIFT)
260 #define SIDLE_SMART             (HWMOD_IDLEMODE_SMART << SLAVE_IDLE_SHIFT)
261 #define SIDLE_SMART_WKUP        (HWMOD_IDLEMODE_SMART_WKUP << SLAVE_IDLE_SHIFT)
262 #define MSTANDBY_FORCE          (HWMOD_IDLEMODE_FORCE << MASTER_STANDBY_SHIFT)
263 #define MSTANDBY_NO             (HWMOD_IDLEMODE_NO << MASTER_STANDBY_SHIFT)
264 #define MSTANDBY_SMART          (HWMOD_IDLEMODE_SMART << MASTER_STANDBY_SHIFT)
265 #define MSTANDBY_SMART_WKUP     (HWMOD_IDLEMODE_SMART_WKUP << MASTER_STANDBY_SHIFT)
267 /* omap_hwmod_sysconfig.sysc_flags capability flags */
268 #define SYSC_HAS_AUTOIDLE       (1 << 0)
269 #define SYSC_HAS_SOFTRESET      (1 << 1)
270 #define SYSC_HAS_ENAWAKEUP      (1 << 2)
271 #define SYSC_HAS_EMUFREE        (1 << 3)
272 #define SYSC_HAS_CLOCKACTIVITY  (1 << 4)
273 #define SYSC_HAS_SIDLEMODE      (1 << 5)
274 #define SYSC_HAS_MIDLEMODE      (1 << 6)
275 #define SYSS_HAS_RESET_STATUS   (1 << 7)
276 #define SYSC_NO_CACHE           (1 << 8)  /* XXX SW flag, belongs elsewhere */
277 #define SYSC_HAS_RESET_STATUS   (1 << 9)
279 /* omap_hwmod_sysconfig.clockact flags */
280 #define CLOCKACT_TEST_BOTH      0x0
281 #define CLOCKACT_TEST_MAIN      0x1
282 #define CLOCKACT_TEST_ICLK      0x2
283 #define CLOCKACT_TEST_NONE      0x3
285 /**
286  * struct omap_hwmod_sysc_fields - hwmod OCP_SYSCONFIG register field offsets.
287  * @midle_shift: Offset of the midle bit
288  * @clkact_shift: Offset of the clockactivity bit
289  * @sidle_shift: Offset of the sidle bit
290  * @enwkup_shift: Offset of the enawakeup bit
291  * @srst_shift: Offset of the softreset bit
292  * @autoidle_shift: Offset of the autoidle bit
293  */
294 struct omap_hwmod_sysc_fields {
295         u8 midle_shift;
296         u8 clkact_shift;
297         u8 sidle_shift;
298         u8 enwkup_shift;
299         u8 srst_shift;
300         u8 autoidle_shift;
301 };
303 /**
304  * struct omap_hwmod_class_sysconfig - hwmod class OCP_SYS* data
305  * @rev_offs: IP block revision register offset (from module base addr)
306  * @sysc_offs: OCP_SYSCONFIG register offset (from module base addr)
307  * @syss_offs: OCP_SYSSTATUS register offset (from module base addr)
308  * @idlemodes: One or more of {SIDLE,MSTANDBY}_{OFF,FORCE,SMART}
309  * @sysc_flags: SYS{C,S}_HAS* flags indicating SYSCONFIG bits supported
310  * @clockact: the default value of the module CLOCKACTIVITY bits
311  *
312  * @clockact describes to the module which clocks are likely to be
313  * disabled when the PRCM issues its idle request to the module.  Some
314  * modules have separate clockdomains for the interface clock and main
315  * functional clock, and can check whether they should acknowledge the
316  * idle request based on the internal module functionality that has
317  * been associated with the clocks marked in @clockact.  This field is
318  * only used if HWMOD_SET_DEFAULT_CLOCKACT is set (see below)
319  *
320  * @sysc_fields: structure containing the offset positions of various bits in
321  * SYSCONFIG register. This can be populated using omap_hwmod_sysc_type1 or
322  * omap_hwmod_sysc_type2 defined in omap_hwmod_common_data.c depending on
323  * whether the device ip is compliant with the original PRCM protocol
324  * defined for OMAP2420 or the new PRCM protocol for new OMAP4 IPs.
325  * If the device follows a different scheme for the sysconfig register ,
326  * then this field has to be populated with the correct offset structure.
327  */
328 struct omap_hwmod_class_sysconfig {
329         u16 rev_offs;
330         u16 sysc_offs;
331         u16 syss_offs;
332         u16 sysc_flags;
333         u8 idlemodes;
334         u8 clockact;
335         struct omap_hwmod_sysc_fields *sysc_fields;
336 };
338 /**
339  * struct omap_hwmod_omap2_prcm - OMAP2/3-specific PRCM data
340  * @module_offs: PRCM submodule offset from the start of the PRM/CM
341  * @prcm_reg_id: PRCM register ID (e.g., 3 for CM_AUTOIDLE3)
342  * @module_bit: register bit shift for AUTOIDLE, WKST, WKEN, GRPSEL regs
343  * @idlest_reg_id: IDLEST register ID (e.g., 3 for CM_IDLEST3)
344  * @idlest_idle_bit: register bit shift for CM_IDLEST slave idle bit
345  * @idlest_stdby_bit: register bit shift for CM_IDLEST master standby bit
346  *
347  * @prcm_reg_id and @module_bit are specific to the AUTOIDLE, WKST,
348  * WKEN, GRPSEL registers.  In an ideal world, no extra information
349  * would be needed for IDLEST information, but alas, there are some
350  * exceptions, so @idlest_reg_id, @idlest_idle_bit, @idlest_stdby_bit
351  * are needed for the IDLEST registers (c.f. 2430 I2CHS, 3430 USBHOST)
352  */
353 struct omap_hwmod_omap2_prcm {
354         s16 module_offs;
355         u8 prcm_reg_id;
356         u8 module_bit;
357         u8 idlest_reg_id;
358         u8 idlest_idle_bit;
359         u8 idlest_stdby_bit;
360 };
363 /**
364  * struct omap_hwmod_omap4_prcm - OMAP4-specific PRCM data
365  * @clkctrl_reg: PRCM address of the clock control register
366  * @rstctrl_reg: address of the XXX_RSTCTRL register located in the PRM
367  * @submodule_wkdep_bit: bit shift of the WKDEP range
368  */
369 struct omap_hwmod_omap4_prcm {
370         u16             clkctrl_offs;
371         u16             rstctrl_offs;
372         u16             context_offs;
373         u8              submodule_wkdep_bit;
374         u8              modulemode;
375 };
378 /*
379  * omap_hwmod.flags definitions
380  *
381  * HWMOD_SWSUP_SIDLE: omap_hwmod code should manually bring module in and out
382  *     of idle, rather than relying on module smart-idle
383  * HWMOD_SWSUP_MSTDBY: omap_hwmod code should manually bring module in and out
384  *     of standby, rather than relying on module smart-standby
385  * HWMOD_INIT_NO_RESET: don't reset this module at boot - important for
386  *     SDRAM controller, etc. XXX probably belongs outside the main hwmod file
387  *     XXX Should be HWMOD_SETUP_NO_RESET
388  * HWMOD_INIT_NO_IDLE: don't idle this module at boot - important for SDRAM
389  *     controller, etc. XXX probably belongs outside the main hwmod file
390  *     XXX Should be HWMOD_SETUP_NO_IDLE
391  * HWMOD_NO_OCP_AUTOIDLE: disable module autoidle (OCP_SYSCONFIG.AUTOIDLE)
392  *     when module is enabled, rather than the default, which is to
393  *     enable autoidle
394  * HWMOD_SET_DEFAULT_CLOCKACT: program CLOCKACTIVITY bits at startup
395  * HWMOD_NO_IDLEST: this module does not have idle status - this is the case
396  *     only for few initiator modules on OMAP2 & 3.
397  * HWMOD_CONTROL_OPT_CLKS_IN_RESET: Enable all optional clocks during reset.
398  *     This is needed for devices like DSS that require optional clocks enabled
399  *     in order to complete the reset. Optional clocks will be disabled
400  *     again after the reset.
401  * HWMOD_16BIT_REG: Module has 16bit registers
402  */
403 #define HWMOD_SWSUP_SIDLE                       (1 << 0)
404 #define HWMOD_SWSUP_MSTANDBY                    (1 << 1)
405 #define HWMOD_INIT_NO_RESET                     (1 << 2)
406 #define HWMOD_INIT_NO_IDLE                      (1 << 3)
407 #define HWMOD_NO_OCP_AUTOIDLE                   (1 << 4)
408 #define HWMOD_SET_DEFAULT_CLOCKACT              (1 << 5)
409 #define HWMOD_NO_IDLEST                         (1 << 6)
410 #define HWMOD_CONTROL_OPT_CLKS_IN_RESET         (1 << 7)
411 #define HWMOD_16BIT_REG                         (1 << 8)
413 /*
414  * omap_hwmod._int_flags definitions
415  * These are for internal use only and are managed by the omap_hwmod code.
416  *
417  * _HWMOD_NO_MPU_PORT: no path exists for the MPU to write to this module
418  * _HWMOD_WAKEUP_ENABLED: set when the omap_hwmod code has enabled ENAWAKEUP
419  * _HWMOD_SYSCONFIG_LOADED: set when the OCP_SYSCONFIG value has been cached
420  * _HWMOD_SKIP_ENABLE: set if hwmod enabled during init (HWMOD_INIT_NO_IDLE) -
421  *     causes the first call to _enable() to only update the pinmux
422  */
423 #define _HWMOD_NO_MPU_PORT                      (1 << 0)
424 #define _HWMOD_WAKEUP_ENABLED                   (1 << 1)
425 #define _HWMOD_SYSCONFIG_LOADED                 (1 << 2)
426 #define _HWMOD_SKIP_ENABLE                      (1 << 3)
428 /*
429  * omap_hwmod._state definitions
430  *
431  * INITIALIZED: reset (optionally), initialized, enabled, disabled
432  *              (optionally)
433  *
434  *
435  */
436 #define _HWMOD_STATE_UNKNOWN                    0
437 #define _HWMOD_STATE_REGISTERED                 1
438 #define _HWMOD_STATE_CLKS_INITED                2
439 #define _HWMOD_STATE_INITIALIZED                3
440 #define _HWMOD_STATE_ENABLED                    4
441 #define _HWMOD_STATE_IDLE                       5
442 #define _HWMOD_STATE_DISABLED                   6
444 /**
445  * struct omap_hwmod_class - the type of an IP block
446  * @name: name of the hwmod_class
447  * @sysc: device SYSCONFIG/SYSSTATUS register data
448  * @rev: revision of the IP class
449  * @pre_shutdown: ptr to fn to be executed immediately prior to device shutdown
450  * @reset: ptr to fn to be executed in place of the standard hwmod reset fn
451  *
452  * Represent the class of a OMAP hardware "modules" (e.g. timer,
453  * smartreflex, gpio, uart...)
454  *
455  * @pre_shutdown is a function that will be run immediately before
456  * hwmod clocks are disabled, etc.  It is intended for use for hwmods
457  * like the MPU watchdog, which cannot be disabled with the standard
458  * omap_hwmod_shutdown().  The function should return 0 upon success,
459  * or some negative error upon failure.  Returning an error will cause
460  * omap_hwmod_shutdown() to abort the device shutdown and return an
461  * error.
462  *
463  * If @reset is defined, then the function it points to will be
464  * executed in place of the standard hwmod _reset() code in
465  * mach-omap2/omap_hwmod.c.  This is needed for IP blocks which have
466  * unusual reset sequences - usually processor IP blocks like the IVA.
467  */
468 struct omap_hwmod_class {
469         const char                              *name;
470         struct omap_hwmod_class_sysconfig       *sysc;
471         u32                                     rev;
472         int                                     (*pre_shutdown)(struct omap_hwmod *oh);
473         int                                     (*reset)(struct omap_hwmod *oh);
474 };
476 /**
477  * struct omap_hwmod - integration data for OMAP hardware "modules" (IP blocks)
478  * @name: name of the hwmod
479  * @class: struct omap_hwmod_class * to the class of this hwmod
480  * @od: struct omap_device currently associated with this hwmod (internal use)
481  * @mpu_irqs: ptr to an array of MPU IRQs
482  * @sdma_reqs: ptr to an array of System DMA request IDs
483  * @prcm: PRCM data pertaining to this hwmod
484  * @main_clk: main clock: OMAP clock name
485  * @_clk: pointer to the main struct clk (filled in at runtime)
486  * @opt_clks: other device clocks that drivers can request (0..*)
487  * @vdd_name: voltage domain name
488  * @voltdm: pointer to voltage domain (filled in at runtime)
489  * @masters: ptr to array of OCP ifs that this hwmod can initiate on
490  * @slaves: ptr to array of OCP ifs that this hwmod can respond on
491  * @dev_attr: arbitrary device attributes that can be passed to the driver
492  * @_sysc_cache: internal-use hwmod flags
493  * @_mpu_rt_va: cached register target start address (internal use)
494  * @_mpu_port_index: cached MPU register target slave ID (internal use)
495  * @opt_clks_cnt: number of @opt_clks
496  * @master_cnt: number of @master entries
497  * @slaves_cnt: number of @slave entries
498  * @response_lat: device OCP response latency (in interface clock cycles)
499  * @_int_flags: internal-use hwmod flags
500  * @_state: internal-use hwmod state
501  * @_postsetup_state: internal-use state to leave the hwmod in after _setup()
502  * @flags: hwmod flags (documented below)
503  * @_lock: spinlock serializing operations on this hwmod
504  * @node: list node for hwmod list (internal use)
505  *
506  * @main_clk refers to this module's "main clock," which for our
507  * purposes is defined as "the functional clock needed for register
508  * accesses to complete."  Modules may not have a main clock if the
509  * interface clock also serves as a main clock.
510  *
511  * Parameter names beginning with an underscore are managed internally by
512  * the omap_hwmod code and should not be set during initialization.
513  */
514 struct omap_hwmod {
515         const char                      *name;
516         struct omap_hwmod_class         *class;
517         struct omap_device              *od;
518         struct omap_hwmod_mux_info      *mux;
519         struct omap_hwmod_irq_info      *mpu_irqs;
520         struct omap_hwmod_dma_info      *sdma_reqs;
521         struct omap_hwmod_rst_info      *rst_lines;
522         union {
523                 struct omap_hwmod_omap2_prcm omap2;
524                 struct omap_hwmod_omap4_prcm omap4;
525         }                               prcm;
526         const char                      *main_clk;
527         struct clk                      *_clk;
528         struct omap_hwmod_opt_clk       *opt_clks;
529         char                            *clkdm_name;
530         struct clockdomain              *clkdm;
531         char                            *vdd_name;
532         struct omap_hwmod_ocp_if        **masters; /* connect to *_IA */
533         struct omap_hwmod_ocp_if        **slaves;  /* connect to *_TA */
534         void                            *dev_attr;
535         u32                             _sysc_cache;
536         void __iomem                    *_mpu_rt_va;
537         spinlock_t                      _lock;
538         struct list_head                node;
539         u16                             flags;
540         u8                              _mpu_port_index;
541         u8                              response_lat;
542         u8                              rst_lines_cnt;
543         u8                              opt_clks_cnt;
544         u8                              masters_cnt;
545         u8                              slaves_cnt;
546         u8                              hwmods_cnt;
547         u8                              _int_flags;
548         u8                              _state;
549         u8                              _postsetup_state;
550 };
552 int omap_hwmod_register(struct omap_hwmod **ohs);
553 struct omap_hwmod *omap_hwmod_lookup(const char *name);
554 int omap_hwmod_for_each(int (*fn)(struct omap_hwmod *oh, void *data),
555                         void *data);
557 int __init omap_hwmod_setup_one(const char *name);
559 int omap_hwmod_enable(struct omap_hwmod *oh);
560 int _omap_hwmod_enable(struct omap_hwmod *oh);
561 int omap_hwmod_idle(struct omap_hwmod *oh);
562 int _omap_hwmod_idle(struct omap_hwmod *oh);
563 int omap_hwmod_shutdown(struct omap_hwmod *oh);
565 int omap_hwmod_assert_hardreset(struct omap_hwmod *oh, const char *name);
566 int omap_hwmod_deassert_hardreset(struct omap_hwmod *oh, const char *name);
567 int omap_hwmod_read_hardreset(struct omap_hwmod *oh, const char *name);
569 int omap_hwmod_enable_clocks(struct omap_hwmod *oh);
570 int omap_hwmod_disable_clocks(struct omap_hwmod *oh);
572 int omap_hwmod_set_master_standbymode(struct omap_hwmod *oh, u8 idlemode);
573 int omap_hwmod_set_slave_idlemode(struct omap_hwmod *oh, u8 idlemode);
574 int omap_hwmod_set_ocp_autoidle(struct omap_hwmod *oh, u8 autoidle);
576 int omap_hwmod_reset(struct omap_hwmod *oh);
577 void omap_hwmod_ocp_barrier(struct omap_hwmod *oh);
579 void omap_hwmod_write(u32 v, struct omap_hwmod *oh, u16 reg_offs);
580 u32 omap_hwmod_read(struct omap_hwmod *oh, u16 reg_offs);
581 int omap_hwmod_softreset(struct omap_hwmod *oh);
583 int omap_hwmod_count_resources(struct omap_hwmod *oh);
584 int omap_hwmod_fill_resources(struct omap_hwmod *oh, struct resource *res);
586 struct powerdomain *omap_hwmod_get_pwrdm(struct omap_hwmod *oh);
587 void __iomem *omap_hwmod_get_mpu_rt_va(struct omap_hwmod *oh);
589 int omap_hwmod_add_initiator_dep(struct omap_hwmod *oh,
590                                  struct omap_hwmod *init_oh);
591 int omap_hwmod_del_initiator_dep(struct omap_hwmod *oh,
592                                  struct omap_hwmod *init_oh);
594 int omap_hwmod_set_clockact_both(struct omap_hwmod *oh);
595 int omap_hwmod_set_clockact_main(struct omap_hwmod *oh);
596 int omap_hwmod_set_clockact_iclk(struct omap_hwmod *oh);
597 int omap_hwmod_set_clockact_none(struct omap_hwmod *oh);
599 int omap_hwmod_enable_wakeup(struct omap_hwmod *oh);
600 int omap_hwmod_disable_wakeup(struct omap_hwmod *oh);
602 int omap_hwmod_for_each_by_class(const char *classname,
603                                  int (*fn)(struct omap_hwmod *oh,
604                                            void *user),
605                                  void *user);
607 int omap_hwmod_set_postsetup_state(struct omap_hwmod *oh, u8 state);
608 int omap_hwmod_get_context_loss_count(struct omap_hwmod *oh);
610 int omap_hwmod_no_setup_reset(struct omap_hwmod *oh);
612 int omap_hwmod_pad_route_irq(struct omap_hwmod *oh, int pad_idx, int irq_idx);
614 /*
615  * Chip variant-specific hwmod init routines - XXX should be converted
616  * to use initcalls once the initial boot ordering is straightened out
617  */
618 extern int omap2420_hwmod_init(void);
619 extern int omap2430_hwmod_init(void);
620 extern int omap3xxx_hwmod_init(void);
621 extern int omap44xx_hwmod_init(void);
622 extern int am33xx_hwmod_init(void);
624 #endif