]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - arch/arm/plat-omap/sram.c
arm:omap:am33xx: Skip parts where cpu_is_omap34xx() is true but NA for AM33XX
[sitara-epos/sitara-epos-kernel.git] / arch / arm / plat-omap / sram.c
1 /*
2  * linux/arch/arm/plat-omap/sram.c
3  *
4  * OMAP SRAM detection and management
5  *
6  * Copyright (C) 2005 Nokia Corporation
7  * Written by Tony Lindgren <tony@atomide.com>
8  *
9  * Copyright (C) 2009 Texas Instruments
10  * Added OMAP4 support - Santosh Shilimkar <santosh.shilimkar@ti.com>
11  *
12  * This program is free software; you can redistribute it and/or modify
13  * it under the terms of the GNU General Public License version 2 as
14  * published by the Free Software Foundation.
15  */
16 #undef DEBUG
18 #include <linux/module.h>
19 #include <linux/kernel.h>
20 #include <linux/init.h>
21 #include <linux/io.h>
23 #include <asm/tlb.h>
24 #include <asm/cacheflush.h>
26 #include <asm/mach/map.h>
28 #include <plat/sram.h>
29 #include <plat/board.h>
30 #include <plat/cpu.h>
32 #include "sram.h"
34 /* XXX These "sideways" includes are a sign that something is wrong */
35 #if defined(CONFIG_ARCH_OMAP2) || defined(CONFIG_ARCH_OMAP3)
36 # include "../mach-omap2/prm2xxx_3xxx.h"
37 # include "../mach-omap2/sdrc.h"
38 #endif
40 #define OMAP1_SRAM_PA           0x20000000
41 #define OMAP2_SRAM_PUB_PA       (OMAP2_SRAM_PA + 0xf800)
42 #define OMAP3_SRAM_PUB_PA       (OMAP3_SRAM_PA + 0x8000)
43 #ifdef CONFIG_OMAP4_ERRATA_I688
44 #define OMAP4_SRAM_PUB_PA       OMAP4_SRAM_PA
45 #else
46 #define OMAP4_SRAM_PUB_PA       (OMAP4_SRAM_PA + 0x4000)
47 #endif
49 #if defined(CONFIG_ARCH_OMAP2PLUS)
50 #define SRAM_BOOTLOADER_SZ      0x00
51 #else
52 #define SRAM_BOOTLOADER_SZ      0x80
53 #endif
55 #define OMAP24XX_VA_REQINFOPERM0        OMAP2_L3_IO_ADDRESS(0x68005048)
56 #define OMAP24XX_VA_READPERM0           OMAP2_L3_IO_ADDRESS(0x68005050)
57 #define OMAP24XX_VA_WRITEPERM0          OMAP2_L3_IO_ADDRESS(0x68005058)
59 #define OMAP34XX_VA_REQINFOPERM0        OMAP2_L3_IO_ADDRESS(0x68012848)
60 #define OMAP34XX_VA_READPERM0           OMAP2_L3_IO_ADDRESS(0x68012850)
61 #define OMAP34XX_VA_WRITEPERM0          OMAP2_L3_IO_ADDRESS(0x68012858)
62 #define OMAP34XX_VA_ADDR_MATCH2         OMAP2_L3_IO_ADDRESS(0x68012880)
63 #define OMAP34XX_VA_SMS_RG_ATT0         OMAP2_L3_IO_ADDRESS(0x6C000048)
65 #define GP_DEVICE               0x300
67 #define ROUND_DOWN(value,boundary)      ((value) & (~((boundary)-1)))
69 static unsigned long omap_sram_start;
70 static void __iomem *omap_sram_base;
71 static unsigned long omap_sram_size;
72 static void __iomem *omap_sram_ceil;
74 /*
75  * Depending on the target RAMFS firewall setup, the public usable amount of
76  * SRAM varies.  The default accessible size for all device types is 2k. A GP
77  * device allows ARM11 but not other initiators for full size. This
78  * functionality seems ok until some nice security API happens.
79  */
80 static int is_sram_locked(void)
81 {
82         if (OMAP2_DEVICE_TYPE_GP == omap_type()) {
83                 /* RAMFW: R/W access to all initiators for all qualifier sets */
84                 if (cpu_is_omap242x()) {
85                         __raw_writel(0xFF, OMAP24XX_VA_REQINFOPERM0); /* all q-vects */
86                         __raw_writel(0xCFDE, OMAP24XX_VA_READPERM0);  /* all i-read */
87                         __raw_writel(0xCFDE, OMAP24XX_VA_WRITEPERM0); /* all i-write */
88                 }
89                 if (cpu_is_omap34xx()) {
90                         __raw_writel(0xFFFF, OMAP34XX_VA_REQINFOPERM0); /* all q-vects */
91                         __raw_writel(0xFFFF, OMAP34XX_VA_READPERM0);  /* all i-read */
92                         __raw_writel(0xFFFF, OMAP34XX_VA_WRITEPERM0); /* all i-write */
93                         __raw_writel(0x0, OMAP34XX_VA_ADDR_MATCH2);
94                         __raw_writel(0xFFFFFFFF, OMAP34XX_VA_SMS_RG_ATT0);
95                 }
96                 return 0;
97         } else
98                 return 1; /* assume locked with no PPA or security driver */
99 }
101 /*
102  * The amount of SRAM depends on the core type.
103  * Note that we cannot try to test for SRAM here because writes
104  * to secure SRAM will hang the system. Also the SRAM is not
105  * yet mapped at this point.
106  */
107 static void __init omap_detect_sram(void)
109         if (cpu_class_is_omap2()) {
110                 if (is_sram_locked()) {
111                         if (cpu_is_omap34xx()) {
112                                 omap_sram_start = OMAP3_SRAM_PUB_PA;
113                                 if ((omap_type() == OMAP2_DEVICE_TYPE_EMU) ||
114                                     (omap_type() == OMAP2_DEVICE_TYPE_SEC)) {
115                                         omap_sram_size = 0x7000; /* 28K */
116                                 } else {
117                                         omap_sram_size = 0x8000; /* 32K */
118                                 }
119                         } else if (cpu_is_omap44xx()) {
120                                 omap_sram_start = OMAP4_SRAM_PUB_PA;
121                                 omap_sram_size = 0xa000; /* 40K */
122                         } else {
123                                 omap_sram_start = OMAP2_SRAM_PUB_PA;
124                                 omap_sram_size = 0x800; /* 2K */
125                         }
126                 } else {
127                         if (cpu_is_omap34xx()) {
128                                 omap_sram_start = OMAP3_SRAM_PA;
129                                 omap_sram_size = 0x10000; /* 64K */
130                         } else if (cpu_is_omap44xx()) {
131                                 omap_sram_start = OMAP4_SRAM_PA;
132                                 omap_sram_size = 0xe000; /* 56K */
133                         } else {
134                                 omap_sram_start = OMAP2_SRAM_PA;
135                                 if (cpu_is_omap242x())
136                                         omap_sram_size = 0xa0000; /* 640K */
137                                 else if (cpu_is_omap243x())
138                                         omap_sram_size = 0x10000; /* 64K */
139                         }
140                 }
141         } else {
142                 omap_sram_start = OMAP1_SRAM_PA;
144                 if (cpu_is_omap7xx())
145                         omap_sram_size = 0x32000;       /* 200K */
146                 else if (cpu_is_omap15xx())
147                         omap_sram_size = 0x30000;       /* 192K */
148                 else if (cpu_is_omap1610() || cpu_is_omap1611() ||
149                                 cpu_is_omap1621() || cpu_is_omap1710())
150                         omap_sram_size = 0x4000;        /* 16K */
151                 else {
152                         pr_err("Could not detect SRAM size\n");
153                         omap_sram_size = 0x4000;
154                 }
155         }
158 /*
159  * Note that we cannot use ioremap for SRAM, as clock init needs SRAM early.
160  */
161 static void __init omap_map_sram(void)
163         int cached = 1;
165         if (omap_sram_size == 0)
166                 return;
168 #ifdef CONFIG_OMAP4_ERRATA_I688
169                 omap_sram_start += PAGE_SIZE;
170                 omap_sram_size -= SZ_16K;
171 #endif
172         if (cpu_is_omap34xx()) {
173                 /*
174                  * SRAM must be marked as non-cached on OMAP3 since the
175                  * CORE DPLL M2 divider change code (in SRAM) runs with the
176                  * SDRAM controller disabled, and if it is marked cached,
177                  * the ARM may attempt to write cache lines back to SDRAM
178                  * which will cause the system to hang.
179                  */
180                 cached = 0;
181         }
183         omap_sram_start = ROUND_DOWN(omap_sram_start, PAGE_SIZE);
184         omap_sram_base = __arm_ioremap_exec(omap_sram_start, omap_sram_size,
185                                                 cached);
186         if (!omap_sram_base) {
187                 pr_err("SRAM: Could not map\n");
188                 return;
189         }
191         omap_sram_ceil = omap_sram_base + omap_sram_size;
193         /*
194          * Looks like we need to preserve some bootloader code at the
195          * beginning of SRAM for jumping to flash for reboot to work...
196          */
197         memset((void *)omap_sram_base + SRAM_BOOTLOADER_SZ, 0,
198                omap_sram_size - SRAM_BOOTLOADER_SZ);
201 /*
202  * Memory allocator for SRAM: calculates the new ceiling address
203  * for pushing a function using the fncpy API.
204  *
205  * Note that fncpy requires the returned address to be aligned
206  * to an 8-byte boundary.
207  */
208 void *omap_sram_push_address(unsigned long size)
210         unsigned long available, new_ceil = (unsigned long)omap_sram_ceil;
212         available = omap_sram_ceil - (omap_sram_base + SRAM_BOOTLOADER_SZ);
214         if (size > available) {
215                 pr_err("Not enough space in SRAM\n");
216                 return NULL;
217         }
219         new_ceil -= size;
220         new_ceil = ROUND_DOWN(new_ceil, FNCPY_ALIGN);
221         omap_sram_ceil = IOMEM(new_ceil);
223         return (void *)omap_sram_ceil;
226 #ifdef CONFIG_ARCH_OMAP1
228 static void (*_omap_sram_reprogram_clock)(u32 dpllctl, u32 ckctl);
230 void omap_sram_reprogram_clock(u32 dpllctl, u32 ckctl)
232         BUG_ON(!_omap_sram_reprogram_clock);
233         /* On 730, bit 13 must always be 1 */
234         if (cpu_is_omap7xx())
235                 ckctl |= 0x2000;
236         _omap_sram_reprogram_clock(dpllctl, ckctl);
239 static int __init omap1_sram_init(void)
241         _omap_sram_reprogram_clock =
242                         omap_sram_push(omap1_sram_reprogram_clock,
243                                         omap1_sram_reprogram_clock_sz);
245         return 0;
248 #else
249 #define omap1_sram_init()       do {} while (0)
250 #endif
252 #if defined(CONFIG_ARCH_OMAP2)
254 static void (*_omap2_sram_ddr_init)(u32 *slow_dll_ctrl, u32 fast_dll_ctrl,
255                               u32 base_cs, u32 force_unlock);
257 void omap2_sram_ddr_init(u32 *slow_dll_ctrl, u32 fast_dll_ctrl,
258                    u32 base_cs, u32 force_unlock)
260         BUG_ON(!_omap2_sram_ddr_init);
261         _omap2_sram_ddr_init(slow_dll_ctrl, fast_dll_ctrl,
262                              base_cs, force_unlock);
265 static void (*_omap2_sram_reprogram_sdrc)(u32 perf_level, u32 dll_val,
266                                           u32 mem_type);
268 void omap2_sram_reprogram_sdrc(u32 perf_level, u32 dll_val, u32 mem_type)
270         BUG_ON(!_omap2_sram_reprogram_sdrc);
271         _omap2_sram_reprogram_sdrc(perf_level, dll_val, mem_type);
274 static u32 (*_omap2_set_prcm)(u32 dpll_ctrl_val, u32 sdrc_rfr_val, int bypass);
276 u32 omap2_set_prcm(u32 dpll_ctrl_val, u32 sdrc_rfr_val, int bypass)
278         BUG_ON(!_omap2_set_prcm);
279         return _omap2_set_prcm(dpll_ctrl_val, sdrc_rfr_val, bypass);
281 #endif
283 #ifdef CONFIG_SOC_OMAP2420
284 static int __init omap242x_sram_init(void)
286         _omap2_sram_ddr_init = omap_sram_push(omap242x_sram_ddr_init,
287                                         omap242x_sram_ddr_init_sz);
289         _omap2_sram_reprogram_sdrc = omap_sram_push(omap242x_sram_reprogram_sdrc,
290                                             omap242x_sram_reprogram_sdrc_sz);
292         _omap2_set_prcm = omap_sram_push(omap242x_sram_set_prcm,
293                                          omap242x_sram_set_prcm_sz);
295         return 0;
297 #else
298 static inline int omap242x_sram_init(void)
300         return 0;
302 #endif
304 #ifdef CONFIG_SOC_OMAP2430
305 static int __init omap243x_sram_init(void)
307         _omap2_sram_ddr_init = omap_sram_push(omap243x_sram_ddr_init,
308                                         omap243x_sram_ddr_init_sz);
310         _omap2_sram_reprogram_sdrc = omap_sram_push(omap243x_sram_reprogram_sdrc,
311                                             omap243x_sram_reprogram_sdrc_sz);
313         _omap2_set_prcm = omap_sram_push(omap243x_sram_set_prcm,
314                                          omap243x_sram_set_prcm_sz);
316         return 0;
318 #else
319 static inline int omap243x_sram_init(void)
321         return 0;
323 #endif
325 #ifdef CONFIG_ARCH_OMAP3
327 static u32 (*_omap3_sram_configure_core_dpll)(
328                         u32 m2, u32 unlock_dll, u32 f, u32 inc,
329                         u32 sdrc_rfr_ctrl_0, u32 sdrc_actim_ctrl_a_0,
330                         u32 sdrc_actim_ctrl_b_0, u32 sdrc_mr_0,
331                         u32 sdrc_rfr_ctrl_1, u32 sdrc_actim_ctrl_a_1,
332                         u32 sdrc_actim_ctrl_b_1, u32 sdrc_mr_1);
334 u32 omap3_configure_core_dpll(u32 m2, u32 unlock_dll, u32 f, u32 inc,
335                         u32 sdrc_rfr_ctrl_0, u32 sdrc_actim_ctrl_a_0,
336                         u32 sdrc_actim_ctrl_b_0, u32 sdrc_mr_0,
337                         u32 sdrc_rfr_ctrl_1, u32 sdrc_actim_ctrl_a_1,
338                         u32 sdrc_actim_ctrl_b_1, u32 sdrc_mr_1)
340         BUG_ON(!_omap3_sram_configure_core_dpll);
341         return _omap3_sram_configure_core_dpll(
342                         m2, unlock_dll, f, inc,
343                         sdrc_rfr_ctrl_0, sdrc_actim_ctrl_a_0,
344                         sdrc_actim_ctrl_b_0, sdrc_mr_0,
345                         sdrc_rfr_ctrl_1, sdrc_actim_ctrl_a_1,
346                         sdrc_actim_ctrl_b_1, sdrc_mr_1);
349 #ifdef CONFIG_PM
350 void omap3_sram_restore_context(void)
352         omap_sram_ceil = omap_sram_base + omap_sram_size;
354         _omap3_sram_configure_core_dpll =
355                 omap_sram_push(omap3_sram_configure_core_dpll,
356                                omap3_sram_configure_core_dpll_sz);
357         omap_push_sram_idle();
359 #endif /* CONFIG_PM */
361 #endif /* CONFIG_ARCH_OMAP3 */
363 static inline int omap34xx_sram_init(void)
365 #if defined(CONFIG_ARCH_OMAP3) && defined(CONFIG_PM)
366         omap3_sram_restore_context();
367 #endif
368         return 0;
371 int __init omap_sram_init(void)
373         if (cpu_is_am33xx())
374                 return 0;
376         omap_detect_sram();
377         omap_map_sram();
379         if (!(cpu_class_is_omap2()))
380                 omap1_sram_init();
381         else if (cpu_is_omap242x())
382                 omap242x_sram_init();
383         else if (cpu_is_omap2430())
384                 omap243x_sram_init();
385         else if (cpu_is_omap34xx())
386                 omap34xx_sram_init();
388         return 0;