]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - block/blk-map.c
arm:omap:am33xx: Reverting gigabit disabling support
[sitara-epos/sitara-epos-kernel.git] / block / blk-map.c
1 /*
2  * Functions related to mapping data to requests
3  */
4 #include <linux/kernel.h>
5 #include <linux/module.h>
6 #include <linux/bio.h>
7 #include <linux/blkdev.h>
8 #include <scsi/sg.h>            /* for struct sg_iovec */
10 #include "blk.h"
12 int blk_rq_append_bio(struct request_queue *q, struct request *rq,
13                       struct bio *bio)
14 {
15         if (!rq->bio)
16                 blk_rq_bio_prep(q, rq, bio);
17         else if (!ll_back_merge_fn(q, rq, bio))
18                 return -EINVAL;
19         else {
20                 rq->biotail->bi_next = bio;
21                 rq->biotail = bio;
23                 rq->__data_len += bio->bi_size;
24         }
25         return 0;
26 }
28 static int __blk_rq_unmap_user(struct bio *bio)
29 {
30         int ret = 0;
32         if (bio) {
33                 if (bio_flagged(bio, BIO_USER_MAPPED))
34                         bio_unmap_user(bio);
35                 else
36                         ret = bio_uncopy_user(bio);
37         }
39         return ret;
40 }
42 static int __blk_rq_map_user(struct request_queue *q, struct request *rq,
43                              struct rq_map_data *map_data, void __user *ubuf,
44                              unsigned int len, gfp_t gfp_mask)
45 {
46         unsigned long uaddr;
47         struct bio *bio, *orig_bio;
48         int reading, ret;
50         reading = rq_data_dir(rq) == READ;
52         /*
53          * if alignment requirement is satisfied, map in user pages for
54          * direct dma. else, set up kernel bounce buffers
55          */
56         uaddr = (unsigned long) ubuf;
57         if (blk_rq_aligned(q, uaddr, len) && !map_data)
58                 bio = bio_map_user(q, NULL, uaddr, len, reading, gfp_mask);
59         else
60                 bio = bio_copy_user(q, map_data, uaddr, len, reading, gfp_mask);
62         if (IS_ERR(bio))
63                 return PTR_ERR(bio);
65         if (map_data && map_data->null_mapped)
66                 bio->bi_flags |= (1 << BIO_NULL_MAPPED);
68         orig_bio = bio;
69         blk_queue_bounce(q, &bio);
71         /*
72          * We link the bounce buffer in and could have to traverse it
73          * later so we have to get a ref to prevent it from being freed
74          */
75         bio_get(bio);
77         ret = blk_rq_append_bio(q, rq, bio);
78         if (!ret)
79                 return bio->bi_size;
81         /* if it was boucned we must call the end io function */
82         bio_endio(bio, 0);
83         __blk_rq_unmap_user(orig_bio);
84         bio_put(bio);
85         return ret;
86 }
88 /**
89  * blk_rq_map_user - map user data to a request, for REQ_TYPE_BLOCK_PC usage
90  * @q:          request queue where request should be inserted
91  * @rq:         request structure to fill
92  * @map_data:   pointer to the rq_map_data holding pages (if necessary)
93  * @ubuf:       the user buffer
94  * @len:        length of user data
95  * @gfp_mask:   memory allocation flags
96  *
97  * Description:
98  *    Data will be mapped directly for zero copy I/O, if possible. Otherwise
99  *    a kernel bounce buffer is used.
100  *
101  *    A matching blk_rq_unmap_user() must be issued at the end of I/O, while
102  *    still in process context.
103  *
104  *    Note: The mapped bio may need to be bounced through blk_queue_bounce()
105  *    before being submitted to the device, as pages mapped may be out of
106  *    reach. It's the callers responsibility to make sure this happens. The
107  *    original bio must be passed back in to blk_rq_unmap_user() for proper
108  *    unmapping.
109  */
110 int blk_rq_map_user(struct request_queue *q, struct request *rq,
111                     struct rq_map_data *map_data, void __user *ubuf,
112                     unsigned long len, gfp_t gfp_mask)
114         unsigned long bytes_read = 0;
115         struct bio *bio = NULL;
116         int ret;
118         if (len > (queue_max_hw_sectors(q) << 9))
119                 return -EINVAL;
120         if (!len)
121                 return -EINVAL;
123         if (!ubuf && (!map_data || !map_data->null_mapped))
124                 return -EINVAL;
126         while (bytes_read != len) {
127                 unsigned long map_len, end, start;
129                 map_len = min_t(unsigned long, len - bytes_read, BIO_MAX_SIZE);
130                 end = ((unsigned long)ubuf + map_len + PAGE_SIZE - 1)
131                                                                 >> PAGE_SHIFT;
132                 start = (unsigned long)ubuf >> PAGE_SHIFT;
134                 /*
135                  * A bad offset could cause us to require BIO_MAX_PAGES + 1
136                  * pages. If this happens we just lower the requested
137                  * mapping len by a page so that we can fit
138                  */
139                 if (end - start > BIO_MAX_PAGES)
140                         map_len -= PAGE_SIZE;
142                 ret = __blk_rq_map_user(q, rq, map_data, ubuf, map_len,
143                                         gfp_mask);
144                 if (ret < 0)
145                         goto unmap_rq;
146                 if (!bio)
147                         bio = rq->bio;
148                 bytes_read += ret;
149                 ubuf += ret;
151                 if (map_data)
152                         map_data->offset += ret;
153         }
155         if (!bio_flagged(bio, BIO_USER_MAPPED))
156                 rq->cmd_flags |= REQ_COPY_USER;
158         rq->buffer = NULL;
159         return 0;
160 unmap_rq:
161         blk_rq_unmap_user(bio);
162         rq->bio = NULL;
163         return ret;
165 EXPORT_SYMBOL(blk_rq_map_user);
167 /**
168  * blk_rq_map_user_iov - map user data to a request, for REQ_TYPE_BLOCK_PC usage
169  * @q:          request queue where request should be inserted
170  * @rq:         request to map data to
171  * @map_data:   pointer to the rq_map_data holding pages (if necessary)
172  * @iov:        pointer to the iovec
173  * @iov_count:  number of elements in the iovec
174  * @len:        I/O byte count
175  * @gfp_mask:   memory allocation flags
176  *
177  * Description:
178  *    Data will be mapped directly for zero copy I/O, if possible. Otherwise
179  *    a kernel bounce buffer is used.
180  *
181  *    A matching blk_rq_unmap_user() must be issued at the end of I/O, while
182  *    still in process context.
183  *
184  *    Note: The mapped bio may need to be bounced through blk_queue_bounce()
185  *    before being submitted to the device, as pages mapped may be out of
186  *    reach. It's the callers responsibility to make sure this happens. The
187  *    original bio must be passed back in to blk_rq_unmap_user() for proper
188  *    unmapping.
189  */
190 int blk_rq_map_user_iov(struct request_queue *q, struct request *rq,
191                         struct rq_map_data *map_data, struct sg_iovec *iov,
192                         int iov_count, unsigned int len, gfp_t gfp_mask)
194         struct bio *bio;
195         int i, read = rq_data_dir(rq) == READ;
196         int unaligned = 0;
198         if (!iov || iov_count <= 0)
199                 return -EINVAL;
201         for (i = 0; i < iov_count; i++) {
202                 unsigned long uaddr = (unsigned long)iov[i].iov_base;
204                 if (!iov[i].iov_len)
205                         return -EINVAL;
207                 /*
208                  * Keep going so we check length of all segments
209                  */
210                 if (uaddr & queue_dma_alignment(q))
211                         unaligned = 1;
212         }
214         if (unaligned || (q->dma_pad_mask & len) || map_data)
215                 bio = bio_copy_user_iov(q, map_data, iov, iov_count, read,
216                                         gfp_mask);
217         else
218                 bio = bio_map_user_iov(q, NULL, iov, iov_count, read, gfp_mask);
220         if (IS_ERR(bio))
221                 return PTR_ERR(bio);
223         if (bio->bi_size != len) {
224                 /*
225                  * Grab an extra reference to this bio, as bio_unmap_user()
226                  * expects to be able to drop it twice as it happens on the
227                  * normal IO completion path
228                  */
229                 bio_get(bio);
230                 bio_endio(bio, 0);
231                 __blk_rq_unmap_user(bio);
232                 return -EINVAL;
233         }
235         if (!bio_flagged(bio, BIO_USER_MAPPED))
236                 rq->cmd_flags |= REQ_COPY_USER;
238         blk_queue_bounce(q, &bio);
239         bio_get(bio);
240         blk_rq_bio_prep(q, rq, bio);
241         rq->buffer = NULL;
242         return 0;
244 EXPORT_SYMBOL(blk_rq_map_user_iov);
246 /**
247  * blk_rq_unmap_user - unmap a request with user data
248  * @bio:               start of bio list
249  *
250  * Description:
251  *    Unmap a rq previously mapped by blk_rq_map_user(). The caller must
252  *    supply the original rq->bio from the blk_rq_map_user() return, since
253  *    the I/O completion may have changed rq->bio.
254  */
255 int blk_rq_unmap_user(struct bio *bio)
257         struct bio *mapped_bio;
258         int ret = 0, ret2;
260         while (bio) {
261                 mapped_bio = bio;
262                 if (unlikely(bio_flagged(bio, BIO_BOUNCED)))
263                         mapped_bio = bio->bi_private;
265                 ret2 = __blk_rq_unmap_user(mapped_bio);
266                 if (ret2 && !ret)
267                         ret = ret2;
269                 mapped_bio = bio;
270                 bio = bio->bi_next;
271                 bio_put(mapped_bio);
272         }
274         return ret;
276 EXPORT_SYMBOL(blk_rq_unmap_user);
278 /**
279  * blk_rq_map_kern - map kernel data to a request, for REQ_TYPE_BLOCK_PC usage
280  * @q:          request queue where request should be inserted
281  * @rq:         request to fill
282  * @kbuf:       the kernel buffer
283  * @len:        length of user data
284  * @gfp_mask:   memory allocation flags
285  *
286  * Description:
287  *    Data will be mapped directly if possible. Otherwise a bounce
288  *    buffer is used. Can be called multple times to append multple
289  *    buffers.
290  */
291 int blk_rq_map_kern(struct request_queue *q, struct request *rq, void *kbuf,
292                     unsigned int len, gfp_t gfp_mask)
294         int reading = rq_data_dir(rq) == READ;
295         unsigned long addr = (unsigned long) kbuf;
296         int do_copy = 0;
297         struct bio *bio;
298         int ret;
300         if (len > (queue_max_hw_sectors(q) << 9))
301                 return -EINVAL;
302         if (!len || !kbuf)
303                 return -EINVAL;
305         do_copy = !blk_rq_aligned(q, addr, len) || object_is_on_stack(kbuf);
306         if (do_copy)
307                 bio = bio_copy_kern(q, kbuf, len, gfp_mask, reading);
308         else
309                 bio = bio_map_kern(q, kbuf, len, gfp_mask);
311         if (IS_ERR(bio))
312                 return PTR_ERR(bio);
314         if (!reading)
315                 bio->bi_rw |= REQ_WRITE;
317         if (do_copy)
318                 rq->cmd_flags |= REQ_COPY_USER;
320         ret = blk_rq_append_bio(q, rq, bio);
321         if (unlikely(ret)) {
322                 /* request is too big */
323                 bio_put(bio);
324                 return ret;
325         }
327         blk_queue_bounce(q, &rq->bio);
328         rq->buffer = NULL;
329         return 0;
331 EXPORT_SYMBOL(blk_rq_map_kern);